Last edited 5 months ago

Android-based OpenSTDroid embedded software architecture overview

Applicable for STM32MP25x lines

Important
OpenSTDroid is validated against the ecosystem release v5.1.0 . It has not been ported yet on STM32 MPU ecosystem release v6. Visit the ecosystem release v5.1.0 wiki to access to user guide explaining how to port Android on top of STM32 MPU ecosystem release v5.

The diagram below shows Android-based OpenSTDroid embedded software distribution's main components:

  • The OpenSTDroid distribution, running on the Arm® Cortex®-A, includes:
    • The OpenSTLinux BSP with:
    • Application frameworks composed of middleware components relying on the BSP and providing a set of APIs:
      • OP-TEE APIs to run Trusted Applications (TA) that allow manipulating secrets (information not visible from Linux® and from the STM32Cube MPU Package).
      • Android APIs to run Applications that typically interact with the user via a display or a touchscreen.
  • The STM32Cube MPU Package running on the Arm® Cortex®-M nonsecure mode: it is based on HAL drivers and middleware, like STM32 microcontrollers, completed with coprocessor management for interaction with the Cortex-A.

The figure below provides an overview of the STM32MPU Embedded Software architecture.


Android-based OpenSTDroid embedded software architecture overview.

1. Open Source Software (OSS) philosophy[edit | edit source]

The Open source software source code is released under a license in which the copyright holder grants users the rights to study, change, and distribute the software to anyone and for any purpose[1].

STMicroelectronics maximizes the using of open source software and contributes to those communities. Notice that, due to the software review life cycle, it can take some time before getting all developments accepted in the communities, so STMicroelectronics can also temporarily provide some source code on GitHub[2], until it is merged in the targeted repository.

2. References[edit | edit source]