This article aims to describe the content of the software release included in the STM32CubeMP2 package, version v1.4.0, which is part of the Yocto-based_OpenSTLinux ecosystem release note v7.0.0.
1. Delivery purpose and scope[edit | edit source]
The STM32CubeMP2 package is a software package running on the Arm® Cortex®-M33 processor and is a fundamental part of the Yocto-based OpenSTLinux embedded software distribution.
This release includes:
- The STM32Cube HAL: STM32 abstraction layer embedded software ensuring maximized portability across the STM32 portfolio. HAL APIs are available for all peripherals.
- Low-layer APIs (LL APIs): Offering a fast, lightweight, expert-oriented layer that is closer to the hardware than the HAL. LL APIs are only available for a limited set of peripherals.
- A consistent set of middleware components: such as FreeRTOS™, OpenAMP, LwIP, STM32_USBPD_Library and MbedTLS.
- All embedded software utilities: delivered with a full set of examples.
- Multi-core components
- OpenAMP
- ResourceManager
- SCMIAgent
- All the STM32MP257F-EV1
, STM32MP257F-DK
, STM32MP257F-DK
for STM32MP23x lines evaluation
, STM32MP215F-DK Discovery kit
projects are available on STM32CubeIDE.
2. Intended Audience[edit | edit source]
The targeted audience is STM32 MPU customers and partners.
3. Licensing[edit | edit source]
All licenses, applicable to STM32CubeMP2 package, are available here.
4. Supported devices[edit | edit source]
The drivers provided within this package support all STM32MP21x lines
, STM32MP23x lines
and STM32MP25x lines
.
5. Supported hardware[edit | edit source]
The software examples and the drivers delivered in this package are applicable for the following boards:
- STM32MP257F-EV1 Evaluation board
, for information about this board, read the article STM32MP257x-EV1 hardware description. - STM32MP257F-DK Discovery kit
, for information about this board, read the article STM32MP257x-DK hardware description. - STM32MP257F-DK Discovery kit
for STM32MP23x lines evaluation
, for information about this board, read the article STM32MP257x-DK hardware description. - STM32MP215F-DK Discovery kit
, for information about this board, read the article STM32MP215x-DK hardware description.
6. Release content[edit | edit source]
This is a maintenance release of the STM32CubeMP2 software package running on Arm® Cortex®-M33 core. The full content is available in STM32CubeMP2 Package content.
6.1. Main changes[edit | edit source]
- OpenAMP_TTY_echo demonstration project, that can be compiled via CMake, is now available for all boards.
- MbedTLS middleware is now supported
- Two new examples are added to demonstrate its usage: SSL_Server and SSL_Client.
- Fixed an issue of stale M33 VRing processing in the StarterApp.
- General improvements in "M33TD_NSAppCore" Utility.
- Fixed RCC HSI calibration save/restore issue.
- Improved Arm-Cortex-M33 nonsecure coprocessor shutdown handling for A35-TD flavor
. - OpenAMP and LwIP middlewares are upgraded with to new versions.
- MISRA and Spellcheck fixes.
6.1.1. HAL drivers[edit | edit source]
- This is a maintenance release of the STM32CubeMP2 package HAL drivers.
- All HAL drivers have been checked for MISRA 2012 compliance, and most warnings have been resolved. The last remaining warnings could be solved by customers if needed.
- Check the overview and all available HAL drivers in HAL drivers.
6.1.2. LL drivers[edit | edit source]
- This is a maintenance release of the STM32CubeMP2 package LL drivers.
- All LL drivers have been checked for MISRA 2012 compliance, and most warnings have been resolved. The last remaining warnings could be solved by customers if needed.
- Check the overview and all available LL drivers here: LL drivers.
6.1.3. BSP[edit | edit source]
- This is a maintenance release of the STM32CubeMP2 package BSP drivers.
- Refer to the BSP Drivers section here: BSP drivers.
6.1.4. CMSIS[edit | edit source]
- Bit and register definitions for
- Support for System, Startup, and Linker files.
- For more details, refer to CMSIS.
6.1.5. Middleware[edit | edit source]
- FreeRTOS
- OpenAMP [1]
- UCPD [2]
- LwIP [3]
- MbedTLS
- Check overview of middleware's in STM32CubeMP2 Package article
6.1.6. Projects[edit | edit source]
- Check project section here for details about implemented projects.
| For detailed information, read file Release_Notes.html delivered with the STM32CubeMP2 Package. |
6.2. Main restrictions[edit | edit source]
- None
6.3. Released components[edit | edit source]
6.3.1. Drivers[edit | edit source]
| Component | Version | Notes |
|---|---|---|
| Cortex®-M CMSIS | v5.9.0 | - |
| STM32MP2xx CMSIS | v1.4.0 | - |
| STM32MP2xx HAL | v1.4.0 | - |
| BSP STM32MP257F_Ev1 | v1.4.0 | - |
| BSP STM32MP257F_DK | v1.4.0 | - |
| BSP STM32MP235F_DK | v1.4.0 | - |
Find here, the list of available HAL, LL and BSP drivers.
6.3.2. Middleware[edit | edit source]
| Component | Version | Notes |
|---|---|---|
| FreeRTOSTM | v10.6.2_20241011 | - |
| OpenAMP | v2025.10_20260902 | - |
| STM32_USBPD_Library - Core | v5.3.1 | |
| STM32_USBPD_Library - Device | v1.0.0_rc2 | |
| Scmiagent | v1.0.5 | - |
| MbedTLS | 3.6.6_20260511 | - |
| LwIP | v2.2.1_20260817 | - |
6.3.3. Utilities[edit | edit source]
| Component | version | Notes |
|---|---|---|
| ResourceManager | v1.4.0 | - |
6.4. Released projects[edit | edit source]
The STM32CubeMP2 package comes with a rich set of examples running on STM32 MPU boards
, organized by board and provided with preconfigured projects.
The main supported development environment is STM32CubeIDE (works on multiple operating systems) and uses the GNU toolchain.
All STM32MP257F-EV1
, STM32MP257F-DK
, STM32MP257F-DK
for STM32MP23x lines evaluation
and STM32MP215F-DK
projects are available with STM32CubeIDE.
Find in the article STM32MP2x Projects, the exhaustive list of available projects for STM32MP215F-DK
, STM32MP257F-DK
for STM32MP23x lines evaluation
, STM32MP257F-DK
and STM32MP257F-EV1
, .
The recommended supported toolchain for STM32MP2 is now STM32CubeIDE (all-in-one multi-OS development tool).
7. How to get started with STM32CubeMP2 Package[edit | edit source]
Refer to How to get software and start with this release article.
8. References[edit | edit source]