Last edited one month ago

STM32 MPU OpenSTLinux release note - v6.2.0

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

This article describes the content of OpenSTLinux distribution software release version openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18, which is part of the STM32 MPU ecosystem release note - v6.2.0.


1. Intended audience[edit | edit source]

The targeted audience is STM32MP1 series and STM32MP2 series customers or partners.

2. Delivery scope and purpose[edit | edit source]

The OpenSTLinux distribution is a Linux® distribution based on the OpenEmbedded build Framework. It runs on the Arm® Cortex® processors, and is a fundamental part of the STM32MPU Embedded Software distribution. This delivery of OpenSTLinux distribution is part of STM32 MPU Ecosystem v6.2.0 (see the STM32 MPU ecosystem release note - v6.2.0).

3. Licensing[edit | edit source]

This software package is licensed under a LIMITED LICENSE AGREEMENT FOR ST MATERIALS EVALUATION (LLA). Customers may not use this package except in compliance with the software license agreement (SLA).

All packages use the same source components. All components and their respective licenses are listed here.

4. Supported hardware[edit | edit source]

This software delivery is compatible with all STM32MP1 series' boards and STM32MP2 series' boards .

5. Release content[edit | edit source]

5.1. Main software components[edit | edit source]

  • Build process
    • OpenEmbedded v5.0.15 (Scarthgap) - Updated
    • GCC version v13.3.0
  • Embedded software components
    • Linux kernel v6.6-stm32mp-r3 (LTS v6.6.116) - Updated
    • TF-A v2.10-stm32mp-r3 (LTS v2.10.24) - Updated
    • U-Boot v2023.10-stm32mp-r3 - Updated
    • OP-TEE 4.0.0-stm32mp-r3 - Updated
    • External DT v6-stm32mp-r3 - Updated
    • OpenOCD version v0.12.0
  • Applicative components
    • Weston version v13.0.1
    • Wayland version 1.22.0
    • GStreamer version v1.22.12
    • GCnano version v6.4.21 - Updated

5.2. Changes[edit | edit source]

5.2.1. OpenSTLinux layers[edit | edit source]

Changes are:‎

  • Rebase on Yocto Release 5.0.15 (Scarthgap)
  • New ST SPLIT Partitions mecanism (refer to ST_SPLIT_Partitions_detailed_information)
  • New machine stm32mp1-efi and stm32mp2-efi machine which boot with EFI kernel image firmware
  • CONF: add support of NAND-CUSTOM via several parameter to define NAND configuration:
    • CUSTOM_NAND_CONFIG = <PageSize>_<BlockSize>-<StorageSize>
    • CUSTOM_NAND_TYPE = fmc or spi
    • MKUBIFS_ARGS_nand_custom ??= "--min-io-size 4096 --leb-size 253952 --max-leb-cnt 4096
    • UBINIZE_ARGS_nand_custom ??= "--min-io-size 4096 --peb-size 256KiB"
    • EXTRA_UBIFS_SIZE_nand_custom ??= "0" to define extra size required for UBIFS volume size (KiB)
  • This custom NAND configuration can be activated by one or the both following configuration on BOOTDEVICE_LABELS:
    • BOOTDEVICE_LABELS += "nand-custom"
    • BOOTDEVICE_LABELS += "nand-custom-sdcard"
  • Add GCC aarch64 none elf for compiling TF-A on arm 64bits
  • OpenOCD: add capstone support
  • WIC: use only rootfs image
  • M33-TD flavor : add rpmsg tool to manage messages between Arm® Cortex®-A and Arm® Cortex®-M
  • Minor fixes

5.2.2. Linux kernel[edit | edit source]

New component release tag v6.6-stm32mp-r3 is available.

The main updated features are:

  • Rebase on Linux® kernel v6.6.116 for OpenSTLinux v6.2.0 delivery
  • Add STM32MP15x lines  PSCI/OSI support
  • Add STM32MP25x lines  PCIE Endpoint support
  • Stabilization and optimization of STM32MP1 & STM32MP2 platforms
  • Improvements for real-time, power management, performance
  • Multimedia enhancements
  • Minor fixes

5.2.3. U-Boot[edit | edit source]

New component release tag v2023.10-stm32mp-r3 is available, rebased on official U-Boot v2023.10.

Changes are:

  • Add stm32mp21 keys in cmd_stm32key command
  • Add support for power supplies in stusb160x driver
  • Add clock provider for TXBYTE and DSI PHY clocks in stm32_dsi driver
  • fastboot: only dequeue IN requests that has been queued
  • QSPI/OSPI indirect mode throughput optimization
  • Migrate U-Boot bootph-all DT properties to kernel DT
  • Use CCF for usb2phy clock provider in phy-stm32-usb2phy driver
  • Minor fixes

5.2.4. TF-A[edit | edit source]

New component release tag v2.10-stm32mp-r3 is available, rebased on official TF-A v2.10.24 (LTS tag lts-v2.10.24.24).

Changes are:

  • Rebase on official lts-v2.10.24
  • Add STM32MP1 PSCI OSI support
  • Add RSE communication support for ST platforms
  • Add secure and encrypted boot support for M33-TD flavor
  • Enable usage of LTO build
  • Multiple fixes and improvements

Full changelog: lts-v2.10.24...2.10-stm32mp-r3

5.2.5. OP-TEE[edit | edit source]

New component release tag 4.0.0-stm32mp-r3 is available, rebased on official OP_TEE OS v4.0.0.

Changes are:

  • STM32MP release 4.0.0-stm32mp-r3 :
    • Add support of PSCI OSI on stm32mp1x
    • Add support of GPU OPP
    • Upgrade to mbedTLS 3.6.4
    • Various fixes

Full Changelog: 4.0.0-stm32mp-r2...4.0.0-stm32mp-r3

5.2.6. External-DT[edit | edit source]

New component release tag v6-stm32mp-r3 is available to take into account rebase of OpenSTLinux v6.2.0.

The external device tree component is used to host STM32 MPU embedded software device tree configurations in addition to the ones present in each software component (TF-A, OP-TEE, U-Boot, Linux kernel, TF-M).

Since this ecosystem release v6.2.0 , it is used for both STM32MP1 series and STM32MP2 series.

6. Release change notification[edit | edit source]

OpenSTLinux attention points to switch from ecosystem release v6.1.0 to ecosystem release v6.2.0 are documented in STM32 MPU OpenSTLinux release changes notification – v6.2.0 article.

7. Recommendations for use[edit | edit source]

7.1. Safe use[edit | edit source]

  • Flash programming and boot from all supported flash devices: SD card, eMMC, ONFI NAND and NOR flash memories.
  • Develop Linux® applications, libraries, kernel modules based on OpenSTLinux delivery.
  • Develop STM32CubeMPU applications based on STM32CubeMP1 and STM32CubeMP2 deliveries.
  • Develop boards based on STM32MP1 series and STM32MP2 series.
  • Prototype applications based on ST boards.

7.2. Non-recommended use[edit | edit source]

  • None

8. Restrictions[edit | edit source]

STM32MP1 series

  • The partition layout always keeps the Firmware Update related partitions even if machine feature fw-update is disabled. To optimize the partition layout without Firmware Update feature, modifications are needed on flashlayout file generation and also on U-Boot source code in case of MTD partitions (storage mapping is hardcoded for MTD partitions, see How_to_configure_U-Boot_for_your_board#MTD_partitions)
  • STM32MP135F-DK : Restriction concerning WoL from PHY feature (missing "/delete-property/ power-domains;" in DT node Ethernet1). Updated procedure is described in Ethernet_device_tree_configuration#How_to_enable_and_use_WoL_from_PHY chapter.

9. Minor release updates[edit | edit source]

STMicroelectronics regularly delivers corrections through github® components which are U-Boot, OP-TEE, TF-A , Linux kernel .


The corrections can be incorporated into the STM32MPU Developer Package or Distribution Package (see below).

Two possibilities exist to update a Distribution Package:

  • Update your existing Distribution Package:
Switch your Distribution Package to # github® mode .
  1. Use the devtool modify <recipe name> command to set up an environment. It fetches and unpacks the source code.
  2. In the extracted source code, use a git command such as git checkout -b WORK <github® TAG> to point to a new revision of the component.
More rarely, STMicroelectronics also delivers fixes on layers through github®. These changes can be integrated (via git commands: git checkout -b WORK <github® commit SHA1>) into the local STM32MPU Distribution Package environment. See below the github® links of the quoted layers :
  • Get a new Distribution Package:
Refer to Installing_the_OpenSTLinux_distribution page for installing instructions, and use the repo command given for the minor version below, if it exists.

10. How to get started with openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18[edit | edit source]

Refer to Yocto-based_OpenSTLinux_embedded_software article.

11. Associated tools[edit | edit source]

Refer to the Referenced tools release notes .

12. Yocto features enabled in the delivery[edit | edit source]

OpenEmbedded[1] build framework engine is named OE-Core.
OpenSTLinux distribution is based on the build framework OpenEmbedded, and can be configured thanks to a mechanism named "features" (machine features, distribution features, ...).

Depending on the features enabled, the resulting distribution can have more capabilities or software embedded.
For example, if the Wifi is enabled then the Wifi software and drivers are present on the filesystem and the Wifi can be used.

12.1. Machine features[edit | edit source]

The variable MACHINE_FEATURES specifies the list of hardware features the machine is capable of supporting.
These features (MACHINE_FEATURES) are defined inside the machine configuration .

Machine feature Purpose
alsa Include ALSA support (OSS compatibility kernel modules installed if available).
autoresize Add support of autoresize through InitRD
bluetooth Add Bluetooth firmware to the filesystem
Broadcom43430 for (STM32MP135x-DK Discovery kit and STM32MP157x-DKx Discovery kit

Broadcom43439 for (STM32MP257F-DK Discovery kit for STM32MP23x lines evaluation and STM32MP257F-DK Discovery kit )
Broadcom4373 for (STM32MP215F-DK Discovery kit via optional M.2 Type 2AE Wi-Fi® + Bluetooth® Module)

ext2 Add Second Extended File System support
fip Enable Firmware In Package (FIP) packaging format
fw-update Enable Firmware update feature
gpu Add GPU support (if EULA is accepted) (STM32MP157 line  and STM32MP2 series only)
initrd Enable Intial ramdisk building
m4copro Add m4projects to userfs (STM32MP15x lines  only)
m33copro Add m33projects to userfs (STM32MP2 series only)
m33td Enable M33-TD flavor (STM32MP2 series only) (deactivates m33copro)
opencl Add OpenCL for GPU support (if EULA is accepted) (STM32MP2 series only)
openvx Add OpenVX for GPU support (if EULA is accepted) (STM32MP2 series only)
optee Add OP-TEE Secure part
pci Add Peripheral Component Interconnect peripheral support
rtc Add Real Time Clock peripheral support
screen Add display screen peripheral support
splashscreen Add splashscreen to U-Boot
tpm2 Add Trusted Platform Module peripheral support
usbg0 Add G0 Firmware for USB support
usbgadget Enable USB Gadget feature
usbhost Enable USB Host feature
vulkan Add Vulkan for GPU support (if EULA is accepted) STM32MP2 series only)
watchdog Add watchdog support and binaries
wifi Add wifi firmware to the filesystem
Broadcom43430 for (STM32MP135x-DK Discovery kit and STM32MP157x-DKx Discovery kit )

Broadcom4373 for (STM32MP215F-DK Discovery kit via optional M.2 Type 2BZ Wi-Fi® + Bluetooth® Module)

12.2. Distribution features[edit | edit source]

The variable DISTRO_FEATURES specifies the list of software features present in the distribution.
These features (DISTRO_FEATURES) are defined inside the distribution configuration .

Distribution feature Purpose
alsa Include ALSA support (OSS compatibility kernel modules installed if available).
argp
autoresize Add support of userfs auto resize feature in OpenSTLinux
bluetooth Include Bluetooth support
bluez5 Add Bluetooth stack
efi Add userland EFI tools
ext2 Add Second Extended File System support
ext4 Add Fourth Extended File System support
gobject-introspection-data Enable GObject Introspection, project for providing machine readable introspection data of the API of C libraries.
gplv3 Add gplv3 binaries in OpenSTLinux
gstreamer Add gstreamer tools in filesystem
initrd Add ramdisk
ipv4 Add ipv4 support
ipv6 Add ipv6 support
kde Add several tools (e.g. cups, fontconfig, ...) to the filesystem
largefile Enable large file support
ldconfig Include support for ldconfig and ld.so.conf on the target
multiarch Enable 64 bits BFD (Binary File Descriptor)
nfs Include NFS client support (for mounting NFS exports on device).
opencl Include the Open Graphics Library
opengl Include the OpenCL Library
optee Install tee service on the filesystem
pam Enable Pluggable Authentication Module
pci Add pci support
pulseaudio Network-capable sound server program
splashscreen Add U-Boot splashscreen
systemd Use systemd as init service
usbgadget USB Gadget Device support (for USB networking/serial/storage)
usbhost USB Host support (allows to connect external keyboard, mouse, storage, network etc)
vulkan Include the Vulkan Library
wayland Add Wayland support
wifi WiFi support
xattr Add "Extended Attributes" support for filesystem
zeroconf Add zeroconf package to set up a ad-hoc network

12.3. Bootscheme labels[edit | edit source]

The variable BOOTSCHEME_LABELS defines which kind of boot is supported on the board.
These settings (BOOTSCHEME_LABELS) are defined inside the machine configuration .

Bootscheme label Purpose
optee Add OP-TEE (System and secure services) in boot scheme
opteemin Add OP-TEE (System services only) in boot scheme
fastboot Add Fastboot and OP-TEE (System and secure services) in boot scheme
fastboot-opteemin Add Fastboot and OP-TEE (System services only) in boot scheme

12.4. Bootdevice labels[edit | edit source]

The variable BOOTDEVICE_LABELS defines which kind of mass storage OpenSTLinux can program.
These settings (BOOTDEVICE_LABELS ) are defined inside the machine configuration .

Bootdevice label Purpose
emmc Add boot on eMMC device
nand-4-256-1024 Add boot on NAND device
nand-4-256-1024-sdcard Add boot stage on NAND device and the filesystem on SD card
nor-emmc Add boot stage on NOR device and the filesystem on eMMC device
nor-sdcard Add boot stage on NOR device and the filesystem on SD card
nor-nor-sdcard M33-TD flavor only: Add boot stages on NOR device (CM33, then CA35) and the filesystem on SD card
sdcard Add boot on SD card