Last edited 4 months ago

TF-M release note

Applicable for STM32MP21x lines, STM32MP23x lines, STM32MP25x lines


This article aims to describe the content of the software release included in the TF-M package, version v2.1.4, which is part of the Yocto-based OpenSTLinux ecosystem release note - v6.2.1.

1. Delivery purpose and scope[edit | edit source]

Trusted Firmware-M (TF-M) implements the Secure Processing Environment (SPE) for Armv8-M, Armv8.1-M architectures. It runs on the Arm® Cortex®-M33 processor of the STM32MP2 series. It can be used for both M33-TD flavor and A35-TD flavor .

2. Intended Audience[edit | edit source]

The targeted audience is STM32 MPU customers and partners.

3. Licensing[edit | edit source]

All licenses applicable to TF-M package are available here.

4. Supported development boards[edit | edit source]

The software examples and the drivers delivered in this package are applicable for the following boards:

  • STM32MP257F-EV1 Evaluation board ,
  • STM32MP257F-DK Discovery kit ,
  • STM32MP257F-DK Discovery kit for STM32MP23x lines evaluation ,
  • STM32MP215F-DK Discovery kit .

5. Release content[edit | edit source]

Updated Component release - v2.1.3-stm32mp-r2
It allows the Arm®Cortex®-M33 firmware to run in secure context.

5.1. Main changes[edit | edit source]

  • Update to TF-M v2.1.4 (LTS update)
  • Update to MbedTLS version to v3.6.5
  • Firmware Update support
  • Warm reset of Arm® Cortex®-A35
  • Add interruption framework
  • Handle Wake-up button
  • Shutdown support
  • Low-power updates
  • Stability improvements and bug fixes

Main information

  • A real time application running on Arm® Cortex®-M33 can be disturbed by an Arm® Cortex®-A35 resource request. The customer has to handle the task priority in its application.

5.2. Main restrictions[edit | edit source]

  • Run1, Run2 Low Power modes (ie Arm® Cortex®-A35 can go in low power) are supported, other low power modes are no yet supported.

5.3. Released components[edit | edit source]

5.3.1. TF-M components[edit | edit source]

Component Repository Version (tag or SHA1)
TF-M https://github.com/STMicroelectronics/trusted-firmware-m v2.1.4-stm32mp-r2.1
tf-m-tests https://github.com/STMicroelectronics/tf-m-tests v2.1.4-stm32mp-r2.1

5.3.2. Dependencies[edit | edit source]

TF-M and tf-m-tests are delivered in their own Github repositories. Some additional components are nevertheless required either to compile or to bring new functionalities. Those components are fetched during the compilation of TF-M, or directly by Yocto.

More information can be found in TF-M Dependency management

Some components, such as QCBOR, MCUBoot, CMSIS and MbedTLS, are opensource, not modified by STMicroelectronics.

The other opensource components, modified by STMicroelectronics, or the STMicroelectronics proprietary software are delivered in STMicroelectronics Github.

Component Repository Version (tag or SHA1)
QCBOR https://github.com/laurencelundblade/QCBOR.git v1.2
MCUBoot https://github.com/mcu-tools/mcuboot.git v2.1.0
CMSIS https://github.com/ARM-software/CMSIS_6.git d0c460c1697d210b49a4b90998195831c0cd325c
MbedTLS https://github.com/Mbed-TLS/mbedtls.git mbedtls-3.6.5
PSA ADAC https://github.com/STMicroelectronics/psa-adac v1.0-stm32mp-r1
SCP-firmware https://github.com/STMicroelectronics/SCP-firmware v2.13.0-stm32mp-r3.1
cmsis-core https://github.com/STMicroelectronics/cmsis-core.git v5.9.0
stm32mp2xx-hal-driver https://github.com/STMicroelectronics/stm32mp2xx-hal-driver.git v1.3.1
cmsis-device-mp2 https://github.com/STMicroelectronics/cmsis-device-mp2.git v1.3.1
stm32mp2-low-power https://github.com/STMicroelectronics/stm32mp2-low-power v1.1.0
ddr https://github.com/STMicroelectronics/stm32-ddr-phy-binary v1.0-stm32mp


6. Documentation[edit | edit source]

More information about TF-M can be found in TF-M official Documentation. Or in STMicroelectronics generated documentation , especially the releases page .

7. How to get started with TF-M Package[edit | edit source]

TF-M package are delivered with Starter package and with Developer package for the Yocto-based_OpenSTLinux_ecosystem.
Refer to Yocto-based_OpenSTLinux_embedded_software article to find the right packages corresponding to your board.

8. References[edit | edit source]



9. Archives [edit | edit source]

STM32MPU release OpenSTLinux release note
STM32 MPU-Ecosystem-v6.2.0 TF-M_release_note - v2.1.3