Last edited 3 weeks ago

STM32CubeMP2 Package release note - v1.3.2

Applicable for STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

This article aims to describe the content of the software release included in the STM32CubeMP2 package, version v1.3.2, which is part of the Yocto-based_OpenSTLinux ecosystem release note v6.2.1.

1. Delivery purpose and scope[edit | edit source]

The STM32CubeMP2 package is a software package running on the Arm® Cortex®-M33 processor and is a fundamental part of the Yocto-based OpenSTLinux embedded software distribution.

This release is made to improve the documentation for StarterApp. Compared to previous release v1.3.1, we highlight the tight coupling of External-DT version with the version of TF-M. These updated README's will help users to correctly compile all StarterAppp like applications.
In functional terms this release is equivalent to v1.3.1.

2. Intended Audience[edit | edit source]

The targeted audience is STM32 MPU customers and partners.

3. Licensing[edit | edit source]

All licenses applicable to STM32CubeMP2 package are available here.

4. Supported devices[edit | edit source]

The drivers provided within this package support all STM32MP21x lines , STM32MP23x lines  and STM32MP25x lines .

5. Supported hardware[edit | edit source]

The software examples and the drivers delivered in this package are applicable for the following boards:


6. Release content[edit | edit source]

This is a maintenance release of the STM32CubeMP2 software package running on Arm® Cortex®-M33 core. The full content is available in STM32CubeMP2 Package content.

6.1. Main changes[edit | edit source]

6.1.1. v1.3.2 changes[edit | edit source]

  • Updates for the M33-TD flavor
    • The documentation for StarterApp like applications is updated and it emphasizes the strong coupling of External-DT version with the version of TF-M.

6.1.2. v1.3.1 changes[edit | edit source]

  • Updates for the M33-TD flavor
    • Firmware update feature is now available in the StarterApp.
    • Low power state management support is enhanced.
    • Utility M33TD_NSAppCore is updated to fully support new use cases of Firmware update and Low Power state management.
    • A new project VisualWatchdogDemo is added to demonstrate how OSTL running on the Arm® Cortex®-A35 processor can be independently rebooted or recovered from a crash.
  • Updates for the A35-TD flavor
    • A new example is added which demonstrates full-duplex SPI transfer between two STM32MP257F-EV1 boards using SPI3 and HPDMA3 in Linked-List mode.
    • A new application is added which demonstrates how you could use the "scmiagent" middleware in your STM32CubeMPU Firmware to communicate using ARM SCMI protocol and enable/disable clocks controlled by Arm® Cortex®-A35.
    • CMSIS device updates for:
      • ETH
      • Bugfix: correct malformed comment delimiters and missing opening parenthesis for some definitions.
    • PWR HAL: updated to use DSB before WFI in low power functions.
    • Bug Fixes and improvements in examples.
6.1.2.1. HAL drivers[edit | edit source]
  • This is a maintenance release of the STM32CubeMP2 package HAL drivers.
  • All HAL drivers have been checked for MISRA 2012 compliance, and most warnings have been resolved. The last remaining warnings could be solved by customers if needed.
  • Check the overview and all available HAL drivers in HAL drivers.
6.1.2.2. LL drivers[edit | edit source]
  • This is a maintenance release of the STM32CubeMP2 package LL drivers.
  • All LL drivers have been checked for MISRA 2012 compliance, and most warnings have been resolved. The last remaining warnings could be solved by customers if needed.
  • Check the overview and all available LL drivers here: LL drivers.
6.1.2.3. BSP[edit | edit source]
  • This is a maintenance release of the STM32CubeMP2 package BSP drivers.
  • Refer to the BSP Drivers section here: BSP drivers.
  • BSP has been added for the DK board with STM32MP21x lines .
6.1.2.4. CMSIS[edit | edit source]
  • Bit and register definitions for
    • STM32MP25x lines 
    • STM32MP23x lines 
    • STM32MP21x lines .
  • Support for System, Startup, and Linker files.
  • For more details, refer to CMSIS.
6.1.2.5. Middleware[edit | edit source]
6.1.2.6. Projects[edit | edit source]
  • Check project section here Projects for details about implemented projects .
Information
Note: For detailed information, read file Release_Notes.html delivered with the STM32CubeMP2 Package.

6.2. Main restrictions[edit | edit source]

None

6.3. Released components[edit | edit source]

6.3.1. Drivers[edit | edit source]

Component Version Notes
Cortex®-M CMSIS V5.9.0 -
STM32MP2xx CMSIS V1.3.1 -
STM32MP2xx HAL V1.3.1 -
BSP STM32MP257F_EV1 V1.3.1 -
BSP STM32MP257F_DK V1.3.1 -
BSP STM32MP235F_DK V1.3.1 -

Find here the list of available HAL , LL and BSP drivers.

6.3.2. Middleware[edit | edit source]

Component Version Notes
FreeRTOSTM v10.6.0_20241011 -
OpenAMP v2022.10_20260511 -
STM32_USBPD_Library - Core v5.3.1
STM32_USBPD_Library - Device v1.0.0_rc2
Scmiagent v1.0.3 -
LwIP v2.2.0_20240202 -

6.3.3. Utilities[edit | edit source]

Component Version Notes
ResourceManager V1.3.1 -

6.4. Released projects[edit | edit source]

The STM32CubeMP2 package comes with a rich set of examples running on STMicroelectronics boards, organized by board and provided with preconfigured projects. The main supported development environment is STM32CubeIDE (works on multiple operating systems) and uses the GNU toolchain.

  • All STM32MP257F-EV1 , STM32MP257F-DK , STM32MP257F-DK for STM32MP23x lines evaluation and STM32MP215F-DK projects are available with STM32CubeIDE.

Find in this article STM32MP2x Projects, the exhaustive list of available projects for STM32MP257F-EV1 Evaluation board , STM32MP257F-DK Discovery kit , STM32MP257F-DK Discovery kit for STM32MP23x lines evaluation and STM32MP215F-DK

The recommended supported toolchain for STM32MP2 is now STM32CubeIDE (all-in-one multi-OS development tool).

7. How to get started with STM32CubeMP2 Package[edit | edit source]

Refer to How to get software and start with this release article.

8. References[edit | edit source]