Last edited 9 months ago

X-LINUX-QT Distribution Package

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

This article explains how to download and install the X-LINUX-QT distribution package

1. Prerequisites[edit | edit source]

Needed prerequisites are described in X-LINUX-QT_expansion_package#Prerequisites.

2. Install the STM32MPU OpenSTLinux distribution package[edit | edit source]

As prerequisite to X-LINUX-QT distribution package, get and install the STM32MPU OpenSTLinux distribution package. Last version is the preferred one : v6.2.1.

The way to proceed is given in STM32MPU_Distribution_Package article.

3. Install X-LINUX-QT distribution package[edit | edit source]

3.1. Install the latest X-LINUX-QT distribution package - v2.3.0[edit | edit source]

To install the X-LINUX-QT distribution package v2.3.0 compatible with ecosystem release v6.2.0, follow the steps below.

3.1.1. Clone the meta-st-x-linux-qt git repository[edit | edit source]

 cd <distribution package installation directory>


 git clone -b v2.3.0 https://github.com/STMicroelectronics/meta-st-x-linux-qt.git layers/meta-st/meta-st-x-linux-qt

3.1.2. Clone the meta-qt git repository[edit | edit source]

 git clone -b 6.8.2 https://code.qt.io/yocto/meta-qt6.git layers/meta-qt6

3.2. Install X-LINUX-QT distribution package v2.2.0 - archive[edit | edit source]

Click on EXPAND, displayed on the right of the line, if you want to know how to install the X-LINUX-QT distribution package v2.2.0

To install the X-LINUX-QT distribution package v2.2.0 compatible with ecosystem release v6.1.0, follow the steps below.

3.2.1. Clone the meta-st-x-linux-qt git repository[edit | edit source]

 cd <distribution package installation directory>
 git clone -b v2.2.0 https://github.com/STMicroelectronics/meta-st-x-linux-qt.git layers/meta-st/meta-st-x-linux-qt

3.2.2. Clone the meta-qt git repository[edit | edit source]

 git clone -b 6.8.0 https://code.qt.io/yocto/meta-qt6.git layers/meta-qt6

Then see "Setup the build environment"

3.3. Install X-LINUX-QT distribution package v2.1.0 - archive[edit | edit source]

Click on EXPAND, displayed on the right of the line, if you want to know how to install the X-LINUX-QT distribution package v2.1.0

To install the X-LINUX-QT distribution package v2.1.0 compatible with ecosystem release v6.0.0, follow the steps below.

3.3.1. Clone the meta-st-x-linux-qt git repository[edit | edit source]

 cd <distribution package installation directory>
 git clone -b v2.1.0 https://github.com/STMicroelectronics/meta-st-x-linux-qt.git layers/meta-st/meta-st-x-linux-qt

3.3.2. Clone the meta-qt git repository[edit | edit source]

 git clone -b 6.6.3 https://code.qt.io/yocto/meta-qt6.git layers/meta-qt6

Then see "Setup the build environment"

3.4. Setup the build environment[edit | edit source]

  • For a new environment
Source the build environment with the correct board and layers:
  • For STM32MP1 series' boards
DISTRO=openstlinux-weston MACHINE=stm32mp1 BSP_DEPENDENCY="layers/meta-qt6 layers/meta-st/meta-st-x-linux-qt" source layers/meta-st/scripts/envsetup.sh
  • For STM32MP2 series' boards
DISTRO=openstlinux-weston MACHINE=stm32mp2 BSP_DEPENDENCY="layers/meta-qt6 layers/meta-st/meta-st-x-linux-qt" source layers/meta-st/scripts/envsetup.sh


  • For an already installed environment
Add the layers to the Yocto environment:
 cd <distribution package installation directory>
 source layers/meta-st/scripts/envsetup.sh
 bitbake-layers add-layer ../layers/meta-qt6 ../layers/meta-st/meta-st-x-linux-qt

4. Re-build the X-LINUX-QT starter package[edit | edit source]

To rebuild the X-LINUX-QT starter package, the user must install the X-LINUX-QT distribution package (as explained in previous chapter), set up the environment, and run the adequate bitbake command as follow:

 bitbake st-image-qt package-index

The output will be the "full image" files for the st-image-qt.

Then jump to X-LINUX-QT_Starter_Package to play with your new X-LINUX-QT starter package.

5. Re-build the X-LINUX-QT developer package[edit | edit source]

To rebuild the X-LINUX-QT developer package, the user must install the X-LINUX-QT distribution package (as explained in previous chapter), set up the environment, and run the adequate bitbake command as below:

 bitbake st-image-qt -c do_populate_sdk

The output will be the full SDK installer for the st-image-qt.

To configure a new STM32MPU Kit for the Qt™ Creator tool, please refer to a kit previously installed with the X-LINUX-QT Developer Package.

Jump to X-LINUX-QT_Developer_Package to play with your new X-LINUX-QT developer package.