Last edited 2 years ago

How to compile the device tree with the Distribution Package

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

1. Introduction[edit | edit source]

This article is intended for Yocto experts, or people who have some practical experience of the Yocto environmment.

This section describes the steps needed to create and configure a demo layer using DeviceTree files from the STM32CubeMX tool, and to add and configure a machine similar to those already supported by the OpenSTLinux Distribution Package (in particular the machine delivered inside the existing STM32MP BSP layer 'addons').

Reminder: this addon-layer is deployed under the following path in the delivery : <path of OpenSTLinux distribution delivery>/layers/meta-st/meta-st-stm32mp-addons/

2. Creating a new open embedded layer for your demo[edit | edit source]

You first need to create a new layer. See the latest How to create a new open embedded layer

After creation, you have under <path of OpenSTLinux distribution delivery>/layers/meta-st/:

$ tree meta-my-demo-layer
meta-my-demo-layer
├── conf
│   └── layer.conf
├── recipes-example
│   └── example
│       └── example.bb
├── COPYING.MIT
└── README

3 directories, 4 files

2.1. Update layer.conf file[edit | edit source]

Open the layer.conf file and add the lines below for the licenses, demo layer path, and dependency with the STM32MP BSP layer 'addons' :

EULA_FILE_ST:stm32mpmydemo = "${LAYERDIR}/conf/eula/${MACHINE}"
EULA_FILE_ST_MD5SUM:stm32mpmydemo = "8b505090fb679839cefbcc784afe8ce9"

#Inform bitbake for adding another location to search for licenses
LICENSE_PATH += "${LAYERDIR}/files/licenses"

# Set a variable to get the STM32MP MX BSP location
STM32MP_MY_DEMO_BASE = "${LAYERDIR}"

# This should only be incremented on significant changes that may
# cause compatibility issues with other layers
LAYERVERSION_meta-my-demo-layer = "1"

LAYERDEPENDS_meta-my-demo-layer = "stm-st-stm32mp-mx"

# OpenEmbedded compatibility information
# This should only be incremented on significant changes that will
# cause compatibility issues with other layers
LAYERVERSION_meta-my-demo-layer = "1"
LAYERSERIES_COMPAT_meta-my-demo-layer = "scarthgap"
Information
LAYERSERIES_COMPAT must be aligned with the version of OpenEmbedded used.
Please refer to https://wiki.yoctoproject.org/wiki/Releases

2.2. Create the machine for your demo[edit | edit source]

2.2.1. Prepare the machine configuration file[edit | edit source]

  • Copy the machine delivered inside the existing STM32MP BSP layer 'addons' into your demo layer
cp <path of OpenSTLinux distribution delivery>/layers/meta-st/meta-st-stm32mp-addons/conf/machine/stm32mpXX-mx.conf  <path of OpenSTLinux distribution delivery>/layers/meta-st/meta-my-demo-layer/conf/machine/stm32mp<X>-demo.conf
  • Open stm32mp<X>-demo.conf and update the line below
#@NEEDED_BSPLAYERS: layers/meta-openembedded/meta-oe layers/meta-openembedded/meta-python layers/meta-st/meta-st-stm32mp-addons
  • Add these lines after the series of includes:
# Define specific common machine name
MACHINEOVERRIDES .= ":stm32mpmydemo"

2.2.2. Configure the machine configuration file for your demo[edit | edit source]

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines


In the customer machine file, move to User machine customization sections paragraph to configure your machine:

  • Boot Scheme
To select your boot scheme configuration(s), comment and uncomment the BOOTSCHEME_LABELS lines.
  • Boot Device Choice
To select your boot device configuration(s), comment and uncomment the BOOTDEVICE_LABELS lines.
  • Support Feature Choice
To select additional features to enable on board, uncomment the MACHINE_FEATURES proposed lines.
  • Specific firmware and kernel modules configuration
This section allows user to configure some specificities related to its board hardware.
- KERNEL_MODULE_AUTOLOAD you may need to feed this variable with the list of kernel modules that need to be loaded at boot time, such as 'goodix' for current touch-screen used on STM32MP157F-EV1 evaluation board.
- BLUETOOTH_LIST in case you enable the bluetooth feature for your machine, you should set, at least, the firmware module to use for your hardware (e.g. 'linux-firmware-bluetooth-bcm4343' for STM32MP157F-DK2 discovery board).
- WIFI_LIST in case you enable the wifi feature for your machine, you should set, at least, the firmware module to use for your hardware (e.g.'linux-firmware-bcm43430' for STM32MP157F-DK2 discovery board).
  • CubeMX Project config
You have to uncomment and configure the following variables to set your CubeMX project:
- CUBEMX_DTB name of CubeMX generated device tree files, without file extension (e.g. stm32mp135f-<ProjectName>-mx)
- CUBEMX_PROJECT path of CubeMX generated device tree files relative to layer path folder (e.g. mx/<ProjectPath>)
- CUBEMX_PROJECT_NAME name of CubeMX project (e.g. <ProjectName>)
Optionally you can also uncomment and configure the CUBEMX_M33_TZ variable to indicate if M33 co-processor is used with Trustzone enabled or not (only for STM32MP2 series).

In order to give a better view on how to configure these variables, some machine samples are provided to show how to set-up a disco and eval board CubeMX machine: refer to conf/machine/examples from meta-st-stm32mp-addons layer.


2.3. Issue with for stm32mp2 machine[edit | edit source]

Warning
Point of attention with M33FW_FIRMWARE configuration on A35-TD flavor

With A35-TD flavor , several ST boards use the Cortex M33 processor (associated to a specific firmware provided by STM32Cube MP2).
For this usage the flag MACHINE_FEATURES have the tag m33copro present.

In this context, you must declare M33FW_FIRMWARE and M33FW_DEFAULT_FIRMWARE variables.

Table of default firmware to use with ST boards:

Board Configuration to have
STM32MP215F-DK M33FW_FIRMWARE[cubemx] ="Projects/STM32MP215F-DK/Demonstrations/OpenAMP/OpenAMP_TTY_echo,OpenAMP_TTY_echo"

M33FW_DEFAULT_FIRMWARE[cubemx] ="OpenAMP_TTY_echo"

STM32MP257F-DK for STM32MP23x lines evaluation M33FW_FIRMWARE[cubemx] ="Projects/STM32MP235F-DK/Demonstrations/USBPD_DRP_UCSI,USBPD_DRP_UCSI"

M33FW_DEFAULT_FIRMWARE[cubemx] ="USBPD_DRP_UCSI"

STM32MP257F-DK M33FW_FIRMWARE[cubemx] ="Projects/STM32MP257F-DK/Demonstrations/USBPD_DRP_UCSI,USBPD_DRP_UCSI"

M33FW_DEFAULT_FIRMWARE[cubemx] ="USBPD_DRP_UCSI"

STM32MP257F-EV1 M33FW_FIRMWARE[cubemx] ="Projects/STM32MP257F-EV1/Demonstrations/USBPD_DRP_UCSI,USBPD_DRP_UCSI"

M33FW_DEFAULT_FIRMWARE[cubemx] ="USBPD_DRP_UCSI"

Information
If you don't need to use the Cortex M33 processor, you can disable it by not providing the tag 'm33copro' on 'MACHINE_FEATURES'


2.4. Associate EULA with the new demo machine[edit | edit source]

Copy the eula folder delivered inside the existing STM32MP BSP layer 'addons' into your demo layer

cp -Rf <path of OpenSTLinux distribution delivery>/layers/meta-st/meta-st-stm32mp-addons/conf/eula/  <path of OpenSTLinux distribution delivery>/layers/meta-st/meta-my-demo-layer/conf/.

Cleanup unexpected symbolic links from eula folder newly populated:

find <path of OpenSTLinux distribution delivery>/layers/meta-st/meta-my-demo-layer/conf/eula -type l -exec rm -f {} \;

Then create the symbolic link with the machine used for your demo:

cd <path of OpenSTLinux distribution delivery>/layers/meta-st/meta-my-demo-layer/conf/eula
ln -sf ST_EULA_SLA stm32mpX-demo

2.5. Move DeviceTree files and project coming from STM32CubeMX tool[edit | edit source]

The principle is that the user generates devicetree files for the targeted demo from the STM32CubeMX tool.

Warning
Most of the time, generated devicetree files - mainly user sections - must be reworked by the end user for compilation and functional purposes. Each demo is delivered with an application note that describe changes applied on STM32CubeMX devicetree files

.

These files are then moved into the “mx” folder created into your demo layer  : <path of OpenSTLinux distribution delivery>/layers/meta-st/meta-my-demo-layer/mx/

Sub-folders are created and populated with the generated devicetree files:

mx/${CUBEMX_PROJECT}/kernel
mx/${CUBEMX_PROJECT}/u-boot
mx/${CUBEMX_PROJECT}/tf-a
mx/${CUBEMX_PROJECT}/optee-os

With CUBEMX_PROJECT that is equal to the value defined inside the machine used for the demo.

2.6. Update the README file[edit | edit source]

Please update the README file with the information needed for building and executing the demo.

2.7. Clean up useless content[edit | edit source]

You can delete the content of the recipes-example folder created by the create-layer command.

After making all of the updates, your demo layer should be similar to:

$ tree meta-my-demo-layer
meta-my-demo-layer
├── conf
│   ├── eula
│   │   ├── ST_EULA_SLA
│   │   ├── stm32mp''X''-demo -> ST_EULA_SLA
│   │   └──  ...
│   ├── machine
│   │   └── stm32mp''X''-demo.conf
│   └── layer.conf
├── mx
│   └── ${CUBEMX_PROJECT}
│            ├── kernel
│            │   └── stm32mpXXXx-my-demo-mx.dts
│            ├── optee-os
│            │   └── stm32mpXXXx-my-demo-mx.dts
│            ├── tf-a
│            │   ├── stm32mpXX-mx.dtsi
│            │   ├── stm32mpXXXx-my-demo-mx.dts
│            │   └── stm32mpXXXx-my-demo-mx-fw-config.dts
│            └── u-boot
│                ├── stm32mpXXXx-my-demo-mx.dts
│                └── stm32mpXXXx-my-demo-mx-u-boot.dtsi
├── COPYING.MIT
└── README

3. Adding specific recipes and content necessary for your demo[edit | edit source]

Examples of further add-on components:

  • Recipes for installing distro-specific configuration files
  • Any image recipes specific to user distribution
  • A psplash append file for a branded splash screen
  • Any other append files to make custom changes

Some other added components (*bb) are more specific: images, system services, and so on (a non-exhaustive list is shown below):

  • Recipes-core for psplash screen, systemd services
  • Recipes-samples for example images

...