Last edited 3 months ago

STM32MP25 Discovery kits - OpenSTDroid Starter Package

(Redirected from STM32MP25 Discovery kits - Starter Package for Android)
Applicable for STM32MP25x lines

This article shows how to start up a STM32MP257x-DK Discovery kits (flexible and complete development platforms for the STM32MP25 microprocessor devices) with the software image for the Android-based OpenSTDroid embedded software. It is valid for the STM32MP257x-DK Discovery kits: the part numbers are specified in the STM32MP25 microprocessor part numbers article.

It lists the required material, points to the board features description, and gives the step-by-step process to set up the system.

Finally, it proposes to run some basic use cases and to discover some of the board capabilities.

1. Starter Package content[edit | edit source]

This Starter Package provides:

  • the OpenSTDroid distribution binaries
  • the partition layout required to flash the device with STM32CubeProgrammer

2. Checking the material[edit | edit source]

Mandatory

PC Linux or Windows operating systems. See PC prerequisites for more details on the required configurations
STM32MP257x-DK Discovery kit Flexible and complete development platform for the STM32MP25 microprocessor device including:
microSDTM card It is populated with OpenSTLinux distribution (Linux software), and provides extra storage capacity. An 16-Gbyte minimum microSD card is needed.
USB type-C cable It connects the STM32MP257x-DK Discovery kit to the PC through the USB type-C (ST-LINK/V3) connector.
USB type-C cable It connects the STM32MP257x-DK Discovery kit to a USB OTG device through the USB type-C connector.


Optional

LCD screen - recommended Two types of screen are possible: LVDS or HDMI
USB keyboard and mouse Thanks to the USB type A connectors, the STM32MP257x-DK Discovery kit can be equipped with a full-size keyboard and mouse.
Ethernet cable It can connect the STM32MP257x-DK Discovery kit to a network through the RJ45 connector.
Camera MIPI CSI-2 Camera

Optionally, devices and extension boards might be plugged to the STM32MP257x-DK Discovery kit thanks to connectors such as:

  • GPIO expansion connector
  • ...


3. Assembling the board[edit | edit source]

The STM32MP257x-DKx Discovery kit package (STM32MP257F-DK ) contains the items listed below.

Position Description
1 MB1605 motherboard
2 microSD™ card


STM32MP257x-DKx Discovery kit out of the box
STM32MP257F-DK Discovery kit shown here (picture not contractual)
Information
LVDS displays and CSI cameras are available for purchase to complete this basic setup.

The complete set contains:

STM32MP257F-DK and additional accessories kits shown here (picture is not contractual)
Position Description
1 MB1605 main board
2 MicroSD card
3 LVDS display cable (provided via B-LVDS7-WSVGA package) (optional)
4 7” LVDS WSVGA display with EDT ETML0700Z9NDHA panel touch panel provided with the B-LVDS7-WSVGA package (optional)
5 Camera board FFC (provided with the B-CAMS-IMX package) (optional)
6 MB1854 board AI camera provided with the B-CAMS-IMX package (optional)


STM32MP257x-DK Discovery kit assembly
STM32MP257F-DK shown here (picture is not contractual)


3.1. Connecting the LVDS display to the board (optional)[edit | edit source]

Display board assembly (picture is not contractual)


  • Check the cable orientation shown above using the black mark and the white twisted pairs.
  • Find the LVDS ports on the STM32MP257x-DK Discovery kit (CN2) and the display (CN1). The LVDS display box contains one cable.
  • Insert the cable into each port as shown below:
Display board assembly (picture is not contractual)


3.2. Connecting the MB1854 camera board to the board (optional)[edit | edit source]

Camera board assembly (picture is not contractual)


  • Find the camera ports on the STM32MP257x-DK Discovery kit (CN8) (#1 in the image above) and MB1854 (CN1) (#2 in the image above). The camera box contains one FFC.
  • For each port:
    • Pull the black plastic (#1 in the image below) lightly to insert the contact side of the FFC towards the board (#2 in the image below).
    • Push the black plastic carefully to hold the FFC (#3 in the image below).
Camera board assembly (picture is not contractual)


3.3. STM32MP257x-DK Discovery kit assembled[edit | edit source]


STM32MP257x-DK Discovery kit assembled
STM32MP257F-DK shown here (picture is not contractual)



4. Installing the tools[edit | edit source]

4.1. Installing the STM32CubeProgrammer tool[edit | edit source]

STM32CubeProgrammer for Linux® host PC STM32CubeProgrammer for Windows® host PC
Download
  • Go on st.com to download the STM32CubeProgrammer software

Version v2.23.0

  • Download the archive file on your host PC in a temporary directory
  • Uncompress the archive file to get the STM32CubeProgrammer installers:

unzip en.stm32cubeprog.zip

Installation
  • Execute the Linux installer, which guides you through the installation process.
$> ./SetupSTM32CubeProgrammer-2.23.0.linux
  • The path to the STM32CubeProgrammer binary must be added to the PATH environment variable
    • either in each Terminal program in which the STM32CubeProgrammer binary needs to be used, using the following command:
$> export PATH=<my STM32CubeProgrammer install directory>/bin:$PATH
  • or once for all by creating a link to the STM32CubeProgrammer binary in a directory already present in PATH. For example, if "/home/bin" is in the PATH environment variable, run the following command:
$> ln -s <my STM32CubeProgrammer install directory>/bin/STM32_Programmer_CLI /home/bin/STM32_Programmer_CLI
  • Execute the Windows installer, which guides you through the installation process.
User manual
Detailed release note
  • Details about the content of this tool version are available from ST web site at Release Note .


4.2. Preparing the USB serial link for flashing[edit | edit source]

It is recommended to use the USB (in DFU mode) for flashing rather than the UART, which is too slow.

Below indications on how to install the USB in DFU mode under Linux and Windows OS, respectively.

  • For Linux host PC or Windows host PC with VMWare:

The libusb1.0 package (including USB DFU mode) must be installed to be able to connect to the board via the USB port. This is achieved by typing the following command from the host PC terminal:

sudo apt-get install libusb-1.0-0

To allow STM32CubeProgrammer to access the USB port through low-level commands, proceed as follows:

cd <your STM32CubeProgrammer install directory>/Drivers/rules 
sudo cp *.* /etc/udev/rules.d/
  • For Windows host PC:

Run the “STM32 Bootloader.bat” file to install the STM32CubeProgrammer DFU driver and activate the STM32 microprocessor device in USB DFU mode. This driver (installed by STM32 Bootloader.bat) is provided within the STM32CubeProgrammer release package. It is located in the DFU driver folder, \Drivers\DFU_Driver.

In case of issue, refer to How to proceed when the DFU driver installation fails on Windows host PC.

To validate the installation, the DFU driver functionality can be verified by following the FAQ instructions provided in how to check if the DFU driver is functional.

4.3. Image download[edit | edit source]

Warning
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.
STM32MPU distribution for Android™
Tag Flash device Link Release note
st-android-16.0.0-2026-05-26 eMMC Go on st.com to download the STM32MP2 OpenSTDroid Starter Package for STM32MP25 (select the adapted board) st-android-16.0.0-2026-05-26 release note (v6.2.0)
st-android-16.0.0-2026-09-08
Coming soon
st-android-16.0.0-2026-09-08 release note (v6.2.1)
Installation
  • Go to the host PC directory where to install the Starter Package (<Starter Package installation directory>); for example:
cd <working directory path>/Android-Starter-Package
  • Download the tarball file (*.tar.gz)) in this directory
  • Uncompress the tarball file to get the binaries for the different partitions of the image, and the flash layout files:
tar xvf st-android-<version>-<date>-stm32mp257f-ev1-<flash device>-starter.tar.gz


4.4. Flashing the eMMC images[edit | edit source]

The STM32CubeProgrammer tool is used to flash the STM32MP25 Discovery kits with the downloaded image.

Several Flash devices (microSD, eMMC...) are available on this board: see the STM32 MPU Flash mapping for Android article if you want to know more about the supported Flash memory technologies, and the Flash partitions. The steps below consider the eMMC as the Flash device.

Let's flash the downloaded image on the eMMC card:

  • Set the boot switches to the off position (boot from UART/USB)
Boot from UART/USB
  • Connect the USB type-C (OTG) port (4) to the host PC that contains the downloaded image
  • Connect the USB type-C (power supply) port (1) to the power connector or a host PC
Warning
If the LEDs (near 1) are red and orange you need to use an adapted power supply (USB PD 5V-3A).
  • Press the reset button (2) to reset the board
Discovery kits connections for flashing
STM32MP257F-DK shown here (picture is not contractual)
  • Go to the Starter Package directory that contains the binaries and the Flash layout files
 cd <Starter Package installation directory>/st-android-<version>-<date>-stm32mp257f-dk-<flash device>-starter
Information
The commands below are for a Linux® host PC; however, they are similar for a Windows host PC except that STM32_Programmer_CLI is replaced by STM32_Programmer_CLI.exe.
  • Check that the STM32CubeProgrammer tool is installed and accessible; if not, go to the installation procedure (installing the tools)
 STM32_Programmer_CLI --h
      -------------------------------------------------------------------
                        STM32CubeProgrammer <tool version>                  
      -------------------------------------------------------------------
  • Get the device port location for the USB link
 STM32_Programmer_CLI -l usb
       -------------------------------------------------------------------
                         STM32CubeProgrammer <tool version>                  
       -------------------------------------------------------------------

=====  DFU Interface   =====

Total number of available STM32 device in DFU mode: 1

  Device Index           : USB1
  USB Bus Number         : 003
  USB Address Number     : 005
  Product ID             : DFU in HS Mode @Device ID /0x505, @Revision ID /0x2000
  Serial number          : 001900364136500100373653
  Firmware version       : 0x0110
  Device ID              : 0x0505
  • Fuse the eMMC RPMB with the RPMB test key
Important
Please read carefully

The starter is using RPMB as secure storage. For that purpose, the RPMB key must be fused on the eMMC.

This procedure must be followed only if the RPMB key has not already been fused on your STM32MP25 Discovery Kit.

By default, the RPMB TEST KEY is used : rpmb/rpmbk.bin

Follow the procedure described in rpmb/README.md of the starter package

Warning
This procedure is not yet available on Windows Host. Waiting availability, please load, flash and start the OpenSTDroid v5.1.1 starter package on st.com. It integrates an automatic mechanism to fuse the RPMB key if not already performed with the TEST KEY
  • Flash the eMMC with the partition images
 STM32_Programmer_CLI -c port=usb1 -w flashlayout/FlashLayout_emmc_cm33tdcid.tsv

This operation takes several minutes.

Go see the STM32CubeProgrammer article to know more about the flashing operation

5. Booting the board[edit | edit source]

Now that the image is flashed on the STM32MP257x-DK Discovery kits, let's finalize the system configuration:

  • Step 0: check that the LVDS display board is well connected or connect a display through HDMI.
  • Step 1: check the configuration of the switches and jumpers:
    • The boot related switches must be configured so that the device (e.g. eMMC) on which the image has been flashed is selected as boot source.
The figure below shows the boot switches for the recommended boot from eMMC (for M33-TD flavor ).
Boot from eMMC for M33-TD flavor
  • Step 2: (optionally) connect a USB keyboard and/or a USB mouse (not provided) using the USB type-A ports (3 in the picture below).
  • Step 3: (optionally) connect an Ethernet cable (not provided) to the dedicated connector (2).
STM3STM32MP257x-DKx Discovery kit connections (picture is not contractual)


  • Step 4: connect the USB Power – TypeC cable to the connector (1).
  • Step 5: (optionally) install and configure a remote Terminal program (e.g. Minicom on Ubuntu Linux PC or Tera Term on Windows PC) onto your host PC, and connect the ST-LINK/V3 USB type-C port (1) to a host PC that runs a Terminal program with ST-LINK/V3 virtual port.
  • Step 6: press the reset button (2) to reset the board

The board boots and the system will be available after few seconds.

6. How to go further?[edit | edit source]

Now that the image is flashed on the STM32MP25 Evaluation board, you might want to switch to the STM32MPU OpenSTDroid Distribution Package, in order to modify or tune the STM32MPU Embedded Software distribution with your own developments.