Last edited 10 months ago

STM32MP257x-DKx - hardware description

Applicable for STM32MP23x lines, STM32MP25x lines

This article provides an overview of STM32MP257x-DK Discovery kits.

1. Article purpose[edit | edit source]

This article briefly describes:

  • How to assemble the different elements provided in the commercial box and additional optional accessories
  • The different components on the boards
  • How to connect the boards to external material
  • How to configure the board for boot
  • The configurations of the connector pins

This article is valid for the STM32MP257F-DK Discovery kit: the part numbers are specified in the STM32MP25 microprocessor part numbers article.

Information
This article is an introduction to the STM32MP257x-DK Discovery kit. For more detailed information, refer to the STM32MP257x-DK Discovery kit user manuals.

2. Board assembly[edit | edit source]

The STM32MP257x-DKx Discovery kit package (STM32MP257F-DK ) contains the items listed below.

Position Description
1 MB1605 motherboard
2 microSD™ card


STM32MP257x-DKx Discovery kit out of the box
STM32MP257F-DK Discovery kit shown here (picture not contractual)
Information
LVDS displays and CSI cameras are available for purchase to complete this basic setup.

The complete set contains:

STM32MP257F-DK and additional accessories kits shown here (picture is not contractual)
Position Description
1 MB1605 main board
2 MicroSD card
3 LVDS display cable (provided via B-LVDS7-WSVGA package) (optional)
4 7” LVDS WSVGA display with EDT ETML0700Z9NDHA panel touch panel provided with the B-LVDS7-WSVGA package (optional)
5 Camera board FFC (provided with the B-CAMS-IMX package) (optional)
6 MB1854 board AI camera provided with the B-CAMS-IMX package (optional)


STM32MP257x-DK Discovery kit assembly
STM32MP257F-DK shown here (picture is not contractual)


2.1. Connecting the LVDS display to the board (optional)[edit | edit source]

Display board assembly (picture is not contractual)


  • Check the cable orientation shown above using the black mark and the white twisted pairs.
  • Find the LVDS ports on the STM32MP257x-DK Discovery kit (CN2) and the display (CN1). The LVDS display box contains one cable.
  • Insert the cable into each port as shown below:
Display board assembly (picture is not contractual)


2.2. Connecting the MB1854 camera board to the board (optional)[edit | edit source]

Camera board assembly (picture is not contractual)


  • Find the camera ports on the STM32MP257x-DK Discovery kit (CN8) (#1 in the image above) and MB1854 (CN1) (#2 in the image above). The camera box contains one FFC.
  • For each port:
    • Pull the black plastic (#1 in the image below) lightly to insert the contact side of the FFC towards the board (#2 in the image below).
    • Push the black plastic carefully to hold the FFC (#3 in the image below).
Camera board assembly (picture is not contractual)


2.3. STM32MP257x-DK Discovery kit assembled[edit | edit source]


STM32MP257x-DK Discovery kit assembled
STM32MP257F-DK shown here (picture is not contractual)



3. Board overview[edit | edit source]

Main board MB1605, revision C-01 : part of the STM32MP257x-DK Discovery kit .

STM32MP257x-DK Discovery kit front side
STM32MP257F-DK shown here (picture is not contractual)


Details about the LEDs:

  • LD11 turns green when a power connection is established (the power cable is inserted into the CN21 connector).
  • Two general-purpose color LEDs (LED1 and LD9) are available as light indicators:
    • The blue LED (LED1) is used as the Linux® Heartbeat LED, which blinks as long as Linux® is running on the Arm® Cortex®-A.
    • The orange LED (LD9) is used as an STM32Cube example verdict LED.
  • The two LEDs, LD7 (red) and LD8 (green), are free user LEDs that can be by configured by the user for any purpose, as explained in the LEDs and buttons on STM32 MPU boards wiki article.
  • The LD5 and LD6 LEDs are used as an ST-LINK status indicator.


STM32MP257x-DK Discovery kit back side
STM32MP257F-DK shown here (picture is not contractual)



4. Board connection[edit | edit source]

The image below shows the recommended connections for getting started with the STM32MP257x-DK Discovery kits. As shown in the board overview, other connectors are available for this board (for example, the GPIO expansion connector).


MB1605 motherboard: STM32MP257F 14x14MicroSD<sup>™</sup> card slot, on back side2 x USB type A (host) (such as a mouse or keyboard USB driver)USB3.0 DRD Type-C (programmable through STM32CubeProgrammer)Reset buttonEthernet (network)USB Power Delivery Type-C (Power or STLINK)HDMI (TV Screen)CSI camera connectorLVDS display connector
STM32MP257x-DKx Discovery kit connections (picture is not contractual)
Warning
To have the possibility to use ST-Link or the consoles, the USB Power Delivery Type-C must be connected to a PC with USB Type-C/Type-C cable. The USB Type-C on the PC must be a USB Power Delivery Type-C.
Information
Via ST-LINK, it is possible to have access to 2 consoles: one for Cortex-M and one for Cortex-A.


5. Boot switches[edit | edit source]

The STM32MP257x-DK Discovery kit can boot from different flash memory devices (microSD, eMMC) based on ROM code selection; using the microSD card is recommended.

boot mode Boot 0 Boot 1 Boot 2 Boot 3 The boot-related switches (SW1 and SW2
in the board overview picture
Storage device used for the Cortex-A35 boot Storage device used for the Cortex-M33 boot
Forced USB boot for flash memory programming 0 0 0 0
USB/UART for programming NA
Boot from microSD card for A35-TD flavor 1 0 0 0
SD card NA
Boot from microSD card for M33-TD flavor 1 1 1 0
|
SD card SD card
Boot from eMMC for A35-TD flavor 0 1 0 0
eMMC NA
Boot from eMMC for M33-TD flavor 0 0 0 1
eMMC eMMC
Developer mode 1 1 0 0
NA NA


When the switch is set to the "ON" position, the BOOTx value is "1"; otherwise it is "0".

6. GPIO mapping[edit | edit source]

6.1. GPIO expansion connector[edit | edit source]

The table below describes the pins of the GPIO expansion connector (CN5 in the board overview picture):

Function STM32 pin Pin Pin STM32 pin Function
3V3 - 1 2 - 5V
GPIO2 / I2C8_SDA PZ3 3 4 - 5V
GPIO3 / I2C8_SDL PZ4 5 6 - GND
GPIO4 / MCO1 PF11 7 8 PF13 GPIO14 / USART6_TX
GND - 9 10 PF14 GPIO15 / USART6_RX
GPIO17 / USART6_RTS PG5 11 12 PD2 GPIO18 / SAI4_SCKA
GPIO27 PZ9 13 14 - GND
GPIO22 PZ0 15 16 PZ1 GPIO23
3V3 - 17 18 PZ6 GPIO24
GPIO10 / SPI6_MOSI PC7 19 20 - GND
GPIO9 / SPI6_MISO PC4 21 22 PZ7 GPIO25
GPIO11 / SPI6_SCK PF7 23 24 PF4 GPIO8 / SPI6_NSS
GND - 25 26 PZ5 GPIO7
I2C2_SDA PF0 27 28 PF2 I2C2_SCL
GPIO5 / TIM8_CH4 PC10 29 30 - GND
GPIO6 / TIM5_CH1 PH8 31 32 PA5 GPIO12 / TIM2_CH4
GPIO13 / TIM4_CH2 PA1 33 34 - GND
GPIO19 / SAI4_FSA PD0 35 36 PF15 GPIO16 / USART6_CTS
GPIO26 PZ8 37 38 PD1 GPIO20 / SAI4_SDA
GND - 39 40 PB5 GPIO21 / SAI4_SDB

6.2. User buttons and LEDs[edit | edit source]

The tables below describe the GPIO assignments for the user buttons and LEDs. Refer to the LEDs and buttons on STM32 MPU boards article for more details.

GPIO for LEDs

LED color and label GPIO
Green LD8 PH5
Red LD7 PH4
Orange LD9 PH6
Blue LED1 PH7

GPIO for user buttons

Button GPIO
USER1 PC5
USER2 PC11

7. References[edit | edit source]