Last edited 2 years ago

Core dump: Difference between revisions

Registered User
mNo edit summary
Registered User
No edit summary
 
(2 intermediate revisions by 2 users not shown)
Line 1: Line 1:
<noinclude>{{ApplicableFor
{{ApplicableFor
|MPUs list=STM32MP13x, STM32MP15x
|MPUs list=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x
|MPUs checklist=STM32MP13x,STM32MP15x
|MPUs checklist=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x
}}</noinclude>
}}
<noinclude></noinclude>
==Article purpose==
==Article purpose==
This article provides the initial information set needed to start the '''core dump''' Linux<sup>&reg;</sup> service.
This article provides the initial information set needed to start the '''core dump''' Linux<sup>&reg;</sup> service.
Line 41: Line 42:


* Verify configuration are present
* Verify configuration are present
  {{Board$}} ls /etc/systemd/coredump.conf.d/
  {{Board$}}ls /etc/systemd/coredump.conf.d/
  coredump-custom.conf
  coredump-custom.conf


* Verify if '''core dump''' is registered by Linux
* Verify if '''core dump''' is registered by Linux
  {{Board$}} cat /proc/sys/kernel/core_pattern
  {{Board$}}cat /proc/sys/kernel/core_pattern
  |/lib/systemd/systemd-coredump %P %u %g %s %t %c %h %e
  |/lib/systemd/systemd-coredump %P %u %g %s %t %c %h %e


Line 56: Line 57:
* Launch a program
* Launch a program
Launch a program (for example: "weston-flower")
Launch a program (for example: "weston-flower")
  {{Board$}} weston-flower &
  {{Board$}}weston-flower &


* Get the pid of this program with the ps command
* Get the pid of this program with the ps command
  {{Board$}} ps ax | grep <program>
  {{Board$}}ps ax | grep <program>


* kill the program with specific '''ILL''' (4) signal (ILL: Illegal instruction)
* kill the program with specific '''ILL''' (4) signal (ILL: Illegal instruction)
  {{Board$}} kill -4 <pid of program>
  {{Board$}}kill -4 <pid of program>
Force to generate core dump (for example)
Force to generate core dump (for example)
  {{Board$}} kill -4 `pidof weston-flower`
  {{Board$}}kill -4 `pidof weston-flower`


* check ''/var/lib/systemd/coredump/'', the core dump associated to this abnormal termination:
* check ''/var/lib/systemd/coredump/'', the core dump associated to this abnormal termination:
  {{Board$}} find /var/lib/systemd/coredump/
  {{Board$}}find /var/lib/systemd/coredump/
/var/lib/systemd/coredump/
/var/lib/systemd/coredump/
/var/lib/systemd/coredump/core.weston-flower.0.47f9def8d0f44af5919d0e4cd5ee04ae.554.1543488316000000.xz
/var/lib/systemd/coredump/core.weston-flower.0.47f9def8d0f44af5919d0e4cd5ee04ae.554.1543488316000000.xz
Line 73: Line 74:


The core dump generated has a size of around 300 Kbytes
The core dump generated has a size of around 300 Kbytes
  {{Board$}} du -sh /var/lib/systemd/coredump/*
  {{Board$}}du -sh /var/lib/systemd/coredump/*
  295K /var/lib/systemd/coredump/core.weston-flower.0.47f9def8d0f44af5919d0e4cd5ee04ae.554.1543488316000000.xz
  295K /var/lib/systemd/coredump/core.weston-flower.0.47f9def8d0f44af5919d0e4cd5ee04ae.554.1543488316000000.xz



Latest revision as of 15:48, 4 November 2024

Applicable for STM32MP13x lines, STM32MP15x lines, Unknown MPU, Unknown MPU, Unknown MPU

1. Article purpose[edit | edit source]

This article provides the initial information set needed to start the core dump Linux® service.

2. Introduction[edit | edit source]

The following table provides a brief description of the tool, as well as its availability depending on the software packages:

Yes: this tool is either present (ready to use or to be activated), or can be integrated and activated on the software package.

No: this tool is not present and cannot be integrated, or it is present but cannot be activated on the software package.

Tool STM32MPU Embedded Software distribution STM32MPU Embedded Software distribution for Android™
Name Category Purpose Starter Package Developer Package Distribution Package Starter Package Developer Package Distribution Package
systemd core dump Debugging tools systemd core dump: generates core dump files on Linux
Yes No Yes No No No

core dump records the states of the working program memory before an abnormal termination. The dump record assists in diagnosing and debugging program errors.

Systemd provides, via a configuration file, a way to generate and store core dump for Linux system.

3. Installing the trace and debug tool on your target board[edit | edit source]

3.1. Using STM32MPU Embedded Software Distribution[edit | edit source]

3.1.1. Distribution Package[edit | edit source]

ST via OpenSTLinux layer provides a recipe named systemd-conf, which provides a core dump configuration for systemd.

The core dump configuration is available only via OpenSTLinux distribution. If this configuration is activated via another distribution, an add-on must be made in the systemd-conf recipe.

recipes-core/systemd/systemd-conf.bbappend:

do_install_append() {
    install -d ${D}${sysconfdir}/systemd/coredump.conf.d/
    echo "[Coredump]" > ${D}${sysconfdir}/systemd/coredump.conf.d/coredump-custom.conf
    echo "Storage=external" >> ${D}${sysconfdir}/systemd/coredump.conf.d/coredump-custom.conf
}

4. Getting started[edit | edit source]

4.1. Verify setup[edit | edit source]

  • Verify configuration are present
ls /etc/systemd/coredump.conf.d/
coredump-custom.conf
  • Verify if core dump is registered by Linux
cat /proc/sys/kernel/core_pattern
|/lib/systemd/systemd-coredump %P %u %g %s %t %c %h %e

4.2. Crash append[edit | edit source]

If an application/program has crashed and generated a core dump while running, the core dump result is stored in /var/lib/systemd/coredump.

(See the How to test core dump service below ).

5. How to test core dump[edit | edit source]

  • Launch a program

Launch a program (for example: "weston-flower")

weston-flower &
  • Get the pid of this program with the ps command
ps ax | grep <program>
  • kill the program with specific ILL (4) signal (ILL: Illegal instruction)
kill -4 <pid of program>

Force to generate core dump (for example)

kill -4 `pidof weston-flower`
  • check /var/lib/systemd/coredump/, the core dump associated to this abnormal termination:
find /var/lib/systemd/coredump/

/var/lib/systemd/coredump/ /var/lib/systemd/coredump/core.weston-flower.0.47f9def8d0f44af5919d0e4cd5ee04ae.554.1543488316000000.xz


The core dump generated has a size of around 300 Kbytes

du -sh /var/lib/systemd/coredump/*
295K /var/lib/systemd/coredump/core.weston-flower.0.47f9def8d0f44af5919d0e4cd5ee04ae.554.1543488316000000.xz

6. To go further[edit | edit source]

To make core analysis please refer to GDB#Core_dump_analysis_using_GDB

7. Documentation and web articles[edit | edit source]


"External links"
Document link Document Type Description
systemd man page for core dump configuration Standard systemd man page