Last edited 3 weeks ago

STM32MPU Developer Package


This article describes how to get and use the Developer Package of the STM32MPU Embedded Software for any development platform of the STM32MP1 series (STM32MP15 boards and STM32MP13 boards) and STM32MP2 series (STM32MP21 boards, STM32MP23 boards and STM32MP25 boards), in order to modify some of its pieces of software, or to add applications on top of it.

It lists some prerequisites in terms of knowledge and development environment, and gives the step-by-step approach to download and install the STM32MPU Embedded Software components for this Package.

Finally, it proposes some guidelines to upgrade (add, remove, configure, improve...) any piece of software.

Linux Yocto developer package.png

1. Developer Package content[edit | edit source]

If you are not yet familiar with the STM32MPU Embedded Software distribution and its Packages, read the following articles:

If you are already familiar with the Developer Package for the STM32MPU Embedded Software distribution, the fast links to essential commands might interest you.

To sum up, this Developer Package provides:

  • for the OpenSTLinux distribution (development on Arm® Cortex®-A processor):
    • the software development kit (SDK), based on Yocto SDK, for cross-development on a host PC
    • the following pieces of software in source code:
      • Linux® kernel
      • gcnano-driver
      • U-Boot
      • Trusted Firmware-A (TF-A)
      • Open source Trusted Execution Environment (OP-TEE)
      • External device tree
  • for the Cortex®-M processor firmware development (only for STM32MP15x lines More info.png and STM32MP2 series with both A35-TD flavor More info green.png and M33-TD flavor More info green.png when supported):
    • the integrated development environment (IDE) (STM32CubeIDE)
    • the STM32CubeMPU Package including all pieces of software (BSP, HAL, middlewares, and applications) in source code
    • the Trusted Firmware-M (TF-M) in source code (for STM32MP2 series only)

Note that the application frameworks for the OpenSTLinux distribution are not available as source code in this Package.

Components of the Developer Package
TF-M is available only for STM32MP2 series

2. Developer Package step-by-step overview[edit | edit source]

The steps to get the STM32MPU Embedded Software Developer Package ready for your developments are:
Checking the prerequisites
Installing the Starter Package for your board and the debug symbol files

Installing the components to develop software running on Arm® Cortex®-A (OpenSTLinux distribution)

Installing the SDK (mandatory for any development on Arm® Cortex®-A)
Installing the OpenSTLinux BSP package (mandatory only if you plan to modify the Linux kernel, to add external out-of-tree Linux kernel modules, to modify U-Boot, TF-A and/or OP-TEE OS)

Installing the components to develop software running Arm Cortex-M (STM32CubeMPU Package)

Installing STM32CubeIDE (mandatory for any development on Arm® Cortex®-M)
Installing the STM32CubeMPU Package (mandatory only if you plan to modify the STM32Cube firmware)

Once these steps are achieved, you are able to:

3. Checking the prerequisites[edit | edit source]

3.1. Knowledge[edit | edit source]

The STM32MPU Developer Package aims at enriching a Linux-based software for the targeted product: basic knowledge about Linux are recommended to make the most of this Package.

Having a look at the STM32MPU Embedded Software architecture overview is also highly recommended.

3.2. Development setup[edit | edit source]

The recommended setup for the development PC (host) is specified in the following article: PC prerequisites.

Whatever the development platform (board) and development PC (host) used, the range of possible development setups is illustrated by the picture below.

Development setup for Developer and Distribution Packages


The following components are mandatory:

  • Host PC for cross-compilation and cross-debugging, installed as specified above
  • Board assembled and configured as specified in the associated Starter Package article
  • Mass storage device (for example, microSD card) to load and update the software images (binaries)

The following components are optional, but recommended:

  • A serial link between the host PC (through Terminal program) and the board for traces (even early boot traces), and access to the board from the remote PC (command lines)
  • An Ethernet link between the host PC and the board for cross-development and cross-debugging through a local network. This is an alternative or a complement to the serial (or USB) link
  • A display connected to the board, depending on the technologies available on the board: DSI LCD display, HDMI monitor (or TV) and so on
  • A mouse and a keyboard connected through USB ports

Additional optional components can be added by means of the connectivity capabilities of the board: cameras, displays, JTAG, sensors, actuators, and much more.

4. Installing the Starter Package[edit | edit source]

Before developing with the Developer Package, it is essential to start up your board thanks to its Starter Package. All articles relative to Starter Packages are found in Category:Starter Package: find the one that corresponds to your board, and follow the installation instructions (if not yet done), before going further.

In brief, it means that:

  • your board boots successfully
  • the flashed image comes from the same release of the STM32MPU Embedded Software distribution as the components that will be downloaded in this article
  • the debug symbol files from the flashed image are available in Starter Package image folder


Thanks to the Starter Package,all Flash partitions are populated.

Then, with the Developer Package, it is possible to modify or to upgrade the partitions independently one from the others.

For example, if you only want to modify the Linux kernel (part of bootfs partition), installing the SDK and the Linux kernel are enough; no need to install anything else.

With the debug symbol files, it is also possible to debug the Linux® kernel, U-Boot, OP-TEE, or TF-A with GDB. Especially, the Debug OpenSTLinux BSP components chapter explains how to load the debug symbol files in GDB.

5. Installing the components to develop software running on Arm Cortex-A (OpenSTLinux distribution)[edit | edit source]

5.1. Installing the SDK[edit | edit source]

Optional step: it is mandatory only if you want to modify or add software running on Arm Cortex-A (for example Linux kernel, Linux user space applications...).

The SDK for OpenSTLinux distribution provides a stand-alone cross-development toolchain and libraries tailored to the contents of the specific image flashed in the board. If you want to know more about this SDK, read the SDK for OpenSTLinux distribution article.

For STM32MP1 series

For STM32MP2 series

5.1.1. Starting up the SDK[edit | edit source]

The SDK environment setup script must be run once in each new working terminal in which you cross-compile:

For STM32MP1 series

For STM32MP2 series

If any of these commands fails or does not return the expected result, try to reinstall the SDK.

5.2. Installing the OpenSTLinux BSP packages[edit | edit source]

Optional step: it is mandatory only if you want to modify the BSP (Linux kernel, TF-A, U-Boot, OP-TEE OS), or to add external out-of-tree Linux kernel modules.

OpenSTLinux BSP packages installation instructions:

5.2.1. Building and deploying OpenSTLinux BSP packages component per component[edit | edit source]

5.2.1.1. Building and deploying the external device tree for the first time[edit | edit source]

Prerequisite: the SDK is installed.

Open the <external device tree installation directory>/README.HOW_TO.txt.<board flavor>[1] helper file, and execute its instructions to:
setup a software configuration management (SCM) system (git) for the external device tree (optional but recommended)
export the path of external device tree directory into the variable EXTDT_DIR

The external device tree is now set-up and can be used during compilation.

5.2.1.2. Building and deploying the ddr firmware for the first time (only on STM32MP2 series)[edit | edit source]

Prerequisite: the SDK is installed.

Open the <ddr firmware installation directory>/README.HOW_TO.txt.<board flavor>[1] helper file, and execute its instructions to:
export the path of ddr firmware tree directory into the variable FWDDR_DIR

The ddr firmware path is now set-up and can be used during compilation.

5.2.1.3. Building and deploying the Linux kernel for the first time[edit | edit source]

Prerequisite: the SDK is installed. It is mandatory to execute once the steps specified below before modifying the Linux kernel, or adding external out-of-tree Linux kernel modules.

The partitions related to the Linux kernel are:

  • the bootfs partition that contains the Linux kernel U-Boot image (uImage) and device tree
  • the rootfs partition that contains the Linux kernel modules

The Linux kernel might be cross-compiled, either in the source code directory, or in a dedicated directory different from the source code directory.
This last method is recommended as it clearly separates the files generated by the cross-compilation from the source code files.


Open the <Linux kernel installation directory>/README.HOW_TO.txt.<board flavor>[1] helper file, and execute its instructions to:
setup a software configuration management (SCM) system (git) for the Linux kernel (optional but recommended)
prepare the Linux kernel (applying the ST patches)
configure the Linux kernel (applying the ST fragments)
cross-compile the Linux kernel
deploy the Linux kernel (that is, update the software on board)

The Linux kernel is now installed: let's modify the Linux kernel.

5.2.1.4. Building and deploying the gcnano-driver for the first time (only on STM32MP15x lines More info.png, STM32MP23x lines More info.png and STM32MP25x lines More info.png)[edit | edit source]

Prerequisite:

It is mandatory to execute once the steps specified below before modifying gcnano-driver.

A kernel module depends on the Linux kernel version. If kernel module is not built with the correct Linux kernel, the kernel could refuse the module to be loaded.

Open the <gcnano-driver installation directory>/README.HOW_TO.txt.<board flavor>[1] helper file, and execute its instructions to:
setup a software configuration management (SCM) system (git) for the gcnano-driver (optional but recommended)
cross-compile the gcnano-driver
deploy the gcnano-driver (that is, update the software on board)

The gcnano-driver is now installed.

5.2.1.5. Building and deploying the U-Boot for the first time[edit | edit source]

Prerequisite: the SDK is installed. It is mandatory to execute once the steps specified below before modifying the U-Boot.

As explained in the boot chain overview, the trusted boot chain is the default solution delivered by STMicroelectronics.

Within this scope, the partition related to the U-Boot is the ssbl one that contains the U-Boot and its device tree blob.

Open the <U-Boot installation directory>/README.HOW_TO.txt.<board flavor>[1] helper file, and execute its instructions to:
setup a software configuration management (SCM) system (git) for the U-Boot (optional but recommended)
prepare the U-Boot (applying the ST patches)
cross-compile the U-Boot
deploy the U-Boot (that is, update the software on board)

The U-Boot is now installed: let's modify the U-Boot.

5.2.1.6. Building and deploying the TF-A for the first time[edit | edit source]

Prerequisite: the SDK is installed. It is mandatory to execute once the steps specified below before modifying the TF-A.

As explained in the boot chain overview, the trusted boot chain is the default solution delivered by STMicroelectronics.

Within this scope, the partition related to the TF-A is the fsbl one.

Open the <TF-A installation directory>/README.HOW_TO.txt.<board flavor>[1] helper file, and execute its instructions to:
setup a software configuration management (SCM) system (git) for the TF-A (optional but recommended)
prepare the TF-A (applying the ST patches)
cross-compile the TF-A
deploy the TF-A (that is, update the software on board)

The TF-A is now installed: let's modify the TF-A.

5.2.1.7. Building and deploying the OP-TEE for the first time[edit | edit source]

Prerequisite: the SDK is installed. It is mandatory to execute once the steps specified below before modifying the OP-TEE.

As explained in the boot chain overview, the trusted boot chain is the default solution delivered by STMicroelectronics. Within this scope, the partition related to the OP-TEE is the fsbl one.

Open the <OP-TEE installation directory>/README.HOW_TO.txt.<board flavor>[1] helper file, and execute its instructions to:
setup a software configuration management (SCM) system (git) for the OP-TEE (optional but recommended)
prepare the OP-TEE (applying the ST patches)
cross-compile the OP-TEE
deploy the OP-TEE (that is, update the software on board)


The OP-TEE is now installed: let's modify the OP-TEE.

5.2.2. Building and deploying the OpensSTLinux BSP packages using SDK-info utilities[edit | edit source]

SDK-infos is an optional component (on top of above ones) that facilitates the extraction, configuration and build of the OpensSTLinux BSP packages. This directory provides a script and README to help to generate a build environment adapted to your needs and to manage OpensSTLinux components diversity.

Prerequisite: the SDK is installed. It is mandatory to execute the build steps specified below.

5.2.2.1. How to use SDK-infos[edit | edit source]

The script "generated_build_script-stm32mpx.sh" uses the whole "README.HOW_TO.txt" files to generate a helper script to compile the component needed for your target.


  • Different options are supported and can be accessed through script help:
$> ./generated_build_script-stm32mpx.sh help
generated_build_script <machine name>
<machine name>: name of the machine which can be use for sdk compilation
     - stm32mp1 or stm32mp1-mx: to compile STM32MP1 series' boards More info green.png either
       - via device tree from components themselves or external-dt source 
       - or via device tree from components themselves or external board provided by STM32CubeMX
     - stm32mp2 or stm32mp2-mx: to compile STM32MP2 series' boards More info green.png for A35-TD flavor More info green.pngeither
       - via device tree from components themselves or external-dt source
       - or via device tree from components themselves or external board provided by STM32CubeMX
     - stm32mp2-m33td or stm32mp2-m33td-mx: to compile STM32MP2 series' boards More info green.png for M33-TD flavor More info green.png either
       - via device tree from components themselves or external-dt source 
       - or via device tree from components themselves or external board provided by STM32CubeMX


  • To generate a helper script for ST board (ex.: stm32mp257f-dk):
$> ./sdk-infos/generated_build_script-stm32mpx.sh stm32mp2

This command generates a script on root directory for all source codes from Developer Package: sources/*/sdk_compilation-stm32mp2-my-custom-board.sh


  • To generate a helper script for board with Cube MX device tree(ex.: stm32mp157f-mx-dk):
$> ./sdk-infos/generated_build_script-stm32mpx.sh stm32mp1-mx

This command generates a script, sources/*/sdk_compilation-stm32mp1-mx-my-custom-board.sh, on root directory for all source codes from Developer Package.


After the helper script was correctly filled with your configuration (see SDK-infos README for examples and explanation), you can start to use it.

Usage helper script, way of working (here we use a helper script named sdk_compilation-stm32mp-xxx.sh as example)

  • To extract the sources codes of components
  $> ./sdk_compilation-stm32mp-xxx.sh extract


  • To generate boot stage of Cortex-A
$> ./sdk_compilation-stm32mp-xxx.sh compile-for-fip
$> ./sdk_compilation-stm32mp-xxx.sh deploy-for-fip

This command generates bl2 and fip binaries for Cortex-A


  • To generate binary to flashing via Cortex-A
$> ./sdk_compilation-stm32mp-xxx.sh programmer

This command generates bl2 and fip binaries for flashing on Cortex-A


  • To generate kernel and kernel modules:
$> ./sdk_compilation-stm32mp-xxx.sh linux-stm32mp-configure
$> ./sdk_compilation-stm32mp-xxx.sh linux-stm32mp-compile
$> ./sdk_compilation-stm32mp-xxx.sh linux-stm32mp-deploy

This command generates the kernel image and device tree and exports kernel modules. The Kernel modules can be found stripped and not stripped on deploy directory.

$> ./sdk_compilation-stm32mp-xxx.sh gcnano-driver-stm32mp-compile
$> ./sdk_compilation-stm32mp-xxx.sh gcnano-driver-stm32mp-deploy
5.2.2.2. Known restrictions[edit | edit source]

6. Installing the components to develop software running on Arm Cortex-M (only on STM32MP15x lines More info.png and STM32MP2 series)[edit | edit source]


6.1. Installing STM32CubeIDE[edit | edit source]

Optional step: it is needed if you want to modify or add software running on Arm Cortex-M.

The table below explains how to download and install STM32CubeIDE which addresses STM32 MCU, and also provides support for Cortex-M inside STM32 MPU.

STM32 MPU support, inside STM32CubeIDE, is available on Linux® and Windows® host PCs, but it is NOT on macOS®.

STM32CubeIDE for Linux® host PC STM32CubeIDE for Windows® host PC
Download

Version 1.19.0

  • Download the preferred all-in-one Linux installer from st.com
    • Generic Linux Installer - STM32CubeIDE-Lnx
    • RPM Linux Installer - STM32CubeIDE-RPM
    • Debian Linux Installer - STM32CubeIDE-DEB

Version 1.19.0

  • Download the all-in-one Windows installer from st.com
    • Windows Installer - STM32CubeIDE-Win
Installation guide
User manual
  • When the installation is completed, see additional information about STM32CubeIDE in st.com:
    • STM32CubeIDE quick start guide (UM2553)
Detailed release note
  • Details about the content of this tool version are available in the STM32CubeIDE release v1.19.0 release note from st.com
Restrictions
  • Main restrictions are identified in this chapter
  • STM32CubeIDE errata (This page is available in the stm32mcu wiki, be aware that, visiting this page, you will leave the stm32mpu wiki)

Minor releases may be available from the update site. Check chapter 10 in (UM2609) for more information on how to update STM32CubeIDE.


6.2. Installing the STM32CubeMPU Package[edit | edit source]

Optional step: it is mandatory only if you want to modify the STM32CubeMPU Package.

Prerequisite: the STM32CubeIDE is installed.

For STM32MP1 series:

For STM32MP2 series:

The STM32CubeMPU Package is now installed: let's develop software running on Arm Cortex-M.


7. Developing software running on Arm Cortex-A[edit | edit source]

7.1. Modifying the Linux kernel[edit | edit source]

Prerequisites:

The <Linux kernel installation directory>/README.HOW_TO.txt helper file gives the commands to:
configure the Linux kernel
cross-compile the Linux kernel
deploy the Linux kernel (that is, update the software on board)

You can refer to the following simple examples:

7.2. Adding Linux user space applications[edit | edit source]

Prerequisites:

Once a suitable cross-toolchain (OpenSTLinux SDK) is installed, it is easy to develop a project outside of the OpenEmbedded build system.
There are different ways to use the SDK toolchain directly, among which Makefile and Autotools.
Whatever the method, it relies on:

  • the sysroot that is associated with the cross-toolchain, and that contains the header files and libraries needed for generating binaries (see target sysroot)
  • the environment variables created by the SDK environment setup script (see SDK startup)

You can refer to the following simple example:

7.3. Modifying the U-Boot[edit | edit source]

Prerequisites:

The <U-Boot installation directory>/README.HOW_TO.txt helper file gives the commands to:
cross-compile the U-Boot
deploy the U-Boot (that is, update the software on board)

You can refer to the following simple example:

7.4. Modifying the TF-A[edit | edit source]

Prerequisites:

The <TF-A installation directory>/README.HOW_TO.txt helper file gives the commands to:
cross-compile the TF-A
deploy the TF-A (that is, update the software on board)

You can refer to the following simple example:

7.5. Modifying the OP-TEE[edit | edit source]

Prerequisites:

The <OP-TEE installation directory>/README.HOW_TO.txt helper file gives the commands to:
cross-compile the OP-TEE
deploy the OP-TEE (that is, update the software on board)

You can refer to the following simple example:


8. Developing software running on Arm Cortex-M[edit | edit source]

This chapters are valid only for STM32MP15x lines More info.png and STM32MP2 series.



Refer to FwST-M_Packages articles to create a STM32CubeMPU project from scratch or open/modify an existing one from STM32CubeMPU package.

9. Fast links to essential commands[edit | edit source]

If you are already familiar with the Developer Package for the STM32MPU Embedded Software distribution, fast links to the essential commands are listed below.

10. How to go further?[edit | edit source]

Now that your developments are ready, you might want to switch to the STM32MPU Distribution Package, in order to create your own distribution and to generate your own SDK and image.

11. References[edit | edit source]

  1. Jump up to: 1.0 1.1 1.2 1.3 1.4 1.5 1.6 The helper file name might be "README.HOW_TO.txt.stm32mp1" for the STM32MP1 series, "README.HOW_TO.txt.stm32mp2" for the A35-TD flavor More info green.png of the STM32MP2 series, or "README.HOW_TO.txt.stm32mp2-m33td" for the M33-TD flavor More info green.png of the STM32MP2 series