1. Article purpose[edit | edit source]
This article aims at proposing a way to organize, on the host PC, the software packages of the different Packages (Starter, Developer and Distribution) for a given release of the STM32MPU Embedded Software distribution (here ecosystem release v6.2.1
).
The main objective of the proposed organization is to keep together the software packages corresponding to a given release because there are links between them. For example:
- Flashing the image from the Starter Package on the board is mandatory before modifying the source code from the Developer Package. Both the image and the source code must belong to the same software release.
- The SDK (Developer Package) and the image (Starter Package) have both been generated from the Distribution Package. A software release thus guarantees that there is no misalignment between the different software packages.
| The objective of this article is to describe one organization among all the possible organizations. Feel free to organize the delivered Packages in any other way that would better match your way of working. |
| In practice, this article uses the release STM32MPU-Ecosystem-v6.2.1 for the STM32MPU Embedded Software distribution as an example to illustrate the proposed organization. If you are using a different release, the names of the directories and files might differ. |
The directories are shown in blue, while the files are in black.
2. Creating the structure[edit | edit source]
- Create your <working directory> and assign a unique name to it (for example by including the release name):
mkdir STM32MPU-Ecosystem-v6.2.1 cd STM32MPU-Ecosystem-v6.2.1
- Create the first-level directories that will host the software packages delivered through the STM32MPU Embedded Software distribution release note:
mkdir Starter-Package mkdir Developer-Package mkdir Distribution-Package
- The resulting directory structure looks as follows:
STM32MPU-Ecosystem-v6.2.1 STM32MPU Embedded Software release ├── Developer-Package Developer Package installation directory ├── Distribution-Package Distribution Package installation directory └── Starter-Package Starter Package(s) installation directory
Once all software packages have been installed according to the instructions given in the STM32MPU Embedded Software distribution release note, the resulting directory structure looks as follows:
STM32MPU-Ecosystem-v6.2.1 STM32MPU Embedded Software release ├── Developer-Package Developer Package installation directory │ ├── stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10/sdk STM32MP1 SDK for OpenSTLinux distribution (32b) │ ├── stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10/sdk STM32MP2 SDK for OpenSTLinux distribution (64b) │ ├── STM32Cube_FW_MP1_V1.7.0 STM32CubeMP1 Package │ ├── STM32Cube_FW_MP2_V1.3.X [X:0;2] STM32CubeMP2 Package │ ├── stm32mpu-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10 Linux kernel, U-Boot, TF-A, OP-TEE OS and TF-M source code (OpenSTLinux distribution) ├── Distribution-Package Distribution Package installation directory │ └── openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10 OpenSTLinux distribution (full source code and OpenEmbedded-based build framework) └── Starter-Package Starter Package installation directory |── stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10 Software image (binaries) for STM32MP1 series |── stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10 Software image (binaries) for STM32MP2 series in A35-TD flavor└── stm32mp2-m33td-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10 Software image (binaries) for STM32MP2 series in M33-TD flavor
![]()
3. Focus on the Starter Package directory[edit | edit source]
The Starter-Package directory contains the software image for the STM32MPU Embedded Software distribution.
The optee boot chain is the default solution delivered by STMicroelectronics. It includes the superset of features (for example, all Flash memory devices are supported). Refer to the Boot chain overview article for details.
Flash memory partitions (e.g. rootfs, bootfs...) are explained in the STM32 MPU Flash mapping article.
Starter-Package └── stm32mp{1,2,2-m33td}-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10 └── images └── stm32mp{1,2,2-m33td} ├── flashlayout_st-image-weston Flash layout files (description of the partitions) for the supported Flash devices and boards │ ├── deleteall │ │ └── [...] │ ├── extensible │ │ ├── FlashLayout_sdcard_stm32mp*-extensible.tsv Flash layout file for microSD card with no userfs partition but a rootfs partition extended to sdcard size (recommended setup for package repository service) │ │ └── [...] │ ├── fastboot │ │ ├── FlashLayout_emmc_stm32mp*-fastboot.tsv Flash layout file for Fastboot flash protocol and op-tee boot chain (System and secure services) │ │ ├── FlashLayout_sdcard_stm32mp*-fastboot.tsv Flash layout file for Fastboot flash protocol and op-tee boot chain (System and secure services) │ │ └── [...] │ ├── fastboot-opteemin │ │ ├── FlashLayout_emmc_stm32mp*-fastboot-opteemin.tsv Flash layout file for Fastboot flash protocol and op-tee boot chain (System services only), with OP-TEE OS │ │ ├── FlashLayout_sdcard_stm32mp*-fastboot-opteemin.tsv Flash layout file for Fastboot flash protocol and op-tee boot chain (System services only), with OP-TEE OS │ │ └── [...] │ ├── optee │ │ ├── FlashLayout_emmc_stm32mp*-optee.tsv Flash layout file for eMMC and op-tee boot chain (System and secure services), with OP-TEE OS │ │ ├── FlashLayout_sdcard_stm32mp*-optee.tsv Flash layout file for microSD card and op-tee boot chain (System and secure services), with OP-TEE OS │ │ └── [...] │ ├── opteemin │ ├── FlashLayout_emmc_stm32mp*-opteemin.tsv Flash layout file for eMMC and op-tee boot chain (System services only), with OP-TEE OS │ ├── FlashLayout_sdcard_stm32mp*-opteemin.tsv Flash layout file for microSD card and op-tee boot chain (System services only), with OP-TEE OS │ └── [...] ├── fip │ ├── fip-<board>-<boot-type>.bin FIP Image to flash ├── arm-trusted-firmware │ ├── bl2 TF-A binary for FIP binaries creation │ │ ├── tf-a-<board name>-<boot chain>-<storage>.bin │ │ └── [...] │ ├── debug Debug binaries for TF-A │ │ ├── debug-tf-a-<board name>-<boot chain>-<storage>.stm32 Debug file for FSBL │ │ ├── tf-a-bl2-<soc name>-<boot chain>-<storage>.elf Debug symbol file for TF-A │ │ └── [...] │ ├── fwconfig TF-A device tree for FIP binaries creation │ │ ├── <board name>-fwconfig-<boot chain>-<storage>.dtb │ │ └── [...] │ ├── metadata.bin Meta data binary for METADATA partition for the supported boards │ ├── tf-a-<board>-<boot-type>.stm32 Intermediate tf-a binary used to build fip image │ └── [...] ├── u-boot │ ├── u-boot-nodtb-soc-<boot-type>.bin Intermediate tf-a binary used to build fip image │ ├── u-boot-<board>.dtb Intermediate tf-a dtb used to build fip image ├── optee │ ├── tee-header_v2-<board>-<boot-type>.bin │ ├── tee-pageable_v2-<board>-<boot-type>.bin │ ├── tee-pager_v2-<board>-<boot-type>.bin ├── kernel │ ├── config-6.6.116 Reference config file for Linux kernel │ ├── [...] │ ├── vmlinux vmlinux copied in bootfs partition ├── scripts │ └── create_sdcard_from_flashlayout.sh ├── st-image-weston-openstlinux-weston-stm32mp{1,2,2-m33td}.rootfs.ext4 Binary for full image content (no split of partition) ├── st-image-weston-openstlinux-weston-stm32mp{1,2,2-m33td}.rootfs.license ├── st-image-weston-openstlinux-weston-stm32mp{1,2,2-m33td}.rootfs-license_content.html License summary for all packages needed to feed all partitions ├── st-image-weston-openstlinux-weston-stm32mp{1,2,2-m33td}.rootfs.manifest ├── st-image-weston-openstlinux-weston-stm32mp{1,2,2-m33td}.splitted-bootfs.ext4 Binary for bootfs partition on eMMC and microSD card devices ├── st-image-weston-openstlinux-weston-stm32mp{1,2,2-m33td}.splitted-vendorfs.ext4 Binary for vendorfs partition on eMMC and microSD card devices ├── st-image-weston-openstlinux-weston-stm32mp{1,2,2-m33td}.splitted-rootfs.ext4 Binary for rootfs partition on eMMC and microSD card devices ├── st-image-weston-openstlinux-weston-stm32mp{1,2,2-m33td}.splitted-userfs.ext4 Binary for userfs partition on eMMC and microSD card devices └── [...]
4. Focus on the Developer Package directory[edit | edit source]
The Developer-Package directory contains:
- The source code for the following OpenSTLinux software packages (development for Arm® Cortex®-A processor):
- Linux® kernel
- GCnano driver
- U-Boot
- TF-A
- OP-TEE OS
- The debug symbol files for Linux kernel, U-Boot, TF-A and OP-TEE OS
- The SDK (for cross-development on an host PC)
- The STM32Cube MPU Package (developed for Arm® Cortex®-M processor)
Developer-Package ├── SDK SDK for OpenSTLinux distribution: details in Standard SDK directory structure article │ ├── st-image-weston-openstlinux-weston-stm32mp1.rootfs-x86_64-toolchain-5.0.17-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10.sh │ ├── [...] │ ├── st-image-weston-openstlinux-weston-stm32mp2.rootfs-x86_64-toolchain-5.0.17-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10.sh │ └── [...]
├── STM32Cube_FW_MP1_V1.7.0 STM32CubeMP1 Package: details in STM32CubeMP15 Package content article │ ├── Drivers │ │ ├── BSP BSP drivers for the supported STM32MPU boards │ │ │ └── [...] │ │ ├── CMSIS │ │ │ └── [...] │ │ └── STM32MP1xx_HAL_Driver HAL drivers for the supported STM32MPU devices │ │ └── [...] │ ├── _htmresc │ │ └── [...] │ ├── License.md License types for the components │ ├── Middlewares Middlewares used by the examples and applications │ │ └── [...] │ ├── package.xml │ ├── Projects │ │ ├── STM32CubeProjectsList.html List of examples and applications for STM32CubeMP1 Package │ │ ├── STM32MP157F-DK2 Set of examples and applications → STM32MP157F-DK2 │ │ │ └── [...] │ │ └── STM32MP157F-EV1 Set of examples and applications → STM32MP157F-EV1 │ │ └── [...] │ ├── Readme.md │ ├── Release_Notes.html Release note for STM32CubeMP1 Package │ └── Utilities │ └── [...] ├── STM32Cube_FW_MP2_V1.3.X [X:0;2] STM32CubeMP2 Package: details in STM32CubeMP2 Package content article └── [...]
└── stm32mp{1,2}-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10 Source code for OpenSTLinux distribution ├── images │ └── stm32mp1 Debug symbol files installation directory │ ├── tf-a-bl2-<soc>-<boot-type>.elf Debug symbol file for TF-A │ ├── u-boot-<soc>-<boot-type>.elf Debug symbol file for U-Boot │ ├── vmlinux Debug symbol file for Linux kernel │ └── [...]
└── sources └── ostl-linux For stm32mp{1,2}x series
├── external-dt-v6.0-stm32mp-r3.1-r0 External DT installation directory │ ├── README.HOW_TO.txt.{stm32mp1,stm32mp2,stm32mp2-m33td} Helper file for External DT module management providing also component compilation guidelines (STM32MP1 series, STM32MP2 series with A35-TD flavorand STM32MP2 series with M33-TD flavor
) │ ├── stm32mp1 Sub-directory for STM32MP1 series │ ├── linux Device tree files for Linux kernel component │ ├── optee Device tree files for optee component │ ├── tf-a Device tree files for tf-a component │ └── u-boot Device tree files for u-boot component │ ├── stm32mp2 Sub-directory for STM32MP2 series │ ├── {a35-td,m33-td} Sub-directory following TD flavor (A35-TD or M33-TD)
│ ├── linux Device tree files for Linux kernel component │ ├── mcuboot Device tree files for mcuboot component (M33-TD flavor
only) │ ├── optee Device tree files for optee component │ ├── tf-a Device tree files for tf-a component │ ├── tf-m Device tree files for tf-m component │ └── u-boot Device tree files for u-boot component
├── gcnano-driver-stm32mp-6.4.21-r1-r0 GCNano linux driver installation directory │ ├── README.HOW_TO.txt.{stm32mp1,stm32mp2,stm32mp2-m33td} Helper file for GCnano kernel module management providing also component compilation guidelines (STM32MP1 series, STM32MP2 series with A35-TD flavorand STM32MP2 series with M33-TD flavor
) │ ├── gcnano-driver-stm32mp-6.4.21-r1-r0 GCnano kernel module source code directory │ └── gcnano-driver-stm32mp-6.4.21-r1-r0.tar.xz
├── linux-stm32mp-6.6.129-stm32mp-r3.1-r0 Linux kernel installation directory │ ├── README.HOW_TO.txt.{stm32mp1,stm32mp2,stm32mp2-m33td} Helper file for Linux kernel module management providing also component compilation guidelines (STM32MP1 series, STM32MP2 series with A35-TD flavorand STM32MP2 series with M33-TD flavor
) │ ├── [*].patch ST patches for Linux kernel │ ├── fragment-[*].config ST configuration fragments for Linux kernel │ ├── optional-fragment-[*].config optional ST configuration fragments for Linux kernel │ ├── linux-6.6.129 Linux kernel source code directory │ ├── linux-6.6.129.tar.xz │ └── series
├── m33tdprojects-starter-stm32mp2-1.3.1-r0 M33TD Starter project installation directory │ ├── README.HOW_TO.txt.stm32mp2-m33td Helper file for M33TD Projects management providing also component compilation guidelines (STM32MP2 series with M33-TD flavoronly) │ ├── mm33tdprojects-starter-stm32mp2-1.3.1-r0 M33TD Starter project source code directory │ ├── m33tdprojects-starter-stm32mp2-1.3.1-r0.tar.xz │ └── Makefile.sdk.stm32mp2-m33td Makefile for the M33TD Starter project compilation
├── optee-os-stm32mp-4.0.0-stm32mp-r3.1-r0 OP-TEE OS installation directory │ ├── README.HOW_TO.txt.{stm32mp1,stm32mp2,stm32mp2-m33td} Helper file for OP-TEE OS module management providing also component compilation guidelines (STM32MP1 series, STM32MP2 series with A35-TD flavorand STM32MP2 series with M33-TD flavor
) │ ├── [*].patch ST patches for OP-TEE OS │ ├── Makefile.sdk.{stm32mp1,stm32mp2,stm32mp2-m33td} Makefile(s) for the OP-TEE OS compilation (STM32MP1 series, STM32MP2 series with A35-TD flavor
and STM32MP2 series with M33-TD flavor
) │ ├── optee-os-stm32mp-4.0.0-stm32mp-r3.1-r0 OP-TEE OS source code directory │ ├── optee-os-stm32mp-4.0.0-stm32mp-r3.1-r0.tar.xz │ └── series
├── sdk-infos-1.0-r0 SDK Infos directory │ ├── README.HOW_TO.txt.{stm32mp1,stm32mp2,stm32mp2-m33td} Helper file for Developer package sources building !!!!!!!!!!!!(STM32MP1 series, STM32MP2 series with A35-TD flavorand STM32MP2 series with M33-TD flavor
) │ └── generated_build_script-stm32mpx.sh Script for !!!!!!!!!!!!!!!!!!!!
├── tf-a-stm32mp-v2.10.24-stm32mp-r3.1-r0 TF-A installation directory │ ├── README.HOW_TO.txt.{stm32mp1,stm32mp2,stm32mp2-m33td} Helper file for TF-A module management providing also component compilation guidelines (STM32MP1 series, STM32MP2 series with A35-TD flavorand STM32MP2 series with M33-TD flavor
) │ ├── [*].patch ST patches for TF-A │ ├── fiptool-stm32mp.{stm32mp1,stm32mp2,stm32mp2-m33td} Script file for creating FIP image (STM32MP1 series, STM32MP2 series with A35-TD flavor
and STM32MP2 series with M33-TD flavor
) │ ├── Makefile.sdk.{stm32mp1,stm32mp2,stm32mp2-m33td} Makefile(s) for the TF-A compilation (STM32MP1 series, STM32MP2 series with A35-TD flavor
and STM32MP2 series with M33-TD flavor
) │ ├── series │ ├── tf-a-stm32mp-v2.10.24-stm32mp-r3.1-r0 TF-A source code directory │ └── tf-a-stm32mp-v2.10.24-stm32mp-r3.1-r0.tar.xz
├── tf-m-stm32mp-v2.1.4-stm32mp-r2.1-r0 TF-M installation directory │ ├── README.HOW_TO.txt Helper file for M33TD Projects management providing also component compilation guidelines │ ├── tf-m-stm32mp-v2.1.4-stm32mp-r2.1-r0 TF-M source code directory │ ├── Makefile.sdk Makefile for the TF-M compilation │ ├── tf-m-stm32mp-v2.1.4-stm32mp-r2.1-r0.tar.xz tar.xz │ └── tf-m-stm32mp-v2.1.4-stm32mp-r2.1-r0.tar.xz diff.gz
├── tf-m-tests-stm32mp-v2.1.4-stm32mp-r2.1-r0 TF-M-tests installation directory │ ├── README.HOW_TO.txt Helper file for TF-M-tests management: reference for TF-M-tests build │ ├── [*].patch ST patches for TF-A │ ├── unknown package TF-M-tests source code directory │ ├── tf-m-tests-stm32mp-v2.1.4-stm32mp-r2.1-r0.tar.xz │ └── series
└── u-boot-stm32mp-v2023.10-stm32mp-r3.1-r0 U-Boot installation directory ├── README.HOW_TO.txt.{stm32mp1,stm32mp2,stm32mp2-m33td} Helper file for U-Boot module management providing also component compilation guidelines (STM32MP1 series, STM32MP2 series with A35-TD flavorand STM32MP2 series with M33-TD flavor
) ├── [*].patch ST patches for U-Boot ├── fiptool-stm32mp.{stm32mp1,stm32mp2,stm32mp2-m33td} Script file for creating FIP image (STM32MP1 series, STM32MP2 series with A35-TD flavor
and STM32MP2 series with M33-TD flavor
) ├── Makefile.sdk.{stm32mp1,stm32mp2,stm32mp2-m33td} Makefile(s) for the U-Boot compilation (STM32MP1 series, STM32MP2 series with A35-TD flavor
and STM32MP2 series with M33-TD flavor
) ├── series ├── u-boot-stm32mp-v2023.10-stm32mp-r3.1-r0 U-Boot source code directory └── u-boot-stm32mp-v2023.10-stm32mp-r3.1-r0.tar.xz
Appendix A shows the structure of the Linux kernel, U-Boot, TF-A and OP-TEE OS installation directories after these software packages have been built.
5. Focus on the Distribution Package directory[edit | edit source]
The Distribution-Package directory contains all the OpenEmbedded layers required to get the source code of any STM32MPU Embedded Software component, as well as a build framework based on OpenEmbedded.
STM32MPU-Ecosystem-v6.2.1 └── Distribution-Package OpenSTLinux distribution └── layers ├── meta-openembedded Collection of layers for the OpenEmbedded-Core universe (OpenEmbedded standard) │ └── [...]
├── meta-st │ ├── meta-st-openstlinux STMicroelectronics layer that contains the settings of the frameworks and images for the OpenSTLinux distribution │ │ ├── recipes-st │ │ │ ├── images │ │ │ │ ├── st-image-core.bb Core image for OpenSTLinux distribution │ │ │ │ └── st-image-weston.bb Weston image with basic Wayland support for OpenSTLinux distribution: recommended setup │ │ │ └── packagegroups │ │ │ └── [...] │ │ └── [...]
│ ├── meta-st-stm32mp STMicroelectronics layer that contains the description of the BSP for the STM32 MPU devices │ │ ├── recipes-bsp │ │ │ ├── alsa Recipes for ALSA control configuration │ │ │ │ └── [...] │ │ │ ├── ddr-firmware │ │ │ │ └── [...] │ │ │ ├── drivers Recipes for Vivante GCNANO GPU kernel drivers │ │ │ │ └── [...] │ │ │ ├── fip-stm32mp │ │ │ │ └── [...] │ │ │ ├── trusted-firmware-a Recipes for TF-A │ │ │ │ └── [...] │ │ │ ├── trusted-firmware-m Recipes for TF-M │ │ │ │ └── [...] │ │ │ └── u-boot Recipes for U-Boot │ │ │ └── [...] │ │ ├── recipes-extended │ │ │ ├── m4projects Recipes for STM32Cube MPU Package within the OpenSTLinux distribution │ │ │ │ └── [...] │ │ │ └── [...] │ │ ├── recipes-graphics │ │ │ ├── gcnano-userland Recipes for Vivante libraries OpenGL ES, OpenVG and EGL (multi backend) │ │ │ │ └── [...] │ │ │ └── [...] │ │ ├── recipes-kernel │ │ │ └── linux Recipes for Linux kernel │ │ │ └── [...] │ │ │ └── linux-firmware Recipes for Linux firmwares (example, Bluetooth firmware) │ │ │ └── [...] │ │ ├── recipes-st │ │ │ └── images │ │ │ ├── st-image-bootfs.bb Recipes for the bootfs partition binary │ │ │ ├── st-image-userfs.bb Recipes for the userfs partition binary │ │ │ └── st-image-vendorfs.bb Recipes for the vendorfs partition binary │ │ └── [...]
│ ├── meta-st-stm32mp-addons STMicroelectronics layer that helps managing the STM32CubeMX integration │ └── [...] │ └── scripts │ ├── envsetup.sh Environment setup script for Distribution Package │ └── [...]
└── openembedded-core Core metadata for current versions of OpenEmbedded (standard) └── [...]
Appendix B shows the structure of the build directory.
6. Appendix A: directory structure after build (Developer Package)[edit | edit source]
Provided you have followed the recommendations of the README.HOW_TO.txt helper files to build the Linux kernel, the U-Boot and the TF-A, then the following new directories and files contain the build outputs.
Developer-Package ├── stm32mpu-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10 Source code for OpenSTLinux distribution │ └── sources │ └── arm-ostl-linux-gnueabi │ ├── FIP_artifacts FIP images to flash │ │ ├── fip/ FIP images to flash, need to edit tsv file to point on that fip images │ │ ├── arm-trusted-firmware/ Intermediate binaries of tf-a required to build fip images │ │ ├── u-boot/ Intermediate binaries of u-boot required to build fip images │ │ ├── optee/ Intermediate binaries of optee required to build fip images
│ ├── linux-6.6.129 │ │ ├── build Linux kernel build directory │ │ │ ├── install_artifact │ │ │ │ ├── lib │ │ │ │ │ └── modules │ │ │ │ │ └── X.Y.Z │ │ │ │ │ └── [...] Kernel modules hierarchy (*.ko files) │ │ │ │ └── boot │ │ │ │ ├── stm32mp[*].dtb Linux kernel device tree blob files for bootfs partition │ │ │ │ ├── uImage Linux kernel binary image file (with U-Boot wrapper) for bootfs partition │ │ │ │ └── [...] │ │ │ ├── vmlinux Debug symbol file for Linux kernel │ │ │ └── [...] │ │ └── [...]
│ ├── optee-os-stm32mp-4.0.0-stm32mp-r3.1-r0 OP-TEE OS installation directory │ │ ├── build OP-TEE OS build directory │ │ │ ├── tee-[header/pageable/pager]_v2-stm32mp[*].stm32 Binaries for OP-TEE OS runtime services │ │ │ └── [...] │ │ └── [...]
│ ├──tf-a-stm32mp-v2.10.24-stm32mp-r3.1-r0 TF-A installation directory │ │ ├── build TF-A build directory │ │ │ ├── optee TF-A, with OP-TEE OS │ │ │ │ ├── tf-a-bl2-optee.elf Debug symbol file for TF-A, with OP-TEE OS → boot firmware stage │ │ │ │ ├── tf-a-stm32mp[*].stm32 TF-A binary for FSBL partition, with OP-TEE OS │ │ │ │ └── [...] │ │ └── [...]
│ └── u-boot-stm32mp-v2023.10-stm32mp-r3.1-r0 U-Boot installation directory
│ └── [...]
7. Appendix B: directory structure after build (Distribution Package)[edit | edit source]
By following the build method explained in OpenSTLinux distribution, the build outputs should look like following file tree.
- Destination of files in purple is the Starter Package: flash layout, binaries for bootfs, rootfs, userfs and vendorfs partitions
- Destination of files in grey is the Starter and Developer Packages: binaries for FSBL and SSBL partitions, and for OP-TEE OS runtime services
- Destination of files in orange is the Developer Package: Linux kernel image and device tree blobs, and debug symbol files
/[...]/build-openstlinuxweston-stm32mp{1,2}/tmp-glibc/deploy Yocto BUILDDIR
├── images
│ └── stm32mp{1,2,2-m33td}
│ ├── flashlayout_st-image-weston/optee Flash layout files (description of the partitions) for the supported flash devices
│ │ ├── FlashLayout_sdcard_stm32mp[*].tsv Flash layout file for SDcard and optee boot chain, with OP-TEE OS
│ │ ├── [...]
│ │ ├── FlashLayout_emmc_stm32mp[*].tsv Flash layout file for eMMC and optee boot chain, with OP-TEE OS → STM32MP157F-EV1
│ │ └── [...]
│ ├── scripts
│ │ └── create_sdcard_from_flashlayout.sh
│ ├── st-image-weston-openstlinux-weston-stm32mp{1,2,2-m33td}.splitted-bootfs.ext4 Binary for bootfs partition
│ ├── st-image-weston-openstlinux-weston-stm32mp{1,2,2-m33td}.splitted-vendorfs.ext4 Binary for vendorfs partition
│ ├── st-image-weston-openstlinux-weston-stm32mp{1,2,2-m33td}.splitted-rootfs.ext4 Binary for rootfs partition
│ ├── st-image-weston-openstlinux-weston-stm32mp{1,2,2-m33td}.splitted-userfs.ext4 Binary for userfs partition
│ ├── fip/ FIP images flashed according flashlayout selected
│ ├── uImage Linux kernel binary image file (with U-Boot wrapper) for bootfs partition
│ ├── vmlinux Debug symbol file for Linux kernel
│ └── [...]
└── [...]