Registered User mNo edit summary |
Registered User Tag: 2017 source edit |
||
(115 intermediate revisions by 6 users not shown) | |||
Line 1: | Line 1: | ||
<noinclude>{{ApplicableFor | |||
|MPUs list=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x | |||
|MPUs checklist=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x | |||
}}</noinclude> | |||
== Das U-Boot == | == Das U-Boot == | ||
[https://en.wikipedia.org/wiki/Das_U-Boot Das U-Boot] ("the Universal Boot Loader" or U-Boot) is an open-source bootloader that can be used on | [https://en.wikipedia.org/wiki/Das_U-Boot Das U-Boot] ("the Universal Boot Loader" or U-Boot) is an open-source bootloader that can be used on STMicroelectronics boards to initialize the platform and load the Linux<sup>®</sup> kernel. | ||
[[File: U-Boot Logo.png|thumb|link=https://u-boot.readthedocs.io/en/stable/]] | |||
* Official '''source code''' is available under [https://git-scm.com/ git] repository <ref name=git>https://source.denx.de/u-boot/u-boot.git or https://github.com/u-boot/u-boot</ref> at [https://source.denx.de/u-boot/u-boot https://source.denx.de/u-boot/u-boot], also available in [https://github.com/u-boot/u-boot https://github.com/u-boot/u-boot] | |||
** source.denx.de also hosts the [https://source.denx.de/u-boot/custodians?sort=name_asc Custodian git trees];<br/>the STMicroelectronics U-Boot Custodian Tree is available in [https://source.denx.de/u-boot/custodians/u-boot-stm https://source.denx.de/u-boot/custodians/u-boot-stm] | |||
** the fork of "U-Boot" Source Tree used in OpenSTLinux is available in ST GITHUB<ref name=github>https://github.com/STMicroelectronics/u-boot</ref> with associated releases <ref name=releases>https://github.com/STMicroelectronics/u-boot/releases</ref>: [https://github.com/STMicroelectronics/u-boot https://github.com/STMicroelectronics/u-boot] | |||
* Official '''manual''': | |||
** [https://docs.u-boot.org https://docs.u-boot.org]:<br/>it is the documentation generated from '''stable''' source code by <code>make htmldocs</code> | |||
** the documentations available in source code: {{CodeSource | U-Boot | README | README file}} and {{CodeSource | U-Boot | doc/}} | |||
Read the {{CodeSource | U-Boot | README | README file}} before starting using U-Boot. It covers the following topics: | Read the {{CodeSource | U-Boot | README | README file}} before starting using U-Boot. It covers the following topics: | ||
* source file tree structure | * source file tree structure | ||
Line 12: | Line 21: | ||
* brief description of the Hush shell | * brief description of the Hush shell | ||
* list of common environment variables | * list of common environment variables | ||
== U-Boot overview == | == U-Boot overview == | ||
[[File: STM32MPU Embedded Software architecture overview.png|link=STM32MPU Embedded Software architecture overview|thumb|Zoom out to STM32MPU Embedded Software]] | [[File: STM32MPU Embedded Software architecture overview.png|link=STM32MPU Embedded Software architecture overview|thumb|Zoom out to STM32MPU Embedded Software]] | ||
The [[Boot_chain_overview | The [[Boot_chain_overview|STM32 MPU boot chain]] uses [[TF-A overview|Trusted Firmware-A (TF-A)]] as FSBL and U-Boot as SSBL, included in a TF-A [[TF-A_BL2_overview#FIP|FIP]]. | ||
<br clear=all> | <br clear=all> | ||
=== SPL === | |||
=== SPL | <div class="mw-collapsible mw-collapsed"> | ||
U-Boot SPL is not supported in OpenSTLinux. | |||
<div class="mw-collapsible-content"> | |||
==== SPL description ==== | ==== SPL description ==== | ||
The '''U-Boot SPL''' or '''SPL''' is an alternate first stage bootloader (FSBL).<br/> | The '''U-Boot SPL''' or '''SPL''' is an alternate first stage bootloader (FSBL).<br/> | ||
Line 33: | Line 38: | ||
* It performs the initial CPU and board configuration (clocks and DDR memory). | * It performs the initial CPU and board configuration (clocks and DDR memory). | ||
* It loads the SSBL (U-Boot) into the DDR memory. | * It loads the SSBL (U-Boot) into the DDR memory. | ||
{{Warning | SPL is not supported in OpenSTLinux as alternate FSBL: it cannot be used for product development.}} | |||
{{Warning | SPL cannot be used for product development.}} | |||
==== SPL execution sequence==== | ==== SPL execution sequence==== | ||
'''SPL''' executes the following main steps in SYSRAM: | '''SPL''' executes the following main steps in SYSRAM: | ||
Line 51: | Line 45: | ||
* '''board_init_r()''': initialization of the other drivers activated in the SPL device tree | * '''board_init_r()''': initialization of the other drivers activated in the SPL device tree | ||
* loading and execution of U-Boot (or Kernel in Falcon mode<ref>https://www.denx.de/wiki/pub/U-Boot/MiniSummitELCE2013/2013-ELCE-U-Boot-Falcon-Boot.pdf</ref>: {{CodeSource | U-Boot | doc/README.falcon | README.falcon }}). | * loading and execution of U-Boot (or Kernel in Falcon mode<ref>https://www.denx.de/wiki/pub/U-Boot/MiniSummitELCE2013/2013-ELCE-U-Boot-Falcon-Boot.pdf</ref>: {{CodeSource | U-Boot | doc/README.falcon | README.falcon }}). | ||
</div></div> | |||
=== U-Boot: SSBL === | === U-Boot: SSBL === | ||
==== U-Boot description ==== | ==== U-Boot description ==== | ||
'''U-Boot''' is the second-stage bootloader (SSBL) of [[Boot_chain_overview | '''U-Boot''' is the second-stage bootloader (SSBL) of [[Boot_chain_overview| boot chain]] for {{MicroprocessorDevice | device=Class}}. | ||
SSBL main features are the following: | SSBL main features are the following: | ||
Line 70: | Line 65: | ||
==== U-Boot execution sequence ==== | ==== U-Boot execution sequence ==== | ||
'''U-Boot''' executes the following main steps in DDR memory: | '''U-Boot''' executes the following main steps in DDR memory: | ||
* '''Pre-relocation''' initialization (common/board_f.c): minimal initialization (such as CPU, clock, reset, DDR and console) running at the | * '''Pre-relocation''' initialization ({{CodeSource | U-Boot | common/board_f.c}}): minimal initialization (such as CPU, clock, reset, DDR and console) running at the CONFIG_TEXT_BASE load address. | ||
* '''Relocation''': copy of the code to the end of DDR memory. | * '''Relocation''': copy of the code to the end of DDR memory. | ||
* '''Post-relocation initialization''':(common/board_r.c): initialization of all the drivers. | * '''Post-relocation initialization''':({{CodeSource | U-Boot | common/board_r.c}}): initialization of all the drivers. | ||
* '''Command execution''' through autoboot (CONFIG_AUTOBOOT) or console shell. | * '''Command execution''' through autoboot (CONFIG_AUTOBOOT) or console shell. | ||
** Execution of the boot command (by default [[#bootcmd|bootcmd=CONFIG_BOOTCOMMAND]]): <br/>for example, execution of the command <code>bootm</code> to: | ** Execution of the boot command (by default [[#bootcmd|bootcmd=CONFIG_BOOTCOMMAND]]): <br/>for example, execution of the command <code>bootm</code> (for uImage or FIT) or <code>booti</code> (for Image.giz) to: | ||
*** load and check images (such as kernel, device tree and ramdisk) | *** load and check images (such as kernel, device tree and ramdisk) | ||
*** fixup the kernel device tree | *** fixup the kernel device tree | ||
Line 85: | Line 80: | ||
** options defined in Kconfig files (CONFIG_ compilation flags) | ** options defined in Kconfig files (CONFIG_ compilation flags) | ||
** the selected configuration file: {{CodeSource | U-Boot | configs/ | configs/stm32mp*_defconfig}}<br/> | ** the selected configuration file: {{CodeSource | U-Boot | configs/ | configs/stm32mp*_defconfig}}<br/> | ||
* '''other compilation flags''' defined in {{CodeSource | U-Boot | include/configs/ | include/configs/stm32mp*.h}} (these flags are progressively migrated to Kconfig)<br/>The file name is configured through CONFIG_SYS_CONFIG_NAME. | * '''other compilation flags''' defined in {{CodeSource | U-Boot | include/configs/ | include/configs/stm32mp*.h}} (these flags are progressively migrated to Kconfig)<br/>The selected file name is configured through CONFIG_SYS_CONFIG_NAME, for example on STMicroelectronics boards: | ||
** {{MicroprocessorDevice | device=13}}: {{CodeSource | U-Boot | include/configs/stm32mp13_st_common.h}} | |||
** {{MicroprocessorDevice | device=15}}: {{CodeSource | U-Boot | include/configs/stm32mp15_st_common.h}} | |||
** {{MicroprocessorDevice | device=21}}: {{CodeSource | U-Boot | include/configs/stm32mp21_st_common.h}} | |||
** {{MicroprocessorDevice | device=23}}: {{CodeSource | U-Boot | include/configs/stm32mp23_st_common.h}} | |||
** {{MicroprocessorDevice | device=25}}: {{CodeSource | U-Boot | include/configs/stm32mp25_st_common.h}} | |||
* '''[[Device_tree|DeviceTree]]''': U-Boot binaries include a device tree blob that is parsed at runtime | * '''[[Device_tree|DeviceTree]]''': U-Boot binaries include a device tree blob that is parsed at runtime | ||
All the configuration flags (prefixed by CONFIG_) are described in the source code, either in the {{CodeSource | U-Boot | README | README}} file or in the {{CodeSource | U-Boot | doc/ | documentation directory}}. | All the configuration flags (prefixed by CONFIG_) are described in the source code, either in the {{CodeSource | U-Boot | README | README}} file or in the {{CodeSource | U-Boot | doc/ |documentation directory}}. | ||
For example, CONFIG_CMD_CLK activates the command <code>clk</code> compilation ({{CodeSource | U-Boot | cmd.clk.c}}). | |||
Hence to compile U-Boot, [[#Kbuild|select the <target>]] and [[#Device_tree|the device tree]] for the board in order to choose a predefined configuration.<br/> | Hence to compile U-Boot, [[#Kbuild|select the <target>]] and [[#Device_tree|the device tree]] for the board in order to choose a predefined configuration.<br/> | ||
Refer to [[#U-Boot_build]] for examples. | Refer to [[#U-Boot_build]] for examples. | ||
Line 97: | Line 100: | ||
Proceed as follows: | Proceed as follows: | ||
* Select a predefined configuration (defconfig file in {{CodeSource | U-Boot | configs/ | configs directory }}) and generate the first '''.config''': | * Select a predefined configuration (defconfig file in {{CodeSource | U-Boot | configs/ | configs directory }}) and generate the first '''.config''': | ||
{{PC$}} make <config>_defconfig. | {{PC$}}make <config>_defconfig. | ||
* Change the U-Boot compile configuration (modify .config) by using one of the following five <code>make</code> commands: | * Change the U-Boot compile configuration (modify .config) by using one of the following five <code>make</code> commands: | ||
{{PC$}} '''make menuconfig''' {{Highlight|--> menu based program}} | {{PC$}}'''make menuconfig''' {{Highlight|--> menu based program}} | ||
{{PC$}} make config {{Highlight|--> line-oriented configuration}} | {{PC$}}make config {{Highlight|--> line-oriented configuration}} | ||
{{PC$}} make xconfig {{Highlight|--> QT program | {{PC$}}make xconfig {{Highlight|--> QT program}} | ||
{{PC$}} make gconfig {{Highlight|--> GTK program}} | {{PC$}}make gconfig {{Highlight|--> GTK program}} | ||
{{PC$}} make nconfig {{Highlight|--> ncurse menu based program}} | {{PC$}}make nconfig {{Highlight|--> ncurse menu based program}} | ||
You can then compile U-Boot with the updated .config. | You can then compile U-Boot with the updated .config. | ||
Line 110: | Line 113: | ||
Save your configuration to be able to use it as a defconfig file: | Save your configuration to be able to use it as a defconfig file: | ||
{{PC$}} make savedefconfig | {{PC$}}make savedefconfig | ||
This target saves the current config as a defconfig file in the build directory. It can then be compared with the predefined configuration (configs/stm32mp*defconfig). | This target saves the current config as a defconfig file in the build directory. It can then be compared with the predefined configuration (configs/stm32mp*defconfig). | ||
The other makefile targets are the following: | The other makefile targets are the following: | ||
{{PC$}} make help | {{PC$}}make help | ||
.... | .... | ||
Configuration targets: | Configuration targets: | ||
Line 139: | Line 142: | ||
=== Device tree === | === Device tree === | ||
Refer to {{CodeSource | U-Boot | doc/ | Refer to {{DocSource | domain=U-Boot | path=/develop/devicetree/control.html|text=U-Boot Documentation}} or {{CodeSource | U-Boot | doc/develop/devicetree/control.rst | doc/develop/devicetree/control.rst }} for details. | ||
The board [[Device_tree|device tree ]] has the same binding as the kernel. | The board [[Device_tree|device tree]] has the same binding as the kernel. By default it is integrated within the U-Boot binaries: [[U-Boot_overview#Output_files|u-boot.bin]]: appended at the end of the code (CONFIG_OF_SEPARATE) or embedded in the U-Boot binary (CONFIG_OF_EMBED). | ||
In OpenSTLinux, the U-Boot device tree ([[U-Boot_overview#Output_files|u-boot.dtb]]) is present inside a FIP and provided to U-Boot as external file loaded by FSBL=TF-A when U-Boot code is started ([[U-Boot_overview#Output_files|u-boot-nodtb.bin]]: code without device tree): the U-Boot device tree address is provided as boot parameter (in r2 register). | |||
A default device tree is available in the defconfig file (by setting CONFIG_DEFAULT_DEVICE_TREE). | A default device tree is available in the defconfig file (by setting CONFIG_DEFAULT_DEVICE_TREE). | ||
You can either select another supported device tree using the DEVICE_TREE make flag. For | You can either select another supported device tree present in U-Boot directories by using the '''DEVICE_TREE''' make flag. For {{MicroprocessorDevice | device=Class}} boards, the corresponding file is {{HighlightParam|<dts-file-name>}}.dts in {{CodeSource | U-Boot | arch/arm/dts/ | arch/arm/dts/stm32mp*.dts}}, with {{HighlightParam|<dts-file-name>}} set to the full name of the board: | ||
{{PC$}} make DEVICE_TREE={{HighlightParam|<dts-file-name>}} | {{PC$}}make {{Highlight|DEVICE_TREE}}={{HighlightParam|<dts-file-name>}} | ||
or provide a device tree blob (dtb file) resulting from the dts file compilation, by using the EXT_DTB option: | or provide a device tree blob (dtb file) resulting from the dts file compilation, by using the '''EXT_DTB''' option: | ||
{{PC$}} make EXT_DTB={{HighlightParam| | {{PC$}}make {{Highlight|EXT_DTB}}={{HighlightParam|<dts-file-name>.dtb}} | ||
To obtain a device tree file '''{{HighlightParam|<dts-file-name>}}.dts''' that is identical to the Linux kernel one, these U-Boot properties are only added for STMicroelectronics boards in the add-on file '''{{HighlightParam|<dts-file-name>}}-u-boot.dtsi'''. This file is automatically included in '''{{HighlightParam|<dts-file-name>}}.dts''' during device tree compilation (the needed "#include" is added during the pre-processing phasis). | |||
<div class="mw-collapsible mw-collapsed">This is a generic U-Boot Makefile behavior defined in {{CodeSource | U-Boot | scripts/Makefile.lib}} that does not generate a compilation error if this file '''{{HighlightParam|<dts-file-name>}}-u-boot.dtsi''' needed for OpenSTLinux is absent. | |||
<div class="mw-collapsible-content"> | |||
<span class="mw-collapsible mw-collapsed"> | |||
# Try these files in order to find the U-Boot-specific .dtsi include file | |||
{{HighlightParam|u_boot_dtsi_options}} = {{Highlight|$(strip $(wildcard $(dir $<)$(basename $(notdir $<))-u-boot.dtsi)}} \ | |||
$(wildcard $(dir $<)$(subst $\",,$(CONFIG_SYS_SOC))-u-boot.dtsi) \ | |||
$(wildcard $(dir $<)$(subst $\",,$(CONFIG_SYS_CPU))-u-boot.dtsi) \ | |||
$(wildcard $(dir $<)$(subst $\",,$(CONFIG_SYS_VENDOR))-u-boot.dtsi) \ | |||
$(wildcard $(dir $<)u-boot.dtsi)) | |||
... | |||
# We use the first match | |||
{{HighlightParam|u_boot_dtsi}} = $(strip $(u_boot_dtsi_options_debug) \ | |||
$(notdir $(firstword $({{HighlightParam|u_boot_dtsi_options}})))) | |||
... | |||
# Modified for U-Boot | |||
# Bring in any U-Boot-specific include at the end of the file | |||
# And finally any custom .dtsi fragments specified with CONFIG_DEVICE_TREE_INCLUDES | |||
cmd_dtc = mkdir -p $(dir ${dtc-tmp}) ; \ | |||
{{Highlight|(cat $<; $(if $(u_boot_dtsi),echo '$(pound)include "$(u_boot_dtsi)"'))}} > $(pre-tmp); \ | |||
$(foreach f,$(subst $(quote),,$(CONFIG_DEVICE_TREE_INCLUDES)), \ | |||
echo '$(pound)include "$(f)"' >> $(pre-tmp);) \ | |||
$(HOSTCC) -E $(dtc_cpp_flags) -x assembler-with-cpp -o $(dtc-tmp) $(pre-tmp) ; \ | |||
$(DTC) -O dtb -o $@ -b 0 \ | |||
-i $(dir $<) $(DTC_FLAGS) \ | |||
-d $(depfile).dtc.tmp $(dtc-tmp) || \ | |||
(echo "Check $(shell pwd)/$(pre-tmp) for errors" && false) \ | |||
; \ | |||
sed "s:$(pre-tmp):$(<):" $(depfile).pre.tmp $(depfile).dtc.tmp > $(depfile); \ | |||
$(DTC) -O dts -I dtb -s $(DTC_FLAGS) -o $@-u-boot.dts $@; \ | |||
$(CPP) $(dtc_cpp_flags) -x assembler-with-cpp -o $(dtc-tmp) $< ; \ | |||
$(DTC) -O dts -I dts -s $(DTC_FLAGS) -o $@-kernel.dts $(dtc-tmp) | |||
</div></div> | |||
To | To do this, U-Boot uses specific device-tree flags to determine if the associated driver is bound and initialized prior to U-Boot relocation and/or if the associated node is present in SPL : | ||
* {{Highlight|'''bootph-all'''}} => '''initialized before relocation in U-Boot''', present in SPL | |||
* '''bootph-some-ram''' => initialized before relocation in U-Boot, not in SPL | |||
* '''bootph-pre-ram''' => present in SPL | |||
In the device tree used by U-Boot, these flags {{Highlight|'''bootph-all'''}} '''need to be added in all the nodes''' used in U-Boot before relocation (or in SPL) and for all used handles (clock, reset, pincontrol). | |||
See example for [[How_to_configure_U-Boot_for_your_board#Console|console configuration]] for example. | |||
<div class="mw-collapsible mw-collapsed"> | |||
'''Device tree in SPL''' (not used in OpenSTLinux): | |||
<div class="mw-collapsible-content"> | |||
<span class="mw-collapsible mw-collapsed"> | |||
The SPL device tree is also generated from this U-Boot device tree. However to reduce its size, the U-Boot makefile uses the fdtgrep tool to parse the full U-Boot DTB and identify all the drivers required by SPL. | |||
</div></div> | |||
== U-Boot command line interface (CLI) == | == U-Boot command line interface (CLI) == | ||
Refer to | Refer to {{DocSource | domain=U-Boot | path=usage/cmdline.html|text=U-Boot Documentation}} or {{CodeSource | U-Boot | doc/usage/cmdline.rst}}. | ||
U-Boot has a command line interface, the U-Boot console, in which you work with U-Boot [[#Commands|commands]] and [[#U-Boot environment variables|environment variables]] to create a customized boot process. | |||
=== Commands === | === Commands === | ||
U-Boot has a set of built-in commands for managing the system and booting the device.By modifying U-Boot source code, you can create your own built-in commands. | |||
The commands are defined in {{CodeSource | U-Boot | cmd/ | cmd/*.c}}. They are activated through the corresponding '''CONFIG_CMD_*''' configuration flag. | The commands are defined in {{CodeSource | U-Boot | cmd/ | cmd/*.c}}. They are activated through the corresponding '''CONFIG_CMD_*''' configuration flag. | ||
Use the <code>help</code> command in the U-Boot shell to list the commands available on your device: | Use the <code>help</code> command in the U-Boot shell to list the commands available on your device: | ||
{{ | {{U-Boot$}}help | ||
Below the list of all commands extracted from | The U-Boot usage is described in {{DocSource | domain=U-Boot | path=usage/index.html|text=U-Boot Documentation}} but only few commands are described here. | ||
* | |||
Below the list of all commands extracted from an old U-Boot Manual] (obsolete and '''not-exhaustive'''): | |||
* '''Information Commands''' | |||
** bdinfo - prints Board Info structure | ** bdinfo - prints Board Info structure | ||
** coninfo - prints console devices and information | ** coninfo - prints console devices and information | ||
Line 183: | Line 230: | ||
** iminfo - prints header information for application image | ** iminfo - prints header information for application image | ||
** help - prints online help | ** help - prints online help | ||
* | * '''Memory Commands''' | ||
** base - prints or sets the address offset | ** base - prints or sets the address offset | ||
** crc32 - checksum calculation | ** crc32 - checksum calculation | ||
Line 194: | Line 241: | ||
** nm - memory modify (constant address) | ** nm - memory modify (constant address) | ||
** loop - infinite loop on address range | ** loop - infinite loop on address range | ||
* | * '''Flash Memory Commands''' | ||
** cp - memory copy | ** cp - memory copy | ||
** flinfo - prints Flash memory information | ** flinfo - prints Flash memory information | ||
Line 200: | Line 247: | ||
** protect - enables or disables Flash memory write protection | ** protect - enables or disables Flash memory write protection | ||
** mtdparts - defines a Linux compatible MTD partition scheme | ** mtdparts - defines a Linux compatible MTD partition scheme | ||
* | * '''Execution Control Commands''' | ||
** source - runs a script from memory | ** source - runs a script from memory | ||
** bootm - boots application image from memory | ** bootm - boots application image from memory | ||
** go - starts application at address 'addr' | ** go - starts application at address 'addr' | ||
* | * '''Download Commands''' | ||
** bootp - boots image via network using BOOTP/TFTP protocol | ** bootp - boots image via network using BOOTP/TFTP protocol | ||
** dhcp - invokes DHCP client to obtain IP/boot params | ** dhcp - invokes DHCP client to obtain IP/boot params | ||
Line 211: | Line 258: | ||
** rarpboot- boots image via network using RARP/TFTP protocol | ** rarpboot- boots image via network using RARP/TFTP protocol | ||
** tftpboot- boots image via network using TFTP protocol | ** tftpboot- boots image via network using TFTP protocol | ||
* | * '''Environment Variables Commands''' | ||
** printenv- prints environment variables | ** printenv- prints environment variables | ||
** saveenv - saves environment variables to persistent storage | ** saveenv - saves environment variables to persistent storage | ||
Line 217: | Line 264: | ||
** run - runs commands in an environment variable | ** run - runs commands in an environment variable | ||
** bootd - default boot, that is run 'bootcmd' | ** bootd - default boot, that is run 'bootcmd' | ||
* | * '''Flattened Device Tree support''' | ||
** fdt addr - selects the FDT to work on | ** fdt addr - selects the FDT to work on | ||
** fdt list - prints one level | ** fdt list - prints one level | ||
Line 226: | Line 273: | ||
** fdt move - moves FDT blob to new address | ** fdt move - moves FDT blob to new address | ||
** fdt chosen - fixup dynamic information | ** fdt chosen - fixup dynamic information | ||
* | * '''Special Commands''' | ||
** i2c - I2C sub-system | ** i2c - I2C sub-system | ||
* | * '''Storage devices''' | ||
* | * '''Miscellaneous Commands''' | ||
** echo - echoes args to console | ** echo - echoes args to console | ||
** reset - performs a CPU reset | ** reset - performs a CPU reset | ||
Line 235: | Line 282: | ||
** version - prints the monitor version | ** version - prints the monitor version | ||
To add a new command, refer to {{CodeSource | U-Boot | doc/ | To add a new command, refer to {{DocSource | domain=U-Boot | path=develop/commands.html|text=U-Boot Documentation}} or to {{CodeSource | U-Boot | doc/develop/commands.rst}}. | ||
=== U-Boot environment variables === | === U-Boot environment variables === | ||
Line 241: | Line 288: | ||
The U-Boot behavior is configured through environment variables. | The U-Boot behavior is configured through environment variables. | ||
Refer to | Refer to {{CodeSource | U-Boot | README | README}} / Environment Variables and to {{DocSource | domain=U-Boot | path=usage/environment.html|text=U-Boot Documentation}}. | ||
On the first boot, U-Boot uses a default environment embedded in the U-Boot binary. You can modify it by changing the content of {{HighlightParam|CONFIG_EXTRA_ENV_SETTINGS}} in your configuration file (for example ./include/configs/stm32mp1.h) (see {{CodeSource | U-Boot | README | README}} / - Default Environment). | |||
This environment can be modified and saved in the boot device. When it is present, it is loaded during U-Boot initialization. | |||
For STMicroelectronics boards the environment location is automatically selected to support multiple boot device on the same board: | |||
* To boot from ''e''•MMC/SD card (CONFIG_ENV_IS_IN_MMC): at the end of the partition indicated by config field "u-boot,mmc-env-partition" in device-tree (partition named " | * To boot from ''e''•MMC/SD card (CONFIG_ENV_IS_IN_MMC): at the end of the partition indicated by config field "u-boot,mmc-env-partition" in device-tree (for STMicroelectronics boards, this partition is named "u-boot-env"). | ||
* To boot from NAND Flash memory (CONFIG_ENV_IS_IN_UBI): in the two UBI volumes "config" (CONFIG_ENV_UBI_VOLUME) and "config_r" (CONFIG_ENV_UBI_VOLUME_REDUND). | * To boot from NAND Flash memory (CONFIG_ENV_IS_IN_UBI): in the two UBI volumes "config" (CONFIG_ENV_UBI_VOLUME) and "config_r" (CONFIG_ENV_UBI_VOLUME_REDUND). | ||
* To boot from NOR Flash memory (CONFIG_ENV_IS_IN_SPI_FLASH): the u- | * To boot from NOR Flash memory (CONFIG_ENV_IS_IN_SPI_FLASH): the "u-boot-env" mtd partition at offset CONFIG_ENV_OFFSET. | ||
==== env command ==== | ==== env command ==== | ||
Line 254: | Line 303: | ||
The <code>env</code> command allows displaying, modifying and saving the environment in U-Boot console. | The <code>env</code> command allows displaying, modifying and saving the environment in U-Boot console. | ||
{{ | {{U-Boot$}}help env | ||
env - environment handling commands | env - environment handling commands | ||
Line 269: | Line 318: | ||
env set -e name [arg ...] - set UEFI variable; unset if 'arg' not specified | env set -e name [arg ...] - set UEFI variable; unset if 'arg' not specified | ||
env set [-f] name [arg ...] | env set [-f] name [arg ...] | ||
See {{DocSource | domain=U-Boot | path=usage/cmd/env.html|text=U-Boot Documentation}} for details. | |||
Example: proceed as follows to restore the default environment and save it. This is useful after a U-Boot upgrade: | Example: proceed as follows to restore the default environment and save it. This is useful after a U-Boot upgrade: | ||
{{ | {{U-Boot$}}env default -a | ||
{{ | {{U-Boot$}}env save | ||
You can also use the command activated by CONFIG_CMD_ERASEENV: | |||
{{U-Boot$}}env erase | |||
==== bootcmd ==== | ==== bootcmd ==== | ||
"bootcmd" variable is the autoboot command. It defines the command executed when U-Boot starts (CONFIG_BOOTCOMMAND). | "bootcmd" variable is the '''autoboot''' command (see {{CodeSource | U-Boot | doc/README.autoboot}}). It defines the command executed when U-Boot starts (CONFIG_BOOTCOMMAND). | ||
In generic stm32mp defconfig, CONFIG_BOOTCOMMAND="run bootcmd_stm32mp": | |||
{{ | {{U-Boot$}}env print bootcmd | ||
bootcmd=run bootcmd_stm32mp | bootcmd=run bootcmd_stm32mp | ||
"bootcmd_stm32mp" is a script that selects the command to be executed for each boot device (see | "bootcmd_stm32mp" is a [[#U-Boot scripting capabilities|script]] that selects the command to be executed for each boot device (see files in include/configs/: stm32mp13_st_common.h, stm32mp15_st_common.h, stm32mp21_st_common.h orstm32mp23_st_common.h or stm32mp25_st_common.h for STMicroelectronics board), based on [[#Generic Distro configuration|generic distro scripts]]: | ||
* To boot from a serial/usb device: execute the <code>stm32prog</code> command. | * To boot from a serial/usb device: execute the <code>stm32prog</code> command. | ||
* To boot from an ''e''•MMC, SD card: boot only on the same device (bootcmd_mmc...). | * To boot from an ''e''•MMC, SD card: boot only on the same device (bootcmd_mmc...). | ||
* To boot from a | * To boot from a NOR Flash memory: use the SD-Card (on SDMMC 0 on STMicroelectronics boards with bootcmd_mmc0). | ||
* To boot from a | * To boot from a NAND Flash memory: boot on ubifs partition on the NAND memory (bootcmd_ubi0) or on the SD-Card (bootcmd_mmc0). | ||
{{ | {{U-Boot$}}env print bootcmd_stm32mp | ||
You can then change this configuration: | You can then change this configuration: | ||
* either permanently in your board file | * either permanently in your board file | ||
** default environment by CONFIG_EXTRA_ENV_SETTINGS (see ./include/configs/ | ** default environment by CONFIG_EXTRA_ENV_SETTINGS (see ./include/configs/stm32mp*.h files) | ||
** change CONFIG_BOOTCOMMAND value in your defconfig | ** change CONFIG_BOOTCOMMAND value in your defconfig | ||
E.g: | |||
CONFIG_BOOTCOMMAND="run bootcmd_mmc0" | CONFIG_BOOTCOMMAND="run bootcmd_mmc0" | ||
Line 302: | Line 359: | ||
* or temporarily in the saved environment: | * or temporarily in the saved environment: | ||
{{ | {{U-Boot$}}env set bootcmd run bootcmd_mmc0 | ||
{{ | {{U-Boot$}}env save | ||
Note: To reset the environment to its default value: | Note: To reset the environment to its default value, use the command: | ||
{{ | {{U-Boot$}}env default bootcmd | ||
{{ | {{U-Boot$}}env save | ||
=== U-Boot scripting capabilities === | |||
"Script" is made up of variables (<code>bootcmd</code> for example) that contain a set of commands that are executed by the U-Boot command interpreter one after another. You run this script with the <code>run</code> command, for example: | |||
{{U-Boot$}}run bootcmd | |||
"Script image" is external binary file with U-Boot header and containing a sequence of commands. It is loaded by U-Boot in memory and executed using the <code>source</code> command, it allows the user to execute a set of predefined U-Boot commands automatically. | |||
To convert an text file commands.txt into a script image for U-Boot, you have to use the mkimage tool as follows: | |||
{{PC$}}mkimage -T script -C none -n 'Demo Script File' -d commands.txt setenv.img | |||
These feature are particularly useful when U-Boot use a the {{DocSource | domain=U-Boot | path=usage/cmdline.html#hush-shell | text=hush shell}} (similar to Bourne shell) as [[#U-Boot command line interface (CLI)|command interpreter]]; it is the default configuration in OpenSTLinux (CONFIG_HUSH_PARSER). | |||
=== Autoboot === | |||
If CONFIG_AUTOBOOT is activated, you have some delay established in <code>bootdelay</code> [[#U-Boot environment variables|variable]] or CONFIG_BOOTDELAY (2s by default, 1s for ST configuration) to enter the console by pressing any key, after the line below is displayed. | |||
Hit any key to stop autoboot: 2 | |||
If U-Boot is not interrupted, [[#bootcmd|bootcmd]] is executed (CONFIG_BOOTCOMMAND), in other words automatic booting have the same effect that the command: | |||
{{U-Boot$}}run bootcmd | |||
or | |||
{{U-Boot$}}boot | |||
=== Generic Distro configuration === | === Generic Distro configuration === | ||
Refer to {{CodeSource | U-Boot | doc/ | Refer to {{DocSource | domain=U-Boot | path=develop/distro.html | text=documentation}} or to {{CodeSource | U-Boot | doc/develop/distro.rst | doc/develop/distro.rst}} for details. | ||
This feature is activated by default on | This feature is activated by default on STMicroelectronics boards (CONFIG_DISTRO_DEFAULTS): | ||
* one boot command (bootmcd_xxx) exists for each bootable device. | * one boot command (bootmcd_xxx) exists for each bootable device. | ||
* U-Boot is independent from the Linux distribution used. | * U-Boot is independent from the Linux distribution used. | ||
Line 331: | Line 411: | ||
bootcmd_ubifs0=setenv devnum 0; run ubifs_boot | bootcmd_ubifs0=setenv devnum 0; run ubifs_boot | ||
U-Boot searches for an '''extlinux.conf''' configuration file for each bootable device. This file defines the kernel configuration to | U-Boot searches for an '''extlinux.conf''' configuration file for each '''bootable''' device. This file defines the files and the kernel configuration used to start the OS with <code>bootm</code> command: | ||
* | * {{highlight|KERNEL}} = '''kernel image''' (uImage or Image.gz)<br/>or '''FIT image''', including all these needed files (for details see {{CodeSource | U-Boot | doc/uImage.FIT/howto.txt}}) | ||
* | * {{highlight|FDT}} = '''device tree''' (optional)<br/>{{highlight|FDTDIR}} = '''path for device tree''', name of device tree is indicated by the variable {{highlightParam|fdtfile}}, build from the board compatible in U-Boot device tree for STMicroelectronics boards in the <code>board_late_init()</code> function, under CONFIG_ENV_VARS_UBOOT_RUNTIME_CONFIG. | ||
* | * {{highlight|KERNEL}} = '''ramdisk files''' (optional) | ||
* {{Highlight|APPEND}} = '''bootargs''', the Linux kernel’s command-line parameter ({{DocSource | domain=Linux kernel | path=admin-guide/kernel-parameters.html}}) | |||
== U-Boot build == | |||
See | See {{DocSource | domain=U-Boot | path=build/index.html|text=U-Boot Documentation}}. | ||
=== Prerequisites === | === Prerequisites === | ||
Line 350: | Line 428: | ||
* U-Boot source code | * U-Boot source code | ||
** the latest STMicroelectronics U-Boot version | ** the latest STMicroelectronics U-Boot version | ||
*** tar.xz file from Developer Package (for example [[ | *** tar.xz file from Developer Package (for example [[STM32MPU_Developer_Package#Installing_the_OpenSTLinux_BSP_packages|STM32MP1]]) or from latest release on ST github <ref name=releases/> | ||
*** from GITHUB<ref | *** from GITHUB<ref name=github/>, with <code>git</code> command | ||
{{PC$}} git clone https://github.com/STMicroelectronics/u-boot | {{PC$}}git clone https://github.com/STMicroelectronics/u-boot | ||
:* from the Mainline U-Boot in official GIT repository <ref | :* from the Mainline U-Boot in official GIT repository <ref name=git/> | ||
{{PC$}} git clone https:// | {{PC$}}git clone https://source.denx.de/u-boot/u-boot.git | ||
=== ARM cross compiler === | === ARM cross compiler === | ||
A cross compiler <ref>https://en.wikipedia.org/wiki/Cross_compiler</ref> must be installed on your Host (X86_64, i686, ...) for the ARM targeted Device architecture. In addition, the $PATH and $CROSS_COMPILE environment variables must be configured in your shell. | A cross compiler <ref>https://en.wikipedia.org/wiki/Cross_compiler</ref> must be installed on your Host (X86_64, i686, ...) for the ARM targeted Device architecture, AArch32 for {{MicroprocessorDevice | device=1}} or AArch64 for {{MicroprocessorDevice | device=2}}. In addition, the $PATH and $CROSS_COMPILE environment variables must be configured in your shell. | ||
You can use gcc for ARM, available in: | You can use gcc for ARM, available in: | ||
* the SDK toolchain (see [[Cross-compile with OpenSTLinux SDK]])<br/>PATH and CROSS_COMPILE are automatically updated. | * the SDK toolchain (see [[Cross-compile with OpenSTLinux SDK]])<br/>PATH and CROSS_COMPILE are automatically updated. | ||
* an existing package<br/>For example, install gcc-arm-linux-gnueabihf on Ubuntu/Debian: | * an existing package<br/>For example, install gcc-arm-linux-gnueabihf on Ubuntu/Debian:<br/>{{PC$}}sudo apt-get install gcc-arm-linux-gnueabihf | ||
<div class="mw-collapsible mw-collapsed"> | |||
* an existing toolchain: | * an existing toolchain: | ||
** latest gcc toolchain provided by arm (https://developer.arm.com/ | ** latest gcc toolchain provided by arm (https://developer.arm.com/downloads/-/arm-gnu-toolchain-downloads) | ||
** | ** Linaro also provides monthly build: (https://www.linaro.org/downloads/) | ||
<div class="mw-collapsible-content"> | |||
Examples for {{MicroprocessorDevice | device=1}}: | |||
1. '''gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf.tar.xz''' provided by arm, extract the toolchain in $HOME and update your environment with: | |||
{{PC$}}export PATH=$HOME/gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf/bin:$PATH | |||
{{PC$}} export PATH=$HOME/gcc-linaro-7.2.1-2017.11-x86_64_arm-linux-gnueabi/bin:$PATH | {{PC$}}export CROSS_COMPILE=arm-none-linux-gnueabihf- | ||
{{PC$}} export CROSS_COMPILE=arm-linux-gnueabi- | |||
2.'''gcc-linaro-7.2.1-2017.11-x86_64_arm-linux-gnueabi.tar.xz''', extract the toolchain in $HOME and update your environment with: | |||
{{PC$}}export PATH=$HOME/gcc-linaro-7.2.1-2017.11-x86_64_arm-linux-gnueabi/bin:$PATH | |||
{{PC$}}export CROSS_COMPILE=arm-linux-gnueabi- | |||
</div></div> | |||
=== Compilation === | === Compilation === | ||
In the U-Boot source directory, select the defconfig for the {{HighlightParam|<target>}} and the {{HighlightParam|<device tree>}} for your board and then execute the <code>make all</code> command: | In the U-Boot source directory, select the defconfig for the {{HighlightParam|<target>}} and the {{HighlightParam|<device tree>}} for your board and then execute the <code>make all</code> command: | ||
{{PC$}} make {{HighlightParam|<target>}}_defconfig | {{PC$}}make {{HighlightParam|<target>}}_defconfig | ||
{{PC$}} make DEVICE_TREE={{HighlightParam|<device tree>}} {{HighlightParam|all}} | {{PC$}}make {{Highlight|DEVICE_TREE}}={{HighlightParam|<device tree>}} {{HighlightParam|all}} | ||
Use help to list other targets than {{HighlightParam|all}}: | Use help to list other targets than {{HighlightParam|all}}: | ||
{{PC$}} make help | {{PC$}}make help | ||
Optionally | Optionally | ||
* | * {{Highlight|KBUILD_OUTPUT}} can be used to change the output build directory in order to compile several targets in the source directory. For example: | ||
{{PC$}} export KBUILD_OUTPUT={{HighlightParam|<path>}} | {{PC$}}export KBUILD_OUTPUT={{HighlightParam|<path>}} | ||
* | * {{Highlight|DEVICE_TREE}} can also be exported to your environment when only one board is supported. For example: | ||
{{PC$}} export DEVICE_TREE={{HighlightParam|<device-tree>}} | {{PC$}}export {{Highlight|DEVICE_TREE}}={{HighlightParam|<device-tree>}} | ||
The result is the following: | The result is the following: | ||
{{PC$}} export KBUILD_OUTPUT={{HighlightParam|<path>}} | {{PC$}}export {{Highlight|KBUILD_OUTPUT}}={{HighlightParam|<path>}} | ||
{{PC$}} export DEVICE_TREE={{HighlightParam|<device tree>}} | {{PC$}}export {{Highlight|DEVICE_TREE}}={{HighlightParam|<device tree>}} | ||
{{PC$}} make {{HighlightParam|<target>}}_defconfig | {{PC$}}make {{HighlightParam|<target>}}_defconfig | ||
{{PC$}} make {{HighlightParam|all}} | {{PC$}}make {{HighlightParam|all}} | ||
{{Highlight|DEVICE_TREE}} can also select a device trees present in the {{CodeSource | External_DT | u-boot/}} directory of the OpenSTLinux seperate [[Git]]: https://github.com/STMicroelectronics/dt-stm32mp by | |||
* using submodule in U-Boot directory {{HighlightParam|arch/arm/dts/external-dt}}, the default path for external device tree. | |||
{{PC$}}git submodule add https://github.com/STMicroelectronics/dt-stm32mp {{HighlightParam|arch/arm/dts/external-dt}} | |||
{{PC$}}make {{Highlight|DEVICE_TREE}}={{HighlightParam|<dts-file-name>}} all | |||
* cloning this [[Git]] in any location indicated with '''EXT_DTS'''in make command | |||
{{PC$}}git clone https://github.com/STMicroelectronics/dt-stm32mp <DTS_PATH> | |||
{{PC$}}make {{Highlight|DEVICE_TREE}}={{HighlightParam|<dts-file-name>}} {{Highlight|EXT_DTS}}=<DTS_PATH> all | |||
See examples in | |||
* [[STM32MP13 U-Boot]] | |||
* [[STM32MP15 U-Boot]] | |||
* [[STM32MP21 U-Boot]] | |||
* [[STM32MP23 U-Boot]] | |||
* [[STM32MP25 U-Boot]] | |||
=== Output files === | |||
The resulting U-Boot files are located in your build directory (U-Boot or KBUILD_OUTPUT). | |||
For OpenSTLinux, two U-Boot files are used by STMicroelectronics boards to generate the FIP file used byTF-A BL2: | |||
* {{HighlightParam|BL33_CFG}}={{Highlight|'''u-boot.dtb'''}} : the U-Boot device tree, selected by DEVICE_TREE, loaded by TF-A BL2 | |||
* {{HighlightParam|BL33}}={{Highlight|'''u-boot-nodtb.bin'''}}: the U-Boot executable, loaded by TF-A BL2 started by secure world = OP-TEE with BL33_CFG as parameter | |||
Nota: All the compiled device tree are available in $KBUILD_OUTPUT/arch/arm/dts/*.dtb.<br/>You can select them as {{HighlightParam|BL33_CFG}} parameter without U-Boot recompilation. | |||
See [[TF-A BL2 overview]] for FIP details. | |||
The [[ | The file used to [[U-Boot_-_How_to_debug|debug with gdb]] is {{Highlight|u-boot}}, the elf file for U-Boot. | ||
<div class="mw-collapsible mw-collapsed"> | |||
The file '''u-boot.stm32''', i.e. the U-Boot binary with [[STM32_header_for_binary_files|STM32 header]], is no more generated and used in OpenSTlinux. | |||
<div class="mw-collapsible-content"> | |||
This file is generated only with stm32mp15_trusted_defconfig, when {{HighlightParam|CONFIG_STM32MP15x_STM32IMAGE}} is activated. This defconfig is kept for compatibility with upstream, it is not supported in OpenSTlinux. | |||
The STM32 image format (*.stm32) is also managed by mkimage U-Boot tools and [[Signing_tool]] to manage this compatibility, stm32mp15_trusted_defconfig and stm32mp15_basic_defconfig. | |||
</div></div> | |||
== | == U-Boot integration in FIP == | ||
U-Boot binary and its associated device tree are part of the FIP binary, [[How to configure TF-A FIP#FIP_binary_creation|created]] with TF-A Makefile option : | |||
* {{HighlightParam|BL33_CFG}} = {{Highlight|'''u-boot.dtb'''}} | |||
* {{HighlightParam|BL33}} = {{Highlight|'''u-boot-nodtb.bin'''}} | |||
or [[How to configure TF-A FIP#Updating_U-Boot|updated]] with <code>fiptools</code>: | |||
* {{HighlightParam|--hw-config}} {{Highlight|'''u-boot.dtb'''}} | |||
* {{HighlightParam|--nt-fw}} {{Highlight|'''u-boot-nodtb.bin'''}} | |||
Example for FIP update : | |||
{{PC$}}fiptool {{HighlightParam|--verbose}} {{Highlight|update}} {{HighlightParam|--nt-fw}} {{Highlight|u-boot-nodtb.bin}} \ | |||
{{HighlightParam|--hw-config}} {{Highlight|u-boot.dtb}} \ | |||
'''fip-<board>.bin''' | |||
DEBUG: Replacing nt-fw with.../u-boot-nodtb.bin | |||
DEBUG: Replacing hw-config with .../u-boot.dtb | |||
DEBUG: Metadata size: ... bytes | |||
DEBUG: Payload size: ... bytes | |||
See [[How_to_configure_TF-A_FIP]] for details. | |||
== References == | == References == | ||
Line 428: | Line 544: | ||
<noinclude> | <noinclude> | ||
[[Category:U-Boot]] | [[Category:U-Boot|U-Boot - 1 overview]] | ||
{{PublicationRequestId | 16007|2020-05-05}} | {{PublicationRequestId | 16007|2020-05-05}} | ||
</noinclude> | </noinclude> |
Latest revision as of 12:03, 8 November 2024
1. Das U-Boot[edit | edit source]
Das U-Boot ("the Universal Boot Loader" or U-Boot) is an open-source bootloader that can be used on STMicroelectronics boards to initialize the platform and load the Linux® kernel.
- Official source code is available under git repository [1] at https://source.denx.de/u-boot/u-boot, also available in https://github.com/u-boot/u-boot
- source.denx.de also hosts the Custodian git trees;
the STMicroelectronics U-Boot Custodian Tree is available in https://source.denx.de/u-boot/custodians/u-boot-stm - the fork of "U-Boot" Source Tree used in OpenSTLinux is available in ST GITHUB[2] with associated releases [3]: https://github.com/STMicroelectronics/u-boot
- source.denx.de also hosts the Custodian git trees;
- Official manual:
- https://docs.u-boot.org:
it is the documentation generated from stable source code bymake htmldocs
- the documentations available in source code: README file and doc/
- https://docs.u-boot.org:
Read the README file before starting using U-Boot. It covers the following topics:
- source file tree structure
- description of CONFIG defines
- instructions for building U-Boot
- brief description of the Hush shell
- list of common environment variables
2. U-Boot overview[edit | edit source]
The STM32 MPU boot chain uses Trusted Firmware-A (TF-A) as FSBL and U-Boot as SSBL, included in a TF-A FIP.
2.1. SPL[edit | edit source]
U-Boot SPL is not supported in OpenSTLinux.
2.2. U-Boot: SSBL[edit | edit source]
2.2.1. U-Boot description[edit | edit source]
U-Boot is the second-stage bootloader (SSBL) of boot chain for STM32 Arm® Cortex® MPUs .
SSBL main features are the following:
- It is configurable and expendable.
- It features a simple command line interface (CLI), allowing users to interact over a serial port console.
- It provides scripting capabilities.
- It loads the kernel into RAM and gives control to the kernel.
- It manages several internal and external devices such as NAND and NOR Flash memories, Ethernet and USB.
- It supports the following features and commands:
- File systems: FAT, UBI/UBIFS, JFFS
- IP stack: FTP
- Display: LCD, HDMI, BMP for splashcreen
- USB: host (mass storage) or device (DFU stack)
2.2.2. U-Boot execution sequence[edit | edit source]
U-Boot executes the following main steps in DDR memory:
- Pre-relocation initialization (common/board_f.c ): minimal initialization (such as CPU, clock, reset, DDR and console) running at the CONFIG_TEXT_BASE load address.
- Relocation: copy of the code to the end of DDR memory.
- Post-relocation initialization:(common/board_r.c ): initialization of all the drivers.
- Command execution through autoboot (CONFIG_AUTOBOOT) or console shell.
- Execution of the boot command (by default bootcmd=CONFIG_BOOTCOMMAND):
for example, execution of the commandbootm
(for uImage or FIT) orbooti
(for Image.giz) to:- load and check images (such as kernel, device tree and ramdisk)
- fixup the kernel device tree
- install the secure monitor (optional) or
- pass the control to the Linux kernel (or to another target application)
- Execution of the boot command (by default bootcmd=CONFIG_BOOTCOMMAND):
3. U-Boot configuration[edit | edit source]
The U-Boot binary configuration is based on
- Kbuild infrastructure (as in Linux Kernel, you can use
make menuconfig
in U-Boot)
The configurations are based on:- options defined in Kconfig files (CONFIG_ compilation flags)
- the selected configuration file: configs/stm32mp*_defconfig
- other compilation flags defined in include/configs/stm32mp*.h (these flags are progressively migrated to Kconfig)
The selected file name is configured through CONFIG_SYS_CONFIG_NAME, for example on STMicroelectronics boards:- STM32MP13 unknown microprocessor device: include/configs/stm32mp13_st_common.h
- STM32MP15x lines
: include/configs/stm32mp15_st_common.h
- STM32MP21 unknown microprocessor device: include/configs/stm32mp21_st_common.h
- STM32MP23 unknown microprocessor device: include/configs/stm32mp23_st_common.h
- STM32MP25 unknown microprocessor device: include/configs/stm32mp25_st_common.h
- DeviceTree: U-Boot binaries include a device tree blob that is parsed at runtime
All the configuration flags (prefixed by CONFIG_) are described in the source code, either in the README file or in the documentation directory .
For example, CONFIG_CMD_CLK activates the command clk
compilation (cmd.clk.c ).
Hence to compile U-Boot, select the <target> and the device tree for the board in order to choose a predefined configuration.
Refer to #U-Boot_build for examples.
3.1. Kbuild[edit | edit source]
Like the kernel, the U-Boot build system is based on configuration symbols (defined in Kconfig files). The selected values are stored in a .config file located in the build directory, with the same makefile target. .
Proceed as follows:
- Select a predefined configuration (defconfig file in configs directory ) and generate the first .config:
PC $>make <config>_defconfig.
- Change the U-Boot compile configuration (modify .config) by using one of the following five
make
commands:
--> menu based program PC $>make config --> line-oriented configuration PC $>make xconfig --> QT program PC $>make gconfig --> GTK program PC $>make nconfig --> ncurse menu based programPC $>'make menuconfig'
You can then compile U-Boot with the updated .config.
Warning: the modification is performed locally in the build directory. It will be lost after a make distclean
.
Save your configuration to be able to use it as a defconfig file:
PC $>make savedefconfig
This target saves the current config as a defconfig file in the build directory. It can then be compared with the predefined configuration (configs/stm32mp*defconfig).
The other makefile targets are the following:
PC $>make help
....
Configuration targets:
config - Update current config utilising a line-oriented program
nconfig - Update current config utilising a ncurses menu based
program
menuconfig - Update current config utilising a menu based program
xconfig - Update current config utilising a Qt based front-end
gconfig - Update current config utilising a GTK+ based front-end
oldconfig - Update current config utilising a provided .config as base
localmodconfig - Update current config disabling modules not loaded
localyesconfig - Update current config converting local mods to core
defconfig - New config with default from ARCH supplied defconfig
savedefconfig - Save current config as ./defconfig (minimal config)
allnoconfig - New config where all options are answered with no
allyesconfig - New config where all options are accepted with yes
allmodconfig - New config selecting modules when possible
alldefconfig - New config with all symbols set to default
randconfig - New config with random answer to all options
listnewconfig - List new options
olddefconfig - Same as oldconfig but sets new symbols to their
default value without prompting
3.2. Device tree[edit | edit source]
Refer to U-Boot Documentation or doc/develop/devicetree/control.rst for details.
The board device tree has the same binding as the kernel. By default it is integrated within the U-Boot binaries: u-boot.bin: appended at the end of the code (CONFIG_OF_SEPARATE) or embedded in the U-Boot binary (CONFIG_OF_EMBED).
In OpenSTLinux, the U-Boot device tree (u-boot.dtb) is present inside a FIP and provided to U-Boot as external file loaded by FSBL=TF-A when U-Boot code is started (u-boot-nodtb.bin: code without device tree): the U-Boot device tree address is provided as boot parameter (in r2 register).
A default device tree is available in the defconfig file (by setting CONFIG_DEFAULT_DEVICE_TREE).
You can either select another supported device tree present in U-Boot directories by using the DEVICE_TREE make flag. For STM32 Arm® Cortex® MPUs boards, the corresponding file is <dts-file-name>.dts in arch/arm/dts/stm32mp*.dts , with <dts-file-name> set to the full name of the board:
DEVICE_TREE=<dts-file-name>PC $>make
or provide a device tree blob (dtb file) resulting from the dts file compilation, by using the EXT_DTB option:
EXT_DTB=<dts-file-name>.dtbPC $>make
To obtain a device tree file <dts-file-name>.dts that is identical to the Linux kernel one, these U-Boot properties are only added for STMicroelectronics boards in the add-on file <dts-file-name>-u-boot.dtsi. This file is automatically included in <dts-file-name>.dts during device tree compilation (the needed "#include" is added during the pre-processing phasis).
To do this, U-Boot uses specific device-tree flags to determine if the associated driver is bound and initialized prior to U-Boot relocation and/or if the associated node is present in SPL :
- bootph-all => initialized before relocation in U-Boot, present in SPL
- bootph-some-ram => initialized before relocation in U-Boot, not in SPL
- bootph-pre-ram => present in SPL
In the device tree used by U-Boot, these flags bootph-all need to be added in all the nodes used in U-Boot before relocation (or in SPL) and for all used handles (clock, reset, pincontrol).
See example for console configuration for example.
Device tree in SPL (not used in OpenSTLinux):
4. U-Boot command line interface (CLI)[edit | edit source]
Refer to U-Boot Documentation or doc/usage/cmdline.rst .
U-Boot has a command line interface, the U-Boot console, in which you work with U-Boot commands and environment variables to create a customized boot process.
4.1. Commands[edit | edit source]
U-Boot has a set of built-in commands for managing the system and booting the device.By modifying U-Boot source code, you can create your own built-in commands.
The commands are defined in cmd/*.c . They are activated through the corresponding CONFIG_CMD_* configuration flag.
Use the help
command in the U-Boot shell to list the commands available on your device:
help
The U-Boot usage is described in U-Boot Documentation but only few commands are described here.
Below the list of all commands extracted from an old U-Boot Manual] (obsolete and not-exhaustive):
- Information Commands
- bdinfo - prints Board Info structure
- coninfo - prints console devices and information
- flinfo - prints Flash memory information
- iminfo - prints header information for application image
- help - prints online help
- Memory Commands
- base - prints or sets the address offset
- crc32 - checksum calculation
- cmp - memory compare
- cp - memory copy
- md - memory display
- mm - memory modify (auto-incrementing)
- mtest - simple RAM test
- mw - memory write (fill)
- nm - memory modify (constant address)
- loop - infinite loop on address range
- Flash Memory Commands
- cp - memory copy
- flinfo - prints Flash memory information
- erase - erases Flash memory
- protect - enables or disables Flash memory write protection
- mtdparts - defines a Linux compatible MTD partition scheme
- Execution Control Commands
- source - runs a script from memory
- bootm - boots application image from memory
- go - starts application at address 'addr'
- Download Commands
- bootp - boots image via network using BOOTP/TFTP protocol
- dhcp - invokes DHCP client to obtain IP/boot params
- loadb - loads binary file over serial line (kermit mode)
- loads - loads S-Record file over serial line
- rarpboot- boots image via network using RARP/TFTP protocol
- tftpboot- boots image via network using TFTP protocol
- Environment Variables Commands
- printenv- prints environment variables
- saveenv - saves environment variables to persistent storage
- setenv - sets environment variables
- run - runs commands in an environment variable
- bootd - default boot, that is run 'bootcmd'
- Flattened Device Tree support
- fdt addr - selects the FDT to work on
- fdt list - prints one level
- fdt print - recursive printing
- fdt mknode - creates new nodes
- fdt set - sets node properties
- fdt rm - removes nodes or properties
- fdt move - moves FDT blob to new address
- fdt chosen - fixup dynamic information
- Special Commands
- i2c - I2C sub-system
- Storage devices
- Miscellaneous Commands
- echo - echoes args to console
- reset - performs a CPU reset
- sleep - delays the execution for a predefined time
- version - prints the monitor version
To add a new command, refer to U-Boot Documentation or to doc/develop/commands.rst .
4.2. U-Boot environment variables[edit | edit source]
The U-Boot behavior is configured through environment variables.
Refer to README / Environment Variables and to U-Boot Documentation.
On the first boot, U-Boot uses a default environment embedded in the U-Boot binary. You can modify it by changing the content of CONFIG_EXTRA_ENV_SETTINGS in your configuration file (for example ./include/configs/stm32mp1.h) (see README / - Default Environment).
This environment can be modified and saved in the boot device. When it is present, it is loaded during U-Boot initialization.
For STMicroelectronics boards the environment location is automatically selected to support multiple boot device on the same board:
- To boot from e•MMC/SD card (CONFIG_ENV_IS_IN_MMC): at the end of the partition indicated by config field "u-boot,mmc-env-partition" in device-tree (for STMicroelectronics boards, this partition is named "u-boot-env").
- To boot from NAND Flash memory (CONFIG_ENV_IS_IN_UBI): in the two UBI volumes "config" (CONFIG_ENV_UBI_VOLUME) and "config_r" (CONFIG_ENV_UBI_VOLUME_REDUND).
- To boot from NOR Flash memory (CONFIG_ENV_IS_IN_SPI_FLASH): the "u-boot-env" mtd partition at offset CONFIG_ENV_OFFSET.
4.2.1. env command[edit | edit source]
The env
command allows displaying, modifying and saving the environment in U-Boot console.
help env
env - environment handling commands
Usage:
env default [-f] -a - [forcibly] reset default environment
env default [-f] var [...] - [forcibly] reset variable(s) to their default values
env delete [-f] var [...] - [forcibly] delete variable(s)
env edit name - edit environment variable
env exists name - tests for existence of variable
env print [-a | name ...] - print environment
env print -e [name ...] - print UEFI environment
env run var [...] - run commands in an environment variable
env save - save environment
env set -e name [arg ...] - set UEFI variable; unset if 'arg' not specified
env set [-f] name [arg ...]
See U-Boot Documentation for details.
Example: proceed as follows to restore the default environment and save it. This is useful after a U-Boot upgrade:
env default -a
env save
You can also use the command activated by CONFIG_CMD_ERASEENV:
env erase
4.2.2. bootcmd[edit | edit source]
"bootcmd" variable is the autoboot command (see doc/README.autoboot ). It defines the command executed when U-Boot starts (CONFIG_BOOTCOMMAND).
In generic stm32mp defconfig, CONFIG_BOOTCOMMAND="run bootcmd_stm32mp":
env print bootcmd
bootcmd=run bootcmd_stm32mp
"bootcmd_stm32mp" is a script that selects the command to be executed for each boot device (see files in include/configs/: stm32mp13_st_common.h, stm32mp15_st_common.h, stm32mp21_st_common.h orstm32mp23_st_common.h or stm32mp25_st_common.h for STMicroelectronics board), based on generic distro scripts:
- To boot from a serial/usb device: execute the
stm32prog
command. - To boot from an e•MMC, SD card: boot only on the same device (bootcmd_mmc...).
- To boot from a NOR Flash memory: use the SD-Card (on SDMMC 0 on STMicroelectronics boards with bootcmd_mmc0).
- To boot from a NAND Flash memory: boot on ubifs partition on the NAND memory (bootcmd_ubi0) or on the SD-Card (bootcmd_mmc0).
env print bootcmd_stm32mp
You can then change this configuration:
- either permanently in your board file
- default environment by CONFIG_EXTRA_ENV_SETTINGS (see ./include/configs/stm32mp*.h files)
- change CONFIG_BOOTCOMMAND value in your defconfig
E.g:
CONFIG_BOOTCOMMAND="run bootcmd_mmc0"
CONFIG_BOOTCOMMAND="run distro_bootcmd"
- or temporarily in the saved environment:
env set bootcmd run bootcmd_mmc0
env save
Note: To reset the environment to its default value, use the command:
env default bootcmd
env save
4.3. U-Boot scripting capabilities[edit | edit source]
"Script" is made up of variables (bootcmd
for example) that contain a set of commands that are executed by the U-Boot command interpreter one after another. You run this script with the run
command, for example:
run bootcmd
"Script image" is external binary file with U-Boot header and containing a sequence of commands. It is loaded by U-Boot in memory and executed using the source
command, it allows the user to execute a set of predefined U-Boot commands automatically.
To convert an text file commands.txt into a script image for U-Boot, you have to use the mkimage tool as follows:
PC $>mkimage -T script -C none -n 'Demo Script File' -d commands.txt setenv.img
These feature are particularly useful when U-Boot use a the hush shell (similar to Bourne shell) as command interpreter; it is the default configuration in OpenSTLinux (CONFIG_HUSH_PARSER).
4.4. Autoboot[edit | edit source]
If CONFIG_AUTOBOOT is activated, you have some delay established in bootdelay
variable or CONFIG_BOOTDELAY (2s by default, 1s for ST configuration) to enter the console by pressing any key, after the line below is displayed.
Hit any key to stop autoboot: 2
If U-Boot is not interrupted, bootcmd is executed (CONFIG_BOOTCOMMAND), in other words automatic booting have the same effect that the command:
run bootcmd
or
boot
4.5. Generic Distro configuration[edit | edit source]
Refer to documentation or to doc/develop/distro.rst for details.
This feature is activated by default on STMicroelectronics boards (CONFIG_DISTRO_DEFAULTS):
- one boot command (bootmcd_xxx) exists for each bootable device.
- U-Boot is independent from the Linux distribution used.
- bootcmd is defined in ./include/config_distro_bootcmd.h
When DISTRO is enabled, the command that is executed by default is include/config_distro_bootcmd.h :
bootcmd=run distro_bootcmd
This script tries any device found in the 'boot_targets' variable and executes the associated bootcmd.
Example for mmc0, mmc1, mmc2, pxe and ubifs devices:
bootcmd_mmc0=setenv devnum 0; run mmc_boot
bootcmd_mmc1=setenv devnum 1; run mmc_boot
bootcmd_mmc2=setenv devnum 2; run mmc_boot
bootcmd_pxe=run boot_net_usb_start; dhcp; if pxe get; then pxe boot; fi
bootcmd_ubifs0=setenv devnum 0; run ubifs_boot
U-Boot searches for an extlinux.conf configuration file for each bootable device. This file defines the files and the kernel configuration used to start the OS with bootm
command:
- KERNEL = kernel image (uImage or Image.gz)
or FIT image, including all these needed files (for details see doc/uImage.FIT/howto.txt ) - FDT = device tree (optional)
FDTDIR = path for device tree, name of device tree is indicated by the variable fdtfile, build from the board compatible in U-Boot device tree for STMicroelectronics boards in theboard_late_init()
function, under CONFIG_ENV_VARS_UBOOT_RUNTIME_CONFIG. - KERNEL = ramdisk files (optional)
- APPEND = bootargs, the Linux kernel’s command-line parameter (admin-guide/kernel-parameters.html)
5. U-Boot build[edit | edit source]
See U-Boot Documentation.
5.1. Prerequisites[edit | edit source]
- a PC with Linux and tools:
- U-Boot source code
https://github.com/STMicroelectronics/u-bootPC $>git clone
- from the Mainline U-Boot in official GIT repository [1]
https://source.denx.de/u-boot/u-boot.gitPC $>git clone
5.2. ARM cross compiler[edit | edit source]
A cross compiler [5] must be installed on your Host (X86_64, i686, ...) for the ARM targeted Device architecture, AArch32 for STM32MP1 Series or AArch64 for STM32MP2 unknown microprocessor device. In addition, the $PATH and $CROSS_COMPILE environment variables must be configured in your shell.
You can use gcc for ARM, available in:
- the SDK toolchain (see Cross-compile with OpenSTLinux SDK)
PATH and CROSS_COMPILE are automatically updated. - an existing package
For example, install gcc-arm-linux-gnueabihf on Ubuntu/Debian:
PC $>sudo apt-get install gcc-arm-linux-gnueabihf
- an existing toolchain:
- latest gcc toolchain provided by arm (https://developer.arm.com/downloads/-/arm-gnu-toolchain-downloads)
- Linaro also provides monthly build: (https://www.linaro.org/downloads/)
5.3. Compilation[edit | edit source]
In the U-Boot source directory, select the defconfig for the <target> and the <device tree> for your board and then execute the make all
command:
<target>_defconfig PC $>make DEVICE_TREE=<device tree> allPC $>make
Use help to list other targets than all:
PC $>make help
Optionally
- KBUILD_OUTPUT can be used to change the output build directory in order to compile several targets in the source directory. For example:
<path>PC $>export KBUILD_OUTPUT=
- DEVICE_TREE can also be exported to your environment when only one board is supported. For example:
DEVICE_TREE=<device-tree>PC $>export
The result is the following:
KBUILD_OUTPUT=<path> PC $>export DEVICE_TREE=<device tree> PC $>make <target>_defconfig PC $>make allPC $>export
DEVICE_TREE can also select a device trees present in the Unsupported domain! directory of the OpenSTLinux seperate Git: https://github.com/STMicroelectronics/dt-stm32mp by
- using submodule in U-Boot directory arch/arm/dts/external-dt, the default path for external device tree.
https://github.com/STMicroelectronics/dt-stm32mp arch/arm/dts/external-dt PC $>make DEVICE_TREE=<dts-file-name> allPC $>git submodule add
- cloning this Git in any location indicated with EXT_DTSin make command
https://github.com/STMicroelectronics/dt-stm32mp <DTS_PATH> PC $>make DEVICE_TREE=<dts-file-name> EXT_DTS=<DTS_PATH> allPC $>git clone
See examples in
5.4. Output files[edit | edit source]
The resulting U-Boot files are located in your build directory (U-Boot or KBUILD_OUTPUT).
For OpenSTLinux, two U-Boot files are used by STMicroelectronics boards to generate the FIP file used byTF-A BL2:
- BL33_CFG=u-boot.dtb : the U-Boot device tree, selected by DEVICE_TREE, loaded by TF-A BL2
- BL33=u-boot-nodtb.bin: the U-Boot executable, loaded by TF-A BL2 started by secure world = OP-TEE with BL33_CFG as parameter
Nota: All the compiled device tree are available in $KBUILD_OUTPUT/arch/arm/dts/*.dtb.
You can select them as BL33_CFG parameter without U-Boot recompilation.
See TF-A BL2 overview for FIP details.
The file used to debug with gdb is u-boot, the elf file for U-Boot.
The file u-boot.stm32, i.e. the U-Boot binary with STM32 header, is no more generated and used in OpenSTlinux.
6. U-Boot integration in FIP[edit | edit source]
U-Boot binary and its associated device tree are part of the FIP binary, created with TF-A Makefile option :
- BL33_CFG = u-boot.dtb
- BL33 = u-boot-nodtb.bin
or updated with fiptools
:
- --hw-config u-boot.dtb
- --nt-fw u-boot-nodtb.bin
Example for FIP update :
--verbose update --nt-fw u-boot-nodtb.bin \ --hw-config u-boot.dtb \ fip-<board>.bin DEBUG: Replacing nt-fw with.../u-boot-nodtb.bin DEBUG: Replacing hw-config with .../u-boot.dtb DEBUG: Metadata size: ... bytes DEBUG: Payload size: ... bytesPC $>fiptool
See How_to_configure_TF-A_FIP for details.
7. References[edit | edit source]
- ↑ Jump up to: 1.0 1.1 https://source.denx.de/u-boot/u-boot.git or https://github.com/u-boot/u-boot
- ↑ Jump up to: 2.0 2.1 https://github.com/STMicroelectronics/u-boot
- ↑ Jump up to: 3.0 3.1 https://github.com/STMicroelectronics/u-boot/releases
- ↑ https://www.denx.de/wiki/pub/U-Boot/MiniSummitELCE2013/2013-ELCE-U-Boot-Falcon-Boot.pdf
- ↑ https://en.wikipedia.org/wiki/Cross_compiler