Registered User mNo edit summary |
Registered User mNo edit summary |
||
Line 17: | Line 17: | ||
rect 144 229 239 286 [[TF-A overview]] | rect 144 229 239 286 [[TF-A overview]] | ||
rect 260 229 356 286 [[U-Boot overview]] | rect 260 229 356 286 [[U-Boot overview]] | ||
rect 364 229 461 287 [[ | rect 364 229 461 287 [[STM32 MPU Linux kernel overview]] | ||
poly 255 203 359 203 359 289 140 289 140 224 255 224 [[Boot_chain_overview|Boot chain overview]] | poly 255 203 359 203 359 289 140 289 140 224 255 224 [[Boot_chain_overview|Boot chain overview]] | ||
rect 32 198 469 296 [[OpenSTLinux BSP architecture overview]] | rect 32 198 469 296 [[OpenSTLinux BSP architecture overview]] |
Revision as of 15:27, 4 November 2021
The OpenSTLinux distribution encompasses the following components:
- The OpenSTLinux BSP that offers services, to the application frameworks in the same context, from:
- The boot chain based on TF-A and U-Boot
- The OP-TEE secure OS running on the Cortex-A in secure mode
- The Linux® kernel running on the Arm® Cortex®-A in non-secure mode
- The Application frameworks that rely on the services provided by the OpenSTLinux BSP, to provide particular functionalities (code libraries, APIs, tool sets...) to facilitate the development of software applications:
- The Linux application frameworks (aka Linux middlewares) running on the user space of the Linux OS: e.g. libusb C library for a generic access to USB devices, ALSA user-space bundle for audio functionalities, GStreamer multimedia framework...
- The U-Boot application frameworks (not shown in the diagram), as part of the boot chain: e.g. configuration scripts
- On OP-TEE side, the Trusted Applications (TA) relies on the OP-TEE core for secrets operations (not visible from the Linux and STM32Cube MPU Package)
The figure below is clickable so that the user can directly jump to one of the sub-levels listed above.

OpenSTLinux architecture overview