deleted>Frq08988 mNo edit summary |
Registered User mNo edit summary |
||
(6 intermediate revisions by 3 users not shown) | |||
Line 1: | Line 1: | ||
<noinclude> | <noinclude>{{ApplicableFor | ||
{{ | |MPUs list=STM32MP13x, STM32MP15x | ||
|MPUs checklist=STM32MP13x,STM32MP15x | |||
}}</noinclude> | |||
</noinclude> | |||
==Peripheral overview== | ==Peripheral overview== | ||
The '''DTS''' peripheral is used to monitor the device temperature and take some preventive action (like frequency scaling or peripheral disabling) in case it is becoming too high and before destroying the component.<br /> | The '''DTS''' peripheral is used to monitor the device temperature and take some preventive action (like frequency scaling or peripheral disabling) in case it is becoming too high and before destroying the component.<br /> | ||
===Features=== | ===Features=== | ||
Refer to the [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]] for the complete list of features , and to the software components, introduced below, to see which features are implemented.<br> | Refer to the [[STM32MP13 resources#Reference manuals|STM32MP13 reference manuals]] or [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]] for the complete list of features , and to the software components, introduced below, to see which features are implemented.<br> | ||
===Security support=== | ===Security support=== | ||
Line 21: | Line 18: | ||
===Runtime=== | ===Runtime=== | ||
====Overview==== | ====Overview==== | ||
The | The monitoring is done from the Cortex-A7 non-secure context with Linux<sup>®</sup> [[Thermal overview|thermal management framework]]. | ||
====Software frameworks==== | ====Software frameworks==== | ||
{{: | ===== On {{MicroprocessorDevice | device=13}} ===== | ||
{{:STM32MP13 internal peripherals software table template}} | |||
| Power & Thermal | |||
| [[DTS internal peripheral|DTS]] | |||
| | |||
| [[Thermal overview|Linux thermal framework]] | |||
| | |||
|- | |||
|} | |||
===== On {{MicroprocessorDevice | device=15}} ===== | |||
{{:STM32MP15_internal_peripherals_software_table_template}} | |||
| Power & Thermal | | Power & Thermal | ||
| [[DTS internal peripheral|DTS]] | | [[DTS internal peripheral|DTS]] | ||
Line 38: | Line 45: | ||
====Peripheral assignment==== | ====Peripheral assignment==== | ||
{{: | ===== On {{MicroprocessorDevice | device=13}} ===== | ||
< | {{:STM32MP13_internal_peripherals_assignment_table_template}} | ||
<section begin=stm32mp13 /> | |||
| rowspan="1" | Power & Thermal | |||
| rowspan="1" | [[DTS internal peripheral|DTS]] | |||
| DTS | |||
| | |||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | |||
| | |||
|- | |||
<section end=stm32mp13 /> | |||
|} | |||
===== On {{MicroprocessorDevice | device=15}} ===== | |||
{{:STM32MP15_internal_peripherals_assignment_table_template}} | |||
<section begin=stm32mp15 /> | |||
| rowspan="1" | Power & Thermal | | rowspan="1" | Power & Thermal | ||
| rowspan="1" | [[DTS internal peripheral|DTS]] | | rowspan="1" | [[DTS internal peripheral|DTS]] | ||
Line 48: | Line 68: | ||
| | | | ||
|- | |- | ||
</ | <section end=stm32mp15 /> | ||
|} | |} | ||
==References== | ==References== | ||
<references/> | <references/> | ||
<noinclude> | |||
[[Category:Power and Thermal peripherals]] | |||
{{PublicationRequestId | 8855 | 2018-09-21 | BrunoB}} | |||
{{ArticleBasedOnModel| Internal peripheral article model}} | |||
</noinclude> |
Revision as of 18:26, 17 June 2022
1. Peripheral overview[edit | edit source]
The DTS peripheral is used to monitor the device temperature and take some preventive action (like frequency scaling or peripheral disabling) in case it is becoming too high and before destroying the component.
1.1. Features[edit | edit source]
Refer to the STM32MP13 reference manuals or STM32MP15 reference manuals for the complete list of features , and to the software components, introduced below, to see which features are implemented.
1.2. Security support[edit | edit source]
The DTS is a non secure peripheral.
2. Peripheral usage and associated software[edit | edit source]
2.1. Boot time[edit | edit source]
DTS is not used at boot time.
2.2. Runtime[edit | edit source]
2.2.1. Overview[edit | edit source]
The monitoring is done from the Cortex-A7 non-secure context with Linux® thermal management framework.
2.2.2. Software frameworks[edit | edit source]
2.2.2.1. On STM32MP13x lines
[edit | edit source]
Domain | Peripheral | Software components | Comment | |
---|---|---|---|---|
OP-TEE | Linux | |||
Power & Thermal | DTS | Linux thermal framework |
2.2.2.2. On STM32MP15x lines
[edit | edit source]
Domain | Peripheral | Software components | Comment | ||
---|---|---|---|---|---|
OP-TEE | Linux | STM32Cube | |||
Power & Thermal | DTS | Linux thermal framework |
2.2.3. Peripheral configuration[edit | edit source]
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the STM32CubeMX tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.
2.2.4. Peripheral assignment[edit | edit source]
2.2.4.1. On STM32MP13x lines
[edit | edit source]
Click on the right to expand the legend...
Domain | Peripheral | Runtime allocation | Comment | ||
---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) | |||
Power & Thermal | DTS | DTS | ☐ |
2.2.4.2. On STM32MP15x lines
[edit | edit source]
Click on the right to expand the legend...
Domain | Peripheral | Runtime allocation | Comment | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) |
Cortex-M4 (STM32Cube) | |||
Power & Thermal | DTS | DTS | ☐ |