1. Article purpose[edit | edit source]
The purpose of this article is to:
- briefly introduce the USB2PHY peripheral and its main features,
- indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
- list the software frameworks and drivers managing the peripheral,
- explain how to configure the peripheral.
2. Peripheral overview[edit | edit source]
The USB2PHY peripheral is a block that contains a USB high-speed UTMI+ PHY. It makes the interface between:
The USB2PHY peripheral is connected to the following controllers:
SoC | USB2PHY1 | USB2PHY2 |
---|---|---|
STM32MP21 unknown microprocessor device | USBH | OTG |
STM32MP23 unknown microprocessor device | USB3DR for USB2.0 speeds. | |
STM32MP25x lines ![]() |
SoC | USB2PHY Block diagram |
---|---|
On STM32MP21 unknown microprocessor device | ![]() |
On STM32MP23 unknown microprocessor device | ![]() |
On STM32MP25x lines ![]() |
Refer to the STM32 MPU reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.
3. Peripheral usage[edit | edit source]
This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.
3.1. Boot time assignment[edit | edit source]
3.1.1. On STM32MP21 unknown microprocessor device[edit | edit source]
One USB2PHY instance, that is, USB2PHY2, is a boot device that support Flash programming with STM32CubeProgrammer.
The USB2PHY2 instance is used by ROM code, FSBL and SSBL when using OTG in Device mode (DFU).
Click on to expand or collapse the legend...
Domain | Peripheral | Boot time allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A35 secure (ROM code) |
Cortex-A35 secure (TF-A BL2) |
Cortex-A35 non-secure (U-Boot) | |||
High speed interface | USB2PHY ![]() |
USB2PHY1 | ⬚ | ⬚ | ☐ | USB2PHY1 can be used in U-boot by USBH with command line tools. |
USB2PHY2 | ☐ | ☐ | ☐ | USB2PHY2 can be used by ROM code, FSBL and SSBL in DFU mode to support serial boot. It can be used also in U-boot by OTG with command line tools. |
3.1.2. On STM32MP23 unknown microprocessor device and STM32MP25x lines
[edit | edit source]
One USB2PHY instance, that is, USB2PHY2, is a boot device that support Flash programming with STM32CubeProgrammer.
The USB2PHY2 instance is used by ROM code, FSBL and SSBL when using USB3DR in Device mode (DFU).
Click on to expand or collapse the legend...
Domain | Peripheral | Boot time allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A35 secure (ROM code) |
Cortex-A35 secure (TF-A BL2) |
Cortex-A35 non-secure (U-Boot) | |||
High speed interface | USB2PHY ![]() |
USB2PHY1 | ⬚ | ⬚ | ☐ | USB2PHY1 can be used in U-boot by USBH with command line tools. |
USB2PHY2 | ☐ | ☐ | ☐ | USB2PHY2 can be used by ROM code, FSBL and SSBL in DFU mode to support serial boot. It can be used also in U-boot by USB3DR with command line tools. |
3.2. Runtime assignment[edit | edit source]
3.2.1. On STM32MP21 unknown microprocessor device[edit | edit source]
USB2PHY| rowspan="2" | High speed interface | rowspan="2" || USB2PHY1 | style="text-align:left;" | ⬚OP-TEE
⬚TF-A BL31 | ☐ | ⬚ | ☐ | Allocation inherited from USBH |- | USB2PHY2 | style="text-align:left;" | ☐OP-TEE
☐TF-A BL31 | ☐ | ☐ | ☐ | Allocation inherited from OTG |-
|}
3.2.2. On STM32MP23 unknown microprocessor device[edit | edit source]
USB2PHY| rowspan="2" | High speed interface | rowspan="2" || USB2PHY1 | style="text-align:left;" | ⬚OP-TEE
⬚TF-A BL31 | ☐ | ⬚ | ☐ | Allocation inherited from USBH |- | USB2PHY2 | style="text-align:left;" | ☐OP-TEE
☐TF-A BL31 | ☐ | ☐ | ☐ | Allocation inherited from USB3DR |-
|}
3.2.3. On STM32MP25x lines
[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Runtime allocation | Comment ![]() | |||||
---|---|---|---|---|---|---|---|---|
Instance | Cortex-A35 secure (OP-TEE / TF-A BL31) |
Cortex-A35 non-secure (Linux) |
Cortex-M33 secure (TF-M) |
Cortex-M33 non-secure (STM32Cube) |
Cortex-M0+![]() (STM32Cube) | |||
High speed interface | USB2PHY ![]() |
USB2PHY1 | ⬚OP-TEE ⬚TF-A BL31 |
☐ | ⬚ | ☐ | Allocation inherited from USBH | |
USB2PHY2 | ☐OP-TEE ☐TF-A BL31 |
☐ | ☐ | ☐ | Allocation inherited from USB3DR |
4. Software frameworks and drivers[edit | edit source]
Below are listed the software frameworks and drivers managing the USB2PHY peripheral for the embedded software components listed in the above tables.
- Linux®: PHY framework, USB2PHY driver (drivers/phy/st/phy-stm32-usb2phy.c )
- U-Boot: PHY uclass (drivers/phy/phy-uclass.c ) and driver (drivers/phy/phy-stm32-usb2phy.c )
5. How to assign and configure the peripheral[edit | edit source]
The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral by generating:
- partial device trees (pin control and clock tree) for the OpenSTLinux software components,
- HAL initialization code for the STM32CubeMPU Package.
The configuration is applied by the firmware running in the context in which the peripheral is assigned.
For U-boot and Linux kernel configuration, please refer to USB2PHY device tree configuration.
6. References[edit | edit source]