Registered User mNo edit summary Tag: 2017 source edit |
Registered User mNo edit summary Tag: 2017 source edit |
||
Line 80: | Line 80: | ||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | | <span title="assignable peripheral" style="font-size:21px">☐</span> | ||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | | <span title="assignable peripheral" style="font-size:21px">☐</span> | ||
| Shareable at internal peripheral level thanks to the RIF: see the [[HPDMA internal peripheral# | | Shareable at internal peripheral level thanks to the RIF: see the [[HPDMA internal peripheral#stm32mp21_HPDMA1-3_a35_runtime_rif | runtime allocation per feature]] | ||
|- | |- | ||
<section end=stm32mp21_a35_runtime /> | <section end=stm32mp21_a35_runtime /> | ||
|} | |} | ||
<span id=" | <span id="stm32mp21_HPDMA1-3_a35_runtime_rif"/>The below table shows the possible runtime allocations for the features of the HPDMA1-3 instance. | ||
{{#lst:STM32MP2_internal_peripherals_assignment_table_template|stm32mp21_runtime_rif}} | {{#lst:STM32MP2_internal_peripherals_assignment_table_template|stm32mp21_runtime_rif}} | ||
| HPDMAx (x = 1 to 3) channel y (y = 0 to 15) | | HPDMAx (x = 1 to 3) channel y (y = 0 to 15) | ||
Line 107: | Line 107: | ||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | | <span title="assignable peripheral" style="font-size:21px">☐</span> | ||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | | <span title="assignable peripheral" style="font-size:21px">☐</span> | ||
| Shareable at internal peripheral level thanks to the RIF: see the [[HPDMA internal peripheral# | | Shareable at internal peripheral level thanks to the RIF: see the [[HPDMA internal peripheral#stm32mp23_HPDMA1-3_a35_runtime_rif | runtime allocation per feature]] | ||
|- | |- | ||
<section end=stm32mp23_a35_runtime /> | <section end=stm32mp23_a35_runtime /> | ||
|} | |} | ||
<span id=" | <span id="stm32mp23_HPDMA1-3_a35_runtime_rif"/>The below table shows the possible runtime allocations for the features of the HPDMA1-3 instance. | ||
{{#lst:STM32MP2_internal_peripherals_assignment_table_template|stm32mp23_runtime_rif}} | {{#lst:STM32MP2_internal_peripherals_assignment_table_template|stm32mp23_runtime_rif}} | ||
| HPDMAx (x = 1 to 3) channel y (y = 0 to 15) | | HPDMAx (x = 1 to 3) channel y (y = 0 to 15) | ||
Line 135: | Line 135: | ||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | | <span title="assignable peripheral" style="font-size:21px">☐</span> | ||
| - | | - | ||
| Shareable at internal peripheral level thanks to the RIF: see the [[HPDMA internal peripheral# | | Shareable at internal peripheral level thanks to the RIF: see the [[HPDMA internal peripheral#stm32mp25_HPDMA1-3_a35_runtime_rif | runtime allocation per feature]] | ||
|- | |- | ||
<section end=stm32mp25_a35_runtime /> | <section end=stm32mp25_a35_runtime /> | ||
|} | |} | ||
<span id=" | <span id="stm32mp25_HPDMA1-3_a35_runtime_rif"/>The below table shows the possible runtime allocations for the features of the HPDMA1-3 instance. | ||
{{#lst:STM32MP2_internal_peripherals_assignment_table_template|stm32mp25_runtime_rif}} | {{#lst:STM32MP2_internal_peripherals_assignment_table_template|stm32mp25_runtime_rif}} | ||
| HPDMAx (x = 1 to 3) channel y (y = 0 to 15) | | HPDMAx (x = 1 to 3) channel y (y = 0 to 15) |
Revision as of 11:22, 7 November 2024
1. Article purpose[edit | edit source]
The purpose of this article is to:
- briefly introduce the HPDMA peripheral and its main features,
- indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
- list the software frameworks and drivers managing the peripheral,
- explain how to configure the peripheral.
2. Peripheral overview[edit | edit source]
The HPDMA peripheral is used to perform high-speed data transfers between memory and memory or between peripherals and memory. The HPDMA controller offers 16 channels. The selection of the device connected to each channel and controlling DMA transfers is done in HPDMA peripheral.
The channels are divided into three performance groups, based on their FIFO size:
- channel 0 to 7 have 8-byte FIFO and belong to Low performance group.
- channel 8 to 11 have 32-byte FIFO and belong to Medium performance group.
- channel 12 to 15 have 128-byte FIFO and belong to High performance group.
- for STM32MP21 unknown microprocessor device
- channel 0 to 7 have 32-byte FIFO and belong to Medium performance group.
- channel 8 to 11 have 64-byte FIFO and belong to Medium performance group.
- channel 12 to 14 have 128-byte FIFO and belong to High performance group.
- channel 15 has 256-byte FIFO and belongs to Very High performance group.
Refer to the STM32MP2xxx reference manual, HPDMA channels chapter, for the implementation of HPDMA channels and their intended use. Refer to HPDMA device tree configuration for the HPDMA device tree bindings and how to select a channel fulfilling the application requirements.
The HPDMA is a RIF-Aware peripheral: transfers can be compartmented, independently at channel level, via compartment IDs (CID). Refer to STM32MP2 firewall configuration and HPDMA device tree configuration.
The HPDMA is a secure peripheral. This means that it performs each transfer in the context of the master that requested it:
- a transfer requested by the Arm® Cortex®-A35 or Arm® Cortex®-M33 nonsecure core propagates nonsecure accesses to the targeted device and/or internal memory.
- a transfer requested by the Arm® Cortex®-A35 or Arm® Cortex®-M33 secure core propagates secure accesses to the targeted device and/or internal memory.
Refer to the STM32 MPU reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.
3. Peripheral usage[edit | edit source]
This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.
3.1. Boot time assignment[edit | edit source]
3.1.1. On STM32MP2 series[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Boot time allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A35 secure (ROM code) |
Cortex-A35 secure (TF-A BL2) |
Cortex-A35 non-secure (U-Boot) | |||
Core/DMA | HPDMA ![]() |
HPDMAx (x = 1 to 3) | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature |
The table below shows the possible boot time allocations for the features of the HPDMAx (x = 1 to 3) instances.
Feature | Boot time allocation ![]() |
Comment | ||
---|---|---|---|---|
Cortex-A35 secure (ROM code) |
Cortex-A35 secure (TF-A BL2) |
Cortex-A35 non-secure (U-Boot) | ||
HPDMAx (x = 1 to 3) channel y (y = 0 to 15) | ⬚ | ⬚ |
3.2. Runtime assignment[edit | edit source]
3.2.1. On STM32MP21 unknown microprocessor device[edit | edit source]
| rowspan="1" | Core/DMA
| rowspan="1" | HPDMA
| HPDMAx (x = 1 to 3)
| ☐OP-TEE
| ☐
| ☐
| ☐
| Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature
|-
|}
The below table shows the possible runtime allocations for the features of the HPDMA1-3 instance.
| HPDMAx (x = 1 to 3) channel y (y = 0 to 15) | ⬚OP-TEE | ☐ | ⬚ | ☐ | |- |}
3.2.2. On STM32MP23 unknown microprocessor device[edit | edit source]
| rowspan="1" | Core/DMA
| rowspan="1" | HPDMA
| HPDMAx (x = 1 to 3)
| ☐OP-TEE
| ☐
| ☐
| ☐
| Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature
|-
|}
The below table shows the possible runtime allocations for the features of the HPDMA1-3 instance.
| HPDMAx (x = 1 to 3) channel y (y = 0 to 15) | ⬚OP-TEE | ☐ | ⬚ | ☐ | |- |}
3.2.3. On STM32MP25x lines
[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Runtime allocation | Comment ![]() | |||||
---|---|---|---|---|---|---|---|---|
Instance | Cortex-A35 secure (OP-TEE / TF-A BL31) |
Cortex-A35 non-secure (Linux) |
Cortex-M33 secure (TF-M) |
Cortex-M33 non-secure (STM32Cube) |
Cortex-M0+![]() (STM32Cube) | |||
Core/DMA | HPDMA ![]()
|
HPDMAx (x = 1 to 3) | ☐OP-TEE | ☐ | ☐ | ☐ | - | Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature |
The below table shows the possible runtime allocations for the features of the HPDMA1-3 instance.
Feature | Runtime allocation ![]() |
Comment | ||||
---|---|---|---|---|---|---|
Cortex-A35 secure (OP-TEE / TF-A BL31) |
Cortex-A35 non-secure (Linux) |
Cortex-M33 secure (TF-M) |
Cortex-M33 non-secure (STM32Cube) |
Cortex-M0+![]() (STM32Cube) | ||
HPDMAx (x = 1 to 3) channel y (y = 0 to 15) | ⬚OP-TEE | ☐ | ⬚ | ☐ | - |
4. Software frameworks and drivers[edit | edit source]
Below are listed the software frameworks and drivers managing the HPDMA peripheral for the embedded software components listed in the above tables.
- Linux®: dmaengine framework
- STM32Cube: DMA HAL driver and header file of DMA HAL module
STM32CubeMX allows to distinguish between nonsecure and secure channels, among all the available channels.
5. How to assign and configure the peripheral[edit | edit source]
The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral by generating:
- partial device trees (pin control and clock tree) for the OpenSTLinux software components,
- HAL initialization code for the STM32CubeMPU Package.
The configuration is applied by the firmware running in the context in which the peripheral is assigned.
6. References[edit | edit source]