Last edited 10 months ago

STM32MP2 OP-TEE overview

(Redirected from STM32MP25 OP-TEE overview)
Applicable for STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

This section gives an overview of the OP-TEE core drivers (UPPERCASE in the figure) implemented for the STM32MP2 series support, with their respective software frameworks (lowercase in the figure).

1. For A35-TD flavor [edit | edit source]

On the STM32MP2 series, when the A35-TD flavor is selected, OP-TEE is the main TEE of the platform.
It is running in the Cortex-A35 secure context (EL2S and EL1S execution level). It is associated to TF-A BL31 secure monitor which is running in Cortex-A35 EL3 and which is providing Cortex-A35 cluster low power functionalities via PSCI interface.

OP-TEE is in charge of:

  • System resources management:
    • Internal and external regulators
    • Clock tree (PLLs and Root clocks)
    • System peripheral clock gating
    • Oscillators calibration
    • Firewall configuration and dynamic management
    • OTP access
    • RNG access
    • Wakeup pins
  • Secure services
    • Cryptography via Global Platform (GP) API
    • PKCS#11
    • Trusted UI
    • StMM for secure UEFI
    • fTPM (firmware TPM) for TPM2 services
    • OTP for provisioning
    • SecCopro for secure Arm® Cortex®-M coprocessor management

As mentioned in the STM32 MPU OP-TEE overview, the different features can be independently activated according to customer needs.

The following figure provides an overview of the STM32MP2 series OP-TEE.

The components are grouped by functional domains.
Each OP-TEE framework is further described in the OP-TEE category articles.
Each STM32 MPU peripheral is introduced in the peripherals overview articles.
Both sections are reusing the same functional domain split.

The color code, explained in the legend, allows to see the code origin for each component.

Zoom out to OpenSTLinux distribution


2. For M33-TD flavor [edit | edit source]

On the STM32MP2 series, when the M33-TD flavor is selected, OP-TEE is the secondary TEE of the platform.
It is running in the Cortex-A35 secure context (EL2S and EL1S execution level). It is associated to TF-A BL31 secure monitor which is running in Cortex-A35 EL3 and which is providing Arm Cortex-A35 cluster low power functionalities via PSCI interface.

OP-TEE is in charge of:

  • Secure services
    • Cryptography via Global Platform (GP) API
    • PKCS#11
    • Trusted UI
    • StMM for secure UEFI
    • fTPM (firmware TPM) for TPM2 services
    • OTP access over PSA client (IPCC based)
    • Cryptographic access over PSA client (IPCC based)

As mentioned in the STM32 MPU OP-TEE overview, the different features can be independently activated according to customer needs.

The following figure provides an overview of the STM32MP2 series OP-TEE.

The components are grouped by functional domains.
Each OP-TEE framework is further described in the OP-TEE category articles.
Each STM32 MPU peripheral is introduced in the peripherals overview articles.
Both sections are reusing the same functional domain split.

The color code, explained in the legend, allows to see the code origin for each component.

Zoom out to OpenSTLinux distribution