Difference between revisions of "USBPHYC device tree configuration"

[unchecked revision] [quality revision]
m (DT configuration (board level))
m
Applicable for STM32MP13x lines, STM32MP15x lines

1 Article purpose[edit]

This article explains how to configure the USBPHYC internal peripheral when it is assigned to the Linux® OS. In that case, it is controlled by the PHY framework.

The configuration is performed using the device tree mechanism.

It is used by the USBPHYC Linux driver[1] which registers the relevant information in PHY framework.

2 DT bindings documentation[edit]

USBPHYC device tree bindings[2] describe all the required and optional functions.

USBPHYC
      |_ PLL
      |
      |_ PHY port#1 _________________ HOST controller
      |                    _                 |
      |                  / 1|________________|
      |_ PHY port#2 ----|   |________________
      |                  \_0|                |
      |_ UTMI switch_______|          OTG controller

3 DT configuration[edit]

This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split.

STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.

3.1 DT configuration (STM32 level)[edit]

The USBPHYC node is declared in:

  • stm32mp131.dtsi[3] on STM32MP13x lines Warning.png
  • stm32mp151.dtsi[4] on STM32MP15x lines More info.png.

It is composed of several nodes:

  • root node e.g. usbphyc describes the USBPHYC hardware block parameters such as registers, clocks, resets and supplies.
  • child nodes e.g. usbphyc_port0 and usbphyc_port1 describe the two high speed PHY ports: port#1 and port#2.
usbphyc: usbphyc@address {
	compatible = "st,stm32mp1-usbphyc";
	...                                         /* usbphyc resources: registers, clocks, resets and supplies */
	usbphyc_port0: usb-phy@0 {
		...                                 /* usbphyc HS PHY port#1 */
	};
	usbphyc_port1: usb-phy@1 {
		...                                 /* usbphyc HS PHY port#2 */
	};
};
Warning white.png Warning
This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.

3.2 DT configuration (board level)[edit]

Follow the sequences described in the below chapters to configure and enable the USBPHYC on your board.

The 'usbphyc' root node must be filled in:

  • Enable the USBPHYC block by setting status = "okay".

The child nodes for each port must be filled in:

  • Configure the USBPHYC 3V3 regulator[5] by setting phy-supply = <&your_regulator>.
Info white.png Information
USB HS PHY ports require an external 3V3 power supply to be provided at VDD3V3_USBHS pin.
  • Optional, you may configure the VBUS 5V regulator[5] by using a connector node with vbus-supply = <&your_regulator>. Have a look at connector bindings [6]
  • Optional, for ecosystem release ≥ v4.0.0 More info.png , each PHY port parameters may be tuned by adding properties directly inside the child node of each port.
Info white.png Information
It may be necessary to adjust the phy settings to compensate parasitics, which can be due to USB connector/receptacle, routing, ESD protection component.

Optional tuning parameter list is available in USBPHYC device tree bindings[2].


3.3 DT configuration example[edit]

The example below shows how to enable and configure USBPHYC ports in the board file.

For ecosystem release ≥ v4.0.0 More info.png

&usbphyc {
	status = "okay";                            /* enable USB HS PHY controller */
};

&usbphyc_port0 {
	phy-supply = <&vdd_usb>;                    /* references the 3V3 voltage regulator on the user board */
	st,tune-hs-dc-level = <2>;                  /* optional USB HS PHY port#1 tuning */
	st,enable-fs-rftime-tuning;
	st,enable-hs-rftime-reduction;
	st,trim-hs-current = <15>;
	st,trim-hs-impedance = <1>;
	st,tune-squelch-level = <3>;
	st,tune-hs-rx-offset = <2>;
	st,no-lsfs-sc;
	connector {
		compatible = "usb-a-connector";
		vbus-supply = <&vbus_sw>;           /* references the optional 5V voltage regulator on the user board */ 
	};
};

&usbphyc_port1 {
	phy-supply = <&vdd_usb>;                    /* references the 3V3 voltage regulator on the user board */
	st,tune-hs-dc-level = <2>;                  /* optional USB HS PHY port#2 tuning */
	st,enable-fs-rftime-tuning;
	st,enable-hs-rftime-reduction;
	st,trim-hs-current = <15>;
	st,trim-hs-impedance = <1>;
	st,tune-squelch-level = <3>;
	st,tune-hs-rx-offset = <2>;
	st,no-lsfs-sc;
};
Info white.png Information
Static configuration of the UTMI switch to assign the port#2 to either USBH or OTG is done by the PHY user node[7]:

usbphyc_port1 user must configure an additional specifier for UTMI switch: 0 to select OTG, 1 to select USBH

Abstract of the example to configure port#2, to be assigned to the USBH:

&usbh_ehci {
	phys = <&usbphyc_port0>, <&usbphyc_port1 1>; /* 1: UTMI switch selects the USBH */
	phy-names = "usb", "usb";
	...
}

Abstract of the example to configure port#2, to be assigned to the OTG:

&usbotg_hs {
	phys = <&usbphyc_port1 0>;                  /* 0: UTMI switch selects the OTG */
	phy-names = "usb2-phy";
	...
}

4 How to configure the DT using STM32CubeMX[edit]

The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.

5 References[edit]

Please refer to the following links for additional information:


<noinclude>{{ApplicableFor
|MPUs list=STM32MP13x, STM32MP15x
|MPUs checklist=STM32MP13x,STM32MP15x
}}</noinclude>

{{ReviewsComments|-- [[User:Nathalie Sangouard|Nathalie Sangouard]] ([[User talk:Nathalie Sangouard|talk]]) 15:28, 30 May 2022 (CEST)<br />General remark : reference to previous ecosystem release should be removed. The previous one could be accepted but not the ones before (v2, v1, ...)}}== Article purpose ==
This article explains how to configure the [[USBPHYC internal peripheral|'''USBPHYC''' internal peripheral]] when it is assigned to the Linux<sup>&reg;</sup> OS. In that case, it is controlled by the [[PHY_overview|PHY framework]].

The configuration is performed using the [[Device tree|device tree]] mechanism.

It is used by the ''USBPHYC Linux driver''<ref>{{CodeSource | Linux kernel | drivers/phy/st/phy-stm32-usbphyc.c}}, STM32 USB PHY Controller driver</ref> which registers the relevant information in [[PHY_overview|PHY framework]].

== DT bindings documentation ==
''USBPHYC device tree bindings''<ref name="phy-stm32-usbphyc.txt">{{CodeSource | Linux kernel | Documentation/devicetree/bindings/phy/phy-stm32-usbphyc.yaml}}, USBPHYC device tree bindings</ref> describe all the required and optional functions.

 USBPHYC
       |_ PLL
       |
       |_ PHY port#1 _________________ HOST controller
       |                    _                 |
       |                  / 1|________________|
       |_ PHY port#2 ----|   |________________
       |                  \_0|                |
       |_ UTMI switch_______|          OTG controller

== DT configuration ==
This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device tree file split.

'''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details.
=== DT configuration (STM32 level) ===
The USBPHYC node is declared in:
* stm32mp131.dtsi<ref name="stm32mp131_dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp131.dtsi}}, STM32MP131 device tree file</ref> on {{MicroprocessorDevice | device=13}}
* stm32mp151.dtsi<ref name="stm32mp151_dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp151.dtsi}}, STM32MP151 device tree file</ref> on {{MicroprocessorDevice | device=15}}.
It is composed of several nodes:
* root node e.g. '''usbphyc''' describes the USBPHYC hardware block parameters such as registers, clocks, resets and supplies.
* child nodes e.g. '''usbphyc_port0''' and '''usbphyc_port1''' describe the two high speed PHY ports: ''port#1'' and ''port#2''.
 usbphyc: usbphyc@address {
 	compatible = "st,stm32mp1-usbphyc";
 	...                                         {{highlight|/* usbphyc resources: registers, clocks, resets and supplies */}}
 	usbphyc_port0: usb-phy@0 {
 		...                                 {{highlight|/* usbphyc HS PHY port#1 */}}
 	};
 	usbphyc_port1: usb-phy@1 {
 		...                                 {{highlight|/* usbphyc HS PHY port#2 */}}
 	};
 };
{{Warning|This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.}}

=== DT configuration (board level) ===
Follow the sequences described in the below chapters to configure and enable the USBPHYC on your board.

The ''''usbphyc'''' '''root node''' must be filled in:
* Enable the USBPHYC block by setting '''status = "okay".'''

The '''child nodes''' for each port must be filled in:
* Configure the USBPHYC 3V3 regulator<ref name="Regulator overview">[[Regulator overview]]</ref> by setting '''phy-supply = <&your_regulator>'''.
{{Info| USB HS PHY ports require an external 3V3 power supply to be provided at VDD3V3_USBHS pin.}}
* Optional, you may configure the VBUS 5V regulator<ref name="Regulator overview">[[Regulator overview]]</ref> by using a connector node with '''vbus-supply = <&your_regulator>'''. Have a look at connector bindings <ref name="connector_bindings>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/connector/usb-connector.yaml}}</ref>


* Optional, '''for {{EcosystemRelease | revision=4.0.0 | range=and after}}''', each PHY port parameters may be tuned by adding properties directly inside the child node of each port.
{{Info| It may be necessary to adjust the phy settings to compensate parasitics, which can be due to USB connector/receptacle, routing, ESD protection component.
Optional tuning parameter list is available in ''USBPHYC device tree bindings''<ref name="phy-stm32-usbphyc.txt"/>.}}
{{ReviewsComments|FGA W902: Later add reference link to the application note that explains how to tune these parameters (once published)}}

=== DT configuration example ===
The example below shows how to enable and configure USBPHYC ports in the board file.

'''For {{EcosystemRelease | revision=4.0.0 | range=and after}}'''
 &usbphyc {
 	status = "okay";                            {{highlight|/* enable USB HS PHY controller */}}
 };

 &usbphyc_port0 {
 	phy-supply = <&vdd_usb>;                    {{highlight|/* references the 3V3 voltage regulator on the user board */}}
 	st,tune-hs-dc-level = <2>;                  {{highlight|/* optional USB HS PHY port#1 tuning */}}
 	st,enable-fs-rftime-tuning;
 	st,enable-hs-rftime-reduction;
 	st,trim-hs-current = <15>;
 	st,trim-hs-impedance = <1>;
 	st,tune-squelch-level = <3>;
 	st,tune-hs-rx-offset = <2>;
 	st,no-lsfs-sc;
 	connector {
 		compatible = "usb-a-connector";
 		vbus-supply = <&vbus_sw>;           {{highlight|/* references the optional 5V voltage regulator on the user board */}} 
 	};
 };

 &usbphyc_port1 {
 	phy-supply = <&vdd_usb>;                    {{highlight|/* references the 3V3 voltage regulator on the user board */}}
 	st,tune-hs-dc-level = <2>;                  {{highlight|/* optional USB HS PHY port#2 tuning */}}
 	st,enable-fs-rftime-tuning;
 	st,enable-hs-rftime-reduction;
 	st,trim-hs-current = <15>;
 	st,trim-hs-impedance = <1>;
 	st,tune-squelch-level = <3>;
 	st,tune-hs-rx-offset = <2>;
 	st,no-lsfs-sc;
 };

{{Info| Static configuration of the UTMI switch to assign the '''port#2''' to either [[USBH_internal_peripheral|USBH]] or [[OTG_internal_peripheral|OTG]] is done by the '''PHY user node'''<ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/phy/phy-bindings.txt}},PHY generic bindings</ref>:
* Please refer to [[USBH_device_tree_configuration]]
* Please refer to [[OTG_device_tree_configuration]]
'''usbphyc_port1''' user must configure an additional specifier for UTMI switch: '''0 to select OTG''', '''1 to select USBH'''
}}
Abstract of the example to configure port#2, to be assigned to the USBH:
 &usbh_ehci {
 	phys = <&usbphyc_port0>, <&usbphyc_port1 {{highlight|'''1'''}}>; {{highlight|/* '''1''': UTMI switch selects the USBH */}}
 	phy-names = "usb", "usb";
 	...
 }
Abstract of the example to configure port#2, to be assigned to the OTG:
 &usbotg_hs {
 	phys = <&usbphyc_port1 {{highlight|'''0'''}}>;                  {{highlight|/* '''0''': UTMI switch selects the OTG */}}
 	phy-names = "usb2-phy";
 	...
 }

==How to configure the DT using STM32CubeMX==
The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32|platform configuration device tree]] files.<br />

The STM32CubeMX may not support all the properties described in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information.

==References==
Please refer to the following links for additional information:
<references />

<noinclude>

[[Category:Device tree configuration]]
[[Category:USB]]
{{PublicationRequestId | 10329 | 2019-01-15 | AlainF}}
{{ArticleBasedOnModel | Peripheral or framework device tree configuration model}}</noinclude>
Line 4: Line 4:
 
}}</noinclude>
 
}}</noinclude>
   
{{ReviewsComments|-- [[User:Nathalie Sangouard|Nathalie Sangouard]] ([[User talk:Nathalie Sangouard|talk]]) 15:28, 30 May 2022 (CEST)<br />General remark : reference to previous ecosystem release should be removed. The previous one could be accepted but not the ones before (v2, v1, ...)}}
 
 
== Article purpose ==
 
== Article purpose ==
 
This article explains how to configure the [[USBPHYC internal peripheral|'''USBPHYC''' internal peripheral]] when it is assigned to the Linux<sup>&reg;</sup> OS. In that case, it is controlled by the [[PHY_overview|PHY framework]].
 
This article explains how to configure the [[USBPHYC internal peripheral|'''USBPHYC''' internal peripheral]] when it is assigned to the Linux<sup>&reg;</sup> OS. In that case, it is controlled by the [[PHY_overview|PHY framework]].