Difference between revisions of "U-Boot overview"
[checked revision] | [quality revision] |
m (restore help env)
|
m
|
Contents
1 Das U-Boot[edit]
Das U-Boot ("the Universal Boot Loader" or U-Boot) is an open-source bootloader that can be used on ST boards to initialize the platform and load the Linux® kernel.
- Official website: https://www.denx.de/wiki/U-Boot
- Official manual: project documentation and https://www.denx.de/wiki/DULG/Manual
- Official source code is available under git repository at [1]
PC $> git clone https://gitlab.denx.de/u-boot/u-boot.git
Read the README file before starting using U-Boot. It covers the following topics:
- source file tree structure
- description of CONFIG defines
- instructions for building U-Boot
- brief description of the Hush shell
- list of common environment variables
2 U-Boot overview[edit]
The same U-Boot source can generate two pieces of firmware used in SPL and U-Boot STM32 MPU boot chain:
- Trusted boot chain: TF-A as FSBL and U-Boot as SSBL
- Basic boot chain: SPL as FSBL and U-Boot as SSBL
![]() |
The basic boot chain cannot be used for product development (see Boot chains overview for details). |
It is provided only as an example of the simplest SSBL and to support upstream U-Boot development. However, several known limitations have been identified when SPL is used in conjunction with the minimal secure monitor provided within U-Boot for basic boot chain. They apply to:
- power
- secure access to registers
- limited features (STM32CubeProgrammer / boot from NAND Flash memory).
No fix is planned for these limitations.
2.1 SPL: FSBL for basic boot[edit]
The U-Boot SPL or SPL is the first stage bootloader (FSBL) for the basic boot chain.
It is a small binary (bootstrap utility) generated from the U-Boot source and stored in the internal limited-size embedded RAM. SPL main features are the following:
- It is loaded by the ROM code.
- It performs the initial CPU and board configuration (clocks and DDR memory).
- It loads the SSBL (U-Boot) into the DDR memory.
2.2 U-Boot: SSBL[edit]
U-Boot is the default second-stage bootloader (SSBL) for STM32 MPU platforms. It is used both for trusted and basic boot chains. SSBL main features are the following:
- It is configurable and expendable.
- It features a simple command line interface (CLI), allowing users to interact over a serial port console.
- It provides scripting capabilities
- It loads the kernel into RAM and gives control to the kernel
- It manages several internal and external devices such as NAND and NOR Flash memories, Ethernet and USB.
- It supports the following features and commands:
- File systems: FAT, UBI/UBIFS, JFFS
- IP stack: FTP
- Display: LCD, HDMI, BMP for splashcreen
- USB: host (mass storage) or device (DFU stack)
2.3 SPL phases[edit]
SPL executes the following main phases in SYSRAM:
- board_init_f(): driver initialization including DDR initialization (mininimal stack and heap: CONFIG_SPL_STACK_R_MALLOC_SIMPLE_LEN)
- configuration of heap in DDR memory (CONFIG_SPL_SYS_MALLOC_F_LEN)
- board_init_r(): initialization of the other drivers activated in the SPL device tree
- loading and execution of U-Boot (or Kernel in Falcon mode[1]: README.falcon ).
2.4 U-Boot phases[edit]
U-Boot executes the following main phases in DDR memory:
- Pre-relocation initialization (common/board_f.c): minimal initialization (such as CPU, clock, reset, DDR and console) running at the CONFIG_SYS_TEXT_BASE load address.
- Relocation: copy of the code to the end of DDR memory.
- Post-relocation initialization:(common/board_r.c): initialization of all the drivers.
-
Command execution through autoboot (CONFIG_AUTOBOOT) or console shell
- Execution of the boot command (by default bootcmd=CONFIG_BOOTCOMMAND):
for example, execution of the command 'bootm' to:- load and check images (such as kernel, device tree and ramdisk)
- fixup the kernel device tree
- install the secure monitor (optional) or
- pass the control to the Linux kernel (or to another target application)
- Execution of the boot command (by default bootcmd=CONFIG_BOOTCOMMAND):
3 U-Boot configuration[edit]
The U-Boot binary configuration is based on
-
Kbuild infrastructure (as in Linux Kernel, you can use "make menuconfig" in U-Boot)
The configurations are based on:- options defined in Kconfig files (CONFIG_ compilation flags)
- the selected configuration file: configs/stm32mp*_defconfig
-
other compilation flags defined in include/configs/stm32mp*.h (these flags are progressively migrated to Kconfig)
The file name is configured through CONFIG_SYS_CONFIG_NAME.
For stm32mp157, the include/configs/stm32mp1.h file is used.
- DeviceTree: U-Boot and SPL binaries include a device tree blob that is parsed at runtime
All the configuration flags (prefixed by CONFIG_) are described in the source code, either in the README file or in the documentation directory .
For example, CONFIG_SPL activates the SPL compilation.
Hence to compile U-Boot, select the <target> and the device tree for the board in order to choose a predefined configuration.
Refer to #U-Boot_build for examples.
3.1 Kbuild[edit]
Like the kernel, the U-Boot build system is based on configuration symbols (defined in Kconfig files). The selected values are stored in a .config file in the build directory, with the same makefile target. .
Proceed as follows:
- Select a pre-defined configuration (defconfig file in configs directory ) and generate the first .config:
PC $> make <config>_defconfig.
- Change the U-Boot compile configuration (modify .config) by using one of the following five make commands:
PC $> make menuconfig --> menu based program PC $> make config --> line-oriented configuration PC $> make xconfig --> QT program[2] PC $> make gconfig --> GTK program PC $> make nconfig --> ncurse menu based program
You can then compile U-Boot with the updated .config.
Warning: the modification is performed locally in the build directory. It will be lost after a "make distclean".
Save your configuration to be able to use it as a defconfig file:
PC $> make savedefconfig
This target saves the current config as a defconfig file in the build directory. It can then be compared with the predefined configuration (configs/stm32mp*defconfig).
The other makefile targets are the following:
PC $> make help .... Configuration targets: config - Update current config utilising a line-oriented program nconfig - Update current config utilising a ncurses menu based program menuconfig - Update current config utilising a menu based program xconfig - Update current config utilising a Qt based front-end gconfig - Update current config utilising a GTK+ based front-end oldconfig - Update current config utilising a provided .config as base localmodconfig - Update current config disabling modules not loaded localyesconfig - Update current config converting local mods to core defconfig - New config with default from ARCH supplied defconfig savedefconfig - Save current config as ./defconfig (minimal config) allnoconfig - New config where all options are answered with no allyesconfig - New config where all options are accepted with yes allmodconfig - New config selecting modules when possible alldefconfig - New config with all symbols set to default randconfig - New config with random answer to all options listnewconfig - List new options olddefconfig - Same as oldconfig but sets new symbols to their default value without prompting
3.2 Device tree[edit]
Refer to doc/README.fdt-control for details.
The board device tree has the same binding as the kernel. It is integrated within the SPL and U-Boot binaries:
- By default, it is appended at the end of the code (CONFIG_OF_SEPARATE).
- It is embedded in the U-Boot binary (CONFIG_OF_EMBED). This is useful for debugging since it enables easy .elf file loading.
A default device tree is available in the defconfig file (by setting CONFIG_DEFAULT_DEVICE_TREE).
You can either select another supported device tree using the DEVICE_TREE make flag. For stm32mp32 boards, the corresponding file is: arch/arm/dts/stm32mp*.dts .
PC $> make DEVICE_TREE=<dts-file-name>
or provide a precompiled device tree blob (using EXT_DTB option):
PC $> make EXT_DTB=boot/<dts-file-name>.dtb
The SPL device tree is also generated from this device tree. However to reduce its size, the U-Boot makefile uses the fdtgrep tool to parse the full U-Boot DTB and identify all the drivers required by SPL.
To do this, U-Boot uses specific device-tree flags to define if the associated driver is initialized prior to U-Boot relocation and/or if the associated node is present in SPL :
- u-boot,dm-pre-reloc => present in SPL, initialized before relocation in U-Boot
- u-boot,dm-pre-proper => initialized before relocation in U-Boot
- u-boot,dm-spl => present in SPL
In the device tree used by U-Boot, these flags need to be added in each node used in SPL or in U-Boot before relocation and for each used handle (clock, reset, pincontrol).
4 U-Boot command line interface (CLI)[edit]
Refer to U-Boot Command Line Interface.
If CONFIG_AUTOBOOT is activated, you have CONFIG_BOOTDELAY seconds (2s by default) to enter the console by pressing any key, after the line below is displayed and bootcmd is executed (CONFIG_BOOTCOMMAND):
Hit any key to stop autoboot: 2
4.1 Commands[edit]
The commands are defined in cmd/*.c . They are activated through the corresponding CONFIG_CMD_* configuration flag.
Use the help command in the U-Boot shell to list the commands available on your device:
Board $> help
Below the list of all commands extracted from U-Boot Manual (not-exhaustive):
-
Information Commands
- bdinfo - prints Board Info structure
- coninfo - prints console devices and information
- flinfo - prints Flash memory information
- iminfo - prints header information for application image
- help - prints online help
-
Memory Commands
- base - prints or sets the address offset
- crc32 - checksum calculation
- cmp - memory compare
- cp - memory copy
- md - memory display
- mm - memory modify (auto-incrementing)
- mtest - simple RAM test
- mw - memory write (fill)
- nm - memory modify (constant address)
- loop - infinite loop on address range
-
Flash Memory Commands
- cp - memory copy
- flinfo - prints Flash memory information
- erase - erases Flash memory
- protect - enables or disables Flash memory write protection
- mtdparts - defines a Linux compatible MTD partition scheme
-
Execution Control Commands
- source - runs a script from memory
- bootm - boots application image from memory
- go - starts application at address 'addr'
-
Download Commands
- bootp - boots image via network using BOOTP/TFTP protocol
- dhcp - invokes DHCP client to obtain IP/boot params
- loadb - loads binary file over serial line (kermit mode)
- loads - loads S-Record file over serial line
- rarpboot- boots image via network using RARP/TFTP protocol
- tftpboot- boots image via network using TFTP protocol
-
Environment Variables Commands
- printenv- prints environment variables
- saveenv - saves environment variables to persistent storage
- setenv - sets environment variables
- run - runs commands in an environment variable
- bootd - boots default, i.e., run 'bootcmd'
-
Flattened Device Tree support
- fdt addr - selects the FDT to work on
- fdt list - prints one level
- fdt print - recursive printing
- fdt mknode - creates new nodes
- fdt set - sets node properties
- fdt rm - removes nodes or properties
- fdt move - moves FDT blob to new address
- fdt chosen - fixup dynamic information
-
Special Commands
- i2c - I2C sub-system
- Storage devices
-
Miscellaneous Commands
- echo - echoes args to console
- reset - Performs a CPU reset
- sleep - delays the execution for a predefined time
- version - prints the monitor version
To add a new command, refer to doc/README.commands .
4.2 U-Boot environment variables[edit]
The U-Boot behavior is configured through environment variables.
Refer to Manual and README / Environment Variables.
On the first boot, U-Boot uses a default environment embedded in the U-Boot binary. You can modify it by changing the content of CONFIG_EXTRA_ENV_SETTINGS in your configuration file (for example ./include/configs/stm32mp1.h) (see README / - Default Environment).
This environment can be modified and saved in the boot device. When it is present, it is loaded during U-Boot initialization:
- for eMMC/SDCARD boot (CONFIG_ENV_IS_IN_EXT4), in the bootable ext4 partition "bootfs" in
in file CONFIG_ENV_EXT4_FILE="uboot.env". - for NAND boot (CONFIG_ENV_IS_IN_UBI), in the two UBI volumes "config" (CONFIG_ENV_UBI_VOLUME) and "config_r" (CONFIG_ENV_UBI_VOLUME_REDUND).
- for NOR boot (CONFIG_ENV_IS_IN_SPI_FLASH), in the u-boot_env mtd parttion (at offset CONFIG_ENV_OFFSET).
4.2.1 env command[edit]
The "env" command allows displaying, modifying and saving the environment in U-Boot console.
Board $> help env env - environment handling commands Usage: env default [-f] -a - [forcibly] reset default environment env default [-f] var [...] - [forcibly] reset variable(s) to their default values env delete [-f] var [...] - [forcibly] delete variable(s) env edit name - edit environment variable env exists name - tests for existence of variable env print [-a | name ...] - print environment env print -e [name ...] - print UEFI environment env run var [...] - run commands in an environment variable env save - save environment env set -e name [arg ...] - set UEFI variable; unset if 'arg' not specified env set [-f] name [arg ...]
Example: proceed as follows to restore the default environment and save it. This is useful after a U-Boot upgrade:
Board $> env default -a Board $> env save
4.2.2 bootcmd[edit]
"bootcmd" is the autoboot command. It defines the command executed when U-Boot starts (CONFIG_BOOTCOMMAND).
For stm32mp, CONFIG_BOOTCOMMAND="run bootcmd_stm32mp":
Board $> env print bootcmd bootcmd=run bootcmd_stm32mp
"bootcmd_stm32mp" is a script that selects the command to be executed for each boot device (see ./include/configs/stm32mp1.h), based on generic distro scripts:
- for serial/usb: execute the stm32prog command.
- for mmc boot (eMMC, SD card), boot only on the same device (bootcmd_mmc...).
- for nand boot, boot with on ubifs partition on nand (bootcmd_ubi0).
- for nor boot, use the default order eMMC (SDMMC 1)/ NAND / SDCARD (SDMMC 0) / SDMMC2 (the default bootcmd: distro_bootcmd).
Board $> env print bootcmd_stm32mp
You can then change this configuration:
- either permanently in your board file (default environment by CONFIG_EXTRA_ENV_SETTINGS or change CONFIG_BOOTCOMMAND value) or
- temporarily in the saved environment:
Board $> env set bootcmd run bootcmd_mmc0 Board $> env save
Note: To reset the environment to its default value:
Board $> env default bootcmd Board $> env save
4.3 Generic Distro configuration[edit]
Refer to doc/README.distro for details.
This feature is activated by default on ST boards (CONFIG_DISTRO_DEFAULTS):
- one boot command (bootmcd_xxx) exists for each bootable device.
- U-Boot is independent of the Linux distribution used.
- bootcmd is defined in ./include/config_distro_bootcmd.h
When DISTRO is enabled, the command that is executed by default is include/config_distro_bootcmd.h :
bootcmd=run distro_bootcmd
This script tries any device found in the 'boot_targets' variable and executes the associated bootcmd.
Example for mmc0, mmc1, mmc2, pxe and ubifs devices:
bootcmd_mmc0=setenv devnum 0; run mmc_boot bootcmd_mmc1=setenv devnum 1; run mmc_boot bootcmd_mmc2=setenv devnum 2; run mmc_boot bootcmd_pxe=run boot_net_usb_start; dhcp; if pxe get; then pxe boot; fi bootcmd_ubifs0=setenv devnum 0; run ubifs_boot
U-Boot searches for a extlinux.conf configuration file for each bootable device. This file defines the kernel configuration to be used:
- bootargs
- kernel + device tree + ramdisk files (optional)
- FIT image
4.4 U-Boot scripting capabilities[edit]
"Script files" are command sequences that are executed by the U-Boot command interpreter. This feature is particularly useful to configure U-Boot to use a real shell (hush) as command interpreter.
See U-Boot script manual for an example.
5 U-Boot build[edit]
5.1 Prerequisites[edit]
- a PC with Linux and tools:
- U-Boot source code
PC $> git clone https://github.com/STMicroelectronics/u-boot
-
- from the Mainline U-Boot in official GIT repository [4]
PC $> git clone https://gitlab.denx.de/u-boot/u-boot.git
5.1.1 ARM cross compiler[edit]
A cross compiler [5] must be installed on your Host (X86_64, i686, ...) for the ARM targeted Device architecture. In addition, the $PATH and $CROSS_COMPILE environment variables must be configured in your shell.
You can use gcc for ARM, available in:
- the SDK toolchain (see Cross-compile with OpenSTLinux SDK)
PATH and CROSS_COMPILE are automatically updated. - an existing package
For example, install gcc-arm-linux-gnueabihf on Ubuntu/Debian: (PC $> sudo apt-get. - an existing toolchain:
- gcc v8 toolchain provided by arm (https://developer.arm.com/open-source/gnu-toolchain/gnu-a/downloads/)
- gcc v7 toolchain provided by linaro: (https://www.linaro.org/downloads/)
For example, to use gcc-linaro-7.2.1-2017.11-x86_64_arm-linux-gnueabi.tar.xz
from https://releases.linaro.org/components/toolchain/binaries/7.2-2017.11/arm-linux-gnueabi/
Unzip the toolchain in $HOME and update your environment with:
PC $> export PATH=$HOME/gcc-linaro-7.2.1-2017.11-x86_64_arm-linux-gnueabi/bin:$PATH PC $> export CROSS_COMPILE=arm-linux-gnueabi-
5.2 Compilation[edit]
In the U-Boot source directory, select the <target> and the <device tree> for your configuration and then execute the "make all" command:
PC $> make <target>_defconfig PC $> make DEVICE_TREE=<device-tree> all
Optionally KBUILD_OUTPUT can be used to change the output directory to compile several targets or not to compile in the source directory. For example:
PC $> export KBUILD_OUTPUT=../build/basic
DEVICE_TREE can also be exported to your environment when only one board is supported. For example:
PC $> export DEVICE_TREE=stm32mp157c-ev1
Three configurations are supported for all stm32mp15 devices, :
- stm32mp15_trusted_defconfig: trusted boot chain, U-Boot (without SPL) is unsecure and uses Secure monitor from TF-A
- stm32mp15_optee_defconfig: trusted boot chain, U-Boot (without SPL) is unsecure and uses Secure monitor from SecureOS = OP-TEE
- stm32mp15_basic_defconfig: basic boot chain, with an SPL as FSBL, U-BOOT is secure and installs monitor with PSCI
The board diversity is only managed with the device tree.
Examples from STM32MP15 U-Boot:
PC $> export KBUILD_OUTPUT=../build/trusted PC $> make stm32mp15_trusted_defconfig PC $> make DEVICE_TREE=stm32mp157c-<board> all
PC $> export KBUILD_OUTPUT=../build/optee PC $> export DEVICE_TREE=stm32mp157c-<board> PC $> make stm32mp15_optee_defconfig PC $> make all
PC $> make stm32mp15_basic_defconfig PC $> make DEVICE_TREE=stm32mp157c-<board> all
Use help to list other targets:
PC $> make help
5.3 Output files[edit]
The resulting U-Boot files are located in your build directory (U-Boot or KBUILD_OUTPUT).
Two binary formats are used for stm32mp devices:
- STM32 image format (*.stm32), managed by mkimage U-Boot tools and Signing_tool . It is requested by ROM code and TF-A (see STM32 header for details).
- uImage (*.img) format, file including a U-Boot header, managed by SPL and U-Boot (for kernel load)
The U-Boot generated files are the following
- For Trusted boot chain (TF-A is used as FSBL, with or without OP-TEE)
- u-boot.stm32 : U-Boot binary with STM32 image header, loaded by TF-A
- For Basic boot chain (SPL is used as FSBL)
- u-boot-spl.stm32 : SPL binary with STM32 image header, loaded by ROM code
- u-boot.img : U-Boot binary with uImage header, loaded by SPL
The files used to debug with gdb are
- u-boot : elf file for U-Boot
- spl/u-boot-spl : elf file for SPL
6 References[edit]
- ↑ https://www.denx.de/wiki/pub/U-Boot/MiniSummitELCE2013/2013-ELCE-U-Boot-Falcon-Boot.pdf
- ↑ https://en.wikipedia.org/wiki/Xconfig
- ↑ https://github.com/STMicroelectronics/u-boot
- ↑ https://gitlab.denx.de/u-boot/u-boot.git or https://github.com/u-boot/u-boot
- ↑ https://en.wikipedia.org/wiki/Cross_compiler
== Das U-Boot == [https://en.wikipedia.org/wiki/Das_U-Boot Das U-Boot] ("the Universal Boot Loader" or U-Boot) is an open-source bootloader that can be used on ST boards to initialize the platform and load the Linux<sup>®</sup> kernel. * Official website: [https://www.denx.de/wiki/U-Boot https://www.denx.de/wiki/U-Boot] * Official manual: [http://www.denx.de/wiki/U-Boot/Documentation|U-Boot project documentation] and [https://www.denx.de/wiki/DULG/Manual https://www.denx.de/wiki/DULG/Manual] * Official [https://www.denx.de/wiki/U-Boot/SourceCode '''source code'''] is available under [https://git-scm.com/ git] repository at [https://gitlab.denx.de/u-boot/u-boot] {{PC$}} git clone https://gitlab.denx.de/u-boot/u-boot.git Read the {{CodeSource | U-Boot | README | README file}} before starting using U-Boot. It covers the following topics: * source file tree structure * description of CONFIG defines * instructions for building U-Boot * brief description of the Hush shell * list of common environment variables == U-Boot overview == [[File: STM32MPU Embedded Software architecture overview.png|link=STM32MPU Embedded Software architecture overview|thumb|Zoom out to STM32MPU Embedded Software]] The same U-Boot source can generate two pieces of firmware used in SPL and U-Boot [[Boot_chains_overview#STM32MP boot chains|STM32 MPU boot chain]]: * Trusted boot chain: TF-A as FSBL and U-Boot as SSBL * Basic boot chain: SPL as FSBL and U-Boot as SSBL <br clear=all> {{Warning | The basic boot chain cannot be used for product development (see [[Boot_chains_overview#Boot_chains_features_set|Boot chains overview]] for details).}} It is provided only as an example of the simplest SSBL and to support upstream U-Boot development. However, several known limitations have been identified when SPL is used in conjunction with the minimal secure monitor provided within U-Boot for basic boot chain. They apply to: * power * secure access to registers * limited features (STM32CubeProgrammer / boot from NAND Flash memory). No fix is planned for these limitations. === SPL: FSBL for basic boot=== The '''U-Boot SPL''' or '''SPL''' is the first stage bootloader (FSBL) for [[Boot_chains_overview#STM32MP boot chains|the basic boot chain]].<br/>It is a small binary (bootstrap utility) generated from the U-Boot source and stored in the internal limited-size embedded RAM. SPL main features are the following: * It is loaded by the ROM code. * It performs the initial CPU and board configuration (clocks and DDR memory). * It loads the SSBL (U-Boot) into the DDR memory. === U-Boot: SSBL === '''U-Boot''' is the default second-stage bootloader (SSBL) for STM32 MPU platforms. It is used both for [[Boot_chains_overview#STM32MP boot chains|trusted and basic]] boot chains. SSBL main features are the following: * It is configurable and expendable. * It features a simple command line interface (CLI), allowing users to interact over a serial port console. * It provides scripting capabilities * It loads the kernel into RAM and gives control to the kernel * It manages several internal and external devices such as NAND and NOR Flash memories, Ethernet and USB. * It supports the following features and commands: ** File systems: FAT, UBI/UBIFS, JFFS ** IP stack: FTP ** Display: LCD, HDMI, BMP for splashcreen ** USB: host (mass storage) or device (DFU stack) === SPL phases === '''SPL''' executes the following main phases in SYSRAM: * '''board_init_f()''': driver initialization including DDR initialization (mininimal stack and heap: CONFIG_SPL_STACK_R_MALLOC_SIMPLE_LEN) * configuration of heap in DDR memory (CONFIG_SPL_SYS_MALLOC_F_LEN) * '''board_init_r()''': initialization of the other drivers activated in the SPL device tree * loading and execution of U-Boot (or Kernel in Falcon mode<ref>https://www.denx.de/wiki/pub/U-Boot/MiniSummitELCE2013/2013-ELCE-U-Boot-Falcon-Boot.pdf</ref>: {{CodeSource | U-Boot | doc/README.falcon | README.falcon }}). === U-Boot phases === '''U-Boot''' executes the following main phases in DDR memory: * '''Pre-relocation''' initialization (common/board_f.c): minimal initialization (such as CPU, clock, reset, DDR and console) running at the CONFIG_SYS_TEXT_BASE load address. * '''Relocation''': copy of the code to the end of DDR memory. * '''Post-relocation initialization''':(common/board_r.c): initialization of all the drivers. * '''Command execution''' through autoboot (CONFIG_AUTOBOOT) or console shell ** Execution of the boot command (by default [[#bootcmd|bootcmd=CONFIG_BOOTCOMMAND]]): <br/>for example, execution of the command 'bootm' to: *** load and check images (such as kernel, device tree and ramdisk) *** fixup the kernel device tree *** install the secure monitor (optional) or *** pass the control to the Linux kernel (or to another target application) == U-Boot configuration == The U-Boot binary configuration is based on * '''Kbuild infrastructure''' (as in [[Menuconfig_or_how_to_configure_kernel|Linux Kernel]], you can use "make menuconfig" in U-Boot)<br/>The configurations are based on: ** options defined in Kconfig files (CONFIG_ compilation flags) ** the selected configuration file: {{CodeSource | U-Boot | configs/ | configs/stm32mp*_defconfig}}<br/> * '''other compilation flags''' defined in {{CodeSource | U-Boot | include/configs/ | include/configs/stm32mp*.h}} (these flags are progressively migrated to Kconfig)<br/>The file name is configured through CONFIG_SYS_CONFIG_NAME.<br/>For stm32mp157, the {{CodeSource | U-Boot | include/configs/stm32mp1.h | include/configs/stm32mp1.h}} file is used. * '''[[Device_tree|DeviceTree]]''': U-Boot and SPL binaries include a device tree blob that is parsed at runtime All the configuration flags (prefixed by CONFIG_) are described in the source code, either in the {{CodeSource | U-Boot | README | README}} file or in the {{CodeSource | U-Boot | doc/ | documentation directory}}.<br/>For example, CONFIG_SPL activates the SPL compilation.<br /> Hence to compile U-Boot, [[#Kbuild|select the <target>]] and [[#Device_tree|the device tree]] for the board in order to choose a predefined configuration.<br/> Refer to [[#U-Boot_build]] for examples. === Kbuild === Like the kernel, the U-Boot build system is based on [[Menuconfig_or_how_to_configure_kernel|configuration symbols]] (defined in Kconfig files). The selected values are stored in a '''.config''' file in the build directory, with the same makefile target. .<br/> Proceed as follows: * Select a pre-defined configuration (defconfig file in {{CodeSource | U-Boot | configs/ | configs directory }}) and generate the first '''.config''': {{PC$}} make <config>_defconfig. * Change the U-Boot compile configuration (modify .config) by using one of the following five make commands: {{PC$}} '''make menuconfig''' {{Highlight|--> menu based program}} {{PC$}} make config {{Highlight|--> line-oriented configuration}} {{PC$}} make xconfig {{Highlight|--> QT program<ref>https://en.wikipedia.org/wiki/Xconfig</ref>}} {{PC$}} make gconfig {{Highlight|--> GTK program}} {{PC$}} make nconfig {{Highlight|--> ncurse menu based program}} You can then compile U-Boot with the updated .config. Warning: the modification is performed locally in the build directory. It will be lost after a "make distclean". Save your configuration to be able to use it as a defconfig file: {{PC$}} make savedefconfig This target saves the current config as a defconfig file in the build directory. It can then be compared with the predefined configuration (configs/stm32mp*defconfig). The other makefile targets are the following: {{PC$}} make help .... Configuration targets: config - Update current config utilising a line-oriented program nconfig - Update current config utilising a ncurses menu based program menuconfig - Update current config utilising a menu based program xconfig - Update current config utilising a Qt based front-end gconfig - Update current config utilising a GTK+ based front-end oldconfig - Update current config utilising a provided .config as base localmodconfig - Update current config disabling modules not loaded localyesconfig - Update current config converting local mods to core defconfig - New config with default from ARCH supplied defconfig savedefconfig - Save current config as ./defconfig (minimal config) allnoconfig - New config where all options are answered with no allyesconfig - New config where all options are accepted with yes allmodconfig - New config selecting modules when possible alldefconfig - New config with all symbols set to default randconfig - New config with random answer to all options listnewconfig - List new options olddefconfig - Same as oldconfig but sets new symbols to their default value without prompting === Device tree === Refer to {{CodeSource | U-Boot | doc/README.fdt-control | doc/README.fdt-control}} for details. The board device tree has the same binding as the kernel. It is integrated within the SPL and U-Boot binaries: * By default, it is appended at the end of the code (CONFIG_OF_SEPARATE). * It is embedded in the U-Boot binary (CONFIG_OF_EMBED). This is useful for debugging since it enables easy .elf file loading. A default device tree is available in the defconfig file (by setting CONFIG_DEFAULT_DEVICE_TREE). You can either select another supported device tree using the DEVICE_TREE make flag. For stm32mp32 boards, the corresponding file is: {{CodeSource | U-Boot | arch/arm/dts/ | arch/arm/dts/stm32mp*.dts}}. {{PC$}} make DEVICE_TREE=<dts-file-name> or provide a precompiled device tree blob (using EXT_DTB option): {{PC$}} make EXT_DTB=boot/<dts-file-name>.dtb The SPL device tree is also generated from this device tree. However to reduce its size, the U-Boot makefile uses the fdtgrep tool to parse the full U-Boot DTB and identify all the drivers required by SPL. To do this, U-Boot uses specific device-tree flags to define if the associated driver is initialized prior to U-Boot relocation and/or if the associated node is present in SPL : * '''u-boot,dm-pre-reloc''' => present in SPL, initialized before relocation in U-Boot * '''u-boot,dm-pre-proper''' => initialized before relocation in U-Boot * '''u-boot,dm-spl''' => present in SPL In the device tree used by U-Boot, these flags '''need to be added in each node''' used in SPL or in U-Boot before relocation and for each used handle (clock, reset, pincontrol). == U-Boot command line interface (CLI) == Refer to [http://www.denx.de/wiki/view/DULG/UBootCommandLineInterface U-Boot Command Line Interface]. If CONFIG_AUTOBOOT is activated, you have CONFIG_BOOTDELAY seconds (2s by default) to enter the console by pressing any key, after the line below is displayed and [[#bootcmd|bootcmd]] is executed (CONFIG_BOOTCOMMAND): Hit any key to stop autoboot: 2 === Commands === The commands are defined in {{CodeSource | U-Boot | cmd/ | cmd/*.c}}. They are activated through the corresponding '''CONFIG_CMD_*''' configuration flag. Use the '''help''' command in the U-Boot shell to list the commands available on your device: {{Board$}} help Below the list of all commands extracted from [http://www.denx.de/wiki/view/DULG/Manual U-Boot Manual] ('''not-exhaustive'''): * [http://www.denx.de/wiki/view/DULG/UBootCmdGroupInfo Information Commands] ** bdinfo - prints Board Info structure ** coninfo - prints console devices and information ** flinfo - prints Flash memory information ** iminfo - prints header information for application image ** help - prints online help * [http://www.denx.de/wiki/view/DULG/UBootCmdGroupMemory Memory Commands] ** base - prints or sets the address offset ** crc32 - checksum calculation ** cmp - memory compare ** cp - memory copy ** md - memory display ** mm - memory modify (auto-incrementing) ** mtest - simple RAM test ** mw - memory write (fill) ** nm - memory modify (constant address) ** loop - infinite loop on address range * [http://www.denx.de/wiki/view/DULG/UBootCmdGroupFlash Flash Memory Commands] ** cp - memory copy ** flinfo - prints Flash memory information ** erase - erases Flash memory ** protect - enables or disables Flash memory write protection ** mtdparts - defines a Linux compatible MTD partition scheme * [http://www.denx.de/wiki/view/DULG/UBootCmdGroupExec Execution Control Commands] ** source - runs a script from memory ** bootm - boots application image from memory ** go - starts application at address 'addr' * [http://www.denx.de/wiki/view/DULG/UBootCmdGroupDownload Download Commands] ** bootp - boots image via network using BOOTP/TFTP protocol ** dhcp - invokes DHCP client to obtain IP/boot params ** loadb - loads binary file over serial line (kermit mode) ** loads - loads S-Record file over serial line ** rarpboot- boots image via network using RARP/TFTP protocol ** tftpboot- boots image via network using TFTP protocol * [http://www.denx.de/wiki/view/DULG/UBootCmdGroupEnvironment Environment Variables Commands] ** printenv- prints environment variables ** saveenv - saves environment variables to persistent storage ** setenv - sets environment variables ** run - runs commands in an environment variable ** bootd - boots default, i.e., run 'bootcmd' * [http://www.denx.de/wiki/view/DULG/UBootCmdFDT Flattened Device Tree support] ** fdt addr - selects the FDT to work on ** fdt list - prints one level ** fdt print - recursive printing ** fdt mknode - creates new nodes ** fdt set - sets node properties ** fdt rm - removes nodes or properties ** fdt move - moves FDT blob to new address ** fdt chosen - fixup dynamic information * [http://www.denx.de/wiki/view/DULG/UBootCmdGroupSpecial Special Commands] ** i2c - I2C sub-system * [http://www.denx.de/wiki/view/DULG/UBootStorageDevices Storage devices] * [http://www.denx.de/wiki/view/DULG/UBootCmdGroupMisc Miscellaneous Commands] ** echo - echoes args to console ** reset - Performs a CPU reset ** sleep - delays the execution for a predefined time ** version - prints the monitor version To add a new command, refer to {{CodeSource | U-Boot | doc/README.commands }}. === U-Boot environment variables === The U-Boot behavior is configured through environment variables. Refer to [http://www.denx.de/wiki/view/DULG/UBootEnvVariables Manual] and {{CodeSource | U-Boot | README | README}} / Environment Variables. On the first boot, U-Boot uses a default environment embedded in the U-Boot binary. You can modify it by changing the content of CONFIG_EXTRA_ENV_SETTINGS in your configuration file (for example ./include/configs/stm32mp1.h) (see {{CodeSource | U-Boot | README | README}} / - Default Environment). This environment can be modified and saved in the boot device. When it is present, it is loaded during U-Boot initialization: * for eMMC/SDCARD boot (CONFIG_ENV_IS_IN_EXT4), in the bootable ext4 partition "bootfs" in <br/>in file CONFIG_ENV_EXT4_FILE="uboot.env". * for NAND boot (CONFIG_ENV_IS_IN_UBI), in the two UBI volumes "config" (CONFIG_ENV_UBI_VOLUME) and "config_r" (CONFIG_ENV_UBI_VOLUME_REDUND). * for NOR boot (CONFIG_ENV_IS_IN_SPI_FLASH), in the u-boot_env mtd parttion (at offset CONFIG_ENV_OFFSET). ==== env command ==== The "env" command allows displaying, modifying and saving the environment in U-Boot console. {{Board$}} help env env - environment handling commands Usage: env default [-f] -a - [forcibly] reset default environment env default [-f] var [...] - [forcibly] reset variable(s) to their default values env delete [-f] var [...] - [forcibly] delete variable(s) env edit name - edit environment variable env exists name - tests for existence of variable env print [-a | name ...] - print environment env print -e [name ...] - print UEFI environment env run var [...] - run commands in an environment variable env save - save environment env set -e name [arg ...] - set UEFI variable; unset if 'arg' not specified env set [-f] name [arg ...] Example: proceed as follows to restore the default environment and save it. This is useful after a U-Boot upgrade: {{Board$}} env default -a {{Board$}} env save ==== bootcmd ==== "bootcmd" is the autoboot command. It defines the command executed when U-Boot starts (CONFIG_BOOTCOMMAND). For stm32mp, CONFIG_BOOTCOMMAND="run bootcmd_stm32mp": {{Board$}} env print bootcmd bootcmd=run bootcmd_stm32mp "bootcmd_stm32mp" is a script that selects the command to be executed for each boot device (see ./include/configs/stm32mp1.h), based on [[#Generic Distro configuration|generic distro scripts]]: * for serial/usb: execute the stm32prog command. * for mmc boot (eMMC, SD card), boot only on the same device (bootcmd_mmc...). * for nand boot, boot with on ubifs partition on nand (bootcmd_ubi0). * for nor boot, use the default order eMMC (SDMMC 1)/ NAND / SDCARD (SDMMC 0) / SDMMC2 (the default bootcmd: distro_bootcmd). {{Board$}} env print bootcmd_stm32mp You can then change this configuration: * either permanently in your board file (default environment by CONFIG_EXTRA_ENV_SETTINGS or change CONFIG_BOOTCOMMAND value) or * temporarily in the saved environment: {{Board$}} env set bootcmd run bootcmd_mmc0 {{Board$}} env save Note: To reset the environment to its default value: {{Board$}} env default bootcmd {{Board$}} env save === Generic Distro configuration === Refer to {{CodeSource | U-Boot | doc/README.distro | doc/README.distro}} for details. This feature is activated by default on ST boards (CONFIG_DISTRO_DEFAULTS): * one boot command (bootmcd_xxx) exists for each bootable device. * U-Boot is independent of the Linux distribution used. * bootcmd is defined in {{CodeSource | U-Boot | ./include/config_distro_bootcmd.h }} When DISTRO is enabled, the command that is executed by default is {{CodeSource | U-Boot | include/config_distro_bootcmd.h}}: bootcmd=run distro_bootcmd This script tries any device found in the 'boot_targets' variable and executes the associated bootcmd. Example for mmc0, mmc1, mmc2, pxe and ubifs devices: bootcmd_mmc0=setenv devnum 0; run mmc_boot bootcmd_mmc1=setenv devnum 1; run mmc_boot bootcmd_mmc2=setenv devnum 2; run mmc_boot bootcmd_pxe=run boot_net_usb_start; dhcp; if pxe get; then pxe boot; fi bootcmd_ubifs0=setenv devnum 0; run ubifs_boot U-Boot searches for a '''extlinux.conf''' configuration file for each bootable device. This file defines the kernel configuration to be used: * bootargs * kernel + device tree + ramdisk files (optional) * FIT image === U-Boot scripting capabilities === "Script files" are command sequences that are executed by the U-Boot command interpreter. This feature is particularly useful to configure U-Boot to use a real shell (hush) as command interpreter. See [http://www.denx.de/wiki/view/DULG/UBootScripts| U-Boot script manual] for an example. == U-Boot build == === Prerequisites === * a PC with Linux and tools: ** see [[PC_prerequisites]] ** [[#ARM cross compiler]] * U-Boot source code ** the latest STMicroelectronics U-Boot version *** tar.xz file from Developer Package (for example [[STM32MP1_Developer_Package#Installing_the_U-Boot|STM32MP1]]) *** from GITHUB<ref>https://github.com/STMicroelectronics/u-boot</ref>, with git command {{PC$}} git clone https://github.com/STMicroelectronics/u-boot :* from the Mainline U-Boot in official GIT repository <ref>https://gitlab.denx.de/u-boot/u-boot.git or https://github.com/u-boot/u-boot</ref> {{PC$}} git clone https://gitlab.denx.de/u-boot/u-boot.git ==== ARM cross compiler ==== A cross compiler <ref>https://en.wikipedia.org/wiki/Cross_compiler</ref> must be installed on your Host (X86_64, i686, ...) for the ARM targeted Device architecture. In addition, the $PATH and $CROSS_COMPILE environment variables must be configured in your shell. You can use gcc for ARM, available in: * the SDK toolchain (see [[Cross-compile with OpenSTLinux SDK]])<br/>PATH and CROSS_COMPILE are automatically updated. * an existing package<br/>For example, install gcc-arm-linux-gnueabihf on Ubuntu/Debian: ({{PC$}} sudo apt-get. * an existing toolchain: ** gcc v8 toolchain provided by arm (https://developer.arm.com/open-source/gnu-toolchain/gnu-a/downloads/) ** gcc v7 toolchain provided by linaro: (https://www.linaro.org/downloads/) For example, to use '''gcc-linaro-7.2.1-2017.11-x86_64_arm-linux-gnueabi.tar.xz'''<br/>from https://releases.linaro.org/components/toolchain/binaries/7.2-2017.11/arm-linux-gnueabi/<br/> Unzip the toolchain in $HOME and update your environment with: {{PC$}} export PATH=$HOME/gcc-linaro-7.2.1-2017.11-x86_64_arm-linux-gnueabi/bin:$PATH {{PC$}} export CROSS_COMPILE=arm-linux-gnueabi- === Compilation === In the U-Boot source directory, select the <target> and the <device tree> for your configuration and then execute the "make all" command: {{PC$}} make <target>_defconfig {{PC$}} make DEVICE_TREE=<device-tree> all Optionally '''KBUILD_OUTPUT''' can be used to change the output directory to compile several targets or not to compile in the source directory. For example: {{PC$}} export KBUILD_OUTPUT=../build/basic '''DEVICE_TREE''' can also be exported to your environment when only one board is supported. For example: {{PC$}} export DEVICE_TREE=stm32mp157c-ev1 Three configurations are supported for all stm32mp15 devices, : * {{Highlight|stm32mp15_trusted_defconfig}}: [[Boot_chains_overview#STM32MP boot chains|trusted boot chain]], U-Boot (without SPL) is unsecure and uses Secure monitor from TF-A * {{Highlight|stm32mp15_optee_defconfig}}: [[Boot_chains_overview#STM32MP boot chains|trusted boot chain]], U-Boot (without SPL) is unsecure and uses Secure monitor from SecureOS = [[OP-TEE overview|OP-TEE]] * stm32mp15_basic_defconfig: [[Boot_chains_overview#STM32MP boot chains|basic boot chain]], with an SPL as FSBL, U-BOOT is secure and installs monitor with PSCI The board diversity is only managed with the device tree. Examples from [[STM32MP15 U-Boot]]: {{PC$}} export KBUILD_OUTPUT=../build/trusted {{PC$}} make stm32mp15_trusted_defconfig {{PC$}} make DEVICE_TREE=stm32mp157c-<board> all {{PC$}} export KBUILD_OUTPUT=../build/optee {{PC$}} export DEVICE_TREE=stm32mp157c-<board> {{PC$}} make stm32mp15_optee_defconfig {{PC$}} make all {{PC$}} make stm32mp15_basic_defconfig {{PC$}} make DEVICE_TREE=stm32mp157c-<board> all Use help to list other targets: {{PC$}} make help === Output files === The resulting U-Boot files are located in your build directory (U-Boot or KBUILD_OUTPUT). Two binary formats are used for stm32mp devices: * STM32 image format (*.stm32), managed by mkimage U-Boot tools and [[Signing_tool ]]. It is requested by ROM code and TF-A (see [[STM32MP15_secure_boot#STM32_Header | STM32 header]] for details). * uImage (*.img) format, file including a U-Boot header, managed by SPL and U-Boot (for kernel load) The U-Boot generated files are the following * For {{Highlight|'''Trusted boot chain'''}} (TF-A is used as FSBL, with or without OP-TEE) ** {{Highlight|'''u-boot.stm32'''}} : U-Boot binary with STM32 image header, loaded by TF-A * For '''Basic boot chain''' (SPL is used as FSBL) ** '''u-boot-spl.stm32''' : SPL binary with STM32 image header, loaded by ROM code ** '''u-boot.img''' : U-Boot binary with uImage header, loaded by SPL The files used to debug with gdb are * u-boot : elf file for U-Boot * spl/u-boot-spl : elf file for SPL == References ==<references/> <noinclude> [[Category:U-Boot]] {{PublicationRequestId | 12893 | 2019-08-01}}</noinclude>
Line 391: | Line 391: | ||
Two binary formats are used for stm32mp devices: |
Two binary formats are used for stm32mp devices: |
||
− | * STM32 image format (*.stm32), managed by mkimage U-Boot tools and [[Signing_tool ]]. It is requested by ROM code and TF-A (see [[STM32MP15_secure_boot#STM32_Header | STM32 header]] for details). |
+ | * STM32 image format (*.stm32), managed by mkimage U-Boot tools and [[Signing_tool]]. It is requested by ROM code and TF-A (see [[STM32MP15_secure_boot#STM32_Header | STM32 header]] for details). |
* uImage (*.img) format, file including a U-Boot header, managed by SPL and U-Boot (for kernel load) |
* uImage (*.img) format, file including a U-Boot header, managed by SPL and U-Boot (for kernel load) |
||