Registered User mNo edit summary |
Registered User mNo edit summary Tag: 2017 source edit |
||
(One intermediate revision by the same user not shown) | |||
Line 1: | Line 1: | ||
<noinclude>{{ApplicableFor | <noinclude>{{ApplicableFor | ||
|MPUs list=STM32MP13x, STM32MP15x | |MPUs list=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x | ||
|MPUs checklist=STM32MP13x, STM32MP15x | |MPUs checklist=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x | ||
}}</noinclude> | }}</noinclude> | ||
Das U-Boot ("the Universal Boot Loader" or U-Boot) is an open-source bootloader that can be used on STMicroelectronics boards to initialize the | Das U-Boot ("the Universal Boot Loader" or U-Boot) is an open-source bootloader that can be used on STMicroelectronics boards to initialize the | ||
Line 20: | Line 20: | ||
|- | |- | ||
| {{MicroprocessorDevice | device=15}}|| [[STM32MP15 U-Boot]] | | {{MicroprocessorDevice | device=15}}|| [[STM32MP15 U-Boot]] | ||
|- | |||
| {{MicroprocessorDevice | device=21}}|| [[STM32MP21 U-Boot]] | |||
|- | |||
| {{MicroprocessorDevice | device=23}}|| [[STM32MP23 U-Boot]] | |||
|- | |||
| {{MicroprocessorDevice | device=25}}|| [[STM32MP25 U-Boot]] | |||
|} | |} | ||
Latest revision as of 14:31, 10 October 2024
Das U-Boot ("the Universal Boot Loader" or U-Boot) is an open-source bootloader that can be used on STMicroelectronics boards to initialize the platform and load the Linux® kernel.
See U-Boot overview for generic information.
Information about U-Boot depends on the microprocessor device.
Several articles have been created to manage STM32 MPU diversity and provide the relevant level of information. Browse the one corresponding to the STM32 MPU you use.
STM32 MPU devices | Associated articles |
---|---|
STM32MP13x lines ![]() |
STM32MP13 U-Boot |
STM32MP15x lines ![]() |
STM32MP15 U-Boot |
STM32MP21 unknown microprocessor device | STM32MP21 U-Boot |
STM32MP23 unknown microprocessor device | STM32MP23 U-Boot |
STM32MP25 unknown microprocessor device | STM32MP25 U-Boot |