Registered User m (Finish review, ref in ref not possible) |
Registered User mNo edit summary Tag: 2017 source edit |
||
(53 intermediate revisions by 11 users not shown) | |||
Line 1: | Line 1: | ||
{{ApplicableFor | |||
|MPUs list=STM32MP13x, STM32MP15x, STM32MP23x, STM32MP25x | |||
|MPUs checklist=STM32MP13x, STM32MP15x, STM32MP23x, STM32MP25x | |||
}} | |||
<noinclude></noinclude> | |||
<noinclude> | <noinclude> | ||
The STM32 header is a STMicroelectronics header needed for binaries loaded by [[:Category:ROM_code|ROM code | The STM32 header is a STMicroelectronics header needed for binaries loaded by [[:Category:ROM_code|ROM code]]. | ||
== Description == | == Description == | ||
</noinclude> | </noinclude> | ||
Each binary image loaded by the [[:Category:ROM_code|ROM code]] needs to include a specific STM32 header added on top of the binary data. This header includes mandatory and optional information: this second one is only needed for the authentication ({{MicroprocessorDevice | device=1}}) and decryption ({{MicroprocessorDevice | device=13}} and {{MicroprocessorDevice | device=2}}) processes. | |||
== On {{MicroprocessorDevice | device=13}} == | |||
=== Base header === | |||
[[File:STM32MP13_header_base.png | right | |400px]] | |||
{| | |||
! Name !! Length !! Byte Offset <ref group="Note">Unless expressed differently, the 32 bits values are stored in little endian.</ref> !! Description | |||
|- | |||
| Magic number || 32 bits || 0 || 4 bytes in big endian:<br> 'S', 'T', 'M', 0x32 = 0x53544D32 | |||
|- | |||
| Image signature || 512 bits || 4 || ECDSA signature for image authentication<ref group="Note">Signature is calculated from first byte of header version field to last byte of image given by image length field.</ref> | |||
|- | |||
| Image checksum || 32 bits || 68 || Checksum of the payload<ref group="Note">32-bit sum of all payload bytes accessed as 8-bit unsigned numbers, discarding any overflow bits. Used to check the downloaded image integrity when signature is not used (if b0=0 in Option flags).</ref> | |||
|- | |||
| Header version || 32 bits || 72 || Header version '''v2.0''' = 0x00020000<br> Byte0: reserved<br> Byte1: major version = 0x02 <br> Byte2: minor version = 0x00 <br> Byte3: reserved | |||
|- | |||
| Image length || 32 bits || 76 || Length of image in bytes<ref group="Note">Length is the length of the built image, it does not include the length of the STM32 header.</ref> | |||
|- | |||
| Image entry Point || 32 bits || 80 || Entry point of image | |||
|- | |||
| Reserved || 96 bits || 84 || Reserved | |||
|- | |||
| Version number || 32 bits || 96 || Image Version (monotonic number)<ref group="Note">Image '''version number''' is an anti rollback monotonic counter. The ROM code checks that it is higher or equal to the monotonic counter stored in OTP.</ref> | |||
|- | |||
| Option flags || 32 bits || 100 || b0=1: Authentication enabled<ref group="Note">Enabling signature verification is mandatory on [[Device life cycle|secured locked device]]. Authentication parameters are stored in "Authentication header extension".</ref><br>b1=1: Decryption enabled.<ref group="Note">When decryption is enabled, authentication is mandatory. Decryption parameters are stored in "Decryption header extension".</ref><br>b31=1: Header padding enabled<ref group="Note">This header padding extension is always used to have a fixed size of 512 bytes for the whole size of header + its extensions.</ref> | |||
|- | |||
| Header extensions length|| 32 bits || 104 || Sizes of header extensions enabled by option flags. | |||
|- | |||
| Padding || 20 Bytes || 108 || Reserved padding bytes<ref group="Note">This padding forces STM32 base header size to '''128 bytes''' (0x80).</ref>. <br>Must all be set to 0 | |||
|} | |||
<references group="Note"/> | |||
=== Authentication header extension === | |||
This header extension contains parameters needed for authentication. | |||
[[File:STM32MP13_header_authentication.png | right | |400px]] | |||
{| | |||
! Name !! Length !! Byte Offset<ref group="Note">Offset is relative to header extension base. Unless expressed differently, the 32 bits values are stored in little endian.</ref> !! Description | |||
|- | |||
| Extension type|| 32 bits || 0 || 4 bytes in big endian:<br> 'S', 'T', 0x00, 0x02 = 0x53540002 | |||
|- | |||
| Extension length|| 32 bits || 4 || Number of bytes of header extension = 340 | |||
|- | |||
| Public key index|| 32 bits || 8 || Index of the public key to be used. | |||
|- | |||
| Public key number|| 32 bits || 12 || Number of public keys in table = 8 | |||
|- | |||
| ECDSA algorithm || 32 bits || 16 || 1: P-256 NIST ; 2: brainpool 256 | |||
|- | |||
| ECDSA public key || 512 bits || 20 || ECDSA public key to be used to verify the signature.<ref group="Note"> Public key is a point on the ECC curve. This field contains the two big numbers in big endian format corresponding to ECC Point coordinates ''x'' and ''y''. (If these coordinates are extracted from a PEM public key file that only kept coordinates in a raw binary format, you shall remove the first byte "04" which is an asn1 tag ; for more info: [http://www.rfc-editor.org/info/rfc5480 RFC 5480]). </ref> | |||
|- | |||
| Public key1 hash || 256 bits || 84 || Hash of (ECDSA Algorithm+Public key1).<ref group="Note"> The Public Key hash computation is the SHA-256 of ECDSA Algorithm expressed in little endian, concatenated to the public key itself. The entry of the public key table referenced by the public key index is compared to the hash of the ECDSA algorithm and public key that are stored in the header.'''</ref>. | |||
|- | |||
| ...||...||...|| Hashes of (ECDSA Algorithm+Public key), for key2 up to key7 | |||
|- | |||
| Public key8 hash<ref group="Note">The table of public key hashes will be hashed with SHA-256 by the ROM code and compared to the '''Hash of Public Keys Hashes Table (PKHTH)''' that is stored in OTP.</ref> || 256 bits || 308 || Hash of (ECDSA Algorithm+Public key8) | |||
|} | |||
<references group="Note"/> | |||
=== Decryption header extension === | |||
[[File:STM32MP13_header_decryption.png | right | |400px]] | |||
This header extension contains parameters needed for decryption. | |||
{| | |||
! Name !! Length !! Byte Offset<ref group="Note">Offset is relative to header extension base. Unless expressed differently, the 32 bits values are stored in little endian.</ref>!! Description | |||
|- | |||
| Extension type|| 32 bits || 0 || 4 bytes in big endian:<br> 'S', 'T', 0x00, 0x01 = 0x53540001 | |||
|- | |||
| Extension length|| 32 bits || 4 || Number of bytes of header extension = 32 | |||
|- | |||
| Key size|| 32 bits || 8 || Size of extension key (128 bits)<ref group="Note">Key size is fixed to 128 bits</ref>. | |||
|- | |||
| Derivation constant|| 32 bits || 12 || Constant used to derive decryption key from master key stored in OTP. | |||
|- | |||
| Plain hash|| 128 bits || 16 || 128 msb bits of plain payload SHA256. | |||
|} | |||
<references group="Note"/> | |||
=== Padding header extension === | |||
[[File:STM32MP13_header_padding.png | right | |400px]] | |||
{| | |||
! Name !! Length !! Byte Offset<ref group="Note">Offset is relative to header extension base. Unless expressed differently, the 32 bits values are stored in little endian.</ref>!! Description | |||
|- | |||
| Extension type|| 32 bits || 0 || 4 bytes in big endian:<br> 'S', 'T', 0xFF, 0xFF = 0x5354FFFF | |||
|- | |||
| Extension length|| 32 bits || 4 || Number of bytes of header extension = N + 8 | |||
|- | |||
| Padding bytes|| N bytes|| 8 || Padding bytes<ref group="Note">N shall be calculated by signing tool so that the size of whole header plus its extension is equal to 512 bytes</ref>. | |||
|} | |||
<references group="Note"/> | |||
== On {{MicroprocessorDevice | device=15}} == | |||
[[File:STM32_header.png | right | |400px]] | [[File:STM32_header.png | right | |400px]] | ||
{| | {| | ||
Line 30: | Line 129: | ||
| Reserved2 || 32 bits || 92 || Reserved | | Reserved2 || 32 bits || 92 || Reserved | ||
|- | |- | ||
| Version number || 32 bits || 96 || Image Version (monotonic number)<ref group="Note">Image '''version number''' is an anti rollback monotonic counter. The ROM code checks that it is higher or equal to the monotonic counter stored in OTP.</ref> | | Version number || 32 bits || 96 || Image Version (monotonic number)<ref group="Note">Image '''version number''' is an anti rollback monotonic counter. The ROM code checks that it is higher or equal to the monotonic counter stored in [[STM32MP15 OTP mapping#version monotonic counter|OTP]].</ref> | ||
|- | |- | ||
| Option flags || 32 bits || 100 || b0=1: no signature verification<ref group="Note">Enabling signature verification is mandatory on | | Option flags || 32 bits || 100 || b0=1: no signature verification<ref group="Note">Enabling signature verification is mandatory on [[Device life cycle|secured locked device]].</ref> | ||
|- | |- | ||
| ECDSA algorithm || 32 bits || 104 || 1: P-256 NIST ; 2: brainpool 256 | | ECDSA algorithm || 32 bits || 104 || 1: P-256 NIST ; 2: brainpool 256 | ||
|- | |- | ||
| ECDSA public key || 512 bits || 108 || ECDSA public key to be used to verify the signature.<ref group="Note"> This field | | ECDSA public key || 512 bits || 108 || ECDSA public key to be used to verify the signature.<ref group="Note"> Public key is a point on the ECC curve. This field contains the two big numbers in big endian format corresponding to ECC Point coordinates ''x'' and ''y''. (If these coordinates are extracted from a PEM public key file that only kept coordinates in a raw binary format, you shall remove the first byte "04" which is an asn1 tag ; for more info: [http://www.rfc-editor.org/info/rfc5480 RFC 5480]). </ref><ref group="Note">The Public Key hash computation is the SHA-256 of the public key itself, then the resulting value is compared to the '''Hash of pubKey''' that is stored in [[STM32MP15 OTP mapping#PKH|OTP]].</ref> | ||
|- | |||
| Padding || 83 Bytes || 172 || Reserved padding bytes<ref group="Note">This padding forces STM32 header size to 256 bytes (0x100).</ref>. Must all be set to 0. | |||
|- | |||
| Binary type || 1 Byte || 255 || Used to check the binary type <br>0x10-0x1F: FSBL <br>0x30: Copro | |||
|} | |||
<references group="Note"/> | |||
== On {{MicroprocessorDevice | device=23}} and {{MicroprocessorDevice | device=25}} == | |||
=== Base header === | |||
[[File:STM32MP25_header_base.png | right | 400px]] | |||
{| | |||
! Name !! Length !! Byte Offset <ref group="Note">Unless expressed differently, the 32 bits values are stored in little endian.</ref> !! Description || Signed | |||
|- | |||
| Magic number || 32 bits || 0 || 4 bytes in big endian:<br> 'S', 'T', 'M', 0x32 = 0x53544D32 || No | |||
|- | |||
| Image signature || 512 bits || 4 || ECDSA signature for image authentication<ref group="Note">Signature is calculated from first byte of header version field to last byte of image given by image length field, excluding the last bytes following the padding field.</ref> || No | |||
|- | |||
| Image checksum || 32 bits || 68 || Checksum of the payload<ref group="Note">32-bit sum of all payload bytes accessed as 8-bit unsigned numbers, discarding any overflow bits. Used to check the downloaded image integrity when signature is not used (if b0=0 in Option flags).</ref> || No | |||
|- | |||
| Header version || 32 bits || 72 || Header version '''v2.2''' = 0x00020200<br> Byte0: reserved<br> Byte1: major version = 0x02 <br> Byte2: minor version = 0x02 <br> Byte3: reserved || Yes | |||
|- | |||
| Image length || 32 bits || 76 || Length of image in bytes<ref group="Note">Length is the length of the built image, it does not include the length of the STM32 header.</ref> || Yes | |||
|- | |||
| Image entry Point || 32 bits || 80 || Entry point of image || Yes | |||
|- | |||
| Reserved || 96 bits || 84 || Reserved || Yes | |||
|- | |||
| Version number || 32 bits || 96 || Image Version (monotonic number)<ref group="Note">Image '''version number''' is an anti rollback monotonic counter. The ROM code checks that it is higher or equal to the monotonic counter stored in OTP.</ref> || Yes | |||
|- | |||
| Option flags || 32 bits || 100 || b0=1: Authentication enabled<ref group="Note">Enabling signature verification is mandatory on [[Device life cycle|secured locked device]]. Authentication parameters are stored in "Authentication header extension".</ref><br>b1=1: Decryption enabled.<ref group="Note">When decryption is enabled, authentication is mandatory. Decryption parameters are stored in "Decryption header extension".</ref><br>b8=1: Aarch32 binary mode support.<ref group="Note">Flag is for ecosystem purpose to detect if the Cortex-A binary is an Aarch32 binary. The ROM code only relies on OTP [[STM32MP23-25_OTP_mapping|a35 mode]] to start directly an Aarch32 FSBL-A.</ref><br>b31=1: Header padding enabled<ref group="Note">This header padding extension is always used to have a fixed size of 512 bytes for the whole size of header + its extensions.</ref> || Yes | |||
|- | |||
| Header extensions length|| 32 bits || 104 || Sizes of header extensions enabled by option flags. || Yes | |||
|- | |||
| Binary type|| 32 bits || 108|| Used to check binary type. Must be set to 0x30 for FSBLM. || Yes | |||
|- | |||
| Padding || 16 Bytes || 112 || Reserved padding bytes<ref group="Note">This padding forces STM32 base header size to '''128 bytes''' (0x80).</ref>. <br>Must all be set to 0 || Yes | |||
|} | |||
<references group="Note"/> | |||
=== Authentication header extension === | |||
Same as the [[#Authentication header extension|authentication header extension on STM32MP13x lines]]. | |||
=== Decryption header extension === | |||
Same as the [[#Decryption header extension|decryption header extension on STM32MP13x lines]] | |||
=== Padding header extension === | |||
Same as the [[#Padding header extension|padding header extension on STM32MP13x lines]]. | |||
== On {{MicroprocessorDevice | device=21}} == | |||
=== Base header === | |||
[[File:STM32MP21 header base.png|right|400x400px]] | |||
{| | |||
! Name !! Length !! Byte Offset <ref group="Note">Unless expressed differently, the 32 bits values are stored in little endian.</ref> !! Description || Signed | |||
|- | |||
| Magic number || 32 bits || 0 || 4 bytes in big endian:<br> 'S', 'T', 'M', 0x32 = 0x53544D32 || No | |||
|- | |||
| Image signature || 768 bits || 4 || ECDSA signature for image authentication<ref group="Note">Signature is calculated from first byte of header version field to last byte of image given by image length field, excluding the last bytes following the padding field.</ref> || No | |||
|- | |||
| Image checksum || 32 bits || 100 || Checksum of the payload<ref group="Note">32-bit sum of all payload bytes accessed as 8-bit unsigned numbers, discarding any overflow bits. Used to check the downloaded image integrity when signature is not used (if b0=0 in Option flags).</ref> || No | |||
|- | |||
| Header version || 32 bits || 104 || Header version '''v2.3''' = 0x00020300<br> Byte0: reserved<br> Byte1: major version = 0x02 <br> Byte2: minor version = 0x03 <br> Byte3: reserved || Yes | |||
|- | |||
| Image length || 32 bits || 108 || Length of image in bytes<ref group="Note">Length is the length of the built image, it does not include the length of the STM32 header.</ref> || Yes | |||
|- | |||
| Image entry Point || 32 bits || 112 || Entry point of image || Yes | |||
|- | |||
| Reserved || 96 bits || 116 || Reserved || Yes | |||
|- | |||
| Version number || 32 bits || 128 || Image Version (monotonic number)<ref group="Note">Image '''version number''' is an anti rollback monotonic counter. The ROM code checks that it is higher or equal to the monotonic counter stored in OTP.</ref> || Yes | |||
|- | |||
| Option flags || 32 bits || 132 || b0=1: Authentication enabled<ref group="Note">Enabling signature verification is mandatory on [[Device life cycle|secured locked device]]. Authentication parameters are stored in "Authentication header extension".</ref><br>b1=1: Decryption enabled.<ref group="Note">When decryption is enabled, authentication is mandatory. Decryption parameters are stored in "Decryption header extension".</ref><br>b8=1: Aarch32 binary mode support.<ref group="Note">Flag is for ecosystem purpose to detect if the Cortex-A binary is an Aarch32 binary. The ROM code only relies on OTP [[STM32MP21_OTP_mapping|a35 mode]] to start directly an Aarch32 FSBL-A.</ref><br>b31=1: Header padding enabled<ref group="Note">This header padding extension is always used to have a fixed size of 512 bytes for the whole size of header + its extensions.</ref> || Yes | |||
|- | |||
| Header extensions length|| 32 bits || 136 || Sizes of header extensions enabled by option flags. || Yes | |||
|- | |||
| Binary type|| 32 bits || 140|| Used to check binary type. Must be set to 0x30 for FSBLM. || Yes | |||
|- | |||
| Padding || 16 Bytes || 144 || Reserved padding bytes<ref group="Note">This padding forces STM32 base header size to '''160 bytes''' (0x80).</ref>. <br>Must all be set to 0 || Yes | |||
|} | |||
<references group="Note"/> | |||
=== Authentication header extension === | |||
This header extension contains parameters needed for authentication. | |||
[[File:STM32MP21 header authentication.png|right|400x400px]] | |||
{| | |||
! Name !! Length !! Byte Offset<ref group="Note">Offset is relative to header extension base. Unless expressed differently, the 32 bits values are stored in little endian.</ref> !! Description | |||
|- | |||
| Extension type|| 32 bits || 0 || 4 bytes in big endian:<br> 'S', 'T', 0x00, 0x02 = 0x53540002 | |||
|- | |||
| Extension length|| 32 bits || 4 || Number of bytes of header extension = 340 | |||
|- | |||
| Public key index|| 32 bits || 8 || Index of the public key to be used. | |||
|- | |||
| Public key number|| 32 bits || 12 || Number of public keys in table = 8 | |||
|- | |||
| ECDSA algorithm || 32 bits || 16 || 1: P-256 NIST ; 2: brainpool 256 ; 3: P-384 NIST ; 4: brainpool 384 | |||
|- | |||
| ECDSA public key || 768 bits || 20 || ECDSA public key to be used to verify the signature.<ref group="Note"> Public key is a point on the ECC curve. This field contains the two big numbers in big endian format corresponding to ECC Point coordinates ''x'' and ''y''. (If these coordinates are extracted from a PEM public key file that only kept coordinates in a raw binary format, you shall remove the first byte "04" which is an asn1 tag ; for more info: [http://www.rfc-editor.org/info/rfc5480 RFC 5480]). </ref> | |||
|- | |||
| Public key1 hash || 256 bits || 116 || Hash of (ECDSA Algorithm+Public key1).<ref group="Note"> The Public Key hash computation is the SHA-256 of ECDSA Algorithm expressed in little endian, concatenated to the public key itself. The entry of the public key table referenced by the public key index is compared to the hash of the ECDSA algorithm and public key that are stored in the header.'''</ref>. | |||
|- | |- | ||
| | | ...||...||...|| Hashes of (ECDSA Algorithm+Public key), for key2 up to key7 | ||
|- | |- | ||
| | | Public key8 hash<ref group="Note">The table of public key hashes will be hashed with SHA-256 by the ROM code and compared to the '''Hash of Public Keys Hashes Table (PKHTH)''' that is stored in OTP.</ref> || 256 bits || 340 || Hash of (ECDSA Algorithm+Public key8) | ||
|} | |} | ||
<references group="Note"/> | <references group="Note"/> | ||
=== Decryption header extension === | |||
[[File:STM32MP21 header decryption.png|right|400x400px]] | |||
This header extension contains parameters needed for decryption. | |||
{| | |||
! Name !! Length !! Byte Offset<ref group="Note">Offset is relative to header extension base. Unless expressed differently, the 32 bits values are stored in little endian.</ref>!! Description | |||
|- | |||
| Extension type|| 32 bits || 0 || 4 bytes in big endian:<br> 'S', 'T', 0x00, 0x01 = 0x53540001 | |||
|- | |||
| Extension length|| 32 bits || 4 || Number of bytes of header extension = 32 | |||
|- | |||
| Key size|| 32 bits || 8 || Size of extension key (128 or 256 bits). | |||
|- | |||
| Derivation constant|| 32 bits || 12 || Constant used to derive decryption key from master key stored in OTP. | |||
|- | |||
| Plain hash|| 128 bits || 16 || 128 msb bits of plain payload SHA256. | |||
|} | |||
<references group="Note"/> | |||
=== Padding header extension === | |||
Same as the [[#Padding header extension|padding header extension on STM32MP13x lines]] | |||
<noinclude> | <noinclude> | ||
[[Category:ROM code|0]] | [[Category:ROM code|0]] | ||
{{PublicationRequestId | 24643 | 2022-09-26 | }} | |||
</noinclude> | </noinclude> |
Latest revision as of 12:56, 7 March 2025
The STM32 header is a STMicroelectronics header needed for binaries loaded by ROM code.
1. Description[edit | edit source]
Each binary image loaded by the ROM code needs to include a specific STM32 header added on top of the binary data. This header includes mandatory and optional information: this second one is only needed for the authentication (STM32MP1 series) and decryption (STM32MP13x lines and STM32MP2 series) processes.
2. On STM32MP13x lines
[edit | edit source]
2.1. Base header[edit | edit source]
Name | Length | Byte Offset [Note 1] | Description |
---|---|---|---|
Magic number | 32 bits | 0 | 4 bytes in big endian: 'S', 'T', 'M', 0x32 = 0x53544D32 |
Image signature | 512 bits | 4 | ECDSA signature for image authentication[Note 2] |
Image checksum | 32 bits | 68 | Checksum of the payload[Note 3] |
Header version | 32 bits | 72 | Header version v2.0 = 0x00020000 Byte0: reserved Byte1: major version = 0x02 Byte2: minor version = 0x00 Byte3: reserved |
Image length | 32 bits | 76 | Length of image in bytes[Note 4] |
Image entry Point | 32 bits | 80 | Entry point of image |
Reserved | 96 bits | 84 | Reserved |
Version number | 32 bits | 96 | Image Version (monotonic number)[Note 5] |
Option flags | 32 bits | 100 | b0=1: Authentication enabled[Note 6] b1=1: Decryption enabled.[Note 7] b31=1: Header padding enabled[Note 8] |
Header extensions length | 32 bits | 104 | Sizes of header extensions enabled by option flags. |
Padding | 20 Bytes | 108 | Reserved padding bytes[Note 9]. Must all be set to 0 |
- ↑ Unless expressed differently, the 32 bits values are stored in little endian.
- ↑ Signature is calculated from first byte of header version field to last byte of image given by image length field.
- ↑ 32-bit sum of all payload bytes accessed as 8-bit unsigned numbers, discarding any overflow bits. Used to check the downloaded image integrity when signature is not used (if b0=0 in Option flags).
- ↑ Length is the length of the built image, it does not include the length of the STM32 header.
- ↑ Image version number is an anti rollback monotonic counter. The ROM code checks that it is higher or equal to the monotonic counter stored in OTP.
- ↑ Enabling signature verification is mandatory on secured locked device. Authentication parameters are stored in "Authentication header extension".
- ↑ When decryption is enabled, authentication is mandatory. Decryption parameters are stored in "Decryption header extension".
- ↑ This header padding extension is always used to have a fixed size of 512 bytes for the whole size of header + its extensions.
- ↑ This padding forces STM32 base header size to 128 bytes (0x80).
2.2. Authentication header extension[edit | edit source]
This header extension contains parameters needed for authentication.
Name | Length | Byte Offset[Note 1] | Description |
---|---|---|---|
Extension type | 32 bits | 0 | 4 bytes in big endian: 'S', 'T', 0x00, 0x02 = 0x53540002 |
Extension length | 32 bits | 4 | Number of bytes of header extension = 340 |
Public key index | 32 bits | 8 | Index of the public key to be used. |
Public key number | 32 bits | 12 | Number of public keys in table = 8 |
ECDSA algorithm | 32 bits | 16 | 1: P-256 NIST ; 2: brainpool 256 |
ECDSA public key | 512 bits | 20 | ECDSA public key to be used to verify the signature.[Note 2] |
Public key1 hash | 256 bits | 84 | Hash of (ECDSA Algorithm+Public key1).[Note 3]. |
... | ... | ... | Hashes of (ECDSA Algorithm+Public key), for key2 up to key7 |
Public key8 hash[Note 4] | 256 bits | 308 | Hash of (ECDSA Algorithm+Public key8) |
- ↑ Offset is relative to header extension base. Unless expressed differently, the 32 bits values are stored in little endian.
- ↑ Public key is a point on the ECC curve. This field contains the two big numbers in big endian format corresponding to ECC Point coordinates x and y. (If these coordinates are extracted from a PEM public key file that only kept coordinates in a raw binary format, you shall remove the first byte "04" which is an asn1 tag ; for more info: RFC 5480).
- ↑ The Public Key hash computation is the SHA-256 of ECDSA Algorithm expressed in little endian, concatenated to the public key itself. The entry of the public key table referenced by the public key index is compared to the hash of the ECDSA algorithm and public key that are stored in the header.
- ↑ The table of public key hashes will be hashed with SHA-256 by the ROM code and compared to the Hash of Public Keys Hashes Table (PKHTH) that is stored in OTP.
2.3. Decryption header extension[edit | edit source]
This header extension contains parameters needed for decryption.
Name | Length | Byte Offset[Note 1] | Description |
---|---|---|---|
Extension type | 32 bits | 0 | 4 bytes in big endian: 'S', 'T', 0x00, 0x01 = 0x53540001 |
Extension length | 32 bits | 4 | Number of bytes of header extension = 32 |
Key size | 32 bits | 8 | Size of extension key (128 bits)[Note 2]. |
Derivation constant | 32 bits | 12 | Constant used to derive decryption key from master key stored in OTP. |
Plain hash | 128 bits | 16 | 128 msb bits of plain payload SHA256. |
2.4. Padding header extension[edit | edit source]
Name | Length | Byte Offset[Note 1] | Description |
---|---|---|---|
Extension type | 32 bits | 0 | 4 bytes in big endian: 'S', 'T', 0xFF, 0xFF = 0x5354FFFF |
Extension length | 32 bits | 4 | Number of bytes of header extension = N + 8 |
Padding bytes | N bytes | 8 | Padding bytes[Note 2]. |
3. On STM32MP15x lines
[edit | edit source]
Name | Length | Byte Offset | Description |
---|---|---|---|
Magic number | 32 bits | 0 | 4 bytes in big endian: 'S', 'T', 'M', 0x32 = 0x53544D32 |
Image signature | 512 bits | 4 | ECDSA signature for image authentication[Note 1] |
Image checksum | 32 bits | 68 | Checksum of the payload[Note 2] |
Header version | 32 bits | 72 | Header version v1.0 = 0x00010000 Byte0: reserved Byte1:major version = 0x01 Byte2: minor version = 0x00 Byte3: reserved |
Image length | 32 bits | 76 | Length of image in bytes[Note 3] |
Image entry Point | 32 bits | 80 | Entry point of image |
Reserved1 | 32 bits | 84 | Reserved |
Load address | 32 bits | 88 | Load address of image[Note 4] |
Reserved2 | 32 bits | 92 | Reserved |
Version number | 32 bits | 96 | Image Version (monotonic number)[Note 5] |
Option flags | 32 bits | 100 | b0=1: no signature verification[Note 6] |
ECDSA algorithm | 32 bits | 104 | 1: P-256 NIST ; 2: brainpool 256 |
ECDSA public key | 512 bits | 108 | ECDSA public key to be used to verify the signature.[Note 7][Note 8] |
Padding | 83 Bytes | 172 | Reserved padding bytes[Note 9]. Must all be set to 0. |
Binary type | 1 Byte | 255 | Used to check the binary type 0x10-0x1F: FSBL 0x30: Copro |
- ↑ Signature is calculated from first byte of header version field to last byte of image given by image length field.
- ↑ 32-bit sum of all payload bytes accessed as 8-bit unsigned numbers, discarding any overflow bits. Used to check the downloaded image integrity when signature is not used (if b0=1 in Option flags).
- ↑ Length is the length of the built image, it does not include the length of the STM32 header.
- ↑ This field is not used by ROM code.
- ↑ Image version number is an anti rollback monotonic counter. The ROM code checks that it is higher or equal to the monotonic counter stored in OTP.
- ↑ Enabling signature verification is mandatory on secured locked device.
- ↑ Public key is a point on the ECC curve. This field contains the two big numbers in big endian format corresponding to ECC Point coordinates x and y. (If these coordinates are extracted from a PEM public key file that only kept coordinates in a raw binary format, you shall remove the first byte "04" which is an asn1 tag ; for more info: RFC 5480).
- ↑ The Public Key hash computation is the SHA-256 of the public key itself, then the resulting value is compared to the Hash of pubKey that is stored in OTP.
- ↑ This padding forces STM32 header size to 256 bytes (0x100).
4. On STM32MP23x lines
and STM32MP25x lines
[edit | edit source]
4.1. Base header[edit | edit source]
Name | Length | Byte Offset [Note 1] | Description | Signed |
---|---|---|---|---|
Magic number | 32 bits | 0 | 4 bytes in big endian: 'S', 'T', 'M', 0x32 = 0x53544D32 |
No |
Image signature | 512 bits | 4 | ECDSA signature for image authentication[Note 2] | No |
Image checksum | 32 bits | 68 | Checksum of the payload[Note 3] | No |
Header version | 32 bits | 72 | Header version v2.2 = 0x00020200 Byte0: reserved Byte1: major version = 0x02 Byte2: minor version = 0x02 Byte3: reserved |
Yes |
Image length | 32 bits | 76 | Length of image in bytes[Note 4] | Yes |
Image entry Point | 32 bits | 80 | Entry point of image | Yes |
Reserved | 96 bits | 84 | Reserved | Yes |
Version number | 32 bits | 96 | Image Version (monotonic number)[Note 5] | Yes |
Option flags | 32 bits | 100 | b0=1: Authentication enabled[Note 6] b1=1: Decryption enabled.[Note 7] b8=1: Aarch32 binary mode support.[Note 8] b31=1: Header padding enabled[Note 9] |
Yes |
Header extensions length | 32 bits | 104 | Sizes of header extensions enabled by option flags. | Yes |
Binary type | 32 bits | 108 | Used to check binary type. Must be set to 0x30 for FSBLM. | Yes |
Padding | 16 Bytes | 112 | Reserved padding bytes[Note 10]. Must all be set to 0 |
Yes |
- ↑ Unless expressed differently, the 32 bits values are stored in little endian.
- ↑ Signature is calculated from first byte of header version field to last byte of image given by image length field, excluding the last bytes following the padding field.
- ↑ 32-bit sum of all payload bytes accessed as 8-bit unsigned numbers, discarding any overflow bits. Used to check the downloaded image integrity when signature is not used (if b0=0 in Option flags).
- ↑ Length is the length of the built image, it does not include the length of the STM32 header.
- ↑ Image version number is an anti rollback monotonic counter. The ROM code checks that it is higher or equal to the monotonic counter stored in OTP.
- ↑ Enabling signature verification is mandatory on secured locked device. Authentication parameters are stored in "Authentication header extension".
- ↑ When decryption is enabled, authentication is mandatory. Decryption parameters are stored in "Decryption header extension".
- ↑ Flag is for ecosystem purpose to detect if the Cortex-A binary is an Aarch32 binary. The ROM code only relies on OTP a35 mode to start directly an Aarch32 FSBL-A.
- ↑ This header padding extension is always used to have a fixed size of 512 bytes for the whole size of header + its extensions.
- ↑ This padding forces STM32 base header size to 128 bytes (0x80).
4.2. Authentication header extension[edit | edit source]
Same as the authentication header extension on STM32MP13x lines.
4.3. Decryption header extension[edit | edit source]
Same as the decryption header extension on STM32MP13x lines
4.4. Padding header extension[edit | edit source]
Same as the padding header extension on STM32MP13x lines.
5. On STM32MP21x lines
[edit | edit source]
5.1. Base header[edit | edit source]
Name | Length | Byte Offset [Note 1] | Description | Signed |
---|---|---|---|---|
Magic number | 32 bits | 0 | 4 bytes in big endian: 'S', 'T', 'M', 0x32 = 0x53544D32 |
No |
Image signature | 768 bits | 4 | ECDSA signature for image authentication[Note 2] | No |
Image checksum | 32 bits | 100 | Checksum of the payload[Note 3] | No |
Header version | 32 bits | 104 | Header version v2.3 = 0x00020300 Byte0: reserved Byte1: major version = 0x02 Byte2: minor version = 0x03 Byte3: reserved |
Yes |
Image length | 32 bits | 108 | Length of image in bytes[Note 4] | Yes |
Image entry Point | 32 bits | 112 | Entry point of image | Yes |
Reserved | 96 bits | 116 | Reserved | Yes |
Version number | 32 bits | 128 | Image Version (monotonic number)[Note 5] | Yes |
Option flags | 32 bits | 132 | b0=1: Authentication enabled[Note 6] b1=1: Decryption enabled.[Note 7] b8=1: Aarch32 binary mode support.[Note 8] b31=1: Header padding enabled[Note 9] |
Yes |
Header extensions length | 32 bits | 136 | Sizes of header extensions enabled by option flags. | Yes |
Binary type | 32 bits | 140 | Used to check binary type. Must be set to 0x30 for FSBLM. | Yes |
Padding | 16 Bytes | 144 | Reserved padding bytes[Note 10]. Must all be set to 0 |
Yes |
- ↑ Unless expressed differently, the 32 bits values are stored in little endian.
- ↑ Signature is calculated from first byte of header version field to last byte of image given by image length field, excluding the last bytes following the padding field.
- ↑ 32-bit sum of all payload bytes accessed as 8-bit unsigned numbers, discarding any overflow bits. Used to check the downloaded image integrity when signature is not used (if b0=0 in Option flags).
- ↑ Length is the length of the built image, it does not include the length of the STM32 header.
- ↑ Image version number is an anti rollback monotonic counter. The ROM code checks that it is higher or equal to the monotonic counter stored in OTP.
- ↑ Enabling signature verification is mandatory on secured locked device. Authentication parameters are stored in "Authentication header extension".
- ↑ When decryption is enabled, authentication is mandatory. Decryption parameters are stored in "Decryption header extension".
- ↑ Flag is for ecosystem purpose to detect if the Cortex-A binary is an Aarch32 binary. The ROM code only relies on OTP a35 mode to start directly an Aarch32 FSBL-A.
- ↑ This header padding extension is always used to have a fixed size of 512 bytes for the whole size of header + its extensions.
- ↑ This padding forces STM32 base header size to 160 bytes (0x80).
5.2. Authentication header extension[edit | edit source]
This header extension contains parameters needed for authentication.
Name | Length | Byte Offset[Note 1] | Description |
---|---|---|---|
Extension type | 32 bits | 0 | 4 bytes in big endian: 'S', 'T', 0x00, 0x02 = 0x53540002 |
Extension length | 32 bits | 4 | Number of bytes of header extension = 340 |
Public key index | 32 bits | 8 | Index of the public key to be used. |
Public key number | 32 bits | 12 | Number of public keys in table = 8 |
ECDSA algorithm | 32 bits | 16 | 1: P-256 NIST ; 2: brainpool 256 ; 3: P-384 NIST ; 4: brainpool 384 |
ECDSA public key | 768 bits | 20 | ECDSA public key to be used to verify the signature.[Note 2] |
Public key1 hash | 256 bits | 116 | Hash of (ECDSA Algorithm+Public key1).[Note 3]. |
... | ... | ... | Hashes of (ECDSA Algorithm+Public key), for key2 up to key7 |
Public key8 hash[Note 4] | 256 bits | 340 | Hash of (ECDSA Algorithm+Public key8) |
- ↑ Offset is relative to header extension base. Unless expressed differently, the 32 bits values are stored in little endian.
- ↑ Public key is a point on the ECC curve. This field contains the two big numbers in big endian format corresponding to ECC Point coordinates x and y. (If these coordinates are extracted from a PEM public key file that only kept coordinates in a raw binary format, you shall remove the first byte "04" which is an asn1 tag ; for more info: RFC 5480).
- ↑ The Public Key hash computation is the SHA-256 of ECDSA Algorithm expressed in little endian, concatenated to the public key itself. The entry of the public key table referenced by the public key index is compared to the hash of the ECDSA algorithm and public key that are stored in the header.
- ↑ The table of public key hashes will be hashed with SHA-256 by the ROM code and compared to the Hash of Public Keys Hashes Table (PKHTH) that is stored in OTP.
5.3. Decryption header extension[edit | edit source]
This header extension contains parameters needed for decryption.
Name | Length | Byte Offset[Note 1] | Description |
---|---|---|---|
Extension type | 32 bits | 0 | 4 bytes in big endian: 'S', 'T', 0x00, 0x01 = 0x53540001 |
Extension length | 32 bits | 4 | Number of bytes of header extension = 32 |
Key size | 32 bits | 8 | Size of extension key (128 or 256 bits). |
Derivation constant | 32 bits | 12 | Constant used to derive decryption key from master key stored in OTP. |
Plain hash | 128 bits | 16 | 128 msb bits of plain payload SHA256. |
- ↑ Offset is relative to header extension base. Unless expressed differently, the 32 bits values are stored in little endian.
5.4. Padding header extension[edit | edit source]
Same as the padding header extension on STM32MP13x lines