STM32MP15 peripherals overview

Revision as of 15:02, 10 June 2022 by Registered User
Applicable for STM32MP15x lines

This article lists all internal peripherals embedded in STM32MP15 device and shows the assignment possibilities to the runtime contexts for each one of them.
Via this article, you can also access to individual peripheral articles in which information related to the overview and configuration can be found.

1. Internal peripherals overview[edit source]

The figure below shows all peripherals embedded in STM32MP15 device, grouped per functional domains that are reused in many places of this wiki to structure the articles.

Several runtime contexts exist on STM32MP15 device[1], corresponding to the different Arm cores and associated security modes:

  •  Arm dual core Cortex-A7 secure  (Trustzone), running a Secure Monitor or Secure OS like OP-TEE
  •  Arm dual core Cortex-A7 non secure , running Linux
  •  Arm Cortex-M4  (non-secure), running STM32Cube


Some peripherals can be strictly assigned to one runtime context: this is the case for most of the peripherals, like USART or I2C.
Other ones can be shared between several runtime contexts: this is the case for system peripherals, like PWR or RCC.
The legend below shows how assigned and shared peripherals are identified in the assignment diagram that follows:

STM32MP1IPsOverview legend.png

Both the diagram below and the following summary table (in Internal peripherals assignment chapter below) are clickable in order to jump to each peripheral overview articles and get more detailed information (like software frameworks used to control them). They list STMicroelectronics recommendations. The STM32MP15 reference manual [2] may expose more possibilities than what is shown here.


STGENSYSCFGRTCEXTIGICNVICIWDGIWDGWWDGDMADMADMAMUXMDMASYSRAMDDR via DDR CTRLBKPSRAMMCU SRAMMCU SRAMRETRAMTIMTIMLPTIMGPIOGPIOIPCCHSEMRCCPWRDTSDDRPERFMDBGMCUHDPSTMBSECQUADSPIFMCSDMMCFDCANETHSDMMCUSBHOTGUSBPHYCUSARTUSARTUSARTI2CI2CI2CSPISPIRNGHASHETZPCCRYPCRCTZCRNGHASHTAMPCRYPCRCGPUDSILTDCDCMICECVREFBUFDACDFSDMADCSPI I2SSPDIFRXSAI
STM32MP1 internal peripherals overview

2. Internal peripherals assignment[edit source]

Click on the right to expand the legend...

STM32MP15 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned () to the given runtime context.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are statically connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

3. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the ADC peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

4. Peripheral overview[edit source]

The ADC peripheral is a successive approximation analog-to-digital converter.

The STM32MP15 has one ADC block with two physical ADCs:

  • Configurable resolution: 8, 10, 12, 14, 16 bits.
  • Each ADC has up to 20 multiplexed channels (including 6 internal channels connected only to ADC2).
  • The conversions can be performed in single, continuous, scan or discontinuous mode.
  • The result can be read in a left- or right-aligned 32-bit data register by using CPU or DMA[3].
  • The analog watchdog feature allows the application to detect if the input voltage goes beyond the user-defined, high or low thresholds.
  • A common input clock for the two ADCs, which can be selected between 2 different clock[4] sources (Synchronous or Asynchronous clock).
  • The common reference voltage can be provided by either VREFBUF[5] or any other external regulator[6] wired to VREF+ pin.

Each ADC supports two contexts to manage conversions:

  • Regular conversions can be done in sequence, running in background
  • Injected conversions have higher priority, and so have the ability to interrupt the regular sequence (either triggered in SW or HW). The regular sequence is resumed, in case it has been interrupted.
  • Each context has its own configurable sequence and trigger: software, TIM[7], LPTIM[8] and EXTI[9].

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

5. Peripheral usage[edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

5.1. Boot time assignment[edit source]

5.1.1. On STM32MP15x lines More info.png[edit source]

The ADC is usually not used at boot time. But it may be used by the SSBL (see Boot chain overview), to check for power supplies for example.

Click on the right to expand the legend...

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given boot time context.
  • means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32 MPU reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Domain Peripheral Boot time allocation Comment
Instance Cortex-A7
secure
(ROM code)
Cortex-A7
secure
(TF-A BL2)
Cortex-A7
non-secure
(U-Boot)
Analog ADC ADC

5.2. Runtime assignment[edit source]

5.2.1. On STM32MP15x lines More info.png[edit source]

Click on the right to expand the legend...

STM32MP15 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Analog ADC ADC Assignment (single choice)

6. Software frameworks and drivers[edit source]

Below are listed the software frameworks and drivers managing the ADC peripheral for the embedded software components listed in the above tables.

7. How to assign and configure the peripheral[edit source]

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:

  • partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
  • HAL initialization code generation for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned.

For the Linux kernel and U-boot configuration, please refer to ADC device tree configuration article.

8. How to go further[edit source]

See application notes:

  • How to get the best ADC accuracy in STM32[10].
  • Getting started with STM32MP15 series hardware development (AN5031)[11].
    It deals with analog domain power supply and reference voltage.

9. References[edit source]



10. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the DAC peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

11. Peripheral overview[edit source]

The DAC peripheral is a voltage output digital-to-analog converter:

  • It may be configured in 8- or 12-bit mode (data could be left- or right-aligned)
  • It has two output channels, each with its own converter
  • The dual DAC channel mode could be done independently or simultaneously
  • It has built-in noise and triangle waveform generator and supports triggers for conversions, using: TIM[1], LPTIM[2] or EXTI[3]
  • The DAC output buffer allows a high drive output current
  • It can operate under Normal mode or low-power Sample and Hold mode (uses LSI clock, from RCC[4]).
  • It may be used in conjunction with the DMA[5] controller (with underrun error detection)
  • The common reference voltage, can be provided by either VREFBUF[6] or any other external regulator[7] wired to VREF+ pin.

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

12. Peripheral usage[edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

12.1. Boot time assignment[edit source]

The DAC peripheral is not used at boot time.

12.2. Runtime assignment[edit source]

12.2.1. On STM32MP15x lines More info.png[edit source]

Click on the right to expand the legend...

STM32MP15 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Analog DAC DAC Assignment (single choice)

13. Software frameworks and drivers[edit source]

Below are listed the software frameworks and drivers managing the DAC peripheral for the embedded software components listed in the above tables.

14. How to assign and configure the peripheral[edit source]

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:

  • partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
  • HAL initialization code generation for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned.

For the Linux kernel configuration, please refer to DAC device tree configuration and DAC Linux driver articles.

15. References[edit source]



16. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the VREFBUF peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

17. Peripheral overview[edit source]

The VREFBUF peripheral is an internal voltage regulator.

The VREFBUF is supplied via the VDDA pin. When enabled, it can provide a reference voltage in the range of: 1,5V, 1,8V, 2,048V or 2,5V.

The VREFBUF can be used to provide an analog voltage reference for:

The VREFBUF can be left unused. In this case, an external voltage regulator can provide reference voltage to VREF+ pin.

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

18. Peripheral usage[edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

18.1. Boot time assignment[edit source]

18.1.1. On STM32MP15x lines More info.png[edit source]

The VREFBUF is not used at boot time.

18.2. Runtime assignment[edit source]

18.2.1. On STM32MP15x lines More info.png[edit source]

Click on the right to expand the legend...

STM32MP15 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Analog VREFBUF VREFBUF Assignment (single choice)

19. Software frameworks and drivers[edit source]

Below are listed the software frameworks and drivers managing the VREFBUF peripheral for the embedded software components listed in the above tables.

Info white.png Information
The VREFBUF is a system resource[1] which needs to be also controlled by the resource manager[1] in case its consumers (e.g. ADC, DAC or an external device connected to VREF+ pin) are spread across:
  • the Arm® Cortex®-A7 non-secure context
  • the Arm® Cortex®-M4 context

For this reason, the direct control of VREFBUF from the Arm® Cortex®-M4 is not recommended in STM32Cube by default.
It's recommended to implement it in STM32Cube only if all consumers and the VDDA supply pin are controlled in the Arm® Cortex®-M4 context.

20. How to assign and configure the peripheral[edit source]

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:

  • partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
  • HAL initialization code generation for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned.

21. References[edit source]

  1. 1.0 1.1 Resource manager for coprocessing, focus on system resources




22. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the IPCC peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

23. Peripheral overview[edit source]

The IPCC (inter-processor communication controller) peripheral is used to exchange data between two processors. It provides a non blocking signaling mechanism to post and retrieve information in an atomic way. Note that shared memory buffers are allocated in the MCU SRAM, which is not part of the IPCC block.

The IPCC peripheral provides a hardware support to manage inter-processor communication between two processor instances. Each processor owns specific register bank and interrupts.

The IPCC provides the signaling for six bidirectional channels.
Each channel is divided into two subchannels that offer a unidirectional signaling from the "sender" processor to the "receiver" processor:

  • P1_TO_P2 subchannel
  • P2_TO_P1 subchannel

A subchannel consists in:

  • One flag that toggles between occupied and free: the flag is set to occupied by the "sender" processor and cleared by the "receiver" processor.
  • Two associated interrupts (shared with the other channels):
    • RXO: RX channel occupied, connected to the "receiver" processor.
    • TXF: TX channel free, connected to the "sender" processor.
  • Two associated interrupt masks multiplexing channel IRQs.


IPCC peripheral.png
The IPCC supports the following channel operating modes:

  • Simplex communication mode:
    • Only one subchannel is used.
    • Unidirectional messages: once the "sender" processor has posted the communication data in the memory, it sets the channel status flag to occupied. The "receiver" processor clears the flag when the message is treated.
  • Half-duplex communication mode:
    • Only one subchannel is used.
    • Bidirectional messages: once the "sender" processor has posted the communication data in the memory, it sets the channel status flag to occupied. The "receiver" processor clears the flag when the message is treated and the response is available in shared memory.
  • Full-duplex communication mode:
    • The subchannels are used in Asynchronous mode.
    • Any processor can post asynchronously a message by setting the subchannel status flag to occupied. The "receiver" processor clears the flag when the message is treated. This mode can be considered as a combination of two simplex modes on a given channel.

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

24. Peripheral usage[edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

24.1. Boot time assignment[edit source]

The IPCC peripheral is not used at boot time.

24.2. Runtime assignment[edit source]

24.2.1. On STM32MP15x lines More info.png[edit source]

STMicroelectronics distribution uses the IPCC peripheral for inter-processor communication with the following configuration:

  • IPCC processor 1 interface is assigned to Arm® Cortex®-A7 non-secure context.
  • IPCC processor 2 interface is assigned to Arm® Cortex®-M4 context.


IPCC overview.png

It does not make sense to allocate the IPCC to a single runtime execution context. It is consequently enabled by default for both cores in the STM32CubeMX.

Click on the right to expand the legend...

STM32MP15 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Coprocessor IPCC IPCC Shared (none or both)

25. Software frameworks and drivers[edit source]

Below are listed the software frameworks and drivers managing the IPCC peripheral for the embedded software components listed in the above tables.

26. How to assign and configure the peripheral[edit source]

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:

  • partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
  • HAL initialization code generation for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned.

The IPCC peripheral is shared between the Arm Cortex-A and Cortex-M contexts. A particular attention must therefore be paid to have a complementary configuration on both contexts. In STMicroelectronics distribution, the IPCC is configured as described below. To ensure the coherency of the system, it is recommended to keep this configuration unchanged in your implementation.

  • Processor interface
Processor interface Context
Cortex-A7 non-secure
(Linux)
Cortex-M4
(STM32Cube)
Processor 1 interface
Processor 2 interface
  • Channel allocation
Channel Mode Usage Software client frameworks
Cortex-A7 non-secure
(Linux)
Cortex-M4
(STM32Cube)
Channel 1 Full-duplex communication RPMsg transfer from Cortex-M to Cortex-A
  • The Cortex-M core uses this channel to indicate that a message is available
  • The Cortex-A core uses this channel to indicate that the message is treated
RPMsg framework OpenAMP
Channel 2 Full-duplex communication RPMsg transfer from Cortex-A to Cortex-M
  • The Cortex-A core uses this channel to indicate that a message is available
  • The Cortex-M core uses this channel to indicate that the message is treated
RPmsg framework OpenAMP
Channel 3 Simplex communication Cortex-M4 shutdown request RemoteProc framework CprocSync cube utility
Channel 4 free
Channel 5 free
Channel 6 free


Applicable for STM32MP15x lines

27. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the HSEM peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

28. Peripheral overview[edit source]

The HSEM (hardware spinlock) peripheral is used to provide synchronization and mutual exclusion between heterogeneous processors.

  • 32 hardware semaphores are available on the platform.
  • semaphores could be accessed by the Arm® Cortex®-A7 core and the Arm® Cortex®-M4

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

29. Peripheral usage[edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

29.1. Boot time assignment[edit source]

29.1.1. On STM32MP15x lines More info.png[edit source]

The hardware semaphore is used at boot time for GPIO access protection between the Arm® Cortex®-A7 and Cortex®-M4 cores. See Protecting GPIO and EXTI system resources by hardware semaphores for details.

Click on the right to expand the legend...

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given boot time context.
  • means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32 MPU reference manuals.

Domain Peripheral Boot time allocation Comment
Instance Cortex-A7
secure
(ROM code)
Cortex-A7
secure
(TF-A BL2)
Cortex-A7
non-secure
(U-Boot)
Coprocessor HSEM HSEM

29.2. Runtime assignment[edit source]

29.2.1. On STM32MP15x lines More info.png[edit source]

It does not make sense to allocate HSEM to a single runtime execution context, that is why it is enabled by default for both cores in the STM32CubeMX.

The hardware semaphore is used at runtime for GPIO and EXTI access protection between the Arm® Cortex®-A7 and Cortex®-M4 cores. See Protecting GPIO and EXTI system resources by hardware semaphores for details.


Click on the right to expand the legend...

STM32MP15 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Coprocessor HSEM HSEM

30. Software frameworks and drivers[edit source]

Below are listed the software frameworks and drivers managing the HSEM peripheral for the embedded software components listed in the above tables.

31. How to assign and configure the peripheral[edit source]

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:

  • partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
  • HAL initialization code generation for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned.

The HSEM peripheral is shared between the Cortex-A and Cortex-M contexts, so a particular attention must be paid to have a complementary configuration on both contexts.


STM32MP15 RTC internal peripheral

STM32MP15 SYSCFG internal peripheral




32. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the NVIC peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

33. Peripheral overview[edit source]

The NVIC peripheral is the Arm® Cortex®-M4 interrupt controller. As a result, it cannot be accessed by the Arm Cortex-A7 core.

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

34. Peripheral usage[edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

34.1. Boot time assignment[edit source]

The NVIC peripheral is not used at boot time.

34.2. Runtime assignment[edit source]

34.2.1. On STM32MP15x lines More info.png[edit source]

Click on the right to expand the legend...

STM32MP15 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Core/Interrupts NVIC NVIC

35. Software frameworks and drivers[edit source]

Below are listed the software frameworks and drivers managing the NVIC peripheral for the embedded software components listed in the above tables.

36. How to assign and configure the peripheral[edit source]

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:

  • partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
  • HAL initialization code generation for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned.




37. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the MCU SRAM internal memory peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

38. Peripheral overview[edit source]

The MCU SRAM peripheral is 384-Kbyte wide and physically near to the Cortex®-M4 for optimized performances from this core. It is split into four separate banks:

  • MCU SRAM1 (128 Kbytes)
  • MCU SRAM2 (128 Kbytes)
  • MCU SRAM3 (64 Kbytes)
  • MCU SRAM4 (64 Kbytes)

Those banks have individual security control (see security support in the runtime assignment table below) and automatic clock gating (for power management optimization), but they are not supplied when the system goes to Standby low power mode, so their content is lost in that case.

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

39. Peripheral usage[edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

39.1. Boot time assignment[edit source]

39.1.1. On STM32MP15x lines More info.png[edit source]

The ROM code uses the MCU SRAM1 to store the USB context during a boot on USB for Flash programming (with STM32CubeProgrammer).

Linux remoteproc framework (running on the Cortex®-A7) loads the Cortex®-M4 firmware code into the MCU SRAM, except the exception table that must be loaded in the RETRAM since the Cortex®-M4 is looking for its reset entry point at address 0x00000000. The overall memory mapping is shown in the platform memory mapping section.

Click on the right to expand the legend...

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given boot time context.
  • means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32 MPU reference manuals.

Domain Peripheral Boot time allocation Comment
Instance Cortex-A7
secure
(ROM code)
Cortex-A7
secure
(TF-A BL2)
Cortex-A7
non-secure
(U-Boot)
Core/RAM MCU SRAM Any instance

39.2. Runtime assignment[edit source]

39.2.1. On STM32MP15x lines More info.png[edit source]

Click on the right to expand the legend...

STM32MP15 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Core/RAM MCU SRAM SRAM1 Assignment (between A7 S and A7 NS / M4)
Shareable (between A7 NS and M4)
SRAM2 Assignment (between A7 S and A7 NS / M4)
Shareable (between A7 NS and M4)
SRAM3 Assignment (between A7 S and A7 NS / M4)
Shareable (between A7 NS and M4)
SRAM4 Assignment (between A7 S and A7 NS / M4)
Shareable (between A7 NS and M4)

40. Software frameworks and drivers[edit source]

Below are listed the software frameworks and drivers managing the XXX peripheral for the embedded software components listed in the above tables.

Notice the and/or allocation between Cortex®-A7 non-secure and Cortex®-M4, meaning that it is possible to share banks between those cores, typically to realize inter process communication between RPMsg on Linux side and OpenAMP on STM32Cube side.

The default assignement set in STMicroelectronics distribution is in line with the platform memory mapping, that can be adapted by the platform user.

41. How to assign and configure the peripheral[edit source]

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:

  • partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
  • HAL initialization code generation for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned.

The several SRAM banks are accessible via different address ranges in order to benefit from the Cortex-M4 multiple ports.




42. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the RETRAM internal memory peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

43. Peripheral overview[edit source]

The RETRAM internal memory is 64 Kbytes wide and is physically near to the Arm® Cortex®-M4 for optimized performance from the core. It is located in the VSW power domain, allowing it to be supplied during Standby low power mode, and to retain retention firmware that can be executed very quickly by the Cortex-M4 on wake up from Standby mode.

The Cortex-M4 firmware has to be loaded to the RETRAM , starting at address 0x00000000. At least, it must load the part of the firmware containing the vector table, since the Cortex-M4 reset entry point is address 0x00000004. The rest of the firmware code is loaded into the MCU SRAM. The overall memory mapping is shown in the platform memory mapping section.

While going to Standby low power mode, the RETRAM can remain supplied, so it can preserve a (small) Cortex-M4 piece of retention firmware that is executed on wake up when the ROM code (running on Cortex-A7) restarts the Cortex-M4.

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

44. Peripheral usage[edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

44.1. Boot time assignment[edit source]

44.1.1. On STM32MP15x lines More info.png[edit source]

At boot time, The RETRAM internal memory can contain the Cortex-M4 firmware, but could also be dedicated tor some other usages.


Click on the right to expand the legend...

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given boot time context.
  • means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32 MPU reference manuals.

Domain Peripheral Boot time allocation Comment
Instance Cortex-A7
secure
(ROM code)
Cortex-A7
secure
(TF-A BL2)
Cortex-A7
non-secure
(U-Boot)
Core/RAM RETRAM RETRAM

44.2. Runtime assignment[edit source]

44.2.1. On STM32MP15x lines More info.png[edit source]

At runtime the RETRAM can be allocated to:

  • the Cortex-M4 (default) for use with the STM32Cube MPU Package, either for runtime firmware that can be mapped in both RETRAM and MCU SRAM, or for retention firmware that only fits into the RETRAM ,

or

  • the Cortex-A7 secure to be used under OP-TEE,

or


Click on the right to expand the legend...

STM32MP15 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Core/RAM RETRAM RETRAM Assignment to the Cortex-M4 if used

45. Software frameworks and drivers[edit source]

The RETRAM is the minimum (and default) memory for the Cortex-M4 firmware.The software frameworks and component managing the RETRAM device to host the Cortex-M4 firmware are listed below.

46. How to assign and configure the peripheral[edit source]

The peripheral assignment can be done manually.

  • In device trees generation for the OpenSTLinux software components:
  • In the linker script for the STM32CubeMPU Package.





47. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the WWDG peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

48. Peripheral overview[edit source]

The WWDG peripheral is a watchdog unit that can be used to protect the Cortex®-M4 based coprocessor firmware from endless loops or to monitor some real-time activities. This peripheral is clocked by the bus on which it is connected, thus it is frozen as soon as the system goes to Stop or Standby low power mode (except if the Stop emulation mode is enabled via DBGSTOP bit in DBGMCU_CR register). This block has an early interrupt feature that allows to get an interrupt (on GIC or NVIC) one cycle before reaching the final reset: this can allow to trigger a recovery mechanism on Cortex®-M4 or on Cortex®-A7.
On WWDG expiration, a MCU reset is generated, reseting Cortex®-M4 sub-system and the WWDG itself. This MCU reset also generates an interrupt on GIC thanks to EXTI. This allows Cortex®-A7 to detect Cortex®-M4 crashed and to recover it by stopping associated services, reloading Cortex®-M4 firmware and restarting Cortex®-M4.

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

49. Peripheral usage[edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

49.1. Boot time assignment[edit source]

The WWDG peripheral is not used at boot time.

49.2. Runtime assignment[edit source]

49.2.1. On STM32MP15x lines More info.png[edit source]

Click on the right to expand the legend...

STM32MP15 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Core/Watchdog WWDG WWDG

50. Software frameworks and drivers[edit source]

Below are listed the software frameworks and drivers managing the WWDG peripheral for the embedded software components listed in the above tables.

As there is only one WWDG counter cycle between the WWDG early interrupt and the WWDG reset generation, ST preconizes to allocate the WWDG early interrupt to Cortex®-M4 for a better reactivity and not to Cortex®-A7.

51. How to assign and configure the peripheral[edit source]

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:

  • partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
  • HAL initialization code generation for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned.









52. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the PWR peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

53. Peripheral overview[edit source]

The PWR peripheral is used to control the device power supply configuration.

It has 6 input pins (named wakeup pins) which can be programmed to wake the system up from low power. The wakeup pins are listed with WKUP prefix in the STM32MP15 Datasheet.

These pins can be used by the Cortex®-A7 non secure (via Cortex®-A7 secure services) or the Cortex®-M4.

The PWR peripheral provides 2 output hardware lines named PWR_ON and PWR_LP:

  • In STPMIC1 configuration, PWR_ON allows to select the register bank (active or low power). PWR_LP is not used.
  • In the power discrete solution they drive VDDcore which feeds the Cortex®-A7, the Cortex®-M4 and the peripherals. They also control the DDR power supplies (VDD_DDR, VREF_DDR, VTT_DDR).

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

54. Peripheral usage[edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

54.1. Boot time assignment[edit source]

54.1.1. On STM32MP15x lines More info.png[edit source]

The PWR is closely configured together with RCC by all the boot components: the ROM code, the FSBL, the SSBL and up to Linux® kernel. Its configuration is carried by the device tree.

Click on the right to expand the legend...

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given boot time context.
  • means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32 MPU reference manuals.

Domain Peripheral Boot time allocation Comment
Instance Cortex-A7
secure
(ROM code)
Cortex-A7
secure
(TF-A BL2)
Cortex-A7
non-secure
(U-Boot)
Power & Thermal PWR PWR

54.2. Runtime assignment[edit source]

54.2.1. On STM32MP15x lines More info.png[edit source]

Click on the right to expand the legend...

STM32MP15 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Power & Thermal PWR PWR

55. Software frameworks and drivers[edit source]

Below are listed the software frameworks and drivers managing the PWR peripheral for the embedded software components listed in the above tables.

56. How to assign and configure the peripheral[edit source]

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:

  • partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
  • HAL initialization code generation for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned:

57. How to go further[edit source]

The PWR is interfaced with the hardware debug port (HDP) of the STM32MP15. This link offers the flexibility to observe the main PWR state signals on debug pins.

Please refer to STM32MP15 reference manuals for the exact list of signals that can be monitored.


STM32MP15 RCC internal peripheral


STM32MP15 CRYP internal peripheral STM32MP15 ETZPC internal peripheral STM32MP15 HASH internal peripheral STM32MP15 RNG internal peripheral

STM32MP15 TAMP internal peripheral




58. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the STM peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

59. Peripheral overview[edit source]

The STM peripheral is used to log STM traces into the embedded trace FIFO (ETF). This trace can include hardware events (the list is given in the STM32MP15 reference manuals) or direct 'printf like' log from the Cortex®-A7. Once in the ETF buffer, the trace can be dumped directly from the Cortex®-A7 or to the trace port interface unit (TPIU), connected to an external probe able to decode it.

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

60. Peripheral usage[edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

60.1. Boot time assignment[edit source]

60.1.1. On STM32MP1 series[edit source]

The STM can be used to debug the boot sequence using an external probe, without any associated embedded software.

60.2. Runtime assignment[edit source]

60.2.1. On STM32MP15x lines More info.png[edit source]

Click on the right to expand the legend...

STM32MP15 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Trace & Debug STM STM

61. Software frameworks and drivers[edit source]

The STM can be used to debug the run time application using an external probe, without any associated embedded software.

There is no software dedicated to the STM internal peripheral delivered with the STM32 MPU ecosystem but the STM trace can be captured using an external probe.

62. How to assign and configure the peripheral[edit source]

Configuration of the STM is done via JTAG scripts. Those scripts must be built by the user using the STM32MP15 reference manuals .



63. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the CEC peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

64. Peripheral overview[edit source]

The CEC (consumer electronics control) or HDMI-CEC peripheral is used to receive/send messages from/to devices, such as TV or tuner, through a HDMI cable.

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

Refer to the STM32 CEC presentation [1] for an overview of the CEC hardware block capabilities.

65. Peripheral usage[edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

65.1. Boot time assignment[edit source]

The CEC peripheral is not used at boot time.

65.2. Runtime assignment[edit source]

65.2.1. On STM32MP15x lines More info.png[edit source]

Click on the right to expand the legend...

STM32MP15 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Visual CEC CEC Assignment (single choice)

66. Software frameworks and drivers[edit source]

Below are listed the software frameworks and drivers managing the CEC peripheral for the embedded software components listed in the above tables.

67. How to assign and configure the peripheral[edit source]

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:

  • partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
  • HAL initialization code generation for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned.

See also additional information in the CEC device tree configuration article for Linux®.

68. How to go further[edit source]

Refer to the STM32 CEC application note (AN4066) [2] for a detailed description of the CEC peripheral and applicable use-cases.

Even if this application note is related to STM32 microcontrollers, it also applies to STM32 MPUs.

69. References[edit source]



70. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the DCMI peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

71. Peripheral overview[edit source]

The DCMI (digital camera memory interface) peripheral is used to receive some video data from an external parallel camera sensor device or any other digital video equipment supporting parallel interface.

The DCMI hardware block can receive raw data frames in RGB565 and YUV422 formats as well as JPEG compressed data.

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

Refer to STM32 DCMI presentation [1] for an overview of DCMI hardware block and its capabilities.

72. Peripheral usage[edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

72.1. Boot time assignment[edit source]

The DCMI peripheral is not used at boot time.

72.2. Runtime assignment[edit source]

72.2.1. On STM32MP15x lines More info.png[edit source]

Click on the right to expand the legend...

STM32MP15 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Visual DCMI DCMI Assignment (single choice)

73. Software frameworks and drivers[edit source]

Below are listed the software frameworks and drivers managing the DCMI peripheral for the embedded software components listed in the above tables.

74. How to assign and configure the peripheral[edit source]

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:

  • partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
  • HAL initialization code generation for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned.

See also additional information in the DCMI device tree configuration article for Linux®.

75. How to go further[edit source]

Refer to STM32 DCMI Application Note (AN5020)[2] for a detailed description of the DCMI peripheral and applicable use-cases.

This application note is related to STM32 microcontrollers but it is also applicable to STM32 MPUs. This document can help to better understand stm32-dcmi V4L2 kernel driver and debug camera sensor and DCMI interactions.

76. References[edit source]



77. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the DSI peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

78. Peripheral overview[edit source]

The DSI peripheral implements all the protocol functions defined in the MIPI® Display Serial Interface (MIPI® DSI) specification. It provides an interface to communicate with a DSI-compliant display. The MIPI® DSI is part of a group of communication protocols defined by the MIPI® Alliance [1].

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

79. Peripheral usage[edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

Even if some MIPI DSI modes are supported by the DSI internal peripheral, in practice:

  • software frameworks like U-Boot or Linux® kernel do not support all the possible modes.
  • hardware integration constraints such as support for all the clock values or the pll configurations make it difficult to use all possible modes.

Select a MIPI DSI panel or bridge supporting the DSI video burst mode [2] because this mode is supported by all software frameworks and is easier to fine tune. Please consider the following recommendations when selecting a MIPI DSI panel or bridge for your project:

  • Pixel data transmission
    • in DSI command mode: not supported by neither U-Boot nor Linux® kernel, use instead the DSI video burst mode.
    • in DSI video mode:
      • burst mode: supported
      • non-burst mode with sync events or pulses: supported with clock constraints to be considered [2].
  • Command transmission (initialization sequence, backlight...)
    • in DSI command mode: supported
    • in DSI video mode:
      • burst mode: supported if there is enough time to send commands before or/and after pixel data [2].
      • non-burst mode with sync events or pulses: supported but there are timing constraints to be considered [2].

If non-burst mode has to be used for a specific MIPI DSI panel or bridge, check non-burst mode constraints.

79.1. Boot time assignment[edit source]

79.1.1. On STM32MP15x lines More info.png[edit source]

The DSI is used at boot time for displaying a splash screen through the U-Boot framework.

Click on the right to expand the legend...

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given boot time context.
  • means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32 MPU reference manuals.

Domain Peripheral Boot time allocation Comment
Instance Cortex-A7
secure
(ROM code)
Cortex-A7
secure
(TF-A BL2)
Cortex-A7
non-secure
(U-Boot)
Visual DSI DSI

79.2. Runtime assignment[edit source]

79.2.1. On STM32MP15x lines More info.png[edit source]

Click on the right to expand the legend...

STM32MP15 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Visual DSI DSI

80. Software frameworks and drivers[edit source]

Below are listed the software frameworks and drivers managing the DSI peripheral for the embedded software components listed in the above tables.

81. How to assign and configure the peripheral[edit source]

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:

  • partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
  • HAL initialization code generation for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned.

See also additional information in the DSI device tree configuration article for Linux®.

82. How to go further[edit source]

Refer to the STM32 DSI application note (AN4860) [2] for a detailed description of the DSI peripheral and applicable use-cases.

Even if this application note is related to STM32 microcontrollers, it also applies to STM32 MPUs.

82.1. Non-burst mode constraints[edit source]

In burst mode the setting for the DSI peripheral's PLL is quite relaxed. The DSI peripheral can send out pixel data in bursts, at rate higher that the pixel clock frequency. The consumer of the pixel data (the MIPI DSI panel or bridge) will internally re-sample such data to the correct clock frequency. This makes easy to configure the DSI in burst mode.

In non-burst mode, instead, the DSI peripheral must send out the pixel data at the exact pixel clock frequency required by the MIPI DSI panel or bridge. But, the set of pixel clock frequencies allowed by the DSI peripheral is limited by:

  • the frequency of the HSE oscillator (the input of the DSI peripheral's PLL);
  • the programmability of the DSI peripheral's PLL;
  • the min and max frequency of the VCO of the DSI peripheral's PLL;
  • the selected bit per pixel.

The following script dumps all the possible pixel clock frequencies allowed, that can be checked against the pixel clock frequency required by the MIPI DSI panel or bridge.

  1. !/bin/bash

hse=24000000 vcomin=1000000000 vcomax=2000000000 n_lanes=2

  1. 24 bpp

byte_per_pixel=3

for i in {1..7}; do

  for n in {10..125}; do
    vco=$(($hse*2*$n/$i))
    if [ $vco -lt $vcomin -o $vco -gt $vcomax ]; then
      continue
    fi
    for o in 1 2 4 8; do
      hs_clk=$(($hse*$n/($i*$o)))
      echo $(($hs_clk*$n_lanes/(8*$byte_per_pixel)))
    done
  done

done | sort -nu

If the required frequency is not listed, you can either:

  • check the spec or contact the vendor of the MIPI DSI panel or bridge to identify other pixel clock frequencies allowed;
  • consider using a different frequency for the HSE oscillator.

It is possible to change the value of the variables in the script to dump the pixel clock frequencies for different HSE oscillators. Please also check in ROM code overview the values of HSE oscillator's frequency accepted by the BootROM. By changing the HSE oscillator, the Clock device tree configuration in TF-A and OP-Tee device tree must be aligned too.

83. References[edit source]



84. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the GPU peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

85. Peripheral overview[edit source]

The GPU peripheral is a dedicated graphics processing unit. It accelerates numerous 3D graphics applications such as graphical user interface (GUI), menu display or animations. It works together with an optimized software stack designed for industry-standard APIs and supporting AndroidTM and Linux® embedded development platforms.

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

86. Peripheral usage[edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

86.1. Boot time assignment[edit source]

The GPU peripheral is not used at boot time.

86.2. Runtime assignment[edit source]

86.2.1. On STM32MP15x lines More info.png[edit source]

Click on the right to expand the legend...

STM32MP15 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Visual GPU GPU

87. Software frameworks and drivers[edit source]

Below are listed the software frameworks and drivers managing the GPU peripheral for the embedded software components listed in the above tables.

  • Linux®: OpenGL®ES framework

88. How to assign and configure the peripheral[edit source]

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:

  • partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
  • HAL initialization code generation for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned.

See also additional information in the GPU device tree configuration article for Linux®.

89. How to go further[edit source]

Please go through the articles belonging to the GPU category.


90. References[edit source]