Last edited 4 months ago

STM32MP13 OTP mapping



1. Memory mapping[edit | edit source]

The table below gives an overview of the BSEC OTP memory mapping with useful information in the context of this article/page reading.
OTP words 0 to 31 are called lower OTP and words 32 to 95 are called upper OTP.
Further information for the words and fields that are not explicitly described here can be found in the reference manual.

OTP word Bit field (size) Name Description
0 31-7 (25 bits) reserved
5, 3 (2 bits) is closed
6, 4, 2-0 (5 bits) reserved
1-2 - - See the reference manual
3 31-30 (2 bits) HSE value
29-27 (3 bits) primary boot source
26-24 (3 bits) secondary boot source
23-16 (8 bits) boot source disable If it is different from zero, each bit disables a boot source.
15 (1 bit) data cache disabling
14-7 (8 bits) UART instances boot source disabling If different from zero then each bit disables an UART instance
6 (1 bit) USB DP pullup disabling
5 (1 bit) PLL disabling
4-3 (2 bits) SD card memory interface
2-1 (2 bits) eMMC™ memory interface
0 (1 bit) QSPI non default AFmux
4 31-0 (32 bits) monotonic counter This is an anti rollback monotonic counter. On closed devices, the ROM code checks if it is less or equal to the one stored in the loaded image header.
5 31-28 (4 bits) AFmux configuration - port1[3:0] Bank id
27-24 (4 bits) AFmux configuration - pin1[3:0] Pin id
23-20 (4 bits) AFmux configuration - afmux1[3:0] AFmux value
19-16 (4 bits) AFmux configuration - mode1[3:0] Pin mode
15-12 (4 bits) AFmux configuration - port0[3:0] Bank id
11-8 (4 bits) AFmux configuration - pin0[3:0] Pin id
7-4 (4 bits) AFmux configuration - afmux0[3:0] AFmux value
3-0 (4 bits) AFmux configuration - mode0[3:0] Pin mode
6 31-28 (4 bits) AFmux configuration - port3[3:0] Bank id
27-24 (4 bits) AFmux configuration - pin3[3:0] Pin id
23-20 (4 bits) AFmux configuration - afmux3[3:0] AFmux value
19-16 (4 bits) AFmux configuration - mode3[3:0] Pin mode
15-12 (4 bits) AFmux configuration - port2[3:0] Bank id
11-8 (4 bits) AFmux configuration - pin2[3:0] Pin id
7-4 (4 bits) AFmux configuration - afmux2[3:0] AFmux value
3-0 (4 bits) AFmux configuration - mode2[3:0] Pin mode
7 31-28 (4 bits) AFmux configuration - port5[3:0] Bank id
27-24 (4 bits) AFmux configuration - pin5[3:0] Pin id
23-20 (4 bits) AFmux configuration - afmux5[3:0] AFmux value
19-16 (4 bits) AFmux configuration - mode5[3:0] Pin mode
15-12 (4 bits) AFmux configuration - port4[3:0] Bank id
11-8 (4 bits) AFmux configuration - pin4[3:0] Pin id
7-4 (4 bits) AFmux configuration - afmux4[3:0] AFmux value
3-0 (4 bits) AFmux configuration - mode4[3:0] Pin mode
8 31-0 (32 bits) reserved
9 31 (1 bit) nand param stored in otp FMC NAND parameters storage flag

Notes:

  • serial NAND parameters must always be stored in OTP. This bit is useless for serial NAND.
  • there are two NAND parameters banks. The value of NAND configuration distribution determines the bank to be used.
30-29 (2 bits) nand page size[1:0] FMC or serial NAND page size

Note: this parameter is part of NAND parameters bank1.

28-27 (2 bits) nand block size[1:0] FMC or serial NAND block size

Note: this parameter is part of NAND parameters bank1.

26-19 (8 bits) nand block nb[7:0] FMC or serial NAND number of blocks in unit of 256 blocks (nb blocks = N * 256)
18 (1 bit) fmc nand width FMC NAND width

Note: this parameter is part of NAND parameters bank1.

17-15 (3 bits) fmc ecc bit nb[2:0] FMC NAND number of ECC bits

Note: this parameter is part of NAND parameters bank1.

14 (1 bit) spinand needs plane select Serial NAND needs plane select.

Note: this parameter is part of NAND parameters bank1.

13-8 (6 bits) reserved
7 (1 bit) FSBL decryption priority
6 (1 bit) SSP success
5 (1 bit) SSP request
4 (1 bit) eMMC 128KB boot partition support
3 (1 bit) disable ddr power optim Disable DDR PLL switch off sequence
2 (1 bit) disable HSE bypass detection
1 (1 bit) disable HSE frequency autodetection
0 (1 bit) disable ROM code traces
10 31-21 (11 bits) reserved
20-18 (3 bits) rng hctr value RNG HCTR value
17-16 (2 bits) nand page size[1:0] NAND parameters bank2 : FMC or serial NAND page size
15-14 (2 bits) nand block size[1:0] NAND parameters bank2 : FMC or serial NAND block size
13-6 (8 bits) nand block nb[7:0] NAND parameters bank2 : FMC or serial NAND number of blocks in unit of 256 blocks (nb blocks = N * 256)
5 (1 bit) fmc nand width NAND parameters bank2 : FMC NAND width
4-2 (3 bits) fmc ecc bit nb[2:0] NAND parameters bank2 : FMC NAND number of ECC bits
1 (1 bit) spinand needs plane select NAND parameters bank2 : serial NAND needs plane select.
0 (1 bit) NAND configuration distribution Distribution of NAND parameters bank1 and bank2.
11-21 - - See the reference manual.
22 31-8 (24 bits) reserved
7-0 (8 bits) signing key id monotonic counter This is a key revocation monotonic counter used by the ROM to check if it is less or equal to the active signing key id stored in the loaded image header.
23 - - See the reference manual.
24 31-0 (32 bits) PKHTH1 The Public Key Hashes Table Hash (PKHTH) is the SHA256 hash of the 8 SHA256 hashes of the 8 ECDSA public keys usable for the secure boot.

If hash = 01 02 03 04 05 06 07 08… then PKHTH1 = 0x01020304, PKHTH2 = 0x05060708, etc,…

25 31-0 (32 bits) PKHTH2
26 31-0 (32 bits) PKHTH3
27 31-0 (32 bits) PKHTH4
28 31-0 (32 bits) PKHTH5
29 31-0 (32 bits) PKHTH6
30 31-0 (32 bits) PKHTH7
31 31-0 (32 bits) PKHTH8
32-55 - - See the reference manual.
56 31-0 (32 bits) rma unlock passwd A password is required for RMA unlock request.
57 31-0 mac1[4 first octets] ETH MAC addresses for STMicroelectronics boards, list of octets
58 15-0 mac1[2 last octets]
31-16 mac2[2 first octets]
59 31-0 mac2[4 last octets]
60-91 - - See the reference manual.
92 31-0 (32 bits) EDMK[31:0] The Encryption Decryption Master Key (EDMK) is used in combination with the derivation constant stored in the header file to derive the FSBL decryption key. This key must use Format 1.
93 31-0 (32 bits) EDMK[63:32]
94 31-0 (32 bits) EDMK[95:64]
95 31-0 (32 bits) EDMK[128:96]

1.1. Key storage in OTP[edit | edit source]

Keys are represented as a string of byte to be stored in consecutive OTP words.

For example a 64-bit key (0xAABBCCDDEEFF5566) is stored into two consecutive OTP words KEY0 and KEY1.

A key is stored in OTP words using one of the following formats

Format 1 KEY0 = 0xAABBCCDD, KEY1 = 0xEEFF5566
Format 2 KEY0 = 0xDDCCBBAA, KEY1 = 0x6655FFEE
Format 3 KEY0 = 0xEEFF5566, KEY1 = 0xAABBCCDD