Difference between revisions of "STM32MP135x-DK - software distributions"
[checked revision] | [quality revision] |
m
|
m
|
Applicable for | STM32MP13x lines |
The STM32MP135x-DK Discovery kit (STM32MP135D-DK
and STM32MP135F-DK
) constitutes a flexible and complete solution for evaluating the capabilities of the STM32MP13 STM32MP13x lines
microprocessor devices.
All useful information in order to start with these boards is accessible through links provided here below.
1 Supported software distribution[edit]
Only one software distribution is supported in these boards:
- The STM32MPU Embedded Software distribution[1]. You might also take a look at the latest STM32 MPU ecosystem release note.
For this distribution, three software Packages are delivered : the Starter Package, the Developer Package, the Distribution Package.
Note that the Which Package better suits your needs article provides hints for selecting the most appropriate Package.
The STM32MP135x-DK Discovery kit include the software packages (image, source code) and the tools needed to get started.
![]() |
||
Starter Package | Developer Package | Distribution Package |
|
Note: these developments require a host PC running the OpenSTLinux SDK, and optionally an IDE |
|
2 Hardware description[edit]
A brief article (see link below) describes the board, and provides indications on how to:
- assemble the board
- configure hardware switches
- connect the board to external material
It also contains a short introduction of the board hardware components and connectors.
Board description |
---|
![]() STM32MP135x-DK - hardware description |
3 References[edit]
<noinclude>{{ApplicableFor |MPUs list=STM32MP13x |MPUs checklist=STM32MP13x, STM32MP15x }}</noinclude> The '''{{Board | type=135x-DK}}''' ({{Board | type=135D-DK | name=short}} and {{Board | type=135F-DK | name=short}}) constitutes a flexible and complete solution for evaluating the capabilities of the STM32MP13 {{MicroprocessorDevice | device=13}} microprocessor devices. All useful information in order to start with these boards is accessible through links provided here below. ==Supported software distribution== Only one software distribution is supported in these boards: * The '''STM32MPU Embedded Software distribution'''<ref name="Embedded Software distribution">[[STM32MPU Embedded Software distribution]]</ref>. You might also take a look at the latest [[STM32 MPU ecosystem release note]]. For this distribution, three software Packages are delivered : the '''Starter Package''', the '''Developer Package''', the '''Distribution Package'''.<br> Note that the [[Which Package better suits your needs]] article provides hints for selecting the most appropriate Package. The {{Board | type=135x-DK}} include the '''software packages''' (image, source code) and the '''tools''' needed to get started. {|class="st-table" |- | colspan="3" | [[File:ST_logo.png | 50px |link=]] '''STM32MPU Embedded Software distribution'''<ref name="Embedded Software distribution" /> |- | style="width:30%; text-align:center" | [[STM32MP13 Discovery kits - Starter Package|'''Starter Package''']] | style="width:30%; text-align:center" | [[STM32MP1 Developer Package|'''Developer Package''']] | style="width:30%; text-align:center" | [[STM32MP1 Distribution Package|'''Distribution Package''']] |- | * to evaluate the board capabilities * to run examples | * to modify the pieces of software delivered as source code in this Package (for example the Linux kernel...) * to add custom applications in the user space (delivered as binary in this Package) Note: these developments require a host PC running the OpenSTLinux SDK, and optionally an IDE | * to create custom distribution |} ==Hardware description== A brief article (see link below) describes the board, and provides indications on how to: * assemble the board * configure hardware switches * connect the board to external material It also contains a short introduction of the board hardware components and connectors. {|class="st-table" |- ! '''Board description''' |- style="text-align:center;" | [[File:STM32MP135x-DK.png | 400px | link=STM32MP135x-DK - hardware description|STM32MP135x-DK - hardware description]]<br>[[STM32MP135x-DK - hardware description|'''STM32MP135x-DK - hardware description''']] |} ==References==<references/> <noinclude> {{PublicationRequestId | TBD| TBD | }} [[Category:STM32MP13 Discovery kits|00]]</noinclude>
Line 3: | Line 3: | ||
|MPUs checklist=STM32MP13x, STM32MP15x |
|MPUs checklist=STM32MP13x, STM32MP15x |
||
}}</noinclude> |
}}</noinclude> |
||
− | The '''{{Board | type=135x-DK}}''' ({{Board | type=135F-DK | name=short}}) constitutes a flexible and complete solution for evaluating the capabilities of the |
+ | The '''{{Board | type=135x-DK}}''' ({{Board | type=135D-DK | name=short}} and {{Board | type=135F-DK | name=short}}) constitutes a flexible and complete solution for evaluating the capabilities of the {{MicroprocessorDevice | device=13}} microprocessor devices. |
All useful information in order to start with these boards is accessible through links provided here below. |
All useful information in order to start with these boards is accessible through links provided here below. |