Last edited 3 weeks ago

STM32CubeProgrammer release note: Difference between revisions

Registered User
mNo edit summary
Registered User
Line 7: Line 7:
STM32CubeProgrammer is the '''official''' STMicroelectronics tool '''to download firmware into STMicroelectronics boards'''.  
STM32CubeProgrammer is the '''official''' STMicroelectronics tool '''to download firmware into STMicroelectronics boards'''.  


==STM32CubeProgrammer - Version v2.11.0==
==STM32CubeProgrammer - Version v2.12.0==
<onlyinclude>
<onlyinclude>
{| class="st-table" width=98%
{| class="st-table" width=98%
Line 15: Line 15:
| '''Download'''
| '''Download'''
| colspan="2" |
| colspan="2" |
'''Version v2.11.0'''
'''Version v2.12.0'''
* Browse [https://www.st.com/en/development-tools/stm32cubeprog.html here] link and follow instructions to download the package, you need a myST account.
* Browse [https://www.st.com/en/development-tools/stm32cubeprog.html here] link and follow instructions to download the package, you need a myST account.
* Download the archive file on your host PC in a temporary directory  
* Download the archive file on your host PC in a temporary directory  
Line 28: Line 28:


* Execute the Linux installer, which guides you through the installation process.
* Execute the Linux installer, which guides you through the installation process.
<pre>$> ./SetupSTM32CubeProgrammer-2.11.0.linux</pre>
<pre>$> ./SetupSTM32CubeProgrammer-2.12.0.linux</pre>
* The path to the STM32CubeProgrammer binary must be added to the PATH environment variable
* The path to the STM32CubeProgrammer binary must be added to the PATH environment variable
** either in each Terminal program in which the STM32CubeProgrammer binary needs to be used, using the following command:
** either in each Terminal program in which the STM32CubeProgrammer binary needs to be used, using the following command:

Revision as of 12:12, 17 November 2022

Applicable for STM32MP13x lines, STM32MP15x lines

STM32CubeProgrammer.png

STM32CubeProgrammer is the official STMicroelectronics tool to download firmware into STMicroelectronics boards.

1. STM32CubeProgrammer - Version v2.12.0[edit | edit source]

STM32CubeProgrammer for Linux® host PC STM32CubeProgrammer for Windows® host PC
Download

Version v2.12.0

  • Browse here link and follow instructions to download the package, you need a myST account.
  • Download the archive file on your host PC in a temporary directory
  • Uncompress the archive file to get the STM32CubeProgrammer installers:


unzip en.stm32cubeprog.zip

Installation
  • Execute the Linux installer, which guides you through the installation process.
$> ./SetupSTM32CubeProgrammer-2.12.0.linux
  • The path to the STM32CubeProgrammer binary must be added to the PATH environment variable
    • either in each Terminal program in which the STM32CubeProgrammer binary needs to be used, using the following command:
$> export PATH=<my STM32CubeProgrammer install directory>/bin:$PATH
  • or once for all by creating a link to the STM32CubeProgrammer binary in a directory already present in PATH. For example, if "/home/bin" is in the PATH environment variable, run the following command:
$> ln -s <my STM32CubeProgrammer install directory>/bin/STM32_Programmer_CLI /home/bin/STM32_Programmer_CLI
  • Execute the Windows installer, which guides you through the installation process.
User manual
Detailed release note
  • Details about the content of this tool version are available from ST web site at Release Note .