Last edited 3 weeks ago

STM32CubeProgrammer release note: Difference between revisions


Latest revision as of 17:54, 3 July 2025


STM32CubeProgrammer.png STM32CubeProgrammer is the official STMicroelectronics tool to download firmware into STMicroelectronics boards.

1. STM32CubeProgrammer - Version v2.20.0 - STM32 MPU support[edit | edit source]

1.1. Main changes coming with new release[edit | edit source]

  • Support of STM32MP21x lines More info.png,
  • Support STPMIC2L and SPMIC1L for PMIC NVM programming via GUI (using STM32PRGFW-UTIL firmware binary on target),

1.2. Features already supported in previous releases[edit | edit source]

  • Support of STM32MP13x lines More info.png,
  • Support of STM32MP15x lines More info.png,
  • Support of STM32MP25x lines More info.png,
  • Support of STM32MP23x lines More info.png,
  • Hash of (RoT Public Keys + Algorithm) hashes (256 bits, ROTPK) generation with KeyGen tool,
  • TF-A BL2 binary signature with stm32header V2.2 with Signing tool for STM32MP25 Rev Y,
  • FSBL encryption with Signing tool,
  • Signing services with PKCS#11,
  • OTP programming via CLI/GUI (using STM32PRGFW-UTIL firmware binary on target),
  • STM32TrustedPackageCreator : Secrets and Backup generation for SSP.
  • PMIC NVM programming via CLI/GUI (using STM32PRGFW-UTIL firmware binary on target),
  • Support of STM32CubeMP13 firmware flashing,
  • STM32CubeProg installer including STM32CubeProgrammer, Keygen and Signing tools,
  • Flash programming of SD card, eMMC, NAND, NOR images through USB and UART,
  • Private and public key generation,
  • Image signatures,
  • OTP fuse management (with console and graphical interfaces),
  • PMIC NVM management).

1.3. Main restrictions[edit | edit source]

  • None

2. How to get STM32CubeProgrammer[edit | edit source]

STM32CubeProgrammer for Linux® host PC STM32CubeProgrammer for Windows® host PC
Download
  • Go on st.com to download the STM32CubeProgrammer software

Version v2.20.0

  • Download the archive file on your host PC in a temporary directory
  • Uncompress the archive file to get the STM32CubeProgrammer installers:

PC $>unzip en.stm32cubeprog.zip

Installation
  • Execute the Linux installer, which guides you through the installation process.
$> ./SetupSTM32CubeProgrammer-2.20.0.linux
  • The path to the STM32CubeProgrammer binary must be added to the PATH environment variable
    • either in each Terminal program in which the STM32CubeProgrammer binary needs to be used, using the following command:
$> export PATH=<my STM32CubeProgrammer install directory>/bin:$PATH
  • or once for all by creating a link to the STM32CubeProgrammer binary in a directory already present in PATH. For example, if "/home/bin" is in the PATH environment variable, run the following command:
$> ln -s <my STM32CubeProgrammer install directory>/bin/STM32_Programmer_CLI /home/bin/STM32_Programmer_CLI
  • Execute the Windows installer, which guides you through the installation process.
User manual
Detailed release note
  • Details about the content of this tool version are available from ST web site at Release Note .