Difference between revisions of "SAI device tree configuration"

[unchecked revision] [quality revision]
m
m (DT configuration)
Applicable for STM32MP13x lines, STM32MP15x lines

1 Article purpose[edit]

This article explains how to configure the SAI internal peripheral when it is assigned to the Linux® OS. In that case, it is controlled by the ALSA framework.

The configuration is performed using the device tree mechanism that provides a hardware description of the SAI peripheral, used by the SAI linux driver.

If the peripheral is assigned to another execution context, refer to How to assign an internal peripheral to a runtime context article for guidelines on peripheral assignment and configuration.

2 DT bindings documentation[edit]

STM32 SAI device tree bindings [1] document describes all the required and optional configuration properties.

3 DT configuration[edit]

This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split.
The SAI is used as a component of a sound card through Linux® kernel ALSA framework. The device tree nodes related to the sound card are described in board device tree.

The STM32 SAI peripheral includes two independent audio subblocks that share common resources. The SAI device tree nodes reflects this architecture, as shown in the SAI DT sample below.

Clock overview Pinctrl overview
SAI device tree configuration

Two parent clocks referred as "x8k" and "x11k", has to be declared for the SAI kernel clock:

  • The "x8k" clock must be a multiple of 8kHz
  • The "x11k" clock must be a multiple of 11.025kHz

Depending on the audio stream sampling rate, the SAI driver selects at runtime the relevant parent clock.

Warning white.png Warning
This peripheral kernel clock is shared by the two SAI sub-blocks, which involves that these two sub-blocks have to run with compatible sampling rates, when they are active at the same time.
Info white.png Information
The parent clock may not be exactly a multiple of the audio stream rate. A debug trace can be enabled in the SAI Linux driver, to report the clock rate accuracy. A deviation of 1000 ppm, on the audio stream frequency, might be considered acceptable for most people.
&saix {
	/* SAIx parent node. Configure common ressources  */
	clock-names = "pclk", "x8k", "x11k"; /* Peripheral and parent clock configuration.  */
	... 

	saixa {
		/* child node. Configure ressources dedicated to SAIxA subblock */
		clock-names = "sai_ck"; /* SAIxA kernel clock confguration.  */
		pinctrl-names = "default"; /* GPIOsA configuration.  */
		... 
	};

	saixb {
		/* child node. Configure ressources dedicated to SAIxB subblock */
		clock-names = "sai_ck"; /* SAIxB kernel clock confguration.  */
		pinctrl-names = "default"; /* GPIOsB configuration.  */
		...
	};
};

The STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.

3.1 DT configuration (STM32 level)[edit]

The SAI nodes are declared in STM32 microprocessor device tree. They describe hardware parameters such as registers address, interrupt and DMA. This set of properties may not vary for a given STM32MPU. For STM32MP1, the corresponding DT file is stm32mp151.dtsi[2].

Warning white.png Warning
This device tree part is related to STM32 microprocessors. It should be kept as is, without being modified by the end-user.

3.2 DT configuration (board level)[edit]

The SAI configuration is board dependent, whether is it connected or not to an external component such as an audio codec. The links between the SAI and the other components define a soundcard. This soundcard has to be configured in the board device tree. Refer to soundcard configuration for examples of SAI configuration on various STM32MPU boards.

3.3 DT configuration examples[edit]

This chapter describes in details advanced SAI configurations. These examples are based on STM32MP1 boards SAI use cases. The corresponding device trees can be found in soundcard article.

Info white.png Information
In this chapter, "SAI" stands for an SAI subblock, SAIxA or SAIxB.

3.3.1 Setting SAI as a master clock provider[edit]

The SAI peripheral can provide a clock to an external component (such as a codec) through the mclk output pin. In this case, it acts as master clock (mclk) provider. The below DT sample gives an example of SAI configuration as mclk provider.

In this example the codec driver supports mclk input based on ASoC DAPM mechanism. If this is not the case, the codec driver has to be adapted. This can be achieved by adding a DAPM clock supply widget to the codec driver. An example of the required DAPM clock supply widget can be found in Cirrus CS42L51 codec source code[3]. In the below device tree example, the codec DAPM clock widget is named "MCLKX".

To allow mclk activation/deactivation, a DAPM route must be defined in the DT. This route is defined in the sound node, as shown below.

soundcard {
	routing =
		"Playback" , "MCLKX", /* Set a route between "MCLKX" and "playback" widgets */
		"Capture" , "MCLKX";
	...
};

codec: {
	clocks = <&sai2a>;     /* The codec is a consumer of SAI2A master clock */
	clock-names = "MCLKX"; /* Feed MCLKX codec clock with SAI2A master clock provider */
	...
};

&sai2 {
	...
		
	sai2a: audio-controller@4400b004 {
		#clock-cells = <0>; /* Set SAI2A as master clock provider */
		...
		sai2a_endpoint: endpoint {
			mclk-fs = <256>; /* Set mclk/fs ratio. (256 or 512) */
		};
	};
};

3.3.2 Sharing master clock between two SAIs[edit]

When an SAI is set as a master clock provider, another SAI can share this master clock. This can be achieved by setting the SAI as a mclk consumer through DT configuration. This means that the mclk consumer SAI can request to change the mclk rate, according to its own audio stream sampling rate. This implies that audio sampling rates must be identical when both SAI subblocks are used.

&sai2 {
	...
		
	sai2a: audio-controller@4400b004 {
		#clock-cells = <0>; /* Set SAI2A as master clock provider */
		...
	};

	sai2b: audio-controller@4400b024 {
		clocks = <&rcc SAI2_K>, <&sai2a>; /* SAI2B is a consumer of SAI2A master clock */
		clock-names = "sai_ck", "MCLK";   /* Feed SAI2B MCLK clock with SAI2A master clock provider */
		...
		sai2b_endpoint: endpoint {
			mclk-fs = <256>; /* Set mclk/fs ratio. (256 or 512) */
		};
	};
};

3.3.3 Sharing the codec interface between two SAIs[edit]

Two SAIs can be connected to the same codec interface, by sharing the I2S bus (i.e. FS and SCK clocks).

SAIs sharing the same codec interface

In such case:

  • The codec has to be master on the I2S bus.
  • Only one SAI is connected to the bus clocks. The other SAI has to be configured as a slave of the SAI connected to the bus.
  • The I2S bus I/O pins must be managed at parent level, so that the corresponding pins are activated whatever the running SAI.

From ASoC point of view:
Two CPU DAIs have to be connected to the same codec DAI. Such topology is not supported natively by the ASoC audio graph card. Indeed, when the audio graph card parses the codec nodes, it expects to find DAI interface indexes, matching the endpoints indexes. A workaround consists in implementing the of_xlate_dai_id callback in the codec driver, to allow using the same DAI interface for both endpoints. An example of code can be found below or in the Cirrus CS42L51 codec source code[3].

  • Code example
static int codec_of_xlate_dai_id(struct snd_soc_component *component,
				   struct device_node *endpoint)
{
	/* return dai id 0, whatever the endpoint index */
	return 0;
}

  • DT example
codec {
	...
	codec_port {
		codec_tx_endpoint {
			remote-endpoint = <&sai2a_endpoint>;
			frame-master;    /* Set codec as master of SAI2A for FS clock. */
			bitclock-master; /* Set codec as master of SAI2A for SCK clock. */
		};

		codec_rx_endpoint { /* Second endpoint mapped on codec DAI 0 via of_xlate */
			remote-endpoint = <&sai2b_endpoint>;
			frame-master;    /* Set codec as master of SAI2B for FS clock. */
			bitclock-master; /* Set codec as master of SAI2B for SCK clock. */
		};
	};
};

&sai2 {
	pinctrl-names = "default", "sleep"; /* Defines SAI2A/B GPIOs at parent level. */
	pinctrl-0 = <&sai2a_pins_a>, <&sai2b_pins_b>;
	pinctrl-1 = <&sai2a_sleep_pins_a>, <&sai2b_sleep_pins_b>;
	...

	sai2a: audio-controller@4400b004 {
		remote-endpoint = <&codec_tx_endpoint>;
		...
	};

	sai2b: audio-controller@4400b024 {
		remote-endpoint = <&codec_rx_endpoint>;
		st,sync = <&sai2a 2>; /* Set SAI2B as slave of SAI2A. */
	};
};

4 How to configure the DT using STM32CubeMX[edit]

The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.

Warning white.png Warning
STM32CubeMX does not allow the generation of all the nodes required to configure a soundcard.

The following nodes have to be filled manually through user sections :

  • soundcard node
  • codec node
  • The SAI node is not fully filled and has to be updated manually. The clock muxings, in STM32CubeMX clock tree panel, allows to configure a single parent clock for the SAI internal peripheral. However, for the SAI peripheral, the device tree has to define two parent clocks "x8k" and "x11k", allowing the SAI Linux driver to choose dynamically the most appropriated clock at runtime. Refer to the SAI device tree bindings [1] and to the SAI driver description for further information.

5 References[edit]



<noinclude>{{ApplicableFor
|MPUs list=STM32MP13x, STM32MP15x
|MPUs checklist=STM32MP13x,STM32MP15x
}}</noinclude>

== Article purpose ==
This article explains how to configure the [[SAI internal peripheral]] when it is assigned to the '''Linux<sup>&reg;</sup> OS'''. In that case, it is controlled by the [[ALSA_overview|ALSA framework]].

The configuration is performed using the [[Device_tree|device tree]] mechanism that provides a hardware description of the SAI peripheral, used by the [[SAI_Linux_driver|SAI linux driver]].

If the peripheral is assigned to another execution context, refer to [[How to assign an internal peripheral to a runtime context]] article for guidelines on peripheral assignment and configuration.

== DT bindings documentation ==
STM32 SAI device tree bindings <ref name="sai bindings">{{CodeSource | Linux kernel | Documentation/devicetree/bindings/sound/st,stm32-sai.yaml}}</ref> document describes all the required and optional configuration properties. 

== DT configuration =={{ReviewsComments|-- [[User:Arnaud Pouliquen|Arnaud Pouliquen]] ([[User talk:Arnaud Pouliquen|talk]]) 16:44, 27 January 2022 (CET)<br />the Cube MX clock panel does not allow to set the "x8k" and "x11k" clock rate but only a static clock tree. need to:
* Add details about  the "x8k", "x11k" usage
* Mention that a debug trace exists in driver to have information about rate accuracy: 	"Rate not accurate. requested (%ld), actual (%ld)\n"
* add info message : "for information only: an error of 100 ppm on the audio frequency is acceptable for most people, some human ears can detect a error of +/-600 ppm."
* mention cubeMX clock set limitation vs audio dynamic clocking need.
}}

{{ReviewsComments | [[User:Olivier Moysan|Olivier Moysan]] ([[User talk:Olivier Moysan|talk]]) 11:55, 19 May 2022 (CEST) - infos added in both SAI DT & driver articles. Same as I2S. }}
This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device tree file split.<br>

The SAI is used as a component of a sound card through Linux<sup>&reg;</sup> kernel ALSA framework. The device tree nodes related to the sound card are described in [[#DT_configuration_.28board_level.29|board device tree]].

The STM32 SAI peripheral includes two independent audio subblocks that share common resources.
The SAI device tree nodes reflects this architecture, as shown in the SAI DT sample below.
{{
ImageMap|
Image:Sai_configuration.png {{!}} frame {{!}} center{{!}} SAI device tree configuration
rect 2 138 164 421 [[Clock_overview]]
rect 653 230 799 420 [[Pinctrl_overview]]
}}

Two parent clocks referred as "x8k" and "x11k", has to be declared for the SAI kernel clock:
*  The  "x8k" clock  must be a multiple of 8kHz
* The "x11k"  clock  must be a multiple of  11.025kHz
Depending on the audio stream sampling rate, the SAI driver selects at runtime the relevant parent clock.

{{warning| This peripheral kernel clock is shared by the two SAI sub-blocks, which involves that these two sub-blocks have to run with compatible sampling rates, when they are active at the same time.}}

{{Info| The parent clock may not be exactly a multiple of the audio stream rate. A [[ALSA_overview#Dynamic_traces | debug trace]] can be enabled in the SAI Linux driver, to report the clock rate accuracy.  A deviation of 1000 ppm, on the audio stream frequency, might be considered acceptable for most people.}}

 &saix {
 	{{highlight|/* SAIx parent node. Configure common ressources  */}}
 	clock-names = "pclk", "x8k", "x11k"; {{highlight|/* Peripheral and parent clock configuration.  */}}
 	... 

 	saixa {
 		{{highlight|/* child node. Configure ressources dedicated to SAIxA subblock */}}
 		clock-names = "sai_ck"; {{highlight|/* SAIxA kernel clock confguration.  */}}
 		pinctrl-names = "default"; {{highlight|/* GPIOsA configuration.  */}}
 		... 
 	};

 	saixb {
 		{{highlight|/* child node. Configure ressources dedicated to SAIxB subblock */}}
 		clock-names = "sai_ck"; {{highlight|/* SAIxB kernel clock confguration.  */}}
 		pinctrl-names = "default"; {{highlight|/* GPIOsB configuration.  */}}
 		...
 	};
 };

The '''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details.

=== DT configuration (STM32 level) ===
The SAI nodes are declared in STM32 microprocessor device tree. They describe hardware parameters such as registers address, interrupt and DMA. This set of properties may not vary for a given STM32MPU. For STM32MP1, the corresponding DT file is stm32mp151.dtsi<ref name="stm32mp151.dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp151.dtsi}}</ref>.
{{Warning|This device tree part is related to STM32 microprocessors. It should be kept as is, without being modified by the end-user.}}

=== DT configuration (board level) ===

The SAI configuration is board dependent, whether is it connected or not to an external component such as an audio codec. The links between the SAI and the other components define a soundcard. This soundcard has to be configured in the board device tree. Refer to [[Soundcard configuration|soundcard configuration]] for examples of SAI configuration on various STM32MPU boards.

=== DT configuration examples ===

This chapter describes in details advanced SAI configurations. These examples are based on [[:Category:Getting_started_with_STM32MP1_boards|STM32MP1 boards]] SAI use cases. The corresponding device trees can be found in [[Soundcard configuration|soundcard]] article.
{{Info|In this chapter, "SAI" stands for an SAI subblock, SAIxA or SAIxB.}}

==== Setting SAI as a master clock provider ====
The SAI peripheral can provide a clock to an external component (such as a codec) through the mclk output pin. In this case, it acts as master clock (mclk) provider. The below DT sample gives an example of SAI configuration as mclk provider.

In this example the codec driver supports mclk input based on ASoC DAPM mechanism.
If this is not the case, the codec driver has to be adapted. This can be achieved by adding a DAPM clock supply widget to the codec driver. An example of the required DAPM clock supply widget can be found in Cirrus CS42L51 codec source code<ref name="CS42L51 code">{{CodeSource | Linux kernel | sound/soc/codecs/cs42l51.c}}</ref>.
In the below device tree example, the codec DAPM clock widget is named "MCLKX". 

To allow mclk activation/deactivation, a DAPM route must be defined in the DT. This route is defined in the sound node, as shown below.

 soundcard {
 	routing =
 		"Playback" , "MCLKX", {{highlight|/* Set a route between "MCLKX" and "playback" widgets */}}
 		"Capture" , "MCLKX";
 	...
 };

 codec: {
 	clocks = <&sai2a>;     {{highlight|/* The codec is a consumer of SAI2A master clock */}}
 	clock-names = "MCLKX"; {{highlight|/* Feed MCLKX codec clock with SAI2A master clock provider */}}
 	...
 };

 &sai2 {
 	...

 	sai2a: audio-controller@4400b004 {
 		#clock-cells = <0>; {{highlight|/* Set SAI2A as master clock provider */}}
 		...
 		sai2a_endpoint: endpoint {
 			mclk-fs = <256>; {{highlight|/* Set mclk/fs ratio. (256 or 512) */}}
 		};
 	};
 };

==== Sharing master clock between two SAIs ====

When an SAI is set as a master clock provider, another SAI can share this master clock.
This can be achieved by setting the SAI as a mclk consumer through DT configuration.
This means that the mclk consumer SAI can request to change the mclk rate, according to its own audio stream sampling rate.
This implies that audio sampling rates must be identical when both SAI subblocks are used.

 &sai2 {
 	...

 	sai2a: audio-controller@4400b004 {
 		#clock-cells = <0>; {{highlight|/* Set SAI2A as master clock provider */}}
 		...
 	};

 	sai2b: audio-controller@4400b024 {
 		clocks = <&rcc SAI2_K>, <&sai2a>; {{highlight|/* SAI2B is a consumer of SAI2A master clock */}}
 		clock-names = "sai_ck", "MCLK";   {{highlight|/* Feed SAI2B MCLK clock with SAI2A master clock provider */}}
 		...
 		sai2b_endpoint: endpoint {
 			mclk-fs = <256>; {{highlight|/* Set mclk/fs ratio. (256 or 512) */}}
 		};
 	};
 };

==== Sharing the codec interface between two SAIs ====

Two SAIs can be connected to the same codec interface, by sharing the I2S bus (i.e. FS and SCK clocks). 

[[Image:sai_shared_codec.png {{!}} frame {{!}} center{{!}} SAIs sharing the same codec interface|link=]]

In such case:
*The codec has to be master on the I2S bus. 
*Only one SAI is connected to the bus clocks. The other SAI has to be configured as a slave of the SAI connected to the bus.
*The I2S bus I/O pins must be managed at parent level, so that the corresponding pins are activated whatever the running SAI.

From ASoC point of view:<BR>

Two CPU DAIs have to be connected to the same codec DAI. Such topology is not supported natively by the ASoC audio graph card. Indeed, when the audio graph card parses the codec nodes, it expects to find DAI interface indexes, matching the endpoints indexes. A workaround consists in implementing the of_xlate_dai_id callback in the codec driver, to allow using the same DAI interface for both endpoints. An example of code can be found below or in the Cirrus CS42L51 codec source code<ref name="CS42L51 code">{{CodeSource | Linux kernel | sound/soc/codecs/cs42l51.c}}</ref>.

* Code example
<syntaxhighlight lang="c">

static int codec_of_xlate_dai_id(struct snd_soc_component *component,
				   struct device_node *endpoint)
{
	/* return dai id 0, whatever the endpoint index */
	return 0;
}</syntaxhighlight>


* DT example

 codec {
 	...
 	codec_port {
 		codec_tx_endpoint {
 			remote-endpoint = <&sai2a_endpoint>;
 			frame-master;    {{highlight|/* Set codec as master of SAI2A for FS clock. */}}
 			bitclock-master; {{highlight|/* Set codec as master of SAI2A for SCK clock. */}}
 		};

 		codec_rx_endpoint { {{highlight|/* Second endpoint mapped on codec DAI 0 via of_xlate */}}
 			remote-endpoint = <&sai2b_endpoint>;
 			frame-master;    {{highlight|/* Set codec as master of SAI2B for FS clock. */}}
 			bitclock-master; {{highlight|/* Set codec as master of SAI2B for SCK clock. */}}
 		};
 	};
 };

 &sai2 {
 	pinctrl-names = "default", "sleep"; {{highlight|/* Defines SAI2A/B GPIOs at parent level. */}}
 	pinctrl-0 = <&sai2a_pins_a>, <&sai2b_pins_b>;
 	pinctrl-1 = <&sai2a_sleep_pins_a>, <&sai2b_sleep_pins_b>;
 	...

 	sai2a: audio-controller@4400b004 {
 		remote-endpoint = <&codec_tx_endpoint>;
 		...
 	};

 	sai2b: audio-controller@4400b024 {
 		remote-endpoint = <&codec_rx_endpoint>;
 		st,sync = <&sai2a 2>; {{highlight|/* Set SAI2B as slave of SAI2A. */}}
 	};
 };

==How to configure the DT using STM32CubeMX==
The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32|platform configuration device tree]] files.<br />

The STM32CubeMX may not support all the properties described in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information.

{{Warning|STM32CubeMX does not allow the generation of all the nodes required to configure a soundcard.
The following nodes have to be filled manually through user sections :
* soundcard node
* codec node
* The SAI node is not fully filled and has to be updated manually. The clock muxings, in STM32CubeMX clock tree panel, allows to configure a single parent clock for the SAI internal peripheral. However, for the SAI peripheral, the device tree has to define two parent clocks "x8k" and "x11k", allowing the [[SAI Linux driver]] to choose dynamically the most appropriated clock at runtime. Refer to the SAI device tree bindings <ref name="sai bindings">{{CodeSource | Linux kernel | Documentation/devicetree/bindings/sound/st,stm32-sai.yaml}}</ref> and to the [[SAI Linux driver#Short_Description | SAI driver description]] for further information.
}}

==References==<references />

<noinclude>

{{ArticleBasedOnModel | Peripheral or framework device tree configuration model}}
{{PublicationRequestId | 14728 | 2020-01-28 | AnneJ (9809)}}

[[Category:Device tree configuration]]
[[Category:ALSA]]</noinclude>
Line 14: Line 14:
   
 
== DT configuration ==
 
== DT configuration ==
{{ReviewsComments|-- [[User:Arnaud Pouliquen|Arnaud Pouliquen]] ([[User talk:Arnaud Pouliquen|talk]]) 16:44, 27 January 2022 (CET)<br />the Cube MX clock panel does not allow to set the "x8k" and "x11k" clock rate but only a static clock tree. need to:
 
* Add details about  the "x8k", "x11k" usage
 
* Mention that a debug trace exists in driver to have information about rate accuracy: "Rate not accurate. requested (%ld), actual (%ld)\n"
 
* add info message : "for information only: an error of 100 ppm on the audio frequency is acceptable for most people, some human ears can detect a error of +/-600 ppm."
 
* mention cubeMX clock set limitation vs audio dynamic clocking need.
 
}}
 
 
{{ReviewsComments | [[User:Olivier Moysan|Olivier Moysan]] ([[User talk:Olivier Moysan|talk]]) 11:55, 19 May 2022 (CEST) - infos added in both SAI DT & driver articles. Same as I2S. }}
 
 
 
This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device tree file split.<br>
 
This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device tree file split.<br>
 
The SAI is used as a component of a sound card through Linux<sup>&reg;</sup> kernel ALSA framework. The device tree nodes related to the sound card are described in [[#DT_configuration_.28board_level.29|board device tree]].
 
The SAI is used as a component of a sound card through Linux<sup>&reg;</sup> kernel ALSA framework. The device tree nodes related to the sound card are described in [[#DT_configuration_.28board_level.29|board device tree]].