Registered User m (→Apt) |
Registered User m (Add warning to explain errors that may occurs with stm32mp13 boards) |
||
(25 intermediate revisions by 4 users not shown) | |||
Line 1: | Line 1: | ||
{{ApplicableFor | |||
|MPUs list=STM32MP13x, STM32MP15x | |||
|MPUs checklist=STM32MP13x, STM32MP15x | |||
}} | |||
<noinclude> | |||
</noinclude> | |||
==Disclaimers== | ==Disclaimers== | ||
STMicroelectronics packages repository service is provided for evaluation purpose only, and therefore not approved for use in production.<br/> | STMicroelectronics packages repository service is provided for evaluation purpose only, and therefore not approved for use in production.<br/> | ||
Line 6: | Line 13: | ||
===Description=== | ===Description=== | ||
OpenSTLinux provides a package repository service hosted at the non-browsable URL <nowiki>http://packages.openstlinux.st.com</nowiki>. | OpenSTLinux provides a package repository service hosted at the non-browsable URL <nowiki>http://packages.openstlinux.st.com</nowiki>. | ||
The package repository service is designed for ''{{Board | type=157x-DKx | name=short}}'', ''{{Board | type=157x-EV1 | name=short}}'' and {{Board | type=135F-DK | name=short}} boards and is enabled by default in the [[:Category:Starter_Package|Starter Package]]. | |||
{{Warning| Some packages provided in the OpenSTLinux distribution can't be installed or run onto the {{Board | type=135F-DK | name=short}} board. This mainly concerns graphical and related packages because of hardware technical characteristics which differ from ''{{Board | type=157x-DKx | name=short}}'' and ''{{Board | type=157x-EV1 | name=short}}'' boards.}} | |||
===Organization=== | ===Organization=== | ||
Within each repository, packages are organized in | Within each repository, packages are organized in three groups (a.k.a ''components'' in the APT terminology): | ||
* the '''main''' group contains a wide selection of packages whose installation is automatically tested by STMicroelectronics | * the '''main''' group contains a wide selection of packages whose installation is automatically tested by STMicroelectronics | ||
* the '''untested''' group contains all the other packages that can be built using the <code>bitbake world</code> command. However their installation is not guaranteed. | * the '''untested''' group contains all the other packages that can be built using the <code>bitbake world</code> command. However their installation is not guaranteed. | ||
* the '''updates''' group contains additional packages not included in the [[OpenSTLinux_distribution|OpenSTLinux distribution releases]] and updated packages. This group is managed by a dedicated layer available through github®. Further details are available by following the github® link: https://github.com/STMicroelectronics/meta-st-pkgrepo-updates. | |||
===Limitations=== | ===Limitations=== | ||
Packages repository service doesn't include the packages that are shipped in the rootfs image, nor the BSP components (TF-A, U-Boot, Linux and OP-TEE). They | Packages repository service doesn't include the packages that are shipped in the rootfs image, nor the BSP components (TF-A, U-Boot, Linux and OP-TEE). They can be installed only from the [[:Category:Starter_Package|Starter Package]] using the [[STM32CubeProgrammer]]. | ||
''rootfs'' available space is about 60MB by default. For a better experience it is recommended to [[STM32CubeProgrammer#How_to_flash_with_STM32CubeProgrammer|flash]] the [[ | ''rootfs'' available space is about 60MB by default. For a better experience it is recommended to [[STM32CubeProgrammer#How_to_flash_with_STM32CubeProgrammer|flash]] the [[:Category:Starter_Package|Starter Package]] using the "extensible" flashlayout (''*-extensible.tsv'').<br/> | ||
{{Grey|'''''Extensible flashlayout''''' does not flash userfs partition to extend the rootfs partition to the size of the sdcard.}} | {{Grey|'''''Extensible flashlayout''''' does not flash userfs partition to extend the rootfs partition to the size of the sdcard.}} | ||
==Usage== | ==Usage== | ||
Line 44: | Line 49: | ||
<nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. | <nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. | ||
Get:1 <nowiki>http://packages.openstlinux.st.com/ | Get:1 <nowiki>http://packages.openstlinux.st.com/4.0</nowiki> dunfell InRelease [3459 B] | ||
Get:2 <nowiki>http://packages.openstlinux.st.com/ | Get:2 <nowiki>http://packages.openstlinux.st.com/4.0</nowiki> dunfell/main armhf Packages [682kB] | ||
Get:3 <nowiki>http://packages.openstlinux.st.com/ | Get:3 <nowiki>http://packages.openstlinux.st.com/4.0</nowiki> dunfell/updates armhf Packages [64.2kB] | ||
Get:4 <nowiki>http://packages.openstlinux.st.com/ | Get:4 <nowiki>http://packages.openstlinux.st.com/4.0</nowiki> dunfell/untested armhf Packages [1223kB] | ||
Fetched | Fetched 1973 kB in 3s (626 kB/s) | ||
Reading package lists... Done | Reading package lists... Done | ||
Line 58: | Line 63: | ||
acl - Utilities for managing POSIX Access Control Lists | acl - Utilities for managing POSIX Access Control Lists | ||
... | ... | ||
xkeyboard-config - Keyboard configuration database for X Window | |||
xxhash - Extremely fast non-cryptographic hash algorithm | |||
xz - Utilities for managing LZMA compressed files | xz - Utilities for managing LZMA compressed files | ||
Line 68: | Line 71: | ||
{{Board$}} apt-cache search emacs | {{Board$}} apt-cache search emacs | ||
libreadline-doc - Library for editing typed command lines - Documentation files | libreadline-doc - Library for editing typed command lines - Documentation files | ||
libreadline-src - Library for editing typed command lines - Source files | |||
emacs-base - Emacs is the extensible, customizable, self-documenting real-time display editor | |||
emacs-doc - Emacs is the extensible, customizable, self-documenting real-time display editor - Documentation files | |||
emacs-full - Emacs is the extensible, customizable, self-documenting real-time display editor | |||
emacs-minimal - Emacs is the extensible, customizable, self-documenting real-time display editor | |||
gpm - Console mouse driver | gpm - Console mouse driver | ||
gpm-doc - Console mouse driver - Documentation files | gpm-doc - Console mouse driver - Documentation files | ||
Line 84: | Line 92: | ||
The following NEW packages will be installed: | The following NEW packages will be installed: | ||
bdwgc zile | bdwgc zile | ||
0 upgraded, 2 newly installed, 0 to remove and | 0 upgraded, 2 newly installed, 0 to remove and 3 not upgraded. | ||
Need to get | Need to get 150 kB of archives. | ||
After this operation, 0 B of additional disk space will be used. | After this operation, 0 B of additional disk space will be used. | ||
Do you want to continue? [Y/n] | Do you want to continue? [Y/n] | ||
Get:1 <nowiki>http://packages.openstlinux.st.com/ | Get:1 <nowiki>http://packages.openstlinux.st.com/4.0</nowiki> dunfell/untested armhf bdwgc armhf 8.2.0-r0 [70.9 kB] | ||
Get:2 <nowiki>http://packages.openstlinux.st.com/ | Get:2 <nowiki>http://packages.openstlinux.st.com/4.0</nowiki> dunfell/untested armhf zile armhf 2.4.15-r0 [79.1 kB] | ||
Fetched | Fetched 150 kB in 1s (287 kB/s) | ||
The software package is provided AS IS, and by downloading it, you agree to be | The software package is provided AS IS, and by downloading it, you agree to be | ||
Line 98: | Line 106: | ||
Selecting previously unselected package bdwgc. | Selecting previously unselected package bdwgc. | ||
(Reading database ... | (Reading database ... 14860 files and directories currently installed.) | ||
Preparing to unpack .../bdwgc_8.0 | Preparing to unpack .../bdwgc_8.2.0-r0_armhf.deb ... | ||
Unpacking bdwgc (8.0 | Unpacking bdwgc (8.2.0-r0) ... | ||
Selecting previously unselected package zile. | Selecting previously unselected package zile. | ||
Preparing to unpack .../zile_2.4. | Preparing to unpack .../zile_2.4.15-r0_armhf.deb ... | ||
Unpacking zile (2.4. | Unpacking zile (2.4.15-r0) ... | ||
Setting up bdwgc (8.0 | Setting up bdwgc (8.2.0-r0) ... | ||
Setting up zile (2.4. | Setting up zile (2.4.15-r0) ... | ||
... or removed: | ... or removed: | ||
Line 118: | Line 126: | ||
The following packages will be REMOVED: | The following packages will be REMOVED: | ||
zile | zile | ||
0 upgraded, 0 newly installed, 1 to remove and | 0 upgraded, 0 newly installed, 1 to remove and 3 not upgraded. | ||
After this operation, 0 B of additional disk space will be used. | After this operation, 0 B of additional disk space will be used. | ||
Do you want to continue? [Y/n] | Do you want to continue? [Y/n] | ||
Line 127: | Line 135: | ||
<nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. | <nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. | ||
(Reading database ... | (Reading database ... 14865 files and directories currently installed.) | ||
Removing zile (2.4. | Removing zile (2.4.15-r0) ... | ||
Line 143: | Line 151: | ||
The following packages will be REMOVED: | The following packages will be REMOVED: | ||
bdwgc | bdwgc | ||
0 upgraded, 0 newly installed, 1 to remove and | 0 upgraded, 0 newly installed, 1 to remove and 3 not upgraded. | ||
After this operation, 0 B of additional disk space will be used. | After this operation, 0 B of additional disk space will be used. | ||
Do you want to continue? [Y/n] | Do you want to continue? [Y/n] | ||
Line 152: | Line 160: | ||
<nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. | <nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. | ||
(Reading database ... | (Reading database ... 14864 files and directories currently installed.) | ||
Removing bdwgc (8.0 | Removing bdwgc (8.2.0-r0) ... | ||
== How to activate a local package repository == | == How to activate a local package repository == | ||
===Prerequisite=== | ===Prerequisite=== | ||
Even if ''Package repository for OpenSTLinux'' offers lots of and various packages, you may need to use a local and personnal package repository. | Even if ''Package repository for OpenSTLinux'' offers lots of and various packages, you may need to use a local and personnal package repository. Using a local and personal package repository is a 'smart' and 'quick' way to update the [[:Category:Starter_Package|Starter Package]] with your developments. | ||
A local package repository is a collection of *.deb organized such <code>apt</code> needs it. The local repository should provide ''Packages'' metafiles. | A local package repository is a collection of *.deb organized such <code>apt</code> needs it. The local repository should provide ''Packages'' metafiles. | ||
Line 183: | Line 191: | ||
{{Board$}} echo "deb [trusted=yes] http://<IP>:8000/all /" >> /etc/apt/sources.list.d/my_custom.list | {{Board$}} echo "deb [trusted=yes] http://<IP>:8000/all /" >> /etc/apt/sources.list.d/my_custom.list | ||
{{Board$}} echo "deb [trusted=yes] http://<IP>:8000/cortexa7t2hf-neon-vfpv4 /" >> /etc/apt/sources.list.d/my_custom.list | {{Board$}} echo "deb [trusted=yes] http://<IP>:8000/cortexa7t2hf-neon-vfpv4 /" >> /etc/apt/sources.list.d/my_custom.list | ||
{{Board$}} echo "deb [trusted=yes] http://<IP>:8000/cortexa7hf-neon-vfpv4 /" >> /etc/apt/sources.list.d/my_custom.list | |||
In the above example, '''[trusted=yes]''' has been specified because the package manifest '''Release''' is not signed.<br/> | In the above example, '''[trusted=yes]''' has been specified because the package manifest '''Release''' is not signed.<br/> | ||
Line 193: | Line 202: | ||
The detailed content licenses can be found at | The detailed content licenses can be found at | ||
<nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. | <nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. | ||
Ign:1 http://<IP>:8000/ | Ign:1 http://<IP>:8000/stm32mp1 InRelease | ||
Ign:2 http://<IP>:8000/ | Ign:2 http://<IP>:8000/all InRelease | ||
Ign:3 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 InRelease | Ign:3 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 InRelease | ||
Get: | Ign:4 http://<IP>:8000/cortexa7hf-neon-vfpv4 InRelease | ||
Get: | Get:5 http://<IP>:8000/stm32mp1 Release [1088 B] | ||
Get: | Get:6 http://<IP>:8000/all Release [1083 B] | ||
Ign: | Get:7 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 Release [1115 B] | ||
Ign: | Get:8 http://<IP>:8000/cortexa7hf-neon-vfpv4 Release [1097 B] | ||
Ign: | Ign:9 http://<IP>:8000/stm32mp1 Release.gpg | ||
Get: | Ign:10 http://<IP>:8000/all Release.gpg | ||
Get: | Ign:11 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 Release.gpg | ||
Get: | Ign:12 http://<IP>:8000/cortexa7hf-neon-vfpv4 Release.gpg | ||
Fetched | Get:13 http://<IP>:8000/stm32mp1 Packages [165 kB] | ||
Get:14 http://<IP>:8000/all Packages [109 kB] | |||
Get:15 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 Packages [2775 kB] | |||
Get:16 http://<IP>:8000/cortexa7hf-neon-vfpv4 Packages [20.5 kB] | |||
Fetched 3073 kB in 7s (463 kB/s) | |||
Reading package lists... Done | Reading package lists... Done | ||
Line 226: | Line 239: | ||
* https://wiki.debian.org/SecureApt | * https://wiki.debian.org/SecureApt | ||
* [[STM32MP15 Discovery kits - Starter Package]] | * [[STM32MP15 Discovery kits - Starter Package]] | ||
* [[STM32MP15_Evaluation boards - Starter Package]] | * [[STM32MP15_Evaluation boards - Starter Package | STM32MP15 Evaluation boards - Starter Package]] | ||
* [[STM32MP1 Developer Package]] | * [[STM32MP1 Developer Package]] | ||
Revision as of 12:58, 17 June 2022
1. Disclaimers[edit | edit source]
STMicroelectronics packages repository service is provided for evaluation purpose only, and therefore not approved for use in production.
The package licenses hosted in these repositories can be found here: OpenSTLinux licenses.
Command outputs described in this document may slightly vary depending on tools version.
1.1. Description[edit | edit source]
OpenSTLinux provides a package repository service hosted at the non-browsable URL http://packages.openstlinux.st.com.
The package repository service is designed for STM32MP157x-DKx , STM32MP157x-EV1
and STM32MP135F-DK
boards and is enabled by default in the Starter Package.
1.2. Organization[edit | edit source]
Within each repository, packages are organized in three groups (a.k.a components in the APT terminology):
- the main group contains a wide selection of packages whose installation is automatically tested by STMicroelectronics
- the untested group contains all the other packages that can be built using the
bitbake world
command. However their installation is not guaranteed. - the updates group contains additional packages not included in the OpenSTLinux distribution releases and updated packages. This group is managed by a dedicated layer available through github®. Further details are available by following the github® link: https://github.com/STMicroelectronics/meta-st-pkgrepo-updates.
1.3. Limitations[edit | edit source]
Packages repository service doesn't include the packages that are shipped in the rootfs image, nor the BSP components (TF-A, U-Boot, Linux and OP-TEE). They can be installed only from the Starter Package using the STM32CubeProgrammer.
rootfs available space is about 60MB by default. For a better experience it is recommended to flash the Starter Package using the "extensible" flashlayout (*-extensible.tsv).
Extensible flashlayout does not flash userfs partition to extend the rootfs partition to the size of the sdcard.
2. Usage[edit | edit source]
2.1. Prequisite[edit | edit source]
We assume your board has an internet connection either through the network cable or through a WiFi connection.
2.2. Apt[edit | edit source]
OpenSTLinux packages can be handled using apt-*
utilities, which are the same utilities used on a Debian system. The first apt-*
command that must be run before any other is:
Board $> apt-get update
The software package is provided AS IS, and by downloading it, you agree to be
bound to the terms of the software license agreement (SLA).
The detailed content licenses can be found at
https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses.
Get:1 http://packages.openstlinux.st.com/4.0 dunfell InRelease [3459 B]
Get:2 http://packages.openstlinux.st.com/4.0 dunfell/main armhf Packages [682kB]
Get:3 http://packages.openstlinux.st.com/4.0 dunfell/updates armhf Packages [64.2kB]
Get:4 http://packages.openstlinux.st.com/4.0 dunfell/untested armhf Packages [1223kB]
Fetched 1973 kB in 3s (626 kB/s)
Reading package lists... Done
This command synchronizes the local packages index from the repositories enumerated in /etc/apt/sources.list{,.d}
. Once it is updated, apt-cache
can be used to get the list of all available packages:
POSIX Access Control Lists ... xkeyboard-config - Keyboard configuration database for X Window xxhash - Extremely fast non-cryptographic hash algorithm xz - Utilities for managing LZMA compressed filesBoard $> apt-cache search . a52dec - ATSC A/52 surround sound stream decoder a52dec-doc - ATSC A/52 surround sound stream decoder acl - Utilities for managing
It is possible to list only packages that match a given pattern, for example:
Board $> apt-cache search emacs
libreadline-doc - Library for editing typed command lines - Documentation files
libreadline-src - Library for editing typed command lines - Source files
emacs-base - Emacs is the extensible, customizable, self-documenting real-time display editor
emacs-doc - Emacs is the extensible, customizable, self-documenting real-time display editor - Documentation files
emacs-full - Emacs is the extensible, customizable, self-documenting real-time display editor
emacs-minimal - Emacs is the extensible, customizable, self-documenting real-time display editor
gpm - Console mouse driver
gpm-doc - Console mouse driver - Documentation files
zile - Zile is lossy Emacs
zile-doc - Zile is lossy Emacs - Documentation files
libreadline8 - Library for editing typed command lines
The desired package(s) can then be easily installed:
Board $> apt-get install zile
Reading package lists... Done
Building dependency tree
Reading state information... Done
The following additional packages will be installed:
bdwgc
The following NEW packages will be installed:
bdwgc zile
0 upgraded, 2 newly installed, 0 to remove and 3 not upgraded.
Need to get 150 kB of archives.
After this operation, 0 B of additional disk space will be used.
Do you want to continue? [Y/n]
Get:1 http://packages.openstlinux.st.com/4.0 dunfell/untested armhf bdwgc armhf 8.2.0-r0 [70.9 kB]
Get:2 http://packages.openstlinux.st.com/4.0 dunfell/untested armhf zile armhf 2.4.15-r0 [79.1 kB]
Fetched 150 kB in 1s (287 kB/s)
The software package is provided AS IS, and by downloading it, you agree to be
bound to the terms of the software license agreement (SLA).
The detailed content licenses can be found at
https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses.
Selecting previously unselected package bdwgc.
(Reading database ... 14860 files and directories currently installed.)
Preparing to unpack .../bdwgc_8.2.0-r0_armhf.deb ...
Unpacking bdwgc (8.2.0-r0) ...
Selecting previously unselected package zile.
Preparing to unpack .../zile_2.4.15-r0_armhf.deb ...
Unpacking zile (2.4.15-r0) ...
Setting up bdwgc (8.2.0-r0) ...
Setting up zile (2.4.15-r0) ...
... or removed:
Board $> apt-get remove zile
Reading package lists... Done
Building dependency tree
Reading state information... Done
The following package was automatically installed and is no longer required:
bdwgc
Use 'apt autoremove' to remove it.
The following packages will be REMOVED:
zile
0 upgraded, 0 newly installed, 1 to remove and 3 not upgraded.
After this operation, 0 B of additional disk space will be used.
Do you want to continue? [Y/n]
The software package is provided AS IS, and by downloading it, you agree to be
bound to the terms of the software license agreement (SLA).
The detailed content licenses can be found at
https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses.
(Reading database ... 14865 files and directories currently installed.)
Removing zile (2.4.15-r0) ...
This command only removes the files that were installed from this package. It does not remove the package from the apt
download cache. If there is not enough space available on the system, it is recommended to clean the cache:
Board $> apt-get clean
Likewise, some packages may have been automatically installed to respect dependencies with other packages. If they are no longer required, they can be removed to free space:
Board $> apt-get autoremove
Reading package lists... Done
Building dependency tree
Reading state information... Done
The following packages will be REMOVED:
bdwgc
0 upgraded, 0 newly installed, 1 to remove and 3 not upgraded.
After this operation, 0 B of additional disk space will be used.
Do you want to continue? [Y/n]
The software package is provided AS IS, and by downloading it, you agree to be
bound to the terms of the software license agreement (SLA).
The detailed content licenses can be found at
https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses.
(Reading database ... 14864 files and directories currently installed.)
Removing bdwgc (8.2.0-r0) ...
3. How to activate a local package repository[edit | edit source]
3.1. Prerequisite[edit | edit source]
Even if Package repository for OpenSTLinux offers lots of and various packages, you may need to use a local and personnal package repository. Using a local and personal package repository is a 'smart' and 'quick' way to update the Starter Package with your developments.
A local package repository is a collection of *.deb organized such apt
needs it. The local repository should provide Packages metafiles.
Natively OpenEmbedded/Yocto build system is able to generate a valid package repository (by using bitbake package-index
command listed below).
So first Install the STM32MP1 OpenSTLinux distribution.
3.2. Update the repo package indexes[edit | edit source]
Execute the bitbake package-index
command:
PC $> cd [your STM32MP1 Distribution path]/build-<DISTRO>-<MACHINE>
PC $> bitbake package-index
3.3. HTTP server execution on the computer[edit | edit source]
SimpleHTTPserver python application is already installed on the board with the OpenSTLinux distribution. You just need to launch this application on your host computer, in the "[your STM32MP1 Distribution path]/build-<DISTRO>-<MACHINE>/tmp-glibc/deploy/deb" folder:
PC $> cd [your STM32MP1 Distribution path]/build-<DISTRO>-<MACHINE>/tmp-glibc/deploy/deb
PC $> python -m SimpleHTTPServer&
3.4. How to use the local OpenSTLinux Distribution[edit | edit source]
We use the physical IP address of the HTTP server we launched above to configure APT. That means this {{<IP>}} address should be defined as static on the host computer.
You can now configure the APT tool directly on the target via a Linux console:
Board $> echo "deb [trusted=yes] http://<IP>:8000/stm32mp1 /" > /etc/apt/sources.list.d/my_custom.list
Board $> echo "deb [trusted=yes] http://<IP>:8000/all /" >> /etc/apt/sources.list.d/my_custom.list
Board $> echo "deb [trusted=yes] http://<IP>:8000/cortexa7t2hf-neon-vfpv4 /" >> /etc/apt/sources.list.d/my_custom.list
Board $> echo "deb [trusted=yes] http://<IP>:8000/cortexa7hf-neon-vfpv4 /" >> /etc/apt/sources.list.d/my_custom.list
In the above example, [trusted=yes] has been specified because the package manifest Release is not signed.
Then you can run the command to synchronize the local packages index:
Board $> apt-get update
The software package is provided AS IS, and by downloading it, you agree to be
bound to the terms of the software license agreement (SLA).
The detailed content licenses can be found at
https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses.
Ign:1 http://<IP>:8000/stm32mp1 InRelease
Ign:2 http://<IP>:8000/all InRelease
Ign:3 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 InRelease
Ign:4 http://<IP>:8000/cortexa7hf-neon-vfpv4 InRelease
Get:5 http://<IP>:8000/stm32mp1 Release [1088 B]
Get:6 http://<IP>:8000/all Release [1083 B]
Get:7 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 Release [1115 B]
Get:8 http://<IP>:8000/cortexa7hf-neon-vfpv4 Release [1097 B]
Ign:9 http://<IP>:8000/stm32mp1 Release.gpg
Ign:10 http://<IP>:8000/all Release.gpg
Ign:11 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 Release.gpg
Ign:12 http://<IP>:8000/cortexa7hf-neon-vfpv4 Release.gpg
Get:13 http://<IP>:8000/stm32mp1 Packages [165 kB]
Get:14 http://<IP>:8000/all Packages [109 kB]
Get:15 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 Packages [2775 kB]
Get:16 http://<IP>:8000/cortexa7hf-neon-vfpv4 Packages [20.5 kB]
Fetched 3073 kB in 7s (463 kB/s)
Reading package lists... Done
The other apt-*
commands are now available as described above.
4. Support[edit | edit source]
Bug reports, request for new packages, or any other kind of support requests can be submitted through https://community.st.com.
5. Further readings[edit | edit source]
- Dpkg
- https://manpages.debian.org/stable/apt/apt-get.8.en.html
- https://manpages.debian.org/stable/apt/sources.list.5.en.html
- https://manpages.debian.org/stable/apt/apt-cache.8.en.html
- https://wiki.debian.org/DebianRepository/Setup
- https://wiki.debian.org/DebianRepository/SetupWithReprepro
- https://wiki.debian.org/SecureApt
- STM32MP15 Discovery kits - Starter Package
- STM32MP15 Evaluation boards - Starter Package
- STM32MP1 Developer Package