Difference between revisions of "NVMEM overview"
[quality revision] | [unchecked revision] |
m
|
m (→How to write BSEC OTPs using NVMEM)
|
Applicable for | STM32MP13x lines, STM32MP15x lines |
This article introduces how NVMEM Linux® framework manages BSEC OTP data and how to read/write from/to it.
Contents
1 Framework purpose[edit]
The NVMEM Linux® framework provides a generic interface for the device non-volatile memory data such as:
- OTP (one-time programmable) fuses
- EEPROM
It offers kernel space and user space interfaces to read and/or write data such as analog calibration data or MAC address.
2 System overview[edit]
2.1 Component description[edit]
- NVMEM user (user space)
The user can use the NVMEM sysfs interface, from a user terminal or a custom application, to read/write data from/to NVMEM device(s) from user space.
- NVMEM user (kernel space)
User drivers can use the NVMEM API to read/write data from/to NVMEM device(s) from kernel space (such as the analog calibration data used by an ADC driver).
- NVMEM framework (kernel space)
The NVMEM core provides sysfs interface and NVMEM API. They can be used to implement NVMEM user and NVMEM controller drivers.
- NVMEM drivers (kernel space)
Provider drivers such as BSEC Linux® driver that exposes OTP data to the core.
- TEE framework (kernel space)
The TEE framework provides TEE client API to communicate with secure services, as the services provided by the OP-TEE Linux® driver.
- OP-TEE (Secure)
The OP-TEE secure OS is running on the Cortex-A in secure mode and exposes secure service with Trusted Applications (TA), as BSEC PTA.
- NVMEM hardware
NVMEM controller(s) such as the BSEC internal peripheral[1]
2.2 API description[edit]
The NVMEM kernel documentation[2] describes:
- Kernel space API for NVMEM providers and NVMEM consumers.
- Userspace binary interface (sysfs).
See also sysfs-bus-nvmem[3] ABI documentation.
3 Configuration[edit]
3.1 Kernel configuration[edit]
Activate NVMEM framework in the kernel configuration through the Linux® menuconfig tool, Menuconfig or how to configure kernel (CONFIG_NVMEM=y):
Device Drivers ---> [*] NVMEM Support ---> <*> STMicroelectronics STM32 factory-programmed memory support
3.2 Device tree configuration[edit]
The NVMEM data device tree bindings describe:
The BSEC internal peripheral[1] device tree bindings are explained in BSEC device tree configuration article.
4 How to use the framework[edit]
4.1 How to use NVMEM with sysfs interface[edit]
4.1.1 How to list NVMEM devices[edit]
The available NVMEM devices can be listed in sysfs directory /sys/bus/nvmem/devices
Example to list nvmem devices: BSEC is stm32-romem0
ls /sys/bus/nvmem/devices/ stm32-romem0
4.1.2 How to read OTPs using NVMEM[edit]
Userspace can read/write the raw NVMEM file located at: /sys/bus/nvmem/devices/*/nvmem
For BSEC, the NVEM stm32-romem0 device, the content of non-secure OTPs can be read but the secured OTPs are masked, theirs values are replaced by 0.
Normally only the 32 lower OTPs can be accessed and the upper OTPS is restricted to security. If user needs more than the 32 lower OTPs, there is an exception management explained in BSEC device tree configuration.
- Example to read all nvmem data content on stm32-romem0 devices
dd if=/sys/bus/nvmem/devices/stm32-romem0/nvmem of=/tmp/file
- Example to display nvmem data content
hexdump -C -v /sys/bus/nvmem/devices/stm32-romem0/nvmem
![]() |
A dedicated page describe the OTP mapping for STM32MP13 and STM32MP15. |
4.1.3 How to write BSEC OTPs using NVMEM[edit]
![]() |
In OpenSTLinux it is not possible The below examples show how to write data to the NVMEM BSEC device with Linux driver; BSEC is defined as a read only NVMEM device. |
an NVMEM device. This may cause unrecoverable damage to the STM32 device (for example when writing to an OTP area) |
The BSEC OTP can be written by 32-bit word starting at OTP N as follows:
# write OTP N word by word dd if=/tmp/file of=/sys/bus/nvmem/devices/stm32-romem0/nvmem bs=4 seek=N
or
# write OTP N, all the file in one request dd if=/tmp/file of=/sys/bus/nvmem/devices/stm32-romem0/nvmem seek=4*N oflag=seek_bytes
With a file /tmp/file containing the OTP data to write, size is 32-bit word aligned; for example:
# Create a 4 bytes length file filled with ones, e.g. 0xffffffff) dd if=/dev/zero count=1 bs=4 | tr '\000' '\377' > file # Create a 4 bytes length file, here 0x01000000 to update one OTP echo -n -e '\x01\x00\x00\x00' > /tmp/file # Create a 8 bytes length file, here 0x01234567 0x89ABCDEF to update two OTPs echo -n -e '\x01\x23\x45\x67\x89\xAB\xCD\xEF' > /tmp/file
An lower OTP can be be written if it is not locked and several time for a bit per bit update.
An upper OTP data can be written only if it is allowed in secure world device tree and only one time; when the upper OTP is written, it is permanent locked at the end of the NVEM request to avoid ECC issue on second update. For the first example with bs=4, this lock is performed after each OTP update and for the second example with oflag=seek_bytes the lock is done when all the OTPs in input file are updated.
5 How to trace and debug the framework[edit]
5.1 How to trace[edit]
Ftrace can be used to trace the NVMEM framework:
cd /sys/kernel/debug/tracing cat available_filter_functions | grep nvmem # Show available filter functions rtc_nvmem_register rtc_nvmem_unregister nvmem_reg_read bin_attr_nvmem_read ...
Enable the kernel function tracer, then start using nvmem and display the result:
echo function > current_tracer echo "*nvmem*" > set_ftrace_filter # Trace all nvmem filter functions echo 1 > tracing_on # start ftrace hexdump -C -v /sys/bus/nvmem/devices/stm32-romem0/nvmem # dump nvmem 00000000 17 00 00 00 01 80 00 00 00 00 00 00 00 00 00 00 |................| ... echo 0 > tracing_on # stop ftrace cat trace # tracer: function # # _-----=> irqs-off # / _----=> need-resched # | / _---=> hardirq/softirq # || / _--=> preempt-depth # ||| / delay # TASK-PID CPU# |||| TIMESTAMP FUNCTION # | | | |||| | | hexdump-478 [000] .... 423.502278: bin_attr_nvmem_read <-sysfs_kf_bin_read hexdump-478 [000] .... 423.502290: nvmem_reg_read <-bin_attr_nvmem_read hexdump-478 [000] .... 423.515804: bin_attr_nvmem_read <-sysfs_kf_bin_read
6 References[edit]
- ↑ 1.01.1 BSEC internal peripheral
- ↑ Documentation/driver-api/nvmem.rst , NVMEM subsytem kernel documentation
- ↑ Documentation/ABI/stable/sysfs-bus-nvmem , NVMEM ABI documentation
- ↑ Documentation/devicetree/bindings/nvmem/nvmem.yaml , NVMEM device tree bindings
- ↑ Documentation/devicetree/bindings/nvmem/nvmem-consumer.yaml , NVMEM consumer device tree bindings
<noinclude>{{ApplicableFor |MPUs list=STM32MP13x, STM32MP15x |MPUs checklist=STM32MP13x,STM32MP15x }}</noinclude> This article introduces how NVMEM Linux<sup>®</sup> framework manages BSEC OTP data and how to read/write from/to it.<p> ==Framework purpose== The NVMEM Linux<sup>®</sup> framework provides a generic interface for the device '''non-volatile memory data''' such as: * OTP (one-time programmable) fuses * EEPROM It offers kernel space and user space interfaces to read and/or write data such as analog calibration data or MAC address. ==System overview== {{ ImageMap|Image:NVMEM_overview.png {{!}} thumb {{!}} 800px {{!}} center{{!}} rect 470 160 600 200 [[NVMEM_overview#API description|NVMEM sysfs interface]] rect 600 260 750 300 [[NVMEM_overview#API description|NVMEM consumers interface]] rect 480 660 600 700 [[BSEC internal peripheral]] rect 480 570 600 615 [[OP-TEE OTP PTA overview|BSEC PTA]] rect 230 560 315 600 [[OP-TEE_overview|OP-TEE]] rect 480 480 600 520 [[OP-TEE_overview#TEE_Linux_driver|OP-TEE linux driver]] rect 525 445 615 475 [[OP-TEE_overview#TEE_Client_API|TEE Client API]] }} ===Component description=== * '''NVMEM user''' (user space) The user can use the NVMEM sysfs interface, from a user terminal or a custom application, to read/write data from/to NVMEM device(s) from user space. * '''NVMEM user''' (kernel space) User drivers can use the NVMEM API to read/write data from/to NVMEM device(s) from kernel space (such as the analog calibration data used by an ADC driver). * '''NVMEM framework''' (kernel space) The NVMEM core provides sysfs interface and NVMEM API. They can be used to implement NVMEM user and NVMEM controller drivers. * '''NVMEM drivers''' (kernel space) Provider drivers such as BSEC Linux<sup>®</sup> driver that exposes OTP data to the core. * '''TEE framework''' (kernel space) The TEE framework provides [[OP-TEE_overview#TEE_Client_API|TEE client API]] to communicate with secure services, as the services provided by the OP-TEE Linux<sup>®</sup> driver. * ''' OP-TEE''' (Secure) The [[OP-TEE overview|'''OP-TEE secure OS''']] is running on the Cortex-A in [[Security_overview|secure mode]] and exposes secure service with '''Trusted Applications (TA)''', as [[OP-TEE OTP PTA overview|BSEC PTA]]. * '''NVMEM hardware''' NVMEM controller(s) such as the ''BSEC internal peripheral''<ref name="BSEC internal peripheral">[[BSEC internal peripheral]]</ref> ===API description=== The NVMEM kernel documentation<ref name="documentation_nvmem">{{CodeSource | Linux kernel | Documentation/driver-api/nvmem.rst}}, NVMEM subsytem kernel documentation</ref> describes: * Kernel space API for NVMEM '''providers''' and NVMEM '''consumers'''. * Userspace binary interface (sysfs). See also ''sysfs-bus-nvmem''<ref name="nvmem_abi">{{CodeSource | Linux kernel | Documentation/ABI/stable/sysfs-bus-nvmem}}, NVMEM ABI documentation</ref> ABI documentation. ==Configuration== ===Kernel configuration=== Activate NVMEM framework in the kernel configuration through the Linux<sup>®</sup> menuconfig tool, [[Menuconfig or how to configure kernel | Menuconfig or how to configure kernel ]] (CONFIG_NVMEM=y): Device Drivers ---> [*] NVMEM Support ---><*> STMicroelectronics STM32 factory-programmed memory support ===Device tree configuration=== The NVMEM data device tree bindings describe: * The location of non-volatile memory data * The NVMEM data providers<ref name="nvmem dt bindings">{{CodeSource | Linux kernel | Documentation/devicetree/bindings/nvmem/nvmem.yaml}}, NVMEM device tree bindings</ref> * The NVMEM data consumers<ref name="nvmem-consumer dt bindings">{{CodeSource | Linux kernel | Documentation/devicetree/bindings/nvmem/nvmem-consumer.yaml}}, NVMEM consumer device tree bindings</ref> The ''BSEC internal peripheral''<ref name="BSEC internal peripheral"/> device tree bindings are explained in [[BSEC device tree configuration]] article. ==How to use the framework== ===How to use NVMEM with sysfs interface=== ====How to list NVMEM devices==== The available NVMEM devices can be listed in sysfs directory {{Highlight|/sys/bus/nvmem/devices}} Example to '''list''' nvmem devices: BSEC is '''stm32-romem0''' {{Board$}} ls /sys/bus/nvmem/devices/ stm32-romem0 ====How to read OTPs using NVMEM==== Userspace can read/write the raw NVMEM file located at: {{Highlight|/sys/bus/nvmem/devices/*/nvmem}} For BSEC, the NVEM '''stm32-romem0''' device, the content of '''non-secure OTPs''' can be read but the '''secured OTPs''' are masked, theirs values are replaced by 0. Normally only the 32 lower OTPs can be accessed and the upper OTPS is restricted to security. If user needs more than the 32 lower OTPs, there is an exception management explained in [[BSEC device tree configuration]]. * Example to '''read''' all nvmem data content on stm32-romem0 devices {{Board$}} dd if=/sys/bus/nvmem/devices/stm32-romem0/nvmem of=/tmp/file * Example to '''display''' nvmem data content {{Board$}} hexdump -C -v /sys/bus/nvmem/devices/stm32-romem0/nvmem {{Info|A dedicated page describe the OTP mapping for [[STM32MP15_OTP_mapping|STM32MP13]] and [[STM32MP15_OTP_mapping|STM32MP15]].}} ====How to write BSEC OTPs using NVMEM==== {{Warning|In OpenSTLinux it is not possible The below examples show how to write data to thean NVMEM BSEC device with Linux driver; BSEC is defined as a read only NVMEM device.}} OTP can be updated by using STM32CubeProgrammer. device. This may cause unrecoverable damage to the STM32 device (for example when writing to an OTP area)}} {{Info| Note that lower BSEC OTPs are using 2:1 redundancy, so they can be written bit per bit, whereas upper BSEC OTPs only support one time 32-bit programming, they are automatically locked by driver. }} The BSEC OTP can be written by 32-bit word starting at OTP {{highlight|N}} as follows: # {{highlight|'''write''' OTP '''N'''}} word by word {{Board$}} dd if={{highlightParam|/tmp/file}} of=/sys/bus/nvmem/devices/stm32-romem0/nvmem bs=4 seek={{highlight|N}} or # {{highlight|'''write''' OTP '''N'''}}, all the file in one request {{Board$}} dd if={{highlightParam|/tmp/file}} of=/sys/bus/nvmem/devices/stm32-romem0/nvmem seek={{highlight|4*N}} oflag=seek_bytes With a file {{highlightParam|/tmp/file}} containing the OTP data to write, size is 32-bit word aligned; for example: # Create a 4 bytes length file filled with ones, e.g. 0xffffffff) {{Board$}} dd if=/dev/zero count=1 bs=4 | tr '\000' '\377' > file # Create a 4 bytes length file, here 0x01000000 to update one OTP {{Board$}} echo -n -e '\x01\x00\x00\x00' > {{highlightParam|/tmp/file}} # Create a 8 bytes length file, here 0x01234567 0x89ABCDEF to update two OTPs {{Board$}} echo -n -e '\x01\x23\x45\x67\x89\xAB\xCD\xEF' > {{highlightParam|/tmp/file}} An lower OTP can be be written if it is not locked and several time for a bit per bit update. An upper OTP data can be written only if it is allowed in [[BSEC_device_tree_configuration#BSEC_node_append|secure world device tree]] and only one time; when the upper OTP is written, it is permanent locked at the end of the NVEM request to avoid ECC issue on second update. For the first example with bs=4, this lock is performed after each OTP update and for the second example with oflag=seek_bytes the lock is done when all the OTPs in input file are updated. {{Info|When a new OTP value has been written using this SYSFS interface, it may be necessary to reboot the board before reading it back. The OTP value can't be read directly after a write because the OTP value is read in a shadow area not directly in the OTP area.}} ==How to trace and debug the framework== ===How to trace=== [[Ftrace]] can be used to trace the NVMEM framework: {{Board$}} cd /sys/kernel/debug/tracing {{Board$}} cat available_filter_functions | grep nvmem # Show available filter functions rtc_nvmem_register rtc_nvmem_unregister nvmem_reg_read bin_attr_nvmem_read ... Enable the kernel function tracer, then start using nvmem and display the result: {{Board$}} echo function > current_tracer {{Board$}} echo "*nvmem*" > set_ftrace_filter # Trace all nvmem filter functions {{Board$}} echo 1 > tracing_on # start ftrace {{Board$}} hexdump -C -v /sys/bus/nvmem/devices/stm32-romem0/nvmem # dump nvmem 00000000 17 00 00 00 01 80 00 00 00 00 00 00 00 00 00 00 |................| ... {{Board$}} echo 0 > tracing_on # stop ftrace {{Board$}} cat trace # tracer: function # # _-----=> irqs-off # / _----=> need-resched # | / _---=> hardirq/softirq # || / _--=> preempt-depth # ||| / delay # TASK-PID CPU# |||| TIMESTAMP FUNCTION # | | | |||| | | hexdump-478 [000] .... 423.502278: bin_attr_nvmem_read <-sysfs_kf_bin_read hexdump-478 [000] .... 423.502290: nvmem_reg_read <-bin_attr_nvmem_read hexdump-478 [000] .... 423.515804: bin_attr_nvmem_read <-sysfs_kf_bin_read ==References== <references /> <noinclude> {{ArticleBasedOnModel | Framework_overview_article_model}} {{PublicationRequestId | 10397 | 2019-01-21 | AnneJ}} [[Category:Persistent storage]]</noinclude>
Line 84: | Line 84: | ||
====How to write BSEC OTPs using NVMEM==== |
====How to write BSEC OTPs using NVMEM==== |
||
− | {{Warning| |
+ | {{Warning|The below examples show how to write data to an NVMEM device. This may cause unrecoverable damage to the STM32 device (for example when writing to an OTP area)}} |
− | OTP can be updated |
+ | {{Info| Note that lower BSEC OTPs are using 2:1 redundancy, so they can be written bit per bit, whereas upper BSEC OTPs only support one time 32-bit programming, they are automatically locked by driver. }} |
+ | |||
+ | The BSEC OTP can be written by 32-bit word starting at OTP {{highlight|N}} as follows: |
||
+ | |||
+ | # {{highlight|'''write''' OTP '''N'''}} word by word |
||
+ | {{Board$}} dd if={{highlightParam|/tmp/file}} of=/sys/bus/nvmem/devices/stm32-romem0/nvmem bs=4 seek={{highlight|N}} |
||
+ | or |
||
+ | # {{highlight|'''write''' OTP '''N'''}}, all the file in one request |
||
+ | {{Board$}} dd if={{highlightParam|/tmp/file}} of=/sys/bus/nvmem/devices/stm32-romem0/nvmem seek={{highlight|4*N}} oflag=seek_bytes |
||
+ | |||
+ | With a file {{highlightParam|/tmp/file}} containing the OTP data to write, size is 32-bit word aligned; for example: |
||
+ | |||
+ | # Create a 4 bytes length file filled with ones, e.g. 0xffffffff) |
||
+ | {{Board$}} dd if=/dev/zero count=1 bs=4 | tr '\000' '\377' > file |
||
+ | # Create a 4 bytes length file, here 0x01000000 to update one OTP |
||
+ | {{Board$}} echo -n -e '\x01\x00\x00\x00' > {{highlightParam|/tmp/file}} |
||
+ | # Create a 8 bytes length file, here 0x01234567 0x89ABCDEF to update two OTPs |
||
+ | {{Board$}} echo -n -e '\x01\x23\x45\x67\x89\xAB\xCD\xEF' > {{highlightParam|/tmp/file}} |
||
+ | |||
+ |
An lower OTP can be be written if it is not locked and several time for a bit per bit update.
|
||
+ | |||
+ |
An upper OTP data can be written only if it is allowed in [[BSEC_device_tree_configuration#BSEC_node_append|secure world device tree]] and only one time; when the upper OTP is written, it is permanent locked at the end of the NVEM request to avoid ECC issue on second update. For the first example with bs=4, this lock is performed after each OTP update and for the second example with oflag=seek_bytes the lock is done when all the OTPs in input file are updated.
|
||
+ | |||
+ |
{{Info|When a new OTP value has been written using this SYSFS interface, it may be necessary to reboot the board before reading it back. The OTP value can't be read directly after a write because the OTP value is read in a shadow area not directly in the OTP area.}}
|
||
==How to trace and debug the framework== |
==How to trace and debug the framework== |