Registered User mNo edit summary |
Registered User |
||
(One intermediate revision by the same user not shown) | |||
Line 27: | Line 27: | ||
===API description=== | ===API description=== | ||
The NVMEM kernel documentation<ref name="documentation_nvmem">{{CodeSource | Linux kernel | Documentation/ | The NVMEM kernel documentation<ref name="documentation_nvmem">{{CodeSource | Linux kernel | Documentation/driver-api/nvmem.rst}}, NVMEM subsytem kernel documentation</ref> describes: | ||
* Kernel space API for NVMEM '''providers''' and NVMEM '''consumers'''. | * Kernel space API for NVMEM '''providers''' and NVMEM '''consumers'''. | ||
* Userspace binary interface (sysfs). | * Userspace binary interface (sysfs). | ||
Line 40: | Line 40: | ||
===Device tree configuration=== | ===Device tree configuration=== | ||
The NVMEM data device tree bindings | The NVMEM data device tree bindings describe: | ||
* The location of non-volatile memory data | * The location of non-volatile memory data | ||
* The NVMEM data providers | * The NVMEM data providers<ref name="nvmem dt bindings">{{CodeSource | Linux kernel | Documentation/devicetree/bindings/nvmem/nvmem.yaml}}, NVMEM device tree bindings</ref> | ||
* The NVMEM data consumers | * The NVMEM data consumers<ref name="nvmem-consumer dt bindings">{{CodeSource | Linux kernel | Documentation/devicetree/bindings/nvmem/nvmem-consumer.yaml}}, NVMEM consumer device tree bindings</ref> | ||
The ''BSEC internal peripheral''<ref name="BSEC internal peripheral"/> device tree bindings are explained in [[BSEC device tree configuration]] article. | The ''BSEC internal peripheral''<ref name="BSEC internal peripheral"/> device tree bindings are explained in [[BSEC device tree configuration]] article. | ||
Revision as of 16:04, 4 November 2020
This article introduces how NVMEM Linux® framework manages BSEC OTP data and how to read/write from/to it.
1. Framework purpose[edit | edit source]
The NVMEM Linux® framework provides a generic interface for the device non-volatile memory data such as:
- OTP (one-time programmable) fuses
- EEPROM
It offers kernel space and user space interfaces to read and/or write data such as analog calibration data or MAC address.
2. System overview[edit | edit source]
2.1. Component description[edit | edit source]
- NVMEM user (user space)
The user can use the NVMEM sysfs interface, from a user terminal or a custom application, to read/write data from/to NVMEM device(s) from user space.
- NVMEM user (kernel space)
User drivers can use the NVMEM API to read/write data from/to NVMEM device(s) from kernel space (such as the analog calibration data used by an ADC driver).
- NVMEM framework (kernel space)
The NVMEM core provides sysfs interface and NVMEM API. They can be used to implement NVMEM user and NVMEM controller drivers.
- NVMEM drivers (kernel space)
Provider drivers such as BSEC Linux® driver that exposes OTP data to the core.
- NVMEM hardware
NVMEM controller(s) such as the BSEC internal peripheral[1]
2.2. API description[edit | edit source]
The NVMEM kernel documentation[2] describes:
- Kernel space API for NVMEM providers and NVMEM consumers.
- Userspace binary interface (sysfs).
See also sysfs-bus-nvmem[3] ABI documentation.
3. Configuration[edit | edit source]
3.1. Kernel configuration[edit | edit source]
Activate NVMEM framework in the kernel configuration through the Linux® menuconfig tool, Menuconfig or how to configure kernel (CONFIG_NVMEM=y):
Device Drivers --->
[*] NVMEM Support --->
<*> STMicroelectronics STM32 factory-programmed memory support
3.2. Device tree configuration[edit | edit source]
The NVMEM data device tree bindings describe:
The BSEC internal peripheral[1] device tree bindings are explained in BSEC device tree configuration article.
4. How to use the framework[edit | edit source]
4.1. How to use NVMEM with sysfs interface[edit | edit source]
4.1.1. How to list NVMEM devices[edit | edit source]
The available NVMEM devices can be listed in sysfs:
Example to list nvmem devices ls /sys/bus/nvmem/devices/ stm32-romem0#
The data content of an NVMEM device can be dumped to a binary file, and then displayed.
4.1.2. How to read BSEC lower OTPs using NVMEM[edit | edit source]
The 32 lower OTPs can be read from non-secure when using either:
- the trusted boot chain (using TF-A)
- the basic boot chain (using U-Boot SPL)
Example to read lower nvmem data content dd if=/sys/bus/nvmem/devices/stm32-romem0/nvmem of=/tmp/file bs=4 count=32 # Example to display nvmem data content hexdump -C -v /tmp/file#
4.1.3. How to read BSEC upper OTPs using NVMEM[edit | edit source]
![]() |
Only the 32 lower OTPs can be accessed when using the basic boot chain, as it doesn't implement secure services (CONFIG_HAVE_ARM_SMCCC). So this section concerns only the trusted boot chain (using TF-A) as SMC feature is available. |
Default behavior for upper OTPS is normally restricted to security. If user needs more than the 32 lower OTPs, there is an exception management explained in BSEC device tree configuration.
It is then possible to access to some upper NVMEM information.
Example to read the MAC address from upper OTP area, using secure services: dd if=/sys/bus/nvmem/devices/stm32-romem0/nvmem of=/tmp/file skip=57 bs=4 count=2 status=none hexdump -C -v /tmp/file#
![]() |
A dedicated chapter of the reference manual describes the OTP mapping. |
4.1.4. How to write BSEC OTPs using NVMEM[edit | edit source]
![]() |
Note that lower OTPs are using 2:1 redundancy, so they can be written bit per bit, whereas upper OTPs only support one time 32-bit programming. |
Whatever the boot chain, the full lower NVMEM data content can be written as follows (if we suppose it has been previously read as described above, and updated directly in /tmp/file):
Example to write lower nvmem data content dd if=/tmp/file of=/sys/bus/nvmem/devices/stm32-romem0/nvmem bs=4 count=32#
Only on Trusted boot chain, and under the condition the device tree authorizes it, an upper NVMEM data can be written.
Example of 32-bit data word writing (filling it with ones) in OTP n°95:
OTP data 95 dd if=/dev/zero count=1 bs=4 | tr '\000' '\377' > file dd if=file bs=4 seek=95 of=/sys/bus/nvmem/devices/stm32-romem0/nvmem# Create a 4 bytes length file filled with ones, e.g. 0xffffffff) # Then, write it (32-bits, e.g. 4bytes) to
![]() |
When a new OTP value has been written using this SYSFS interface, it may be necessary to reboot the board before reading it back. The OTP value can't be read directly after a write because the OTP value is read in a shadow area not directly in the OTP area. |
5. How to trace and debug the framework[edit | edit source]
5.1. How to trace[edit | edit source]
Ftrace can be used to trace the NVMEM framework:
cd /sys/kernel/debug/tracing
cat available_filter_functions | grep nvmem # Show available filter functions
rtc_nvmem_register
rtc_nvmem_unregister
nvmem_reg_read
bin_attr_nvmem_read
...
Enable the kernel function tracer, then start using nvmem and display the result:
CPU# |||| TIMESTAMP FUNCTION # | | | |||| | | hexdump-478 [000] .... 423.502278: bin_attr_nvmem_read <-sysfs_kf_bin_read hexdump-478 [000] .... 423.502290: nvmem_reg_read <-bin_attr_nvmem_read hexdump-478 [000] .... 423.515804: bin_attr_nvmem_read <-sysfs_kf_bin_readecho function > current_tracer echo "*nvmem*" > set_ftrace_filter # Trace all nvmem filter functions echo 1 > tracing_on # start ftrace hexdump -C -v /sys/bus/nvmem/devices/stm32-romem0/nvmem # dump nvmem 00000000 17 00 00 00 01 80 00 00 00 00 00 00 00 00 00 00 |................| ... echo 0 > tracing_on # stop ftrace cat trace # tracer: function # # _-----=> irqs-off # / _----=> need-resched # | / _---=> hardirq/softirq # || / _--=> preempt-depth # ||| / delay # TASK-PID
6. References[edit | edit source]
- ↑ Jump up to: 1.0 1.1 BSEC internal peripheral
- ↑ Documentation/driver-api/nvmem.rst , NVMEM subsytem kernel documentation
- ↑ Documentation/ABI/stable/sysfs-bus-nvmem , NVMEM ABI documentation
- ↑ Documentation/devicetree/bindings/nvmem/nvmem.yaml , NVMEM device tree bindings
- ↑ Documentation/devicetree/bindings/nvmem/nvmem-consumer.yaml , NVMEM consumer device tree bindings