Approved version. Approved on: 07:33, 14 September 2021
You are viewing an old version of this page. Return to the latest version.
Difference between revisions of "How to use the RTC"
[unchecked revision] | [quality revision] |
m
|
Applicable for | STM32MP13x lines, STM32MP15x lines |
Contents
1 Purpose[edit]
This article describes how to use the RTC.
2 How to set a hardware clock using the hwclock tool[edit]
The correct system time must first be set with the date command. Type the date command to see the date and time format of the string:
date Fri Mar 9 12:18:51 UTC 2018
date --set="Fri Mar 9 19:18:51 UTC 2018" Fri Mar 9 19:18:51 UTC 2018
Set the hardware clock to this date:
hwclock Fri Mar 9 12:21:03 2018 0.000000 seconds hwclock --systohc --utc hwclock Fri Mar 9 19:19:52 2018 0.000000 seconds
See [1] for more about date settings. See [2] for more about hwclock settings.
3 How to set an alarm[edit]
# disable the alarm
echo 0 > /sys/class/rtc/rtc0/wakealarm
# calculate alarm with 1 minute later
wakeuptime=`date -d "1 minute" +%s`
# set the alarm
echo $wakeuptime > /sys/class/rtc/rtc0/wakealarm
root@stm32mp1:~# [ 829.279019] rtc rtc0: Alarm occurred
You can also set an alarm 'n' seconds later:
echo +10 > /sys/class/rtc/rtc0/wakealarm
4 How to set an alarm and go into a system sleep state with the rtcwake tool[edit]
# calculate an alarm 1 minute later
wakeuptime=`date -d "1 minute" +%s`
# set wakeup on /dev/rtc0
rtcwake -lt$wakeuptime -m mem
rtcwake: wakeup from "mem" using /dev/rtc0 at Sun Mar 11 10:48:06 2018
[ 154.022303] PM: suspend entry (deep)
[ 154.024421] PM: Syncing filesystems ... done.
[ 154.037258] Freezing user space processes ... (elapsed 0.001 seconds) done.
[ 154.044397] OOM killer disabled.
[ 154.047555] Freezing remaining freezable tasks ... (elapsed 0.001 seconds) done.
[ 154.055039] Suspending console(s) (use no_console_suspend to debug)
One minute later...
NOTICE: CPU: STM32MP157CAA Rev.B NOTICE: Model: STMicroelectronics STM32MP157C eval daughter on eval mother NOTICE: Board: MB1263 Var1 Rev.C-01 INFO: Reset reason (0x810): INFO: System exits from STANDBY INFO: Using SDMMC INFO: Instance 1 INFO: Boot used partition fsbl1 INFO: Product_below_2v5=1: HSLVEN update is INFO: destructive, no update as VDD>2.7V NOTICE: BL2: v2.0(debug):v2.0-stm32mp-19-01-29 NOTICE: BL2: Built : 15:58:42, Jan 29 2019 INFO: BL2: Doing platform setup INFO: PMIC version = 0x10 INFO: RAM: DDR3-1066/888 bin G 2x4Gb 533MHz v1.41 INFO: BL2 runs SP_MIN setup INFO: BL2: Loading image id 4 INFO: Loading image id=4 at address 0x2ffe5000 INFO: Image id=4 loaded: 0x2ffe5000 - 0x30000000 INFO: BL2: Skip loading image id 5 INFO: read version 0 current version 0 NOTICE: BL2: Booting BL32 INFO: Entry point address = 0x2ffe5000 INFO: SPSR = 0x1d3 INFO: PMIC version = 0x10 NOTICE: SP_MIN: v2.0(debug):v2.0-stm32mp-19-01-29 NOTICE: SP_MIN: Built : 15:58:42, Jan 29 2019 INFO: ARM GICv2 driver initialized INFO: stm32mp HSI (18): Secure only INFO: stm32mp HSE (20): Secure only INFO: stm32mp PLL2 (27): Secure only INFO: stm32mp PLL2_R (30): Secure only INFO: SP_MIN: Initializing runtime services INFO: SP_MIN: Preparing exit to normal world [ 154.074319] dwc2 49000000.usb-otg: suspending usb gadget configfs-gadget [ 154.196804] Disabling non-boot CPUs ... [ 154.250046] CPU1 killed. [ 154.251704] Enabling non-boot CPUs ... [ 154.252697] CPU1 is up [ 154.254885] rtc rtc0: Alarm occurred [ 154.273940] dwmac4: Master AXI performs any burst length [ 154.273972] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found [ 154.276938] usb usb2: root hub lost power or was reset [ 154.284703] dwc2 49000000.usb-otg: resuming usb gadget configfs-gadget [ 154.491151] dwc2 49000000.usb-otg: new device is high-speed [ 154.619589] dwc2 49000000.usb-otg: new device is high-speed [ 154.669343] usb 2-1: reset high-speed USB device number 2 using ehci-platform [ 154.697272] dwc2 49000000.usb-otg: new address 2 [ 154.722774] configfs-gadget gadget: high-speed config #1: c [ 155.066198] OOM killer enabled. [ 155.069339] Restarting tasks ... done. [ 155.075470] PM: suspend exit
See [3] for more about rtcwake settings.
5 How to get RTC status[edit]
cat /proc/driver/rtc
rtc_time : 07:25:13
rtc_date : 2000-01-01
alrm_time : 00:00:00
alrm_date : 2165-01-01
alarm_IRQ : no
alrm_pending : no
update IRQ enabled : no
periodic IRQ enabled : no
periodic IRQ frequency : 1
max user IRQ frequency : 64
24hr : yes
6 References[edit]
{{ApplicableFor |MPUs list=STM32MP13x, STM32MP15x |MPUs checklist=STM32MP13x, STM32MP15x }} __TOC__ ==Purpose== This article describes how to use the RTC. == How to set a hardware clock using the hwclock tool == The correct system time must first be set with the date command. Type the date command to see the date and time format of the string: {{Board$}} date Fri Mar 9 12:18:51 UTC 2018 {{Board$}} date --set="Fri Mar 9 19:18:51 UTC 2018" Fri Mar 9 19:18:51 UTC 2018 Set the hardware clock to this date: {{Board$}} hwclock Fri Mar 9 12:21:03 2018 0.000000 seconds {{Board$}} hwclock --systohc --utc {{Board$}} hwclock Fri Mar 9 19:19:52 2018 0.000000 seconds See <ref name="date">http://man7.org/linux/man-pages/man1/date.1.html</ref> for more about date settings. See <ref name="hwclock">http://man7.org/linux/man-pages/man8/hwclock.8.html</ref> for more about hwclock settings. == How to set an alarm == {{highlight|# disable the alarm}} {{Board$}} echo 0 > /sys/class/rtc/rtc0/wakealarm {{highlight|# calculate alarm with 1 minute later}} {{Board$}} wakeuptime=`date -d "1 minute" +%s` {{highlight|# set the alarm}} {{Board$}} echo $wakeuptime > /sys/class/rtc/rtc0/wakealarm root@stm32mp1:~# [ 829.279019] rtc rtc0: Alarm occurred You can also set an alarm 'n' seconds later: {{Board$}} echo +10 > /sys/class/rtc/rtc0/wakealarm == How to set an alarm and go into a system sleep state with the rtcwake tool == {{highlight|# calculate an alarm 1 minute later}} {{Board$}} wakeuptime=`date -d "1 minute" +%s` {{highlight|# set wakeup on /dev/rtc0}} {{Board$}} rtcwake -lt$wakeuptime -m mem rtcwake: wakeup from "mem" using /dev/rtc0 at Sun Mar 11 10:48:06 2018 [ 154.022303] PM: suspend entry (deep) [ 154.024421] PM: Syncing filesystems ... done. [ 154.037258] Freezing user space processes ... (elapsed 0.001 seconds) done. [ 154.044397] OOM killer disabled. [ 154.047555] Freezing remaining freezable tasks ... (elapsed 0.001 seconds) done. [ 154.055039] Suspending console(s) (use no_console_suspend to debug) One minute later... NOTICE: CPU: STM32MP157CAA Rev.B NOTICE: Model: STMicroelectronics STM32MP157C eval daughter on eval mother NOTICE: Board: MB1263 Var1 Rev.C-01 INFO: Reset reason (0x810): INFO: System exits from STANDBY INFO: Using SDMMC INFO: Instance 1 INFO: Boot used partition fsbl1 INFO: Product_below_2v5=1: HSLVEN update is INFO: destructive, no update as VDD>2.7V NOTICE: BL2: v2.0(debug):v2.0-stm32mp-19-01-29 NOTICE: BL2: Built : 15:58:42, Jan 29 2019 INFO: BL2: Doing platform setup INFO: PMIC version = 0x10 INFO: RAM: DDR3-1066/888 bin G 2x4Gb 533MHz v1.41 INFO: BL2 runs SP_MIN setup INFO: BL2: Loading image id 4 INFO: Loading image id=4 at address 0x2ffe5000 INFO: Image id=4 loaded: 0x2ffe5000 - 0x30000000 INFO: BL2: Skip loading image id 5 INFO: read version 0 current version 0 NOTICE: BL2: Booting BL32 INFO: Entry point address = 0x2ffe5000 INFO: SPSR = 0x1d3 INFO: PMIC version = 0x10 NOTICE: SP_MIN: v2.0(debug):v2.0-stm32mp-19-01-29 NOTICE: SP_MIN: Built : 15:58:42, Jan 29 2019 INFO: ARM GICv2 driver initialized INFO: stm32mp HSI (18): Secure only INFO: stm32mp HSE (20): Secure only INFO: stm32mp PLL2 (27): Secure only INFO: stm32mp PLL2_R (30): Secure only INFO: SP_MIN: Initializing runtime services INFO: SP_MIN: Preparing exit to normal world [ 154.074319] dwc2 49000000.usb-otg: suspending usb gadget configfs-gadget [ 154.196804] Disabling non-boot CPUs ... [ 154.250046] CPU1 killed. [ 154.251704] Enabling non-boot CPUs ... [ 154.252697] CPU1 is up [ 154.254885] rtc rtc0: Alarm occurred [ 154.273940] dwmac4: Master AXI performs any burst length [ 154.273972] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found [ 154.276938] usb usb2: root hub lost power or was reset [ 154.284703] dwc2 49000000.usb-otg: resuming usb gadget configfs-gadget [ 154.491151] dwc2 49000000.usb-otg: new device is high-speed [ 154.619589] dwc2 49000000.usb-otg: new device is high-speed [ 154.669343] usb 2-1: reset high-speed USB device number 2 using ehci-platform [ 154.697272] dwc2 49000000.usb-otg: new address 2 [ 154.722774] configfs-gadget gadget: high-speed config #1: c [ 155.066198] OOM killer enabled. [ 155.069339] Restarting tasks ... done. [ 155.075470] PM: suspend exit See <ref name="rtcwake">http://man7.org/linux/man-pages/man8/rtcwake.8.html</ref> for more about rtcwake settings. == How to get RTC status == {{Board$}} cat /proc/driver/rtc rtc_time : 07:25:13 rtc_date : 2000-01-01 alrm_time : 00:00:00 alrm_date : 2165-01-01 alarm_IRQ : no alrm_pending : no update IRQ enabled : no periodic IRQ enabled : no periodic IRQ frequency : 1 max user IRQ frequency : 64 24hr : yes ==References==<references/> <noinclude> [[Category:RTC|3]] {{PublicationRequestId |15042 | 2020-02-21}}</noinclude>
Line 113: | Line 113: | ||
See <ref name="rtcwake">http://man7.org/linux/man-pages/man8/rtcwake.8.html</ref> for more about rtcwake settings. |
See <ref name="rtcwake">http://man7.org/linux/man-pages/man8/rtcwake.8.html</ref> for more about rtcwake settings. |
||
+ | |||
+ | == How to get RTC status == |
||
+ | {{Board$}} cat /proc/driver/rtc |
||
+ | rtc_time : 07:25:13 |
||
+ | rtc_date : 2000-01-01 |
||
+ | alrm_time : 00:00:00 |
||
+ | alrm_date : 2165-01-01 |
||
+ | alarm_IRQ : no |
||
+ | alrm_pending : no |
||
+ | update IRQ enabled : no |
||
+ | periodic IRQ enabled : no |
||
+ | periodic IRQ frequency : 1 |
||
+ | max user IRQ frequency : 64 |
||
+ | 24hr : yes |
||
==References== |
==References== |