Difference between revisions of "How to use U-Boot stm32key command"
[quality revision] | [unchecked revision] |
m
|
m
|
Applicable for | STM32MP13x lines, STM32MP15x lines |
Contents
1 Purpose[edit]
In this article, the stm32key
U-Boot command is used to illustrate and experiment the steps to provision the keys in the correct OTP needed to activate secure boot features: authentication and encryption.
It also allows to directly set the device to CLOSED state.
1.1 Prerequisite[edit]
All the required keys have to be generated to provision the OTP.
![]() |
Make sure that a device with Secure boot enabled is used: this is mentioned in the chip part number, for STM32MP13 and STM32MP15, otherwise the device will become permanently unusable. |
2 stm32key command[edit]
U-Boot in OpenSTLinux embeds a stm32key
command that can be called from U-Boot command line interface to manage the keys in OTPs.
stm32key help
stm32key - Manage key on STM32
Usage:
stm32key list : list the supported key with description
stm32key select [<key>] : Select the key identified by <key> or display the key used for read/fuse command
stm32key read [<addr> | -a ] : Read the curent key at <addr> or current / all (-a) key in OTP
stm32key fuse [-y] <addr> : Fuse the current key at addr in OTP
stm32key close [-y] : Close the device, force use of PKH stored in OTP
The optional option -y
is used to skip the confirmation message.
The name of the used <key> is
stm32key list PKHTH : Hash of the 8 ECC Public Keys Hashes Table (ECDSA is the authentication algorithm) OTP24..32 EDMK : Encryption/Decryption Master Key" OTP92..95
stm32key list
PKH : Hash of the ECC Public Key (ECDSA is the authentication algorithm)
OTP24..32
3 Authentication keys provisioning[edit]
The key provisioning is the first step to enable the authentication: burn the keys in OTPs with the key hash output file from STM32 KeyGen.
3.1 Select keys[edit]
Key is selected with the command sm32key select <key>
, with <key>=
sm32key select PKHTH
PKHTH selected
sm32key select PKH
PKH selected
3.2 Load keys file in DDR[edit]
The keys hash file, output file from STM32 KeyGen, must be available in DDR before proceeding the stm32key
command;
this file is loaded at 0xc0000000 in the next examples.
The file publicKeysHash.bin can be loaded from a filesystem partition on a storage device by using the load
command. For example, the file publicKeysHash.bin is in the bootfs (partition 7) on SD card (mmc0):
load mmc 0:7 0xc0000000 publicKeysHash.bin 32 bytes read in 50 ms (0 Bytes/s)
3.3 Verify keys file in DDR[edit]
Once the publicKeysHash.bin file is loaded in DDR, you can verify the content of the file with the command:
stm32key read 0xc0000000
Example for STM32MP13x lines with PKHTH
stm32key read 0xC0000000 Read PKHTH at 0xc0000000 PKHTH OTP 24: [c0000000] 27051956 PKHTH OTP 25: [c0000004] b56aef2d PKHTH OTP 26: [c0000008] 6215263c PKHTH OTP 27: [c000000c] 00000439 PKHTH OTP 28: [c0000010] 00000000 PKHTH OTP 29: [c0000014] 00000000 PKHTH OTP 30: [c0000018] 72429173 PKHTH OTP 31: [c000001c] 05020600
Example for STM32MP15x lines with PKH
stm32key read 0xC0000000 Read PKH at 0xc0000000 PKH OTP 24: [c0000000] 27051956 PKH OTP 25: [c0000004] b56aef2d PKH OTP 26: [c0000008] 6215263c PKH OTP 27: [c000000c] 00000439 PKH OTP 28: [c0000010] 00000000 PKH OTP 29: [c0000014] 00000000 PKH OTP 30: [c0000018] 72429173 PKH OTP 31: [c000001c] 05020600
3.4 Key provisioning[edit]
To write and lock the keys in OTP, you use the command:
stm32key fuse 0xc0000000
![]() |
Verify keys before to confirm the operation, it is a irreversible operation ! |
3.5 Verify keys file in OTP[edit]
After the previous command, the device contains the keys to authenticate images and it can be verified with the command:
stm32key read
Result for STM32MP13x lines with PKHTH
stm32key read PKHTH OTP 24: 27051956 lock : 50000000 PKHTH OTP 25: b56aef2d lock : 50000000 PKHTH OTP 26: 6215263c lock : 50000000 PKHTH OTP 27: 00000439 lock : 50000000 PKHTH OTP 28: 00000000 lock : 50000000 PKHTH OTP 29: 00000000 lock : 50000000 PKHTH OTP 30: 72429173 lock : 50000000 PKHTH OTP 31: 05020600 lock : 50000000
Result for STM32MP15x lines with PKH
stm32key read PKH OTP 24: 27051956 lock : 50000000 PKH OTP 25: b56aef2d lock : 50000000 PKH OTP 26: 6215263c lock : 50000000 PKH OTP 27: 00000439 lock : 50000000 PKH OTP 28: 00000000 lock : 50000000 PKH OTP 29: 00000000 lock : 50000000 PKH OTP 30: 72429173 lock : 50000000 PKH OTP 31: 05020600 lock : 50000000
4 Encryption Decryption Master Key provisioning[edit]
The EDMK key provisioning is the first step to enable the image decryption.
It is only available on STM32MP13x lines .
4.1 Select EDMK[edit]
Key is selected with the command sm32key select <key>
, with <key>=
stm32key select EDMK
EDMK selected
4.2 Load EDMK file in DDR[edit]
The keys file must be available in DDR before proceeding the stm32key
command;
this file is loaded at 0xc0000000 in the next examples.
The file edmk.bin can be loaded from a filesystem partition on a storage device by using the load
command. For example, the file edmk.bin is in the bootfs (partition 7) on SD card (mmc0):
load mmc 0:7 0xc0000000 edmk.bin 32 bytes read in 50 ms (0 Bytes/s)
4.3 Verify EDMK in DDR[edit]
Then you can verify the content of keys files loaded in DDR with the command: sm32key read <addr>
Result for STM32MP13x lines with EDMK and <addr>=0xc0000000
stm32key read 0xc0000000
Read EDMK at 0xc0000000
EDMK OTP 92: [c0000000] 27051956
EDMK OTP 93: [c0000004] b56aef2d
EDMK OTP 94: [c0000008] 6215263c
EDMK OTP 95: [c000000c] 00000439
4.4 EDMK provisioning[edit]
To write and lock the EDMK in OTP, you use the command with the same address:
stm32key fuse 0xc0000000
![]() |
Verify keys before to confirm the operation, it is a irreversible operation ! |
4.5 Verify EDMK in OTP[edit]
After the previous command, the device contains the keys to decrypt the images and it can be verified with the command:
stm32key read
Result for STM32MP13x lines with EDMK
stm32key read EDMK OTP 92: 00000000 lock : 50000000 EDMK OTP 93: 00000000 lock : 50000000 EDMK OTP 94: 00000000 lock : 50000000 EDMK OTP 95: 00000000 lock : 50000000
Warning the content of the key can't be read, it is masked, but the lock property can be verified to ensure the key as been written.
5 Closing the device[edit]
Once the authentication process is confirmed in ROM code and in TF-A, the device can be closed to ensure that only signed images can be used.
This operation is perform with the U-Boot command:
stm32key close
![]() |
This must not be done on STM32MP13 or STM32MP15 part numbers without Secure boot enabled, otherwise the chip will be bricked and could not be used anymore |
{{ApplicableFor |MPUs list=STM32MP13x, STM32MP15x |MPUs checklist=STM32MP13x, STM32MP15x }} __TOC__ == Purpose == In this article, the <code>stm32key</code> U-Boot command is used to '''illustrate''' and '''experiment''' the steps to provision the [[How_to_secure_STM32_MPU#STM32MPU_keys|keys]] in the correct OTP needed to activate [[How_to_secure_STM32_MPU#Secure_Boot|secure boot]] features: authentication and encryption. It also allows to directly set the device to [[How_to_secure_STM32_MPU#Device_life_cycle|'''CLOSED''']] state. === Prerequisite === All the required [[How_to_secure_STM32_MPU#STM32MPU_keys|keys]] have to be generated to provision the OTP. {{Warning| Make sure that a device with Secure boot enabled is used: this is mentioned in the chip part number, for [[STM32MP13_microprocessor#Part_number_codification|STM32MP13]] and [[STM32MP15_microprocessor#Part_number_codification|STM32MP15]], otherwise the device will become permanently unusable.}} == stm32key command == U-Boot in OpenSTLinux embeds a <code>stm32key</code> command that can be called from [[U-Boot_overview#U-Boot command line interface (CLI)|U-Boot command line interface]] to manage the keys in OTPs. {{U-Boot$}} stm32key help stm32key - Manage key on STM32 Usage: stm32key list : list the supported key with description stm32key select [{{HighlightParam|<key>}}] : Select the key identified by <key> or display the key used for read/fuse command stm32key read [<addr> | -a ] : Read the curent key at <addr> or current / all (-a) key in OTP stm32key fuse [-y] <addr> : Fuse the current key at addr in OTP stm32key close [-y] : Close the device, force use of PKH stored in OTP The optional option <code>-y</code> is used to skip the confirmation message. The name of the used {{HighlightParam|<key>}} is * for {{MicroprocessorDevice | device=13}}: {{Highlight|PKHTH}} for authentication and {{Highlight|EDMK}} for encryption {{U-Boot$}} stm32key list {{Highlight|PKHTH}} : Hash of the 8 ECC Public Keys Hashes Table (ECDSA is the authentication algorithm) OTP24..32 {{Highlight|EDMK}} : Encryption/Decryption Master Key" OTP92..95 * for {{MicroprocessorDevice | device=15}}: {{Highlight|PKH}} for authentication {{U-Boot$}} stm32key list {{Highlight|PKH}} : Hash of the ECC Public Key (ECDSA is the authentication algorithm) OTP24..32 ==Authentication keys provisioning== The [[How_to_secure_STM32_MPU#Provisioning|key provisioning]] is the first step to enable the authentication: burn the keys in OTPs with the key hash output file from [[KeyGen_tool|STM32 KeyGen]]. ===Select keys=== Key is selected with the command <code>sm32key select {{HighlightParam|<key>}}</code>, with {{HighlightParam|<key>}}= :* {{Highlight|PKHTH}} for {{MicroprocessorDevice | device=13}} {{U-Boot$}} sm32key select {{Highlight|PKHTH}} PKHTH selected :* {{Highlight|PKH}} for {{MicroprocessorDevice | device=15}} {{U-Boot$}} sm32key select {{Highlight|PKH}} PKH selected ===Load keys file in DDR=== The keys hash file, output file from [[KeyGen_tool|STM32 KeyGen]], must be available in DDR before proceeding the <code>stm32key</code> command;<br/>this file is loaded at {{HighlightParam|0xc0000000}} in the next examples. <div class="mw-collapsible mw-collapsed"> The file {{Highlight|publicKeysHash.bin}} can be loaded from a filesystem partition on a storage device by using the <code>load</code> command. For example, the file {{Highlight|publicKeysHash.bin}} is in the bootfs (partition {{HighlightParam|7}}) on SD card ({{HighlightParam|mmc0}}): {{U-Boot$}} load {{HighlightParam|mmc}} {{HighlightParam|0}}:{{HighlightParam|7}} {{HighlightParam|0xc0000000}} {{Highlight|publicKeysHash.bin}} 32 bytes read in 50 ms (0 Bytes/s)</div></div> ===Verify keys file in DDR=== Once the {{Highlight|publicKeysHash.bin}} file is loaded in DDR, you can verify the content of the file with the command: {{U-Boot$}} stm32key read {{HighlightParam|0xc0000000}} Example for {{MicroprocessorDevice | device=13}} with {{Highlight|PKHTH}} {{U-Boot$}} stm32key read 0xC0000000 Read PKHTH at 0xc0000000 PKHTH OTP 24: [c0000000] 27051956 PKHTH OTP 25: [c0000004] b56aef2d PKHTH OTP 26: [c0000008] 6215263c PKHTH OTP 27: [c000000c] 00000439 PKHTH OTP 28: [c0000010] 00000000 PKHTH OTP 29: [c0000014] 00000000 PKHTH OTP 30: [c0000018] 72429173 PKHTH OTP 31: [c000001c] 05020600 Example for {{MicroprocessorDevice | device=15}} with {{Highlight|PKH}} {{U-Boot$}} stm32key read 0xC0000000 Read PKH at 0xc0000000 PKH OTP 24: [c0000000] 27051956 PKH OTP 25: [c0000004] b56aef2d PKH OTP 26: [c0000008] 6215263c PKH OTP 27: [c000000c] 00000439 PKH OTP 28: [c0000010] 00000000 PKH OTP 29: [c0000014] 00000000 PKH OTP 30: [c0000018] 72429173 PKH OTP 31: [c000001c] 05020600 ===Key provisioning=== To write and lock the keys in OTP, you use the command: {{U-Boot$}} stm32key fuse {{HighlightParam|0xc0000000}} {{Warning| Verify keys before to confirm the operation, it is a irreversible operation !}} ===Verify keys file in OTP=== After the previous command, the device contains the keys to authenticate images and it can be verified with the command: {{U-Boot$}} stm32key read Result for {{MicroprocessorDevice | device=13}} with {{Highlight|PKHTH}} {{U-Boot$}} stm32key read PKHTH OTP 24: 27051956 lock : 50000000 PKHTH OTP 25: b56aef2d lock : 50000000 PKHTH OTP 26: 6215263c lock : 50000000 PKHTH OTP 27: 00000439 lock : 50000000 PKHTH OTP 28: 00000000 lock : 50000000 PKHTH OTP 29: 00000000 lock : 50000000 PKHTH OTP 30: 72429173 lock : 50000000 PKHTH OTP 31: 05020600 lock : 50000000 Result for {{MicroprocessorDevice | device=15}} with {{Highlight|PKH}} {{U-Boot$}} stm32key read PKH OTP 24: 27051956 lock : 50000000 PKH OTP 25: b56aef2d lock : 50000000 PKH OTP 26: 6215263c lock : 50000000 PKH OTP 27: 00000439 lock : 50000000 PKH OTP 28: 00000000 lock : 50000000 PKH OTP 29: 00000000 lock : 50000000 PKH OTP 30: 72429173 lock : 50000000 PKH OTP 31: 05020600 lock : 50000000 ==Encryption Decryption Master Key provisioning== The [[How_to_secure_STM32_MPU#Provisioning|EDMK key provisioning]] is the first step to enable the image decryption. It is only available on {{MicroprocessorDevice | device=13}}. ===Select EDMK=== Key is selected with the command <code>sm32key select {{HighlightParam|<key>}}</code>, with {{HighlightParam|<key>}}= :* {{Highlight|EDMK}} for {{MicroprocessorDevice | device=13}} {{U-Boot$}} stm32key select {{Highlight|EDMK}} EDMK selected ===Load EDMK file in DDR=== The keys file must be available in DDR before proceeding the <code>stm32key</code> command;<br/>this file is loaded at {{HighlightParam|0xc0000000}} in the next examples. <div class="mw-collapsible mw-collapsed"> The file {{Highlight|edmk.bin}} can be loaded from a filesystem partition on a storage device by using the <code>load</code> command. For example, the file {{Highlight|edmk.bin}} is in the bootfs (partition {{HighlightParam|7}}) on SD card ({{HighlightParam|mmc0}}): {{U-Boot$}} load {{HighlightParam|mmc}} {{HighlightParam|0}}:{{HighlightParam|7}} {{HighlightParam|0xc0000000}} {{Highlight|edmk.bin}} 32 bytes read in 50 ms (0 Bytes/s)</div></div> ===Verify EDMK in DDR=== Then you can verify the content of keys files loaded in DDR with the command: <code>sm32key read {{HighlightParam|<addr>}}</code> Result for {{MicroprocessorDevice | device=13}} with {{Highlight|EDMK}} and <addr>=0xc0000000 {{U-Boot$}} stm32key read {{HighlightParam|0xc0000000}} Read EDMK at 0xc0000000 EDMK OTP 92: [c0000000] 27051956 EDMK OTP 93: [c0000004] b56aef2d EDMK OTP 94: [c0000008] 6215263c EDMK OTP 95: [c000000c] 00000439 ===EDMK provisioning=== To write and lock the EDMK in OTP, you use the command with the same address: {{U-Boot$}} stm32key fuse {{HighlightParam|0xc0000000}} {{Warning| Verify keys before to confirm the operation, it is a irreversible operation !}} ===Verify EDMK in OTP=== After the previous command, the device contains the keys to decrypt the images and it can be verified with the command: {{U-Boot$}} stm32key read Result for {{MicroprocessorDevice | device=13}} with {{Highlight|EDMK}} {{U-Boot$}} stm32key read EDMK OTP 92: 00000000 lock : {{HighlightParam|50000000}} EDMK OTP 93: 00000000 lock : {{HighlightParam|50000000}} EDMK OTP 94: 00000000 lock : {{HighlightParam|50000000}} EDMK OTP 95: 00000000 lock : {{HighlightParam|50000000}} Warning the content of the key can't be read, it is masked, but the lock property can be verified to ensure the key as been written. ==Closing the device== Once the authentication process is confirmed in [[How_to_secure_STM32_MPU#ROM_code_secure_boot_validation|ROM code]] and in TF-A, the device can be [[How_to_secure_STM32_MPU#Device_life_cycle|closed]] to ensure that {{Highlight|only signed images}} can be used. [[How_to_secure_STM32_MPU#Close_the_device|This operation]] is perform with the U-Boot command: {{U-Boot$}} stm32key close {{Warning| This must not be done on [[STM32MP13_microprocessor#Security_and_Cortex-A7_frequency|STM32MP13]] or [[STM32MP15_microprocessor#Security_and_Cortex-A7_frequency|STM32MP15]] part numbers without '''Secure boot enabled''', otherwise the chip will be bricked and could not be used anymore}} <noinclude> [[Category:How to populate boards]] [[Category:U-Boot|U-Boot - 9]]{{PublicationRequestId | No TLMS yet | 2022-08-29 | TLMS to be entered by NSA}}</noinclude>
Line 212: | Line 212: | ||
[[Category:How to populate boards]] |
[[Category:How to populate boards]] |
||
[[Category:U-Boot|U-Boot - 9]] |
[[Category:U-Boot|U-Boot - 9]] |
||
+ | {{PublicationRequestId | No TLMS yet | 2022-08-29 | TLMS to be entered by NSA}} |
||
</noinclude> |
</noinclude> |