Registered User mNo edit summary |
Registered User mNo edit summary Tag: 2017 source edit |
||
(176 intermediate revisions by 6 users not shown) | |||
Line 1: | Line 1: | ||
<noinclude> | <noinclude>{{ApplicableFor | ||
{{ | |MPUs list=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x | ||
|MPUs checklist=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x | |||
}} | |||
</noinclude> | </noinclude> | ||
This page explains how to manually update the bootloaders binary (including [[U-Boot_overview|U-Boot]] and [[TF-A_overview|TF-A]]) on boot device (SD card, ''e''•MMC, NOR, NAND) | |||
== Update of SD card == | |||
The user has access to the SD card device partitions: | |||
* on a Linux<sup>®</sup>PC, with a card reader of this PC | |||
* on target, with Linux<sup>®</sup> console or U-Boot console. | |||
[[STM32_MPU_Flash_mapping#SD_card_memory_mapping|The 7 first GPT partitions on the SD card]] are by default in OpenSTLinux BSP: | |||
# {{highlightParam|fsbl1}} or {{highlight|fsbla1}} = TF-A BL2 | |||
# {{highlightParam|fbsl2}} or {{highlight|fsbla2}} = TF-A BL2: second copy (a manual update is not needed by default, only used for fail-safe update) | |||
# '''metadata1''' = TF-A firmware update data : select FIP-A | |||
# '''metadata2''' = TF-A firmware update data : select FIP-A, second copy of the same binary | |||
# '''fip-a''' = FIP, first slot | |||
# '''fip-b''' = FIP, second slot, not required as the first slot is selected in metadata | |||
# '''u-boot-env''' = U-Boot environment | |||
See [[Boot_chain_overview]] for the bootloader definitions. | |||
In the next chapters, the examples are provided for {{MicroprocessorDevice | device=1}} with FSBL partition name {{highlightParam|fsbl1}}/{{highlightParam|fsbl2}} but it is also applicable for {{MicroprocessorDevice | device=2}} with partition name for cortex-A35, with name {{highlight|fsbla1}}/{{highlight|fsbla2}}. | |||
=== On a Linux<sup>®</sup> console with the Linux<sup>®</sup> dd command === | |||
Use the Linux<sup>®</sup> <code>dd</code> command to copy the bootloader files directly to the correct partition: | |||
{{PC$}} dd if={{HighlightParam|<file>}} of=/dev/{{HighlightParam|<dev>}} conv={{HighlightParam|fdatasync}} | |||
{{HighlightParam|<dev>}} is: | |||
* mmcblk{{Highlight|<X>}}p{{Highlight|<n>}}: PC-embedded card reader case or target Linux<sup>®</sup> console | |||
* sd{{Highlight|<X>}}{{Highlight|<n>}}: USB-connected SD card reader case | |||
where {{Highlight|<X>}} is the ID of the device, and {{Highlight|<n>}} the ID of the partition. | |||
The <code>dd</code> command must be repeated for each GPT partition to update. | |||
Note: the dd option {{HighlightParam|conv}}={{HighlightParam|fdatasync}} is used to force synchronous copying. | |||
The U-Boot environment is saved in the partition, named "u-boot-env": ID = {{HighlightParam|7}} in OpenSTLinux BSP. <br> | |||
You can erase this partition to clear this environment; for example, by using the <code>dd</code> command this input file: if={{HighlightParam|/dev/zero}}. | |||
{{PC$}} | When SD card device is {{Highlight|mmcblk0}}, the GPT partition {{HighlightParam|p<n>}} is '''/dev/{{Highlight|mmcblk0}}{{HighlightParam|p<n>}}''' (for example in OpenSTLinux target console or for a PC internal card reader), the update of the SD card is done with: | ||
{{PC$}}dd if={{HighlightParam|tf-a-sdcard.stm32}} of=/dev/{{Highlight|mmcblk0}}{{HighlightParam|p1}} conv=fdatasync | |||
{{PC$}}dd if={{HighlightParam|tf-a-sdcard.stm32}} of=/dev/{{Highlight|mmcblk0}}{{HighlightParam|p2}} conv=fdatasync | |||
{{PC$}}dd if={{HighlightParam|metadata.bin}} of=/dev/{{Highlight|mmcblk0}}{{HighlightParam|p3}} conv=fdatasync | |||
{{PC$}}dd if={{HighlightParam|metadata.bin}} of=/dev/{{Highlight|mmcblk0}}{{HighlightParam|p4}} conv=fdatasync | |||
{{PC$}}dd if={{HighlightParam|fip.bin}} of=/dev/{{Highlight|mmcblk0}}{{HighlightParam|p5}} conv=fdatasync | |||
{{PC$}}dd if=/dev/zero of=/dev/{{Highlight|mmcblk0}}{{HighlightParam|p7}} conv=fdatasync | |||
=== On a U-Boot console === | |||
==== With ums command ==== | |||
Alternatively, with U-Boot [[How to use USB mass storage in U-Boot|<code>ums</code> command]], on mmc dev = {{Highlight|0}},the SD card device on STMicroelectronics board: | |||
{{U-Boot$}}ums 0 mmc {{Highlight|0}} | |||
The exported SD card is mounted on the Linux<sup>®</sup> PC as a block device named sd{{Highlight|<X>}} and the GPT partitions are exported by '''sd{{Highlight|<X>}}{{Highlight|<n>}}''' where: | |||
The | * {{Highlight|<X>}} is the ID of the device starting at '''a''' | ||
* {{Highlight|<n>}} the ID of the partition. | |||
If the block device SD card is available in '''/dev/{{Highlight|sda}}''' (with {{Highlight|<X>}} = '''a''' but this value must be verified on your PC), the partitions are updated with the dd command: | |||
== | {{PC$}}dd if={{HighlightParam|tf-a-sdcard.stm32}} of=/dev/{{Highlight|sda}}{{HighlightParam|1}} conv=fdatasync | ||
{{PC$}}dd if={{HighlightParam|tf-a-sdcard.stm32}} of=/dev/{{Highlight|sda}}{{HighlightParam|2}} conv=fdatasync | |||
{{PC$}}dd if={{HighlightParam|metadata.bin}} of=/dev/{{Highlight|sda}}{{HighlightParam|3}} conv=fdatasync | |||
{{PC$}}dd if={{HighlightParam|metadata.bin}} of=/dev/{{Highlight|sda}}{{HighlightParam|4}} conv=fdatasync | |||
{{PC$}}dd if={{HighlightParam|fip.bin}} of=/dev/{{Highlight|sda}}{{HighlightParam|5}} conv=fdatasync | |||
{{PC$}}dd if=/dev/zero of=/dev/{{Highlight|sda}}{{HighlightParam|7}} conv=fdatasync | |||
{{ | ==== With mmc command ==== | ||
{{ | |||
{{PC$}} dd if=u-boot. | {{DocSource | domain=U-Boot | path=usage/cmd/mmc.html|text=The command <code>mmc</code>}} can be used also to directly write file previously loaded in memory by other U-boot command. | ||
For example, to check partition offset on dev 0, SD card on STMicroelectonics boards: | |||
{{U-Boot$}}mmc dev 0 | |||
{{U-Boot$}}mmc part | |||
Partition Map for MMC device 0 -- Partition Type: EFI | |||
Part Start LBA End LBA Name | |||
Attributes | |||
Type GUID | |||
Partition GUID | |||
1 {{HighlightParam|0x00000022}} {{Highlight|0x00000221}} "fsbl1" | |||
.... | |||
To write TF-A, loaded at {{Highlight|0xC000000}} at blk# = {{HighlightParam|22}} for 256KB ({{Highlight|0x200}}*512) | |||
{{U-Boot$}}mmc write {{Highlight|0xC0000000}} {{HighlightParam|22}} {{Highlight|200}} | |||
With block address (blk#) and clock count (ctn), multiple of block size = LBA of 512 bytes. | |||
== Update of ''e''•MMC == | |||
The user has access to the ''e''•MMC device partitions on target, with Linux<sup>®</sup> console or U-Boot console. | |||
[[STM32_MPU_Flash_mapping#e•MMC_memory_mapping|The ''e''•MMC memory mapping]] are by default: | |||
* FSBL = TF-A is saved in the ''e''•MMC boot partitions (2 copy for fail-safe update) | |||
* Other binaries are in the GPT partitions of the ''e''•MMC user area | |||
# '''metadata1''' = TF-A firmware update data : select FIP-A | |||
# '''metadata2''' = TF-A firmware update data : select FIP-A, second copy of the same binary | |||
# '''fip-a''' = FIP, first slot | |||
# '''fip-b''' = FIP, second slot, not required as the first slot is selected in metadata | |||
# '''u-boot-env''' = U-Boot environment | |||
The user must select the ''e''•MMC hardware partition to update: user data, boot1, or boot2. | |||
=== On a Linux<sup>®</sup> console === | |||
If dev = {{Highlight|mmcblk1}} for ''e''•MMC device (default on STMicroelectronics board). | |||
The boot partitions are available in /dev/{{Highlight|mmcblk1}}{{HighlightParam|boot0}} and /dev/{{Highlight|mmcblk1}}{{HighlightParam|boot1}} <ref>https://www.kernel.org/doc/Documentation/mmc/mmc-dev-parts.txt</ref>. | |||
The user could need to allow access, for example with: | |||
{{Board$}} echo 0 > /sys/class/block/{{Highlight|mmcblk1}}{{HighlightParam|boot0}}/force_ro | |||
The <code>mmc</code> tools allow the boot partition that can be selected <ref>https://manpages.debian.org/buster/mmc-utils/mmc.1.en.html</ref>. | |||
The [[STM32_MPU_ROM_code_overview|ROM code]] requires: | |||
* <send_ack> =1 to enable the boot acknowledge bit in the ''e''•MMC ''ext_csd'' register | |||
* the eMMC boot configuration is: 1 wire configuration and 25 MHz, it is done with the command: | |||
{{Board$}} mmc bootbus set single_backward x1 x1 dev/{{Highlight|mmcblk1}} | |||
To update TF-A in boot1 and select this boot partition (default): | |||
{{Board$}}dd if={{HighlightParam|tf-a-emmc.stm32}} of=/dev/{{Highlight|mmcblk1}}{{HighlightParam|boot0}} conv=fdatasync | |||
{{Board$}}mmc bootpart enable {{HighlightParam|1}} 1 /dev/{{Highlight|mmcblk1}} | |||
To update TF-A in boot2 and select this boot partition (not needed by default, only required for fail-safe update): | |||
{{Board$}}dd if={{HighlightParam|tf-a-emmc.stm32}} of=/dev/{{Highlight|mmcblk1}}{{HighlightParam|boot1}} conv=fdatasync | |||
{{Board$}}mmc bootpart enable {{HighlightParam|2}} 1 /dev/{{Highlight|mmcblk1}} | |||
To update the GPT partitions: | |||
{{Board$}}dd if=/dev/zero of=/dev/{{Highlight|mmcblk1}}{{HighlightParam|p1}} conv=fdatasync | |||
{{Board$}}dd if={{HighlightParam|metadata.bin}} of=/dev/{{Highlight|mmcblk1}}{{HighlightParam|p1}} conv=fdatasync | |||
{{Board$}}dd if={{HighlightParam|metadata.bin}} of=/dev/{{Highlight|mmcblk1}}{{HighlightParam|p2}} conv=fdatasync | |||
{{Board$}}dd if={{HighlightParam|fip.bin}} of=/dev/{{Highlight|mmcblk1}}{{HighlightParam|p3}} conv=fdatasync | |||
The U-Boot environment is saved in the partition, named "u-boot-env": ID = {{HighlightParam|5}} in OpenSTLinux. <br> | |||
You can erase this partition to clear this environment; for example, by using the dd command this input file: if={{HighlightParam|/dev/zero}}. | |||
{{Board$}}dd if=/dev/zero of=/dev/{{Highlight|mmcblk1}}{{HighlightParam|p5}} conv=fdatasync | |||
See also <ref>https://www.emcraft.com/som/stm32mp1/booting-linux-from-emmc</ref>. | |||
=== On a U-Boot console === | |||
If mmc device [dev] = {{Highlight|1}} for ''e''•MMC device in U-Boot (default on STMicroelectronics board). | |||
{{DocSource | domain=U-Boot | path=usage/cmd/mmc.html|text=The command <code>mmc</code>}} is used in U-Boot console for ''e''•MMC device configuration. | |||
mmc {{Highlight|bootbus}} <dev> <boot_bus_width> <reset_boot_bus_width> <boot_mode> | |||
Before the first boot, select the right ''e''•MMC boot configuration (1 wire, 25 MHz) with the command: | |||
{{U-Boot$}}mmc bootbus {{Highlight|1}} 0 0 0 | |||
==== Select boot partition ==== | |||
The targeted ''e''•MMC HW partition is selected in U-Boot by {{DocSource | domain=U-Boot | path=usage/cmd/mmc.html|text= the command <code>mmc partconf</code>}}: | |||
mmc partconf <dev> [[varname] | [<boot_ack> <boot_partition> <partition_access>]] | |||
With: | |||
* dev = {{Highlight|1}} (''e''•MMC device on STMicroelectronics board) | |||
* boot_ack=1 (the boot acknowledge bit in the ''e''•MMC ''ext_csd'' register is needed by [[STM32_MPU_ROM_code_overview|ROM code]]) | |||
* boot_partition = {{HighlightParam|1}} (boot partition 1 enabled for boot) | |||
* partition_access = 0 | |||
** {{HighlightParam|0}}: user data partition (default) | |||
** {{HighlightParam|1}}: boot partition 1 | |||
** {{HighlightParam|2}}: boot partition 2 | |||
Do not change the last parameter {{HighlightParam|partition_access}} value if you do not manually access the boot partition content with <code>mmc read</code> or <code>mmc write</code>. | |||
The command to '''select the boot partition used by ROM code''' on ''e''•MMC at next reboot is: | |||
* for {{Highlight|boot1}}: | |||
{{U-Boot$}}mmc partconf {{Highlight|1}} 1 {{HighlightParam|1}} 0 | |||
* for {{Highlight|boot2}} (not needed by default, only required for fail-safe update): | |||
{{U-Boot$}}mmc partconf {{Highlight|1}} 1 {{HighlightParam|2}} 0 | |||
==== With ums command ==== | |||
The ''e''•MMC update is done with the [[How to use USB mass storage in U-Boot|<code>ums</code> command]], with the U-Boot's partition syntax {{DocSource | domain=U-Boot | path=usage/partitions.html|text=U-Boot's partition syntax }}: | |||
<command> <interface> [devnum][.hwpartnum][:partnum|#partname] | |||
The exported ''e''•MMC is mounted on the Linux<sup>®</sup> PC as a block device named sd{{Highlight|<X>}} and the GPT partitions are exported by '''sd{{Highlight|<X>}}{{Highlight|<n>}}''' where | |||
* {{Highlight|<X>}} is the ID of the device starting at '''a''' | |||
* {{Highlight|<n>}} the ID of the partition. | |||
In the next examples, we assume {{Highlight|<X>}} = '''a''', so the block device ''e''•MMC available in '''/dev/{{Highlight|sda}}''' but this value must be verified on your PC. | |||
'''boot partitions''' | |||
This boot partition by ROM code is selected in previous step [[#select boot partition]], only the selected on needed to be updated. | |||
To update FSBL=TF-A in the {{HighlightParam|boot1}} HW partition. | |||
{{U-Boot$}}ums 0 mmc {{Highlight|1}}.{{HighlightParam|1}} | |||
UMS: LUN 0, dev {{Highlight|1}}, hwpart {{HighlightParam|1}}, sector 0x0, count 0x1000 | |||
On boot partitions, without GPT partitions, just copy TF-A binary on the block device /dev/{{Highlight|sda}} exported by U-Boot. | |||
{{PC$}}dd if={{HighlightParam|tf-a-emmc.stm32}} of=/dev/{{Highlight|sda}} conv=fdatasync | |||
To update {{HighlightParam|boot2}}, change the mmc device to {{Highlight|1}}.{{HighlightParam|2}}; but it not needed by default if [[#select boot partition|'''boot1''' is selected]]: <code>mmc partconf 1 1 {{HighlightParam|1}} 0</code>. | |||
It is only required for fail-safe update, when the boot partition is selected after update with <code>mmc partconf</code>. | |||
{{U-Boot$}}ums 0 mmc {{Highlight|1}}.{{HighlightParam|2}} | |||
UMS: LUN 0, dev {{Highlight|1}}, hwpart {{HighlightParam|2}}, sector 0x0, count 0x1000 | |||
{{PC$}}dd if={{HighlightParam|tf-a-emmc.stm32}} of=/dev/{{Highlight|sda}} conv=fdatasync | |||
And select ''boot2'' partition after update: | |||
{{U-Boot$}}mmc partconf {{Highlight|1}} 1 {{HighlightParam|2}} 0 | |||
'''user data partition''' | |||
To export all the ''e''•MMC in {{HighlightParam|/dev/sda}}, including all GPT partitions in /dev/{{Highlight|sda}}{{HighlightParam|N}}: | |||
{{U-Boot$}}ums 0 mmc {{Highlight|1}} | |||
And copy each binary in the GPT partitions of this block device: | |||
{{PC$}}dd if={{HighlightParam|metadata.bin}} of=/dev/{{Highlight|sda}}{{HighlightParam|1}} conv=fdatasync | |||
{{PC$}}dd if={{HighlightParam|metadata.bin}} of=/dev/{{Highlight|sda}}{{HighlightParam|2}} conv=fdatasync | |||
{{PC$}}dd if={{HighlightParam|fip.bin}} of=/dev/{{Highlight|sda}}{{HighlightParam|3}} conv=fdatasync | |||
And clear the U-Boot environment with | |||
{{PC$}}dd if=/dev/zero of=/dev/{{Highlight|mmcblk1}}{{HighlightParam|p5}} conv=fdatasync | |||
==== With mmc command ==== | |||
{{DocSource | domain=U-Boot | path=usage/cmd/mmc.html|text=The command <code>mmc</code>}} can be used also to directly write file previously loaded in memory by an other U-Boot command. | |||
For example, to check the GPT partition of ''e''•MMC, on dev=1 for STMicroelectronics board: | |||
{{U-Boot$}}mmc dev 1 | |||
{{U-Boot$}}mmc part | |||
To write TF-A , loaded at 0xC000000 at blk# = {{HighlightParam|0}} for boot{{Highlight|1}} for 256KB ({{Highlight|0x200}}*512): | |||
{{U-Boot$}}mmc partconf 1 1 {{HighlightParam|1}} {{Highlight|1}} | |||
{{U-Boot$}}mmc write 0xC0000000 {{HighlightParam|0}} {{Highlight|200}} | |||
{{U-Boot$}}mmc partconf 1 1 {{HighlightParam|1}} {{Highlight|0}} | |||
See in [[#select boot partition]] for details on ''boot_partition''={{HighlightParam|1}} and ''partition_access''={{Highlight|1}} and {{Highlight|0}} of <code>mmc partconf</code>. | |||
To write metadata1, loaded at {{Highlight|0xC000000}} at blk# = {{HighlightParam|0x00}}, size = 1KB ({{Highlight|0x2}}*512) | |||
{{U-Boot$}}mmc write {{Highlight|0xC0000000}} {{HighlightParam|00}} {{Highlight|2}} | |||
With block address (blk#) and clock count (ctn), multiple of block size = LBA of 512 bytes. | |||
== Update of NOR == | |||
The user has access to the NOR device partitions on target, with Linux<sup>®</sup> console or U-Boot console. | |||
[[STM32_MPU_Flash_mapping#NOR_memory_mapping|The 7 first partitions on the NOR device]] are by default in OpenSTLinux BSP: | |||
# {{highlightParam|fsbl1}} or {{highlight|fsbla1}} = TF-A BL2 | |||
# {{highlightParam|fbsl2}} or {{highlight|fsbla2}} = TF-A BL2: second copy (a manual update is not needed by default, only used for fail-safe update) | |||
# '''metadata1''' = TF-A firmware update data : select FIP-A | |||
# '''metadata2''' = TF-A firmware update data : select FIP-A, second copy of the same binary | |||
# '''fip-a''' = FIP, first slot | |||
# '''fip-b''' = FIP, second slot, not required as the first slot is selected in metadata | |||
# '''u-boot-env''' = U-Boot environment | |||
In the next chapters, the examples are provided for {{MicroprocessorDevice | device=1}} with FSBL partition name {{highlightParam|fsbl1}}/{{highlightParam|fsbl2}} but it is also applicable for {{MicroprocessorDevice | device=2}} with partition name for cortex-A35, with name {{highlight|fsbla1}}/{{highlight|fsbla2}}. | |||
=== On a Linux<sup>®</sup> console with the Linux<sup>®</sup> mtd_debug command === | |||
NOR device partitions can be listed using the [[MTD_overview#How_to_use_the_framework|mtdinfo]] command | |||
root:~# mtdinfo -a | |||
Count of MTD devices: 8 | |||
Present MTD devices: mtd0, mtd1, mtd2, mtd3, mtd4, mtd5, mtd6, mtd7 | |||
Sysfs interface supported: yes | |||
mtd0 | |||
Name: fsbl1 | |||
Type: nor | |||
Eraseblock size: 65536 bytes, 64.0 KiB | |||
Amount of eraseblocks: 4 (262144 bytes, 256.0 KiB) | |||
Minimum input/output unit size: 1 byte | |||
Sub-page size: 1 byte | |||
Character device major/minor: 90:0 | |||
Bad blocks are allowed: false | |||
Device is writable: true | |||
mtd1 | |||
Name: fsbl2 | |||
Type: nor | |||
Eraseblock size: 65536 bytes, 64.0 KiB | |||
Amount of eraseblocks: 4 (262144 bytes, 256.0 KiB) | |||
Minimum input/output unit size: 1 byte | |||
Sub-page size: 1 byte | |||
Character device major/minor: 90:2 | |||
Bad blocks are allowed: false | |||
Device is writable: true | |||
mtd2 | |||
Name: metadata1 | |||
Type: nor | |||
Eraseblock size: 65536 bytes, 64.0 KiB | |||
Amount of eraseblocks: 4 (262144 bytes, 256.0 KiB) | |||
Minimum input/output unit size: 1 byte | |||
Sub-page size: 1 byte | |||
Character device major/minor: 90:4 | |||
Bad blocks are allowed: false | |||
Device is writable: true | |||
mtd3 | |||
Name: metadata2 | |||
Type: nor | |||
Eraseblock size: 65536 bytes, 64.0 KiB | |||
Amount of eraseblocks: 4 (262144 bytes, 256.0 KiB) | |||
Minimum input/output unit size: 1 byte | |||
Sub-page size: 1 byte | |||
Character device major/minor: 90:6 | |||
Bad blocks are allowed: false | |||
Device is writable: true | |||
mtd4 | |||
Name: fip-a | |||
Type: nor | |||
Eraseblock size: 65536 bytes, 64.0 KiB | |||
Amount of eraseblocks: 64 (4194304 bytes, 4.0 MiB) | |||
Minimum input/output unit size: 1 byte | |||
Sub-page size: 1 byte | |||
Character device major/minor: 90:8 | |||
Bad blocks are allowed: false | |||
Device is writable: true | |||
mtd5 | |||
Name: fip-b | |||
Type: nor | |||
Eraseblock size: 65536 bytes, 64.0 KiB | |||
Amount of eraseblocks: 64 (4194304 bytes, 4.0 MiB) | |||
Minimum input/output unit size: 1 byte | |||
Sub-page size: 1 byte | |||
Character device major/minor: 90:10 | |||
Bad blocks are allowed: false | |||
Device is writable: true | |||
mtd6 | |||
Name: u-boot-env | |||
Type: nor | |||
Eraseblock size: 65536 bytes, 64.0 KiB | |||
Amount of eraseblocks: 8 (524288 bytes, 512.0 KiB) | |||
Minimum input/output unit size: 1 byte | |||
Sub-page size: 1 byte | |||
Character device major/minor: 90:12 | |||
Bad blocks are allowed: false | |||
Device is writable: true | |||
mtd7 | |||
Name: nor-user | |||
Type: nor | |||
Eraseblock size: 65536 bytes, 64.0 KiB | |||
Amount of eraseblocks: 872 (57147392 bytes, 54.5 MiB) | |||
Minimum input/output unit size: 1 byte | |||
Sub-page size: 1 byte | |||
Character device major/minor: 90:14 | |||
Bad blocks are allowed: false | |||
Device is writable: true | |||
Before writing a NOR partition, it must be erased. | |||
To erase NOR partitions : | |||
root:~# mtd_debug erase /dev/{{HighlightParam|mtd0}} {{Highlight|0}} {{Highlight|0x40000}} | |||
root:~# mtd_debug erase /dev/{{HighlightParam|mtd1}} {{Highlight|0}} {{Highlight|0x40000}} | |||
root:~# mtd_debug erase /dev/{{HighlightParam|mtd2}} {{Highlight|0}} {{Highlight|0x40000}} | |||
root:~# mtd_debug erase /dev/{{HighlightParam|mtd3}} {{Highlight|0}} {{Highlight|0x40000}} | |||
root:~# mtd_debug erase /dev/{{HighlightParam|mtd4}} {{Highlight|0}} {{Highlight|0x400000}} | |||
root:~# mtd_debug erase /dev/{{HighlightParam|mtd5}} {{Highlight|0}} {{Highlight|0x400000}} | |||
root:~# mtd_debug erase /dev/{{HighlightParam|mtd6}} {{Highlight|0}} {{Highlight|0x80000}} | |||
To write binaries in their respective partition : | |||
root:~# mtd_debug write /dev/{{HighlightParam|mtd0}} {{Highlight|0}} {{Highlight|0x40000}} tf-a-nor.stm32 | |||
root:~# mtd_debug write /dev/{{HighlightParam|mtd1}} {{Highlight|0}} {{Highlight|0x40000}} tf-a-nor.stm32 | |||
root:~# mtd_debug write /dev/{{HighlightParam|mtd2}} {{Highlight|0}} {{Highlight|0x40000}} metadata.bin | |||
root:~# mtd_debug write /dev/{{HighlightParam|mtd3}} {{Highlight|0}} {{Highlight|0x40000}} metadata.bin | |||
root:~# mtd_debug write /dev/{{HighlightParam|mtd4}} {{Highlight|0}} {{Highlight|0x400000}} fip.bin | |||
root:~# mtd_debug write /dev/{{HighlightParam|mtd5}} {{Highlight|0}} {{Highlight|0x400000}} fip.bin | |||
=== On a U-Boot console === | |||
NOR device partitions can be listed using the command mtd list which shows start and end offset of all partitions | |||
{{U-Boot$}}mtd list | |||
List of MTD devices: | |||
* {{Highlight|nor1}} | |||
- device: flash@0 | |||
- parent: spi@40430000 | |||
- driver: jedec_spi_nor | |||
- path: /soc@0/ommanager@40500000/spi@40430000/flash@0 | |||
- type: NOR flash | |||
- block size: 0x10000 bytes | |||
- min I/O: 0x1 bytes | |||
- 0x000000000000-0x000004000000 : "nor1" | |||
- 0x000000000000-0x000000040000 : "fsbl1" | |||
- 0x000000040000-0x000000080000 : "fsbl2" | |||
- 0x000000080000-0x0000000c0000 : "metadata1" | |||
- 0x0000000c0000-0x000000100000 : "metadata2" | |||
- {{HighlightParam|0x000000100000}}-{{HighlightParam|0x000000500000}} : "fip-a" | |||
- 0x000000500000-0x000000900000 : "fip-b" | |||
- 0x000000900000-0x000000980000 : "u-boot-env" | |||
- 0x000000980000-0x000004000000 : "nor-user" | |||
In this example, "fip-a" partition is located on {{Highlight|nor1}} device, starts at offset {{HighlightParam|0x000000100000}} and ends at offset {{HighlightParam|0x000000500000}}, fip-a partition size is {{Highlight|0x400000}}. | |||
Before writing NOR partitions, it must be erased. | |||
To erase NOR partitions : | |||
{{U-Boot$}}mtd erase {{Highlight|nor1}} {{HighlightParam|0x000000000000}} {{Highlight|0x40000}} | |||
{{U-Boot$}}mtd erase {{Highlight|nor1}} {{HighlightParam|0x000000040000}} {{Highlight|0x40000}} | |||
{{U-Boot$}}mtd erase {{Highlight|nor1}} {{HighlightParam|0x000000080000}} {{Highlight|0x40000}} | |||
{{U-Boot$}}mtd erase {{Highlight|nor1}} {{HighlightParam|0x0000000c0000}} {{Highlight|0x40000}} | |||
{{U-Boot$}}mtd erase {{Highlight|nor1}} {{HighlightParam|0x000000100000}} {{Highlight|0x400000}} | |||
{{U-Boot$}}mtd erase {{Highlight|nor1}} {{HighlightParam|0x000000500000}} {{Highlight|0x400000}} | |||
{{U-Boot$}}mtd erase {{Highlight|nor1}} {{HighlightParam|0x000000900000}} {{Highlight|0x80000}} | |||
To write "fip-a" binaries previously loaded in DDR at {{HighlightParam|0xC0000000}} in {{Highlight|nor1}} in "fip-a" partition | |||
{{U-Boot$}}mtd write {{Highlight|nor1}} {{HighlightParam|0xC0000000}} {{Highlight|0x000000100000}} {{HighlightParam|0x2DB1C9}} | |||
Writing 2994633 byte(s) at offset 0x00100000 | |||
Or with MTD partition name and with variable $filesize, the size of file loaded with <code>load</code> command in DDR at {{HighlightParam|0xC0000000}}: | |||
{{U-Boot$}}mtd erase {{Highlight|fip-a}} | |||
{{U-Boot$}}mtd write {{Highlight|fip-a}} {{HighlightParam|0xC0000000}} $filesize | |||
== Update of NAND == | |||
The user has access to the NAND device partitions on target, with Linux<sup>®</sup> console or U-Boot console. | |||
[[STM32 MPU Flash mapping#NAND memory mapping|The 8 first partitions on the NAND device]] are by default in OpenSTLinux BSP: | |||
# {{highlightParam|fsbl1}} or {{highlight|fsbla1}} = TF-A BL2 | |||
# {{highlightParam|fbsl2}} or {{highlight|fsbla2}} = TF-A BL2: second copy (a manual update is not needed by default, only used for fail-safe update) | |||
# '''metadata1''' = TF-A firmware update data : select FIP-A | |||
# '''metadata2''' = TF-A firmware update data : select FIP-A, second copy of the same binary | |||
# '''fip-a1''' = FIP, first slot | |||
# '''fip-a2''' = FIP, copy of first slot | |||
# '''fip-b1''' = FIP, second slot, not required as the first slot is selected in metadata | |||
# '''fip-b2''' = FIP, copy of second slot, not required as the first slot is selected in metadata | |||
In the next chapters, the examples are provided for {{MicroprocessorDevice | device=1}} with FSBL partition name {{highlightParam|fsbl1}}/{{highlightParam|fsbl2}} but it is also applicable for {{MicroprocessorDevice | device=2}} with partition name for cortex-A35, with name {{highlight|fsbla1}}/{{highlight|fsbla2}}. | |||
=== On a Linux<sup>®</sup> console with the Linux<sup>®</sup> flash_erase and nandwrite commands === | |||
NAND device partitions can be listed using the [[MTD_overview#How_to_use_the_framework|mtdinfo]] command | |||
root:~# mtdinfo -a | |||
Count of MTD devices: 8 | |||
Present MTD devices: mtd0, mtd1, mtd2, mtd3, mtd4, mtd5, mtd6, mtd7, mtd8 | |||
Sysfs interface supported: yes | |||
mtd0 | |||
Name: fsbl1 | |||
Type: nand | |||
Eraseblock size: 262144 bytes, 256.0 KiB | |||
Amount of eraseblocks: 2 (524288 bytes, 512.0 KiB) | |||
Minimum input/output unit size: 4096 bytes | |||
Sub-page size: 4096 bytes | |||
OOB size: 224 bytes | |||
Character device major/minor: 90:18 | |||
Bad blocks are allowed: true | |||
Device is writable: true | |||
mtd1 | |||
Name: fsbl2 | |||
Type: nand | |||
Eraseblock size: 262144 bytes, 256.0 KiB | |||
Amount of eraseblocks: 2 (524288 bytes, 512.0 KiB) | |||
Minimum input/output unit size: 4096 bytes | |||
Sub-page size: 4096 bytes | |||
OOB size: 224 bytes | |||
Character device major/minor: 90:20 | |||
Bad blocks are allowed: true | |||
Device is writable: true | |||
mtd2 | |||
Name: metadata1 | |||
Type: nand | |||
Eraseblock size: 262144 bytes, 256.0 KiB | |||
Amount of eraseblocks: 2 (524288 bytes, 512.0 KiB) | |||
Minimum input/output unit size: 4096 bytes | |||
Sub-page size: 4096 bytes | |||
OOB size: 224 bytes | |||
Character device major/minor: 90:22 | |||
Bad blocks are allowed: true | |||
Device is writable: true | |||
mtd3 | |||
Name: metadata2 | |||
Type: nand | |||
Eraseblock size: 262144 bytes, 256.0 KiB | |||
Amount of eraseblocks: 2 (524288 bytes, 512.0 KiB) | |||
Minimum input/output unit size: 4096 bytes | |||
Sub-page size: 4096 bytes | |||
OOB size: 224 bytes | |||
Character device major/minor: 90:24 | |||
Bad blocks are allowed: true | |||
Device is writable: true | |||
{{Highlight|mtd4}} | |||
Name: fip-a1 | |||
Type: nand | |||
Eraseblock size: 262144 bytes, 256.0 KiB | |||
Amount of eraseblocks: 16 (4194304 bytes, 4.0 MiB) | |||
Minimum input/output unit size: 4096 bytes | |||
Sub-page size: 4096 bytes | |||
OOB size: 224 bytes | |||
Character device major/minor: 90:26 | |||
Bad blocks are allowed: true | |||
Device is writable: true | |||
mtd5 | |||
Name: fip-a2 | |||
Type: nand | |||
Eraseblock size: 262144 bytes, 256.0 KiB | |||
Amount of eraseblocks: 16 (4194304 bytes, 4.0 MiB) | |||
Minimum input/output unit size: 4096 bytes | |||
Sub-page size: 4096 bytes | |||
OOB size: 224 bytes | |||
Character device major/minor: 90:28 | |||
Bad blocks are allowed: true | |||
Device is writable: true | |||
mtd6 | |||
Name: fip-b1 | |||
Type: nand | |||
Eraseblock size: 262144 bytes, 256.0 KiB | |||
Amount of eraseblocks: 16 (4194304 bytes, 4.0 MiB) | |||
Minimum input/output unit size: 4096 bytes | |||
Sub-page size: 4096 bytes | |||
OOB size: 224 bytes | |||
Character device major/minor: 90:30 | |||
Bad blocks are allowed: true | |||
Device is writable: true | |||
mtd7 | |||
Name: fip-b2 | |||
Type: nand | |||
Eraseblock size: 262144 bytes, 256.0 KiB | |||
Amount of eraseblocks: 16 (4194304 bytes, 4.0 MiB) | |||
Minimum input/output unit size: 4096 bytes | |||
Sub-page size: 4096 bytes | |||
OOB size: 224 bytes | |||
Character device major/minor: 90:32 | |||
Bad blocks are allowed: true | |||
Device is writable: true | |||
mtd8 | |||
Name: UBI | |||
Type: nand | |||
Eraseblock size: 262144 bytes, 256.0 KiB | |||
Amount of eraseblocks: 4024 (1054867456 bytes, 1006.0 MiB) | |||
Minimum input/output unit size: 4096 bytes | |||
Sub-page size: 4096 bytes | |||
OOB size: 224 bytes | |||
Character device major/minor: 90:34 | |||
Bad blocks are allowed: true | |||
Device is writable: true | |||
In this example, "fip-a1" partition is located in /dev/{{Highlight|mtd4}} device | |||
Before writing NAND partitions, it must be erased. | |||
To erase NAND partitions | |||
root:~# flash_erase /dev/{{Highlight|mtd0}} {{HighlightParam|0}} {{HighlightParam|0}} | |||
root:~# flash_erase /dev/{{Highlight|mtd1}} {{HighlightParam|0}} {{HighlightParam|0}} | |||
root:~# flash_erase /dev/{{Highlight|mtd2}} {{HighlightParam|0}} {{HighlightParam|0}} | |||
root:~# flash_erase /dev/{{Highlight|mtd3}} {{HighlightParam|0}} {{HighlightParam|0}} | |||
root:~# flash_erase /dev/{{Highlight|mtd4}} {{HighlightParam|0}} {{HighlightParam|0}} | |||
root:~# flash_erase /dev/{{Highlight|mtd5}} {{HighlightParam|0}} {{HighlightParam|0}} | |||
root:~# flash_erase /dev/{{Highlight|mtd6}} {{HighlightParam|0}} {{HighlightParam|0}} | |||
root:~# flash_erase /dev/{{Highlight|mtd7}} {{HighlightParam|0}} {{HighlightParam|0}} | |||
To write binaries in NAND | |||
root:~# root@stm32mp1:~# nandwrite -p /dev/{{Highlight|mtd0}} tf-a-nand.stm32 | |||
root:~# root@stm32mp1:~# nandwrite -p /dev/{{Highlight|mtd1}} tf-a-nand.stm32 | |||
root:~# root@stm32mp1:~# nandwrite -p /dev/{{Highlight|mtd2}} metadata.bin | |||
root:~# root@stm32mp1:~# nandwrite -p /dev/{{Highlight|mtd3}} metadata.bin | |||
root:~# root@stm32mp1:~# nandwrite -p /dev/{{Highlight|mtd4}} fip.bin | |||
root:~# root@stm32mp1:~# nandwrite -p /dev/{{Highlight|mtd5}} fip.bin | |||
root:~# root@stm32mp1:~# nandwrite -p /dev/{{Highlight|mtd6}} fip.bin | |||
root:~# root@stm32mp1:~# nandwrite -p /dev/{{Highlight|mtd7}} fip.bin | |||
=== On a U-Boot console === | |||
==== With nand command ==== | |||
NAND device partitions can be listed using the command mtd list which shows start and end offset of all partitions | |||
{{U-Boot$}}mtd list | |||
List of MTD devices: | |||
*nand0 | |||
- type: NAND flash | |||
- block size: 0x40000 bytes | |||
- min I/O: 0x1000 bytes | |||
- OOB size: 224 bytes | |||
- OOB available: 118 bytes | |||
- ECC strength: 8 bits | |||
- ECC step size: 512 bytes | |||
- bitflip threshold: 6 bits | |||
- 0x000000000000-0x000040000000 : "nand0" | |||
- 0x000000000000-0x000000080000 : "fsbl1" | |||
- 0x000000080000-0x000000100000 : "fsbl2" | |||
- 0x000000100000-0x000000180000 : "metadata1" | |||
- 0x000000180000-0x000000200000 : "metadata2" | |||
- {{HighlightParam|0x000000200000}}-{{HighlightParam|0x000000600000}} : "fip-a1" | |||
- 0x000000600000-0x000000a00000 : "fip-a2" | |||
- 0x000000a00000-0x000000e00000 : "fip-b1" | |||
- 0x000000e00000-0x000001200000 : "fip-b2" | |||
- 0x000001200000-0x000040000000 : "UBI" | |||
In this example, "fip-a1" partition starts at offset {{HighlightParam|0x000000200000}} and ends at offset {{HighlightParam|0x000000600000}}, fip-a1 partition size is {{HighlightParam|0x400000}}. | |||
Before writing NAND partitions, it must be erased. | |||
{{U-Boot$}}nand erase {{HighlightParam|0x000000000000}} {{HighlightParam|0x80000}} | |||
{{U-Boot$}}nand erase {{HighlightParam|0x000000800000}} {{HighlightParam|0x80000}} | |||
{{U-Boot$}}nand erase {{HighlightParam|0x000001000000}} {{HighlightParam|0x80000}} | |||
{{U-Boot$}}nand erase {{HighlightParam|0x000001800000}} {{HighlightParam|0x80000}} | |||
{{U-Boot$}}nand erase {{HighlightParam|0x000002000000}} {{HighlightParam|0x400000}} | |||
{{U-Boot$}}nand erase {{HighlightParam|0x000006000000}} {{HighlightParam|0x400000}} | |||
{{U-Boot$}}nand erase {{HighlightParam|0x00000a000000}} {{HighlightParam|0x400000}} | |||
{{U-Boot$}}nand erase {{HighlightParam|0x00000e000000}} {{HighlightParam|0x400000}} | |||
To write "fip-a1" binary previously loaded in DDR at {{HighlightParam|0xC0000000}} in "fip-a1" partition | |||
{{U-Boot$}}nand write {{HighlightParam|0xC0000000}} {{HighlightParam|0x000000200000}} {{HighlightParam|400000}} | |||
Or you can use command with MTD partition name (with ${filesize}: the size of the loaded binary set by many command as <code>load</code>) : | |||
{{U-Boot$}}nand erase.part {{Highlight|fip-a1}} | |||
{{U-Boot$}}nand write {{HighlightParam|0xC0000000}} {{Highlight|fip-a1}} $filesize | |||
==== With mtd command ==== | |||
NAND device partitions can be listed using the command mtd list which shows start and end offset of all partitions | |||
{{U-Boot$}}mtd list | |||
List of MTD devices: | |||
*{{Highlight|nand0}} | |||
- type: NAND flash | |||
- block size: 0x40000 bytes | |||
- min I/O: 0x1000 bytes | |||
- OOB size: 224 bytes | |||
- OOB available: 118 bytes | |||
- ECC strength: 8 bits | |||
- ECC step size: 512 bytes | |||
- bitflip threshold: 6 bits | |||
- 0x000000000000-0x000040000000 : "nand0" | |||
- 0x000000000000-0x000000080000 : "fsbl1" | |||
- 0x000000080000-0x000000100000 : "fsbl2" | |||
- 0x000000100000-0x000000180000 : "metadata1" | |||
- 0x000000180000-0x000000200000 : "metadata2" | |||
- {{HighlightParam|0x000000200000}}-{{HighlightParam|0x000000600000}} : "fip-a1" | |||
- 0x000000600000-0x000000a00000 : "fip-a2" | |||
- 0x000000a00000-0x000000e00000 : "fip-b1" | |||
- 0x000000e00000-0x000001200000 : "fip-b2" | |||
- 0x000001200000-0x000040000000 : "UBI" | |||
In this example, "fip-a1" partition starts at offset {{HighlightParam|0x000000200000}} and ends at offset {{HighlightParam|0x000000600000}}, fip-a1 partition size is {{HighlightParam|0x400000}}. | |||
Before writing NAND partitions, it must be erased with offset and size in MTD device. | |||
{{U-Boot$}}mtd erase {{Highlight|nand0}} {{HighlightParam|0x000000000000}} {{HighlightParam|0x80000}} | |||
{{U-Boot$}}mtd erase {{Highlight|nand0}} {{HighlightParam|0x000000800000}} {{HighlightParam|0x80000}} | |||
{{U-Boot$}}mtd erase {{Highlight|nand0}} {{HighlightParam|0x000001000000}} {{HighlightParam|0x80000}} | |||
{{U-Boot$}}mtd erase {{Highlight|nand0}} {{HighlightParam|0x000001800000}} {{HighlightParam|0x80000}} | |||
{{U-Boot$}}mtd erase {{Highlight|nand0}} {{HighlightParam|0x000002000000}} {{HighlightParam|0x400000}} | |||
{{U-Boot$}}mtd erase {{Highlight|nand0}} {{HighlightParam|0x000006000000}} {{HighlightParam|0x400000}} | |||
{{U-Boot$}}mtd erase {{Highlight|nand0}} {{HighlightParam|0x00000a000000}} {{HighlightParam|0x400000}} | |||
{{U-Boot$}}mtd erase {{Highlight|nand0}} {{HighlightParam|0x00000e000000}} {{HighlightParam|0x400000}} | |||
To write "fip-a1" binary previously loaded in DDR at {{HighlightParam|0xC0000000}} in "fip-a1" partition. | |||
Be careful to use {{Highlight|.dontskipff}} option which forces writing empty pages<ref>http://www.linux-mtd.infradead.org/doc/ubi.html#L_flasher_algo: indicated the expected content of empty page for UBI<br>The {{highlightParam|.dontskipff}} option of <code>mtd</code>command forces writing empty pages; it must be used for boot-loader images, it must be not used for UBI images.<br>The inverse option {{highlightParam|.trimfss}} is defined for {{CodeSource|U-Boot|doc/README.nand|nand}} command, it is required only when flashing UBI images or by default empty pages are written.</ref> | |||
{{U-Boot$}}mtd write{{Highlight|.dontskipff}} {{Highlight|nand0}} {{HighlightParam|0xC0000000}} {{HighlightParam|0x000000200000}} {{HighlightParam|400000}} | |||
Or you can use the MTD partition name, for example to write binary previously loaded in DDR at {{HighlightParam|0xC0000000}} in the {{Highlight|fip-a1}} partition and $filesize is the size of the loaded binary. | |||
{{U-Boot$}}mtd erase {{Highlight|fip-a1}} | |||
{{U-Boot$}}mtd write{{Highlight|.dontskipff}} {{Highlight|fip-a1}} {{HighlightParam|0xC0000000}} $filesize | |||
==References== | |||
Please refer to the following links for additional information: | |||
<references /> | |||
<noinclude> | |||
[[Category:How to populate boards]] | |||
{{PublicationRequestId | 26963| 2023-04-24}} | |||
</noinclude> |
Latest revision as of 19:26, 4 November 2024
This page explains how to manually update the bootloaders binary (including U-Boot and TF-A) on boot device (SD card, e•MMC, NOR, NAND)
1. Update of SD card[edit | edit source]
The user has access to the SD card device partitions:
- on a Linux®PC, with a card reader of this PC
- on target, with Linux® console or U-Boot console.
The 7 first GPT partitions on the SD card are by default in OpenSTLinux BSP:
- fsbl1 or fsbla1 = TF-A BL2
- fbsl2 or fsbla2 = TF-A BL2: second copy (a manual update is not needed by default, only used for fail-safe update)
- metadata1 = TF-A firmware update data : select FIP-A
- metadata2 = TF-A firmware update data : select FIP-A, second copy of the same binary
- fip-a = FIP, first slot
- fip-b = FIP, second slot, not required as the first slot is selected in metadata
- u-boot-env = U-Boot environment
See Boot_chain_overview for the bootloader definitions.
In the next chapters, the examples are provided for STM32MP1 series with FSBL partition name fsbl1/fsbl2 but it is also applicable for STM32MP2 series with partition name for cortex-A35, with name fsbla1/fsbla2.
1.1. On a Linux® console with the Linux® dd command[edit | edit source]
Use the Linux® dd
command to copy the bootloader files directly to the correct partition:
<file> of=/dev/<dev> conv=fdatasyncdd if=
<dev> is:
- mmcblk<X>p<n>: PC-embedded card reader case or target Linux® console
- sd<X><n>: USB-connected SD card reader case
where <X> is the ID of the device, and <n> the ID of the partition.
The dd
command must be repeated for each GPT partition to update.
Note: the dd option conv=fdatasync is used to force synchronous copying.
The U-Boot environment is saved in the partition, named "u-boot-env": ID = 7 in OpenSTLinux BSP.
You can erase this partition to clear this environment; for example, by using the dd
command this input file: if=/dev/zero.
When SD card device is mmcblk0, the GPT partition p<n> is /dev/mmcblk0p<n> (for example in OpenSTLinux target console or for a PC internal card reader), the update of the SD card is done with:
tf-a-sdcard.stm32 of=/dev/mmcblk0p1 conv=fdatasync dd if=tf-a-sdcard.stm32 of=/dev/mmcblk0p2 conv=fdatasync dd if=metadata.bin of=/dev/mmcblk0p3 conv=fdatasync dd if=metadata.bin of=/dev/mmcblk0p4 conv=fdatasync dd if=fip.bin of=/dev/mmcblk0p5 conv=fdatasync dd if=/dev/zero of=/dev/mmcblk0p7 conv=fdatasyncdd if=
1.2. On a U-Boot console[edit | edit source]
1.2.1. With ums command[edit | edit source]
Alternatively, with U-Boot ums
command, on mmc dev = 0,the SD card device on STMicroelectronics board:
0ums 0 mmc
The exported SD card is mounted on the Linux® PC as a block device named sd<X> and the GPT partitions are exported by sd<X><n> where:
- <X> is the ID of the device starting at a
- <n> the ID of the partition.
If the block device SD card is available in /dev/sda (with <X> = a but this value must be verified on your PC), the partitions are updated with the dd command:
tf-a-sdcard.stm32 of=/dev/sda1 conv=fdatasync dd if=tf-a-sdcard.stm32 of=/dev/sda2 conv=fdatasync dd if=metadata.bin of=/dev/sda3 conv=fdatasync dd if=metadata.bin of=/dev/sda4 conv=fdatasync dd if=fip.bin of=/dev/sda5 conv=fdatasync dd if=/dev/zero of=/dev/sda7 conv=fdatasyncdd if=
1.2.2. With mmc command[edit | edit source]
The command mmc
can be used also to directly write file previously loaded in memory by other U-boot command.
For example, to check partition offset on dev 0, SD card on STMicroelectonics boards:
MMC device 0 -- Partition Type: EFImmc dev 0 mmc part Partition Map for
LBA End LBA Name Attributes Type GUID Partition GUID 1 0x00000022 0x00000221 "fsbl1" ....Part Start
To write TF-A, loaded at 0xC000000 at blk# = 22 for 256KB (0x200*512)
0xC0000000 22 200mmc write
With block address (blk#) and clock count (ctn), multiple of block size = LBA of 512 bytes.
2. Update of e•MMC[edit | edit source]
The user has access to the e•MMC device partitions on target, with Linux® console or U-Boot console.
The e•MMC memory mapping are by default:
- FSBL = TF-A is saved in the e•MMC boot partitions (2 copy for fail-safe update)
- Other binaries are in the GPT partitions of the e•MMC user area
- metadata1 = TF-A firmware update data : select FIP-A
- metadata2 = TF-A firmware update data : select FIP-A, second copy of the same binary
- fip-a = FIP, first slot
- fip-b = FIP, second slot, not required as the first slot is selected in metadata
- u-boot-env = U-Boot environment
The user must select the e•MMC hardware partition to update: user data, boot1, or boot2.
2.1. On a Linux® console[edit | edit source]
If dev = mmcblk1 for e•MMC device (default on STMicroelectronics board).
The boot partitions are available in /dev/mmcblk1boot0 and /dev/mmcblk1boot1 [1].
The user could need to allow access, for example with:
mmcblk1boot0/force_roecho 0 > /sys/class/block/
The mmc
tools allow the boot partition that can be selected [2].
The ROM code requires:
- <send_ack> =1 to enable the boot acknowledge bit in the e•MMC ext_csd register
- the eMMC boot configuration is: 1 wire configuration and 25 MHz, it is done with the command:
mmcblk1mmc bootbus set single_backward x1 x1 dev/
To update TF-A in boot1 and select this boot partition (default):
tf-a-emmc.stm32 of=/dev/mmcblk1boot0 conv=fdatasync mmc bootpart enable 1 1 /dev/mmcblk1dd if=
To update TF-A in boot2 and select this boot partition (not needed by default, only required for fail-safe update):
tf-a-emmc.stm32 of=/dev/mmcblk1boot1 conv=fdatasync mmc bootpart enable 2 1 /dev/mmcblk1dd if=
To update the GPT partitions:
mmcblk1p1 conv=fdatasync dd if=metadata.bin of=/dev/mmcblk1p1 conv=fdatasync dd if=metadata.bin of=/dev/mmcblk1p2 conv=fdatasync dd if=fip.bin of=/dev/mmcblk1p3 conv=fdatasyncdd if=/dev/zero of=/dev/
The U-Boot environment is saved in the partition, named "u-boot-env": ID = 5 in OpenSTLinux.
You can erase this partition to clear this environment; for example, by using the dd command this input file: if=/dev/zero.
mmcblk1p5 conv=fdatasyncdd if=/dev/zero of=/dev/
See also [3].
2.2. On a U-Boot console[edit | edit source]
If mmc device [dev] = 1 for e•MMC device in U-Boot (default on STMicroelectronics board).
The command mmc
is used in U-Boot console for e•MMC device configuration.
bootbus <dev> <boot_bus_width> <reset_boot_bus_width> <boot_mode>mmc
Before the first boot, select the right e•MMC boot configuration (1 wire, 25 MHz) with the command:
1 0 0 0mmc bootbus
2.2.1. Select boot partition[edit | edit source]
The targeted e•MMC HW partition is selected in U-Boot by the command mmc partconf
:
mmc partconf <dev> [[varname] | [<boot_ack> <boot_partition> <partition_access>]]
With:
- dev = 1 (e•MMC device on STMicroelectronics board)
- boot_ack=1 (the boot acknowledge bit in the e•MMC ext_csd register is needed by ROM code)
- boot_partition = 1 (boot partition 1 enabled for boot)
- partition_access = 0
- 0: user data partition (default)
- 1: boot partition 1
- 2: boot partition 2
Do not change the last parameter partition_access value if you do not manually access the boot partition content with mmc read
or mmc write
.
The command to select the boot partition used by ROM code on e•MMC at next reboot is:
- for boot1:
1 1 1 0mmc partconf
- for boot2 (not needed by default, only required for fail-safe update):
1 1 2 0mmc partconf
2.2.2. With ums command[edit | edit source]
The e•MMC update is done with the ums
command, with the U-Boot's partition syntax U-Boot's partition syntax:
<command> <interface> [devnum][.hwpartnum][:partnum|#partname]
The exported e•MMC is mounted on the Linux® PC as a block device named sd<X> and the GPT partitions are exported by sd<X><n> where
- <X> is the ID of the device starting at a
- <n> the ID of the partition.
In the next examples, we assume <X> = a, so the block device e•MMC available in /dev/sda but this value must be verified on your PC.
boot partitions
This boot partition by ROM code is selected in previous step #select boot partition, only the selected on needed to be updated.
To update FSBL=TF-A in the boot1 HW partition.
1.1 UMS: LUN 0, dev 1, hwpart 1, sector 0x0, count 0x1000ums 0 mmc
On boot partitions, without GPT partitions, just copy TF-A binary on the block device /dev/sda exported by U-Boot.
tf-a-emmc.stm32 of=/dev/sda conv=fdatasyncdd if=
To update boot2, change the mmc device to 1.2; but it not needed by default if boot1 is selected: mmc partconf 1 1 1 0
.
It is only required for fail-safe update, when the boot partition is selected after update with mmc partconf
.
1.2 UMS: LUN 0, dev 1, hwpart 2, sector 0x0, count 0x1000 dd if=tf-a-emmc.stm32 of=/dev/sda conv=fdatasyncums 0 mmc
And select boot2 partition after update:
1 1 2 0mmc partconf
user data partition
To export all the e•MMC in /dev/sda, including all GPT partitions in /dev/sdaN:
1ums 0 mmc
And copy each binary in the GPT partitions of this block device:
metadata.bin of=/dev/sda1 conv=fdatasync dd if=metadata.bin of=/dev/sda2 conv=fdatasync dd if=fip.bin of=/dev/sda3 conv=fdatasyncdd if=
And clear the U-Boot environment with
mmcblk1p5 conv=fdatasyncdd if=/dev/zero of=/dev/
2.2.3. With mmc command[edit | edit source]
The command mmc
can be used also to directly write file previously loaded in memory by an other U-Boot command.
For example, to check the GPT partition of e•MMC, on dev=1 for STMicroelectronics board:
mmc dev 1
mmc part
To write TF-A , loaded at 0xC000000 at blk# = 0 for boot1 for 256KB (0x200*512):
1 1 mmc write 0xC0000000 0 200 mmc partconf 1 1 1 0mmc partconf 1 1
See in #select boot partition for details on boot_partition=1 and partition_access=1 and 0 of mmc partconf
.
To write metadata1, loaded at 0xC000000 at blk# = 0x00, size = 1KB (0x2*512)
0xC0000000 00 2mmc write
With block address (blk#) and clock count (ctn), multiple of block size = LBA of 512 bytes.
3. Update of NOR[edit | edit source]
The user has access to the NOR device partitions on target, with Linux® console or U-Boot console.
The 7 first partitions on the NOR device are by default in OpenSTLinux BSP:
- fsbl1 or fsbla1 = TF-A BL2
- fbsl2 or fsbla2 = TF-A BL2: second copy (a manual update is not needed by default, only used for fail-safe update)
- metadata1 = TF-A firmware update data : select FIP-A
- metadata2 = TF-A firmware update data : select FIP-A, second copy of the same binary
- fip-a = FIP, first slot
- fip-b = FIP, second slot, not required as the first slot is selected in metadata
- u-boot-env = U-Boot environment
In the next chapters, the examples are provided for STM32MP1 series with FSBL partition name fsbl1/fsbl2 but it is also applicable for STM32MP2 series with partition name for cortex-A35, with name fsbla1/fsbla2.
3.1. On a Linux® console with the Linux® mtd_debug command[edit | edit source]
NOR device partitions can be listed using the mtdinfo command
MTD devices: 8 Present MTD devices: mtd0, mtd1, mtd2, mtd3, mtd4, mtd5, mtd6, mtd7 Sysfs interface supported: yes mtd0 Name: fsbl1 Type: nor Eraseblock size: 65536 bytes, 64.0 KiB Amount of eraseblocks: 4 (262144 bytes, 256.0 KiB) Minimum input/output unit size: 1 byte Sub-page size: 1 byte Character device major/minor: 90:0 Bad blocks are allowed: false Device is writable: true mtd1 Name: fsbl2 Type: nor Eraseblock size: 65536 bytes, 64.0 KiB Amount of eraseblocks: 4 (262144 bytes, 256.0 KiB) Minimum input/output unit size: 1 byte Sub-page size: 1 byte Character device major/minor: 90:2 Bad blocks are allowed: false Device is writable: true mtd2 Name: metadata1 Type: nor Eraseblock size: 65536 bytes, 64.0 KiB Amount of eraseblocks: 4 (262144 bytes, 256.0 KiB) Minimum input/output unit size: 1 byte Sub-page size: 1 byte Character device major/minor: 90:4 Bad blocks are allowed: false Device is writable: true mtd3 Name: metadata2 Type: nor Eraseblock size: 65536 bytes, 64.0 KiB Amount of eraseblocks: 4 (262144 bytes, 256.0 KiB) Minimum input/output unit size: 1 byte Sub-page size: 1 byte Character device major/minor: 90:6 Bad blocks are allowed: false Device is writable: true mtd4 Name: fip-a Type: nor Eraseblock size: 65536 bytes, 64.0 KiB Amount of eraseblocks: 64 (4194304 bytes, 4.0 MiB) Minimum input/output unit size: 1 byte Sub-page size: 1 byte Character device major/minor: 90:8 Bad blocks are allowed: false Device is writable: true mtd5 Name: fip-b Type: nor Eraseblock size: 65536 bytes, 64.0 KiB Amount of eraseblocks: 64 (4194304 bytes, 4.0 MiB) Minimum input/output unit size: 1 byte Sub-page size: 1 byte Character device major/minor: 90:10 Bad blocks are allowed: false Device is writable: true mtd6 Name: u-boot-env Type: nor Eraseblock size: 65536 bytes, 64.0 KiB Amount of eraseblocks: 8 (524288 bytes, 512.0 KiB) Minimum input/output unit size: 1 byte Sub-page size: 1 byte Character device major/minor: 90:12 Bad blocks are allowed: false Device is writable: true mtd7 Name: nor-user Type: nor Eraseblock size: 65536 bytes, 64.0 KiB Amount of eraseblocks: 872 (57147392 bytes, 54.5 MiB) Minimum input/output unit size: 1 byte Sub-page size: 1 byte Character device major/minor: 90:14 Bad blocks are allowed: false Device is writable: trueroot:~# mtdinfo -a Count of
Before writing a NOR partition, it must be erased. To erase NOR partitions :
mtd0 0 0x40000 root:~# mtd_debug erase /dev/mtd1 0 0x40000 root:~# mtd_debug erase /dev/mtd2 0 0x40000 root:~# mtd_debug erase /dev/mtd3 0 0x40000 root:~# mtd_debug erase /dev/mtd4 0 0x400000 root:~# mtd_debug erase /dev/mtd5 0 0x400000 root:~# mtd_debug erase /dev/mtd6 0 0x80000root:~# mtd_debug erase /dev/
To write binaries in their respective partition :
mtd0 0 0x40000 tf-a-nor.stm32 root:~# mtd_debug write /dev/mtd1 0 0x40000 tf-a-nor.stm32 root:~# mtd_debug write /dev/mtd2 0 0x40000 metadata.bin root:~# mtd_debug write /dev/mtd3 0 0x40000 metadata.bin root:~# mtd_debug write /dev/mtd4 0 0x400000 fip.bin root:~# mtd_debug write /dev/mtd5 0 0x400000 fip.binroot:~# mtd_debug write /dev/
3.2. On a U-Boot console[edit | edit source]
NOR device partitions can be listed using the command mtd list which shows start and end offset of all partitions
MTD devices: * nor1 - device: flash@0 - parent: spi@40430000 - driver: jedec_spi_nor - path: /soc@0/ommanager@40500000/spi@40430000/flash@0 - type: NOR flash - block size: 0x10000 bytes - min I/O: 0x1 bytes - 0x000000000000-0x000004000000 : "nor1" - 0x000000000000-0x000000040000 : "fsbl1" - 0x000000040000-0x000000080000 : "fsbl2" - 0x000000080000-0x0000000c0000 : "metadata1" - 0x0000000c0000-0x000000100000 : "metadata2" - 0x000000100000-0x000000500000 : "fip-a" - 0x000000500000-0x000000900000 : "fip-b" - 0x000000900000-0x000000980000 : "u-boot-env" - 0x000000980000-0x000004000000 : "nor-user"mtd list List of
In this example, "fip-a" partition is located on nor1 device, starts at offset 0x000000100000 and ends at offset 0x000000500000, fip-a partition size is 0x400000.
Before writing NOR partitions, it must be erased. To erase NOR partitions :
nor1 0x000000000000 0x40000 mtd erase nor1 0x000000040000 0x40000 mtd erase nor1 0x000000080000 0x40000 mtd erase nor1 0x0000000c0000 0x40000 mtd erase nor1 0x000000100000 0x400000 mtd erase nor1 0x000000500000 0x400000 mtd erase nor1 0x000000900000 0x80000mtd erase
To write "fip-a" binaries previously loaded in DDR at 0xC0000000 in nor1 in "fip-a" partition
nor1 0xC0000000 0x000000100000 0x2DB1C9 Writing 2994633 byte(s) at offset 0x00100000mtd write
Or with MTD partition name and with variable $filesize, the size of file loaded with load
command in DDR at 0xC0000000:
fip-a mtd write fip-a 0xC0000000 $filesizemtd erase
4. Update of NAND[edit | edit source]
The user has access to the NAND device partitions on target, with Linux® console or U-Boot console.
The 8 first partitions on the NAND device are by default in OpenSTLinux BSP:
- fsbl1 or fsbla1 = TF-A BL2
- fbsl2 or fsbla2 = TF-A BL2: second copy (a manual update is not needed by default, only used for fail-safe update)
- metadata1 = TF-A firmware update data : select FIP-A
- metadata2 = TF-A firmware update data : select FIP-A, second copy of the same binary
- fip-a1 = FIP, first slot
- fip-a2 = FIP, copy of first slot
- fip-b1 = FIP, second slot, not required as the first slot is selected in metadata
- fip-b2 = FIP, copy of second slot, not required as the first slot is selected in metadata
In the next chapters, the examples are provided for STM32MP1 series with FSBL partition name fsbl1/fsbl2 but it is also applicable for STM32MP2 series with partition name for cortex-A35, with name fsbla1/fsbla2.
4.1. On a Linux® console with the Linux® flash_erase and nandwrite commands[edit | edit source]
NAND device partitions can be listed using the mtdinfo command
MTD devices: 8 Present MTD devices: mtd0, mtd1, mtd2, mtd3, mtd4, mtd5, mtd6, mtd7, mtd8 Sysfs interface supported: yes mtd0 Name: fsbl1 Type: nand Eraseblock size: 262144 bytes, 256.0 KiB Amount of eraseblocks: 2 (524288 bytes, 512.0 KiB) Minimum input/output unit size: 4096 bytes Sub-page size: 4096 bytes OOB size: 224 bytes Character device major/minor: 90:18 Bad blocks are allowed: true Device is writable: true mtd1 Name: fsbl2 Type: nand Eraseblock size: 262144 bytes, 256.0 KiB Amount of eraseblocks: 2 (524288 bytes, 512.0 KiB) Minimum input/output unit size: 4096 bytes Sub-page size: 4096 bytes OOB size: 224 bytes Character device major/minor: 90:20 Bad blocks are allowed: true Device is writable: true mtd2 Name: metadata1 Type: nand Eraseblock size: 262144 bytes, 256.0 KiB Amount of eraseblocks: 2 (524288 bytes, 512.0 KiB) Minimum input/output unit size: 4096 bytes Sub-page size: 4096 bytes OOB size: 224 bytes Character device major/minor: 90:22 Bad blocks are allowed: true Device is writable: true mtd3 Name: metadata2 Type: nand Eraseblock size: 262144 bytes, 256.0 KiB Amount of eraseblocks: 2 (524288 bytes, 512.0 KiB) Minimum input/output unit size: 4096 bytes Sub-page size: 4096 bytes OOB size: 224 bytes Character device major/minor: 90:24 Bad blocks are allowed: true Device is writable: true mtd4 Name: fip-a1 Type: nand Eraseblock size: 262144 bytes, 256.0 KiB Amount of eraseblocks: 16 (4194304 bytes, 4.0 MiB) Minimum input/output unit size: 4096 bytes Sub-page size: 4096 bytes OOB size: 224 bytes Character device major/minor: 90:26 Bad blocks are allowed: true Device is writable: true mtd5 Name: fip-a2 Type: nand Eraseblock size: 262144 bytes, 256.0 KiB Amount of eraseblocks: 16 (4194304 bytes, 4.0 MiB) Minimum input/output unit size: 4096 bytes Sub-page size: 4096 bytes OOB size: 224 bytes Character device major/minor: 90:28 Bad blocks are allowed: true Device is writable: true mtd6 Name: fip-b1 Type: nand Eraseblock size: 262144 bytes, 256.0 KiB Amount of eraseblocks: 16 (4194304 bytes, 4.0 MiB) Minimum input/output unit size: 4096 bytes Sub-page size: 4096 bytes OOB size: 224 bytes Character device major/minor: 90:30 Bad blocks are allowed: true Device is writable: true mtd7 Name: fip-b2 Type: nand Eraseblock size: 262144 bytes, 256.0 KiB Amount of eraseblocks: 16 (4194304 bytes, 4.0 MiB) Minimum input/output unit size: 4096 bytes Sub-page size: 4096 bytes OOB size: 224 bytes Character device major/minor: 90:32 Bad blocks are allowed: true Device is writable: true mtd8 Name: UBI Type: nand Eraseblock size: 262144 bytes, 256.0 KiB Amount of eraseblocks: 4024 (1054867456 bytes, 1006.0 MiB) Minimum input/output unit size: 4096 bytes Sub-page size: 4096 bytes OOB size: 224 bytes Character device major/minor: 90:34 Bad blocks are allowed: true Device is writable: trueroot:~# mtdinfo -a Count of
In this example, "fip-a1" partition is located in /dev/mtd4 device
Before writing NAND partitions, it must be erased. To erase NAND partitions
mtd0 0 0 root:~# flash_erase /dev/mtd1 0 0 root:~# flash_erase /dev/mtd2 0 0 root:~# flash_erase /dev/mtd3 0 0 root:~# flash_erase /dev/mtd4 0 0 root:~# flash_erase /dev/mtd5 0 0 root:~# flash_erase /dev/mtd6 0 0 root:~# flash_erase /dev/mtd7 0 0root:~# flash_erase /dev/
To write binaries in NAND
mtd0 tf-a-nand.stm32 root:~# root@stm32mp1:~# nandwrite -p /dev/mtd1 tf-a-nand.stm32 root:~# root@stm32mp1:~# nandwrite -p /dev/mtd2 metadata.bin root:~# root@stm32mp1:~# nandwrite -p /dev/mtd3 metadata.bin root:~# root@stm32mp1:~# nandwrite -p /dev/mtd4 fip.bin root:~# root@stm32mp1:~# nandwrite -p /dev/mtd5 fip.bin root:~# root@stm32mp1:~# nandwrite -p /dev/mtd6 fip.bin root:~# root@stm32mp1:~# nandwrite -p /dev/mtd7 fip.binroot:~# root@stm32mp1:~# nandwrite -p /dev/
4.2. On a U-Boot console[edit | edit source]
4.2.1. With nand command[edit | edit source]
NAND device partitions can be listed using the command mtd list which shows start and end offset of all partitions
MTD devices: *nand0 - type: NAND flash - block size: 0x40000 bytes - min I/O: 0x1000 bytes - OOB size: 224 bytes - OOB available: 118 bytes - ECC strength: 8 bits - ECC step size: 512 bytes - bitflip threshold: 6 bits - 0x000000000000-0x000040000000 : "nand0" - 0x000000000000-0x000000080000 : "fsbl1" - 0x000000080000-0x000000100000 : "fsbl2" - 0x000000100000-0x000000180000 : "metadata1" - 0x000000180000-0x000000200000 : "metadata2" - 0x000000200000-0x000000600000 : "fip-a1" - 0x000000600000-0x000000a00000 : "fip-a2" - 0x000000a00000-0x000000e00000 : "fip-b1" - 0x000000e00000-0x000001200000 : "fip-b2" - 0x000001200000-0x000040000000 : "UBI"mtd list List of
In this example, "fip-a1" partition starts at offset 0x000000200000 and ends at offset 0x000000600000, fip-a1 partition size is 0x400000.
Before writing NAND partitions, it must be erased.
0x000000000000 0x80000 nand erase 0x000000800000 0x80000 nand erase 0x000001000000 0x80000 nand erase 0x000001800000 0x80000 nand erase 0x000002000000 0x400000 nand erase 0x000006000000 0x400000 nand erase 0x00000a000000 0x400000 nand erase 0x00000e000000 0x400000nand erase
To write "fip-a1" binary previously loaded in DDR at 0xC0000000 in "fip-a1" partition
0xC0000000 0x000000200000 400000nand write
Or you can use command with MTD partition name (with ${filesize}: the size of the loaded binary set by many command as load
) :
fip-a1 nand write 0xC0000000 fip-a1 $filesizenand erase.part
4.2.2. With mtd command[edit | edit source]
NAND device partitions can be listed using the command mtd list which shows start and end offset of all partitions
MTD devices: *nand0 - type: NAND flash - block size: 0x40000 bytes - min I/O: 0x1000 bytes - OOB size: 224 bytes - OOB available: 118 bytes - ECC strength: 8 bits - ECC step size: 512 bytes - bitflip threshold: 6 bits - 0x000000000000-0x000040000000 : "nand0" - 0x000000000000-0x000000080000 : "fsbl1" - 0x000000080000-0x000000100000 : "fsbl2" - 0x000000100000-0x000000180000 : "metadata1" - 0x000000180000-0x000000200000 : "metadata2" - 0x000000200000-0x000000600000 : "fip-a1" - 0x000000600000-0x000000a00000 : "fip-a2" - 0x000000a00000-0x000000e00000 : "fip-b1" - 0x000000e00000-0x000001200000 : "fip-b2" - 0x000001200000-0x000040000000 : "UBI"mtd list List of
In this example, "fip-a1" partition starts at offset 0x000000200000 and ends at offset 0x000000600000, fip-a1 partition size is 0x400000.
Before writing NAND partitions, it must be erased with offset and size in MTD device.
nand0 0x000000000000 0x80000 mtd erase nand0 0x000000800000 0x80000 mtd erase nand0 0x000001000000 0x80000 mtd erase nand0 0x000001800000 0x80000 mtd erase nand0 0x000002000000 0x400000 mtd erase nand0 0x000006000000 0x400000 mtd erase nand0 0x00000a000000 0x400000 mtd erase nand0 0x00000e000000 0x400000mtd erase
To write "fip-a1" binary previously loaded in DDR at 0xC0000000 in "fip-a1" partition.
Be careful to use .dontskipff option which forces writing empty pages[4]
.dontskipff nand0 0xC0000000 0x000000200000 400000mtd write
Or you can use the MTD partition name, for example to write binary previously loaded in DDR at 0xC0000000 in the fip-a1 partition and $filesize is the size of the loaded binary.
fip-a1 mtd write.dontskipff fip-a1 0xC0000000 $filesizemtd erase
5. References[edit | edit source]
Please refer to the following links for additional information:
- ↑ https://www.kernel.org/doc/Documentation/mmc/mmc-dev-parts.txt
- ↑ https://manpages.debian.org/buster/mmc-utils/mmc.1.en.html
- ↑ https://www.emcraft.com/som/stm32mp1/booting-linux-from-emmc
- ↑ http://www.linux-mtd.infradead.org/doc/ubi.html#L_flasher_algo: indicated the expected content of empty page for UBI
The .dontskipff option ofmtd
command forces writing empty pages; it must be used for boot-loader images, it must be not used for UBI images.
The inverse option .trimfss is defined for nand command, it is required only when flashing UBI images or by default empty pages are written.