Last edited 8 months ago

How to manually update bootloaders: Difference between revisions


Revision as of 08:48, 7 November 2018

Template:ArticleMainWriter Template:ArticleApprovedVersion


This page explains how to manually update the U-Boot binaries on an SD Card.

1. Copying a binary to an SD card with the Linux dd command[edit | edit source]

When you have access to the device (with the card reader of a PC, or the UMS command on a target), the 3 first partitions on the SDCard are:

  1. FSBL1
  2. FSBL2
  3. SSBL

See Boot_chains_overview, for the bootloader definitions.

You can use the Linux dd command to copy the FSBL and SSBL directly to the correct partition:

 Template:PC$  dd if=<file> of=/dev/<dev> conv=fdatasync

<dev> is:

  • mmcblk<X>p<n> : PC-embedded card reader case
  • sd<X><N> : USB-connected SD card reader case

where <X> is the ID of the device, and <n> the ID of the partition.

Note: the dd option conv=fdatasync is used to force synchronous copying.

2. Trusted boot chain update example[edit | edit source]

The internal card reader is /dev/mmcblk0, partition <n> is /dev/mmcblk0p<n>:

 Template:PC$  dd if=tf-a.stm32 of=/dev/mmcblk0p1 conv=fdatasync
 Template:PC$  dd if=tf-a.stm32 of=/dev/mmcblk0p2 conv=fdatasync
 Template:PC$  dd if=u-boot.stm32 of=/dev/mmcblk0p3 conv=fdatasync

3. Basic boot chain udpate example[edit | edit source]

The USB card reader is /dev/sdb, partition <n> is /dev/sdb<n>

 Template:PC$  dd if=u-boot-spl.stm32 of=/dev/sdb1 conv=fdatasync
 Template:PC$  dd if=u-boot-spl.stm32 of=/dev/sdb2 conv=fdatasync
 Template:PC$  dd if=u-boot.img of=/dev/sdb3 conv=fdatasync