This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Template:ArticleMainWriter Template:ReviewersList Template:ArticleApprovedVersion
1 Article purpose[edit source]
The article aims to give some information useful to start with the scp Linux command.
2 Introduction[edit source]
The scp[1] copies files between hosts on a network. It uses ssh[2] (remote login program) for data transfer, uses the same authentication and provides the same security as ssh.
This article focuses on the file transfer between a host PC and a STMicroelectronics board over a network connection.
3 Installation on your target[edit source]
The scp is installed on the STMicroelectronics images via the package openssh.
4 Installation on your PC[edit source]
The package openssh-client must be installed on your host PC to perform a file transfer over network with the scp.
On Ubuntu:
sudo apt-get install openssh-client
5 Getting started[edit source]
- Your host PC and your board are connected to your local network through
- The board IP address (<board ip address>) has been retrieved thanks to the ip Linux command line
- Upload a file (<host file path>/<example.txt>) from your host PC to your board:
scp <host file path>/<example.txt> root@<board ip address>:/<board file path>/
Example (assuming that <board ip address> is a.b.c.d): Copy the example.txt host PC file in the /home/root/ board directory echo "scp example: from host PC to board" > ./example.txt scp ./example.txt root@a.b.c.d:/home/root Check the result on the board cat /home/root/example.txt scp example
- Download a file (/<board file path>/<example.txt>) from your board to your host PC:
scp root@<board ip address>:/<board file path>/<example.txt> <host file path>/
Example (assuming that <board ip address> is a.b.c.d): Copy the example.txt board file in the current directory of the host PC echo "scp example: from board to host PC" > /home/root/example.txt scp root@a.b.c.d:/home/root/example.txt ./ Check the result on the host PC cat ./example.txt scp example: from board to host PC