deleted>Frq08988 mNo edit summary |
Registered User mNo edit summary |
||
(3 intermediate revisions by the same user not shown) | |||
Line 1: | Line 1: | ||
==Article purpose== | ==Article purpose== | ||
The article aims to give some information useful to start with the '''''scp''''' Linux command. | The article aims to give some information useful to start with the '''''scp''''' Linux command. | ||
Line 26: | Line 18: | ||
==Getting started == | ==Getting started == | ||
* Your host PC and your board are connected to your local network through {{UpdateNeededForNewBoard|Point to the Ethernet connector (if any) of the new board}} | * Your host PC and your board are connected to your local network through {{UpdateNeededForNewBoard|Point to the Ethernet connector (if any) of the new board}} | ||
:* the [[ | :* the [[STM32MP157x-EV1 - hardware description#MB1262-CN3|STM32MP157x-EV1 Evaluation board CN3 Ethernet connector]] | ||
:* the [[ | :* the [[STM32MP157x-DKx - hardware_description#MB1272-CN8|STM32MP157x-DKx Discovery kit CN8 Ethernet connector]] | ||
* The board IP address (''<board ip address>'') has been retrieved thanks to the [[IP Linux command line|''ip'' Linux command line]] | * The board IP address (''<board ip address>'') has been retrieved thanks to the [[IP Linux command line|''ip'' Linux command line]] | ||
Line 58: | Line 50: | ||
<references /> | <references /> | ||
<noinclude> | |||
[[Category:How to run use cases]] | |||
[[Category:How to populate boards]] | |||
{{PublicationRequestId | 7893 | 2018-07-03 | AlainF}} | |||
</noinclude> |
Revision as of 17:11, 10 April 2020
1. Article purpose[edit | edit source]
The article aims to give some information useful to start with the scp Linux command.
2. Introduction[edit | edit source]
The scp[1] copies files between hosts on a network. It uses ssh[2] (remote login program) for data transfer, uses the same authentication and provides the same security as ssh.
This article focuses on the file transfer between a host PC and a STMicroelectronics board over a network connection.
3. Installation on your target[edit | edit source]
The scp is installed on the STMicroelectronics images via the package openssh.
4. Installation on your PC[edit | edit source]
The package openssh-client must be installed on your host PC to perform a file transfer over network with the scp.
On Ubuntu:
Template:PC$ sudo apt-get install openssh-client
5. Getting started[edit | edit source]
- Your host PC and your board are connected to your local network through Template:UpdateNeededForNewBoard
- The board IP address (<board ip address>) has been retrieved thanks to the ip Linux command line
- Upload a file (<host file path>/<example.txt>) from your host PC to your board:
Template:PC$ scp <host file path>/<example.txt> root@<board ip address>:/<board file path>/
Template:PC$ echo "scp example: from host PC to board" > ./example.txt Template:PC$ scp ./example.txt root@a.b.c.d:/home/root Check the result on the board Template:Board$ cat /home/root/example.txt scp exampleExample (assuming that <board ip address> is a.b.c.d): Copy the example.txt host PC file in the /home/root/ board directory
- Download a file (/<board file path>/<example.txt>) from your board to your host PC:
Template:PC$ scp root@<board ip address>:/<board file path>/<example.txt> <host file path>/
Template:Board$ echo "scp example: from board to host PC" > /home/root/example.txt Template:PC$ scp root@a.b.c.d:/home/root/example.txt ./ Check the result on the host PC Template:Board$ cat ./example.txt scp example: from board to host PCExample (assuming that <board ip address> is a.b.c.d): Copy the example.txt board file in the current directory of the host PC
6. References[edit | edit source]