Registered User mNo edit summary |
Registered User No edit summary |
||
(4 intermediate revisions by 2 users not shown) | |||
Line 1: | Line 1: | ||
{{ApplicableFor | |||
|MPUs list=STM32MP13x, STM32MP15x | |MPUs list=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x | ||
|MPUs checklist=STM32MP13x,STM32MP15x | |MPUs checklist=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x | ||
}}</noinclude> | }} | ||
<noinclude></noinclude> | |||
==Purpose== | ==Purpose== | ||
The purpose of this article is to introduce EXT4 filesystem: | The purpose of this article is to introduce EXT4 filesystem: | ||
Line 48: | Line 49: | ||
* Mount "userfs". | * Mount "userfs". | ||
{{Board$}} mount /dev/mmcblk0p7 /media/ | {{Board$}}mount /dev/mmcblk0p7 /media/ | ||
* Check that "userfs" partition is mounted. | * Check that "userfs" partition is mounted. | ||
{{Board$}} mount | grep "/media" | {{Board$}}mount | grep "/media" | ||
/dev/mmcblk0p7 on /media type ext4 (rw,sync,relatime) | /dev/mmcblk0p7 on /media type ext4 (rw,sync,relatime) | ||
Line 58: | Line 59: | ||
* Format a MMC partition (mmcblk0p7 will be used in this example). | * Format a MMC partition (mmcblk0p7 will be used in this example). | ||
{{Board$}} mke2fs -t ext4 -L "testfs" /dev/mmcblk0p7 | {{Board$}}mke2fs -t ext4 -L "testfs" /dev/mmcblk0p7 | ||
mke2fs 1.43.5 (04-Aug-2017) | mke2fs 1.43.5 (04-Aug-2017) | ||
/dev/mmcblk0p7 contains a ext4 file system | /dev/mmcblk0p7 contains a ext4 file system | ||
Line 74: | Line 75: | ||
* Mount "testfs" with device partition path or with label. | * Mount "testfs" with device partition path or with label. | ||
{{Board$}} mount /dev/mmcblk0p7 /media | {{Board$}}mount /dev/mmcblk0p7 /media | ||
{{Board$}} mount /dev/disk/by-label/testfs /media | {{Board$}}mount /dev/disk/by-label/testfs /media | ||
* Check that the file system is empty. | * Check that the file system is empty. | ||
{{Board$}} ls -la /media | {{Board$}}ls -la /media | ||
total 21 | total 21 | ||
drwxr-xr-x 3 root root 4096 Aug 7 08:34 . | drwxr-xr-x 3 root root 4096 Aug 7 08:34 . | ||
Line 86: | Line 87: | ||
* Create a random data file. | * Create a random data file. | ||
{{Board$}} dd if=/dev/urandom of=/tmp/random.hex bs=1M count=100 conv=fsync | {{Board$}}dd if=/dev/urandom of=/tmp/random.hex bs=1M count=100 conv=fsync | ||
100+0 records in | 100+0 records in | ||
100+0 records out | 100+0 records out | ||
Line 92: | Line 93: | ||
* Copy the random data file in /media. | * Copy the random data file in /media. | ||
{{Board$}} cp /tmp/random.hex /media/ | {{Board$}}cp /tmp/random.hex /media/ | ||
* Un-mount /media. | * Un-mount /media. | ||
{{Board$}} umount /media | {{Board$}}umount /media | ||
* Mount "testfs". | * Mount "testfs". | ||
{{Board$}} mount /dev/disk/by-label/testfs /media | {{Board$}}mount /dev/disk/by-label/testfs /media | ||
* Check that the random data file created is identical in /tmp and /media. | * Check that the random data file created is identical in /tmp and /media. | ||
{{Board$}} md5sum /tmp/random.hex /media/random.hex | {{Board$}}md5sum /tmp/random.hex /media/random.hex | ||
6ab2f920c81bba53b01f9e758116a172 /tmp/random.hex | 6ab2f920c81bba53b01f9e758116a172 /tmp/random.hex | ||
6ab2f920c81bba53b01f9e758116a172 /media/random.hex | 6ab2f920c81bba53b01f9e758116a172 /media/random.hex | ||
* Un-mount /media. | * Un-mount /media. | ||
{{Board$}} umount /media | {{Board$}}umount /media | ||
==References== | ==References== | ||
Line 115: | Line 116: | ||
[[Category:How to run use cases]] | [[Category:How to run use cases]] | ||
[[Category:Mass storage]] | [[Category:Mass storage]] | ||
{{PublicationRequestId | 24680 | 2022-09-26}} | |||
</noinclude> | </noinclude> |
Latest revision as of 13:22, 17 October 2024
1. Purpose[edit | edit source]
The purpose of this article is to introduce EXT4 filesystem:
- General information
- Main components
- How to use EXT4
2. Overview[edit | edit source]
EXT4 (fourth extended file system)[1][2] is an advanced level of the EXT3 filesystem which incorporates scalability and reliability enhancements for supporting large filesystems (64 bit) in keeping with increasing disk capacities and state-of-the-art feature requirements.
- EXT4 is backward-compatible with EXT3 and EXT2. It is possible to mount both EXT3 and EXT2 filesystems directly using the EXT4 filesystem driver.
- EXT4 can support volumes with sizes up to 1 exbibyte (EiB) and files with sizes up to 16 tebibytes (TiB).
This file system may be used on emmc/sd-card (please refer to the MMC framework). It does not work for raw Flash memory like NOR/NAND.
3. Kernel configuration[edit | edit source]
EXT4 support is activated by default in ST deliveries. Nevertheless, if a specific configuration is needed, this section indicates how EXT4 can be activated/deactivated in the kernel.
Activate EXT4 in the kernel configuration with the Linux Menuconfig tool: Menuconfig or how to configure kernel.
File systems --->
<*> The Extended 4 (ext4) filesystem
[*] Use ext4 for ext2 file systems
4. Using a EXT4 partition as root file system[edit | edit source]
Assuming a rootfs EXT4 image is already flashed to the memory device, the user has to provide:
- The partition that has to be mounted, using root=<partition_device_path> or root=PARTUUID=XXXX where X represents the unique id of a partition.
- The file system type (rootfstype=ext4 in that case). Optional, by default the kernel find the file system type of partition.
Please refer to the SD card memory mapping to check the "rootfs" location in ST deliveries.
In this case, the kernel command-line parameters [3] that have to be added are:
- In case PARTUUID is used.
root=PARTUUID=45e5fc02-d536-43a4-a941-94a8329afeaf
- In case the partition device path is used.
root=/dev/mmcblk0p6
5. Mounting an EXT4 partition[edit | edit source]
Assuming that the "userfs" partition has been flashed on partition 7, the below steps show how to mount this partition.
Please refer to the SD card memory mapping to check the "userfs" location in ST deliveries.
- Mount "userfs".
Board $>mount /dev/mmcblk0p7 /media/
- Check that "userfs" partition is mounted.
Board $>mount | grep "/media"
/dev/mmcblk0p7 on /media type ext4 (rw,sync,relatime)
6. Create a default EXT4 filesystem on a MMC partition[edit | edit source]
- Format a MMC partition (mmcblk0p7 will be used in this example).
UUID: b7c6e8f5-373c-4c91-aace-0c8f69649165 Superblock backups stored on blocks: 32768, 98304 Allocating group tables: done Writing inode tables: done Creating journal (4096 blocks): done Writing superblocks and filesystem accounting information: doneBoard $>mke2fs -t ext4 -L "testfs" /dev/mmcblk0p7 mke2fs 1.43.5 (04-Aug-2017) /dev/mmcblk0p7 contains a ext4 file system created on Tue Aug 7 08:28:50 2018 Proceed anyway? (y,N) y Creating filesystem with 163595 4k blocks and 40960 inodes Filesystem
- Mount "testfs" with device partition path or with label.
Board $>mount /dev/mmcblk0p7 /media
Board $>mount /dev/disk/by-label/testfs /media
- Check that the file system is empty.
Board $>ls -la /media
total 21
drwxr-xr-x 3 root root 4096 Aug 7 08:34 .
drwxr-xr-x 3 root root 1024 Aug 7 08:38 ..
drwx------ 2 root root 16384 Aug 7 08:34 lost+found
- Create a random data file.
Board $>dd if=/dev/urandom of=/tmp/random.hex bs=1M count=100 conv=fsync
100+0 records in
100+0 records out
104857600 bytes (105 MB, 100 MiB) copied, 6.49739 s, 16.1 MB/s
- Copy the random data file in /media.
Board $>cp /tmp/random.hex /media/
- Un-mount /media.
Board $>umount /media
- Mount "testfs".
Board $>mount /dev/disk/by-label/testfs /media
- Check that the random data file created is identical in /tmp and /media.
Board $>md5sum /tmp/random.hex /media/random.hex
6ab2f920c81bba53b01f9e758116a172 /tmp/random.hex
6ab2f920c81bba53b01f9e758116a172 /media/random.hex
- Un-mount /media.
Board $>umount /media
7. References[edit | edit source]
Please refer to the following links for full description: