Template:ArticleMainWriter Template:ArticleApprovedVersion
Even if the example is related to the RTL8723BU chip (this chip calls for a WiFi (minimally 802.11g/n) and Bluetooth 4.0 LE), most of the commands are generic ones and can be applied to any platform.
1. ifconfig[edit | edit source]
Verify the wlan0 interface is present (that means drivers have been started and the WiFi firmware loaded):
1.1. Check WLAN interface[edit | edit source]
RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)ifconfig -a lo Link encap:Local Loopback LOOPBACK MTU:65536 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:1 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:10 (10.0 B)wlan0 Link encap:Ethernet HWaddr 60:F1:89:3F:F6:0E BROADCAST MULTICAST MTU:1500 Metric:1
1.2. Initialize WLAN interface[edit | edit source]
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 /* UP indicate that your interface is UP */ RX packets:19 errors:0 dropped:0 overruns:0 frame:0 TX packets:19 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:1774 (1.7 KiB) TX bytes:2326 (2.2 KiB)ifconfig wlan0 up wlan0 Link encap:Ethernet HWaddr 60:F1:89:3F:F6:0E inet addr:192.168.43.135 Bcast:192.168.43.255 Mask:255.255.255.0
2. iw[edit | edit source]
The next phase is to scan for any wireless access points with the command:
2.1. Scan available SSID (AP)[edit | edit source]
- Get only SSID name
iw dev wlan0 scan |grep SSID
SSID: NETWORK1
SSID: NETWORK2
- List full SSID information
iw dev wlan0 scan
BSS 00:23:5e:4a:28:f9(on wlan0)
TSF: 0 usec (0d, 00:00:00)
freq: 2412
beacon interval: 100 TUs
capability: ESS ShortPreamble ShortSlotTime (0x0421)
signal: -72.00 dBm
last seen: 0 ms ago
SSID: NETWORK1
Supported rates: 1.0* 2.0* 5.5* 6.0 9.0 11.0* 12.0 18.0
DS Parameter set: channel 1
TIM: DTIM Count 0 DTIM Period 1 Bitmap Control 0x0 Bitmap[0] 0x2
Country: FR Environment: Indoor/Outdoor
Channels [1 - 13] @ 20 dBm
BSS Load:
* station count: 1
* channel utilisation: 30/255
* available admission capacity: 23437 [*32us]
ERP: <no flags>
Extended supported rates: 24.0 36.0 48.0 54.0
WMM: * Parameter version 1
* u-APSD
* BE: CW 15-1023, AIFSN 3
* BK: CW 15-1023, AIFSN 7
* VI: CW 7-15, AIFSN 2, TXOP 3008 usec
* VO: CW 3-7, AIFSN 2, TXOP 1504 usec
BSS 00:23:5e:96:57:20(on wlan0)
TSF: 0 usec (0d, 00:00:00)
freq: 2412
beacon interval: 100 TUs
capability: ESS Privacy ShortPreamble ShortSlotTime (0x0431)
signal: -66.00 dBm
last seen: 0 ms ago
SSID: NETWORK2
Supported rates: 1.0* 2.0* 5.5* 6.0 9.0 11.0* 12.0 18.0
DS Parameter set: channel 1
Country: FR Environment: Indoor/Outdoor
Channels [1 - 13] @ 20 dBm
BSS Load:
* station count: 8
* channel utilisation: 48/255
* available admission capacity: 23437 [*32us]
ERP: <no flags>
RSN: * Version: 1
* Group cipher: CCMP
* Pairwise ciphers: CCMP
* Authentication suites: IEEE 802.1X 00-40-96:0
* Capabilities: 4-PTKSA-RC 4-GTKSA-RC (0x0028)
Extended supported rates: 24.0 36.0 48.0 54.0
WMM: * Parameter version 1
* u-APSD
* BE: CW 15-1023, AIFSN 3
* BK: CW 15-1023, AIFSN 7
* VI: CW 7-15, AIFSN 2, TXOP 3008 usec
* VO: CW 3-7, AIFSN 2, TXOP 1504 usec
3. Wlan Network attachment (without system which manage systemd-networkd configuration)[edit | edit source]
3.1. Configure your WiFi connection[edit | edit source]
Configure WiFi connection by using wpa_supplicant tool
- Check current configuration
cat /etc/wpa_supplicant.conf
ctrl_interface=/var/run/wpa_supplicant
ctrl_interface_group=0
update_config=1
network={
key_mgmt=NONE
}
- Set the WiFi network name and password
wpa_passphrase <your_ssid_name> <your_ssid_key> >> /etc/wpa_supplicant.conf
- Check new configuration
psk="your_ssid_key" }cat /etc/wpa_supplicant.conf ctrl_interface=/var/run/wpa_supplicant ctrl_interface_group=0 update_config=1 network={ ssid="your_ssid_name"
![]() |
If no WPA key replace psk=... with key_mgmt=NONE |
3.1.1. Connect to SSID[edit | edit source]
wpa_supplicant -B -iwlan0 -c /etc/wpa_supplicant.conf
Successfully initialized wpa_supplicant
3.1.2. link to SSID[edit | edit source]
RX: 501 bytes (3 packets) TX: 4056 bytes (22 packets) signal: -75 dBm tx bitrate: 12.0 MBit/s bss flags: short-preamble short-slot-time dtim period: 1 beacon int: 100iw wlan0 link SSID: NETWORK1 freq: 2462
3.1.3. Assign IP address to WLAN interface[edit | edit source]
Use the DHCP client to obtain an address (assuming wireless network (associated to) has a DHCP server):
dhclient wlan0
Use the ip command to verify the IP address assigned by the DHCP. The IP address is 192.168.43.135 from below.
UP qlen 1000 link/ether 74:e5:43:a1:ce:65 brd ff:ff:ff:ff:ff:ff inet 192.168.43.135/24 brd 192.168.1.255 scope global wlan0 inet6 fe80::76e5:43ff:fea1:ce65/64 scope link valid_lft forever preferred_lft foreverip addr show wlan0 3: wlan0: mtu 1500 qdisc mq state
3.1.4. Check connectivity[edit | edit source]
The most basic connectivity test is to use the “ping” command. In this example, the wireless router (associated to) has an IP address of 192.168.43.1:
ping 192.168.43.1
PING 192.168.43.1 (192.168.43.1): 56 data bytes
64 bytes from 192.168.43.1: seq=0 ttl=64 time=14.905 ms
64 bytes from 192.168.43.1: seq=1 ttl=64 time=30.387 ms
64 bytes from 192.168.43.1: seq=2 ttl=64 time=20.462 ms
- Note : Enter <CTRL+C> to terminate the ping session.
4. Automatic WiFi configuration at start up[edit | edit source]
4.1. networkctl[edit | edit source]
Systemd has a specific service for the network named systemd-networkd, this service comes with the tool networkctl which allows to show the status of each network interface.
networkctl --no-pager
IDX LINK TYPE OPERATIONAL SETUP
1 lo loopback carrier unmanaged
2 eth0 ether routable configured
3 sit0 sit off unmanaged
4 ip6tnl0 tunnel6 off unmanaged
5 wlan0 wlan off unmanaged
6 wlan1 wlan off unmanaged
6 links listed.
We can see that the eth0 interface is managed by networked via the information configured and the interface is used (routable).
4.2. How to set a wireless configuration with networkd[edit | edit source]
The goal is to configure an wlan network interface via systemd-networkd configuration.
All the network configurations are stored on /lib/systemd/network or /etc/systemd/network
Create the file dedicated to wireless interface:
DHCP=ipv4cat /lib/systemd/network/51-wireless.network [Match] Name=wlan0 [Network]
For attaching this wireless interface to a specific network, we need to have some information like SSID of network and password.
To see the list of wireless network available:
ifconfig wlan0 up
iw dev wlan0 scan |grep SSID
SSID: NETWORK1
SSID: NETWORK2
Associate the wireless network to wireless interface, here wlan0:
mkdir -p /etc/wpa_supplicant/
echo "ctrl_interface=/var/run/wpa_supplicant" > /etc/wpa_supplicant/wpa_supplicant-wlan0.conf
echo "eapol_version=1" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf
echo "ap_scan=1" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf
echo "fast_reauth=1" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf
echo "" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf
wpa_passphrase SSID_OF_NETWORK PASSWORD_OF_NETWORK >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf
Where SSID_OF_NETWORK PASSWORD_OF_NETWORK correspond to the SSID and password of wireless network.
![]() |
the name of file on /etc/wpa_supplicant must contains the name of wireless interface: wpa_supplicant-wlan0.conf |
To enable and start the wireless configuration:
systemctl enable wpa_supplicant@wlan0.service
systemctl restart systemd-networkd.service
systemctl restart wpa_supplicant@wlan0.service