deleted>Frq08988 mNo edit summary |
Registered User mNo edit summary |
||
(5 intermediate revisions by 4 users not shown) | |||
Line 1: | Line 1: | ||
==Introduction== | ==Introduction== | ||
STMicroelectronics delivers also a script runing on '''Linux''' host PC to populate '''ONLY''' the microSD card device.<br> | STMicroelectronics delivers also a script runing on '''Linux''' host PC to populate '''ONLY''' the microSD card device.<br> | ||
This script is located here : build-<DISTRO>-<MACHINE>/tmp-glibc/deploy/images/<MACHINE>/scripts/<br> | This script is located here : build-<DISTRO>-<MACHINE>/tmp-glibc/deploy/images/<MACHINE>/scripts/<br> | ||
This script is also located in the Starter Package/<VERSION>/ images/stm32mp1/scripts. | |||
This script as [[STM32CubeProgrammer]] tool is using ''Flashlayout.tsv'' file in input parameter<br> | This script as [[STM32CubeProgrammer]] tool is using ''Flashlayout.tsv'' file in input parameter<br> | ||
Line 140: | Line 135: | ||
{{PC$}} cd build-openstlinuxweston-stm32mp1/tmp-glibc/deploy/images/stm32mp1/scripts/ | {{PC$}} cd build-openstlinuxweston-stm32mp1/tmp-glibc/deploy/images/stm32mp1/scripts/ | ||
{{PC$}} sudo dd if=../flashlayout_st-image-weston_FlashLayout_sdcard_stm32mp157c-ev1-trusted.raw of=/dev/mmcblk0 bs=8M conv=fdatasync | {{PC$}} sudo dd if=../flashlayout_st-image-weston_FlashLayout_sdcard_stm32mp157c-ev1-trusted.raw of=/dev/mmcblk0 bs=8M conv=fdatasync status=progress | ||
The dd command takes few minutes (depending mainly of your rootfs size) | The dd command takes few minutes (depending mainly of your rootfs size) | ||
Line 234: | Line 229: | ||
) | ) | ||
</pre> | </pre> | ||
<noinclude> | |||
[[Category:How to populate boards]] | |||
{{PublicationRequestId | 9332 | 2018-11-07 | AlainF}} | |||
</noinclude> |
Revision as of 18:17, 29 January 2020
1. Introduction[edit | edit source]
STMicroelectronics delivers also a script runing on Linux host PC to populate ONLY the microSD card device.
This script is located here : build-<DISTRO>-<MACHINE>/tmp-glibc/deploy/images/<MACHINE>/scripts/
This script is also located in the Starter Package/<VERSION>/ images/stm32mp1/scripts.
This script as STM32CubeProgrammer tool is using Flashlayout.tsv file in input parameter
This script creates a raw file <FlashLayoutName>.raw and a txt file <FlashLayoutName>.how_to_update.txt
Then you can use this raw file to populate your microSD card inserted on your HOST PC
2. Usage[edit | edit source]
Template:PC$ cd build-<DISTRO>-<MACHINE>/tmp-glibc/deploy/images/<MACHINE>/scripts
Template:PC$ ./create_sdcard_from_flashlayout.sh ../flashlayout_<built-image>/<FlashLayout file>
Example :
PC $> cd build-openstlinuxweston-stm32mp1/tmp-glibc/deploy/images/stm32mp1/scripts/
PC $> ./create_sdcard_from_flashlayout.sh ../flashlayout_st-image-weston/FlashLayout_sdcard_stm32mp157c-ev1-trusted.tsv
Create Raw empty image: ../flashlayout_st-image-weston/../flashlayout_st-image-weston_FlashLayout_sdcard_stm32mp157c-ev1-trusted.raw of 1536MB
Create partition table:
[CREATED] part 1: fsbl1 [partition size 256.0 KiB]
[CREATED] part 2: fsbl2 [partition size 256.0 KiB]
[CREATED] part 3: ssbl [partition size 2.5 MiB]
[CREATED] part 4: bootfs [partition size 64.0 MiB]
[CREATED] part 5: vendorfs [partition size 16.0 MiB]
[CREATED] part 6: rootfs [partition size 750.4 MiB]
[CREATED] part 7: userfs [partition size 702.5 MiB]
Partition table from ../flashlayout_st-image-weston/../flashlayout_st-image-weston_FlashLayout_sdcard_stm32mp157c-ev1-trusted.raw
Disk ../flashlayout_st-image-weston/../flashlayout_st-image-weston_FlashLayout_sdcard_stm32mp157c-ev1-trusted.raw: 3145728 sectors, 1.5 GiB
Logical sector size: 512 bytes
Disk identifier (GUID): 8E3FE74B-3B58-4617-B71B-5EC498875478
Partition table holds up to 128 entries
First usable sector is 34, last usable sector is 3145694
Partitions will be aligned on 2-sector boundaries
Total free space is 0 sectors (0 bytes)
Number Start (sector) End (sector) Size Code Name
1 34 545 256.0 KiB 8300 fsbl1
2 546 1057 256.0 KiB 8300 fsbl2
3 1058 6177 2.5 MiB 8300 ssbl
4 6178 137249 64.0 MiB 8300 bootfs
5 137250 170017 16.0 MiB 8300 vendorfs
6 170018 1706881 750.4 MiB 8300 rootfs
7 1706882 3145694 702.5 MiB 8300 userfs
Populate raw image with image content:
[ FILLED ] part 1: fsbl1, image: tf-a-stm32mp157c-ev1-trusted.stm32
[ FILLED ] part 2: fsbl2, image: tf-a-stm32mp157c-ev1-trusted.stm32
[ FILLED ] part 3: ssbl, image: u-boot-stm32mp157c-ev1-trusted.stm32
[ FILLED ] part 4: bootfs, image: st-image-bootfs-openstlinux-weston-stm32mp1.ext4
[ FILLED ] part 5: vendorfs, image: st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
[ FILLED ] part 6: rootfs, image: st-image-weston-openstlinux-weston-stm32mp1.ext4
[ FILLED ] part 7: userfs, image: st-image-userfs-openstlinux-weston-stm32mp1.ext4
###########################################################################
###########################################################################
RAW IMAGE generated: ../flashlayout_st-image-weston/../flashlayout_st-image-weston_FlashLayout_sdcard_stm32mp157c-ev1-trusted.raw
WARNING: before to use the command dd, please umount all the partitions
associated to SDCARD.
sudo umount `lsblk --list | grep mmcblk0 | grep part | gawk '{ print $7 }' | tr '\n' ' '`
To put this raw image on sdcard:
sudo dd if=../flashlayout_st-image-weston/../flashlayout_st-image-weston_FlashLayout_sdcard_stm32mp157c-ev1-trusted.raw of=/dev/mmcblk0 bs=8M conv=fdatasync
(mmcblk0 can be replaced by:
sdX if it's a device dedicated to receive the raw image
(where X can be a, b, c, d, e)
###########################################################################
###########################################################################
3. Populate the microSD card inserted on your linux host PC with the created raw file[edit | edit source]
You need first to retrieve the volume name of your drive (USB Key or MMC card)
To connect a USB device to the virtual machine manually, select VM > Removable Devices > Device Name > Connect (Disconnect from host)
More explanations for this specific case here
Insert your drive then use the following command :
- In this example, the volume name is sdd (microSD card is inserted with USB key)
PC $> cat /proc/partitions
major minor #blocks name
8 0 488386584 sda
8 1 999424 sda1
8 2 1 sda2
8 5 487384064 sda5
11 0 1048575 sr0
252 0 487382016 dm-0
252 1 19996672 dm-1
252 2 8335360 dm-2
252 3 459046912 dm-3
8 48 1921024 sdd
- In this example, the volume name is mmcblk0 (microSD card is inserted directly with microSD card adapter)
PC $> cat /proc/partitions
major minor #blocks name
8 0 488386584 sda
8 1 999424 sda1
8 2 1 sda2
8 5 487384064 sda5
11 0 1048575 sr0
252 0 487382016 dm-0
252 1 19996672 dm-1
252 2 8335360 dm-2
252 3 459046912 dm-3
8 48 1921024 mmcblk0
- Before using the command dd, please umount all the partitions associated to microSD card.
Template:PC$ sudo umount `lsblk --list | grep mmcblk0 | grep part | gawk '{ print $7 }' | tr '\n' ' '`
- Populate microSD card with dd command:
Template:PC$ cd build-openstlinuxweston-stm32mp1/tmp-glibc/deploy/images/stm32mp1/scripts/
Template:PC$ sudo dd if=../flashlayout_st-image-weston_FlashLayout_sdcard_stm32mp157c-ev1-trusted.raw of=/dev/mmcblk0 bs=8M conv=fdatasync status=progress
The dd command takes few minutes (depending mainly of your rootfs size)
4. Update manually some partitions with dd command[edit | edit source]
Once you have populated your microSD card with the raw file, it is possible to update manually some partitions as explained in txt file.
Example :
PC $> cat flashlayout_st-image-weston_FlashLayout_sdcard_stm32mp157c-ev1-trusted.how_to_update.txt
This file describes how to update manually the partition of SDCARD:
1. SDCARD schema of partition
2. How to populate each partition
3. How to update the kernel/devicetree
1. SDCARD schema of partition:
------------------------------
============================================================================================
= = = = = = = =
= fsbl1 = fsbl2 = ssbl = bootfs = vendorfs = rootfs = userfs =
= = = = = = = =
= mmcblk0p1 = mmcblk0p2 = mmcblk0p3 = mmcblk0p4 = mmcblk0p5 = mmcblk0p6 = mmcblk0p7 =
= (1 ) = (2 ) = (3 ) = (4 ) = (5 ) = (6 ) = (7 ) =
= = = = = = = =
============================================================================================
(1):
Device: /dev/mmcblk0p1
Label: fsbl1
Image: tf-a-stm32mp157c-ev1-trusted.stm32
(2):
Device: /dev/mmcblk0p2
Label: fsbl2
Image: tf-a-stm32mp157c-ev1-trusted.stm32
(3):
Device: /dev/mmcblk0p3
Label: ssbl
Image: u-boot-stm32mp157c-ev1-trusted.stm32
(4):
Device: /dev/mmcblk0p4
Label: bootfs
Image: st-image-bootfs-openstlinux-weston-stm32mp1.ext4
(5):
Device: /dev/mmcblk0p5
Label: vendorfs
Image: st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
(6):
Device: /dev/mmcblk0p6
Label: rootfs
Image: st-image-weston-openstlinux-weston-stm32mp1.ext4
(7):
Device: /dev/mmcblk0p7
Label: userfs
Image: st-image-userfs-openstlinux-weston-stm32mp1.ext4
2. How to populate each partition
---------------------------------
- Populate partition fsbl1 (/dev/mmcblk0p1)
dd if=tf-a-stm32mp157c-ev1-trusted.stm32 of=/dev/mmcblk0p1 bs=1M conv=fdatasync
- Populate partition fsbl2 (/dev/mmcblk0p2)
dd if=tf-a-stm32mp157c-ev1-trusted.stm32 of=/dev/mmcblk0p2 bs=1M conv=fdatasync
- Populate partition ssbl (/dev/mmcblk0p3)
dd if=u-boot-stm32mp157c-ev1-trusted.stm32 of=/dev/mmcblk0p3 bs=1M conv=fdatasync
- Populate partition bootfs (/dev/mmcblk0p4)
dd if=st-image-bootfs-openstlinux-weston-stm32mp1.ext4 of=/dev/mmcblk0p4 bs=1M conv=fdatasync
- Populate partition vendorfs (/dev/mmcblk0p5)
dd if=st-image-vendorfs-openstlinux-weston-stm32mp1.ext4 of=/dev/mmcblk0p5 bs=1M conv=fdatasync
- Populate partition rootfs (/dev/mmcblk0p6)
dd if=st-image-weston-openstlinux-weston-stm32mp1.ext4 of=/dev/mmcblk0p6 bs=1M conv=fdatasync
- Populate partition userfs (/dev/mmcblk0p7)
dd if=st-image-userfs-openstlinux-weston-stm32mp1.ext4 of=/dev/mmcblk0p7 bs=1M conv=fdatasync
3. How to update the kernel/devicetree
--------------------------------------
The kernel and devicetree are present on "bootfs" partition.
To change kernel and devicetree, you can copy the file on this partition:
- plug SDCARD on your PC
- copy kernel uImage on SDCARD
sudo cp uImage /media/$USER/bootfs/
- copy devicetree uImage on SDCARD
sudo cp stm32mp1*.dtb /media/$USER/bootfs/
- umount partitions of SDCARD
sudo umount /media/$USER/bootfs/
(dont't forget to umount the other partitions of SDCARD:
sudo umount `lsblk --list | grep mmcblk0 | grep part | gawk '{ print $7 }' | tr '\n' ' '`
)