Last edited 9 months ago

How to modify the panel backlight

The printable version is no longer supported and may have rendering errors. Please update your browser bookmarks and please use the default browser print function instead.


First identify the backlight device linked to your panel, thanks to the sysfs:

ls /sys/class/backlight
5a000000.dsi.0

In the above example, there is a single entry named "5a000000.dsi.0", which is replaced by "*" in the below command.


To adjust the panel backlight, enter the following command:

echo 32 > /sys/class/backlight/*/brightness    # set the dsi panel backlight to the value 32

Note: Only values between 0 and max_brightness must be used.

To get the maximum panel backlight value, enter:

cat /sys/class/backlight/*/max_brightness
255

To get the actual panel backlight value, enter:

cat /sys/class/backlight/*/actual_brightness
32


Use one of the following commands to quickly test the panel backlight:

export bl=/sys/class/backlight/5a000000.dsi.0/brightness
export max=/sys/class/backlight/5a000000.dsi.0/max_brightness

# switch on/off test
(while true; do echo 0 > $bl; sleep 0.5; echo $max > $bl; sleep 0.5; done)

# slow 32-step tests (only for pwm-based backlights)
(i=0; while true; do i=$(((i+32)%256)); echo $i > $bl; sleep 0.5; done)

# fast 1-step test  (only for pwm-based backlights)
(i=0; while true; do i=$(((i+1)%256)); echo $i > $bl; done)