Approved version. Approved on: 16:44, 18 February 2019
You are viewing an old version of this page. Return to the latest version.
Difference between revisions of "How to modify the panel backlight"
[quality revision] | [quality revision] |
m
|
[quality revision] | [quality revision] |
m
|
Template:ArticleMainWriter Template:ReviewersList Template:ArticleApprovedVersion
First identify the backlight device linked to your panel, thanks to the sysfs:
ls /sys/class/backlight 5a000000.dsi.0
In the above example, there is a single entry named "5a000000.dsi.0", which is replaced by "*" in the below command.
To adjust the panel backlight, enter the following command:
echo 32 > /sys/class/backlight/*/brightness # set the dsi panel backlight to the value 32
Note: Only values between 0 and max_brightness must be used.
To get the maximum panel backlight value, enter:
cat /sys/class/backlight/*/max_brightness 255
To get the actual panel backlight value, enter:
cat /sys/class/backlight/*/actual_brightness 32
Use one of the following commands to quickly test the panel backlight:
export bl=/sys/class/backlight/5a000000.dsi.0/brightness # switch on/off test (while true; do echo 0 > $bl; sleep 0.5; echo 255 > $bl; sleep 0.5; done) # slow 32-step tests (i=0; while true; do i=$(((i+32)%256)); echo $i > $bl; sleep 0.5; done) # fast 1-step test (i=0; while true; do i=$(((i+1)%256)); echo $i > $bl; done)
<noinclude> {{ArticleMainWriter | PhilippeC }} {{ReviewersList | YannickF}} {{ArticleApprovedVersion | PhilippeC | YannickF (Passed, 5feb'19)| No previous approved version | AnneJ - 18Feb'19 - 10715 | 18Feb'19}} [[Category:How to run use cases]] [[Category:DRM KMS]]</noinclude> First identify the backlight device linked to your panel, thanks to the sysfs: {{Board$}} ls /sys/class/backlight 5a000000.dsi.0 In the above example, there is a single entry named "5a000000.dsi.0", which is '''replaced by "*"''' in the below command. To adjust the panel backlight, enter the following command: {{Board$}} echo '''32''' > /sys/class/backlight/*/'''brightness''' # set the dsi panel backlight to the value '''32''' Note: Only values between 0 and '''max_brightness''' must be used. To get the maximum panel backlight value, enter: {{Board$}} cat /sys/class/backlight/*/'''max_brightness''' 255 To get the actual panel backlight value, enter: {{Board$}} cat /sys/class/backlight/*/'''actual_brightness''' 32 Use one of the following commands to quickly test the panel backlight: {{Board$}} export bl=/sys/class/backlight/5a000000.dsi.0/brightness {{Board$}} # switch on/off test {{Board$}} (while true; do echo 0 > $bl; sleep 0.5; echo 255 > $bl; sleep 0.5; done) {{Board$}} # slow 32-step tests {{Board$}} (i=0; while true; do i=$(((i+32)%256)); echo $i > $bl; sleep 0.5; done) {{Board$}} # fast 1-step test {{Board$}} (i=0; while true; do i=$(((i+1)%256)); echo $i > $bl; done) <noinclude> {{PublicationRequestId | 10715 | 2019-02-18 | AnneJ}} [[Category:How to run use cases]] [[Category:DRM KMS]]</noinclude>
Line 1: | Line 1: | ||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
First identify the backlight device linked to your panel, thanks to the sysfs: |
First identify the backlight device linked to your panel, thanks to the sysfs: |
||
{{Board$}} ls /sys/class/backlight |
{{Board$}} ls /sys/class/backlight |
||
Line 38: | Line 30: | ||
{{Board$}} # fast 1-step test |
{{Board$}} # fast 1-step test |
||
{{Board$}} (i=0; while true; do i=$(((i+1)%256)); echo $i > $bl; done) |
{{Board$}} (i=0; while true; do i=$(((i+1)%256)); echo $i > $bl; done) |
||
+ | |||
+ | |||
+ | <noinclude> |
||
+ | {{PublicationRequestId | 10715 | 2019-02-18 | AnneJ}} |
||
+ | [[Category:How to run use cases]] |
||
+ | [[Category:DRM KMS]] |
||
+ | </noinclude> |