Last edited 8 months ago

How to install JAVA JDK: Difference between revisions


Latest revision as of 16:55, 15 November 2024



The goal of this page is to describe the OpenJDK installation procedure on your STM32 MPU board and (native) desktop, in a STM32MPU Distribution Package environment.
It is the "Open Standard Edition Java Development Kit" installation process. According to the OpenstLinux Weston software architecture, XWayland is used for all Java applications based on X11, which means AWT/SWING Java display/graphical applications.
By default the Java Development Kit is installed on the rootfs partition of the target.


1. Prerequisites[edit | edit source]

1.1. Hardware prerequisites[edit | edit source]

  • STM32MP157x-DKx Discovery kit More info green.png or STM32MP157x-EV1 Evaluation board More info green.png
  • a keyboard and a mouse connected to the board

1.2. Software prerequisites[edit | edit source]

The STM32MPU Distribution Package must be installed on your host. To do this, follow the procedure described in the STM32MPU Distribution Package#Installing the OpenSTLinux distribution article.

The process has been verified with ecosystem release unknown revision 5.0.0 Warning.png of the OpenSTlinux distribution.

2. The yoctoproject meta-java[edit | edit source]

JAVA for Linux-based embedded systems is available as metadata in the Yocto project.

  • Clone the following git repository into [your STM32MPU Distribution path]/layers
PC $>cd [your STM32MPU Distribution path]/layers
PC $>git clone git://git.yoctoproject.org/meta-java

Depending on the Yocto release, select the right branch. (for example, branch mickledore for the ecosystem release unknown revision 5.0.0 Warning.png )

PC $>cd meta-java
PC $>git checkout remotes/origin/mickledore
  • Two patches need to be applied to meta-java layers:
PC $>cd [your STM32MPU Distribution path]/layers/meta-java

1- In recipes-core/xml-commons/xml-commons-resolver1.1_1.2.bb

-SRC_URI = "http://archive.apache.org/dist/xml/commons/xml-commons-resolver-${PV}.tar.gz"
+SRC_URI = "http://archive.apache.org/dist/xml/commons/binaries/xml-commons-resolver-${PV}.tar.gz"

2- In recipes-core/openjdk/openjdk-8_272.bb

+ERROR_QA:remove = "patch-fuzz"
  • If not already done, set up your build environment
PC $>cd [your STM32MPU Distribution path]
PC $>source layers/meta-st/scripts/envsetup.sh
(Select for the DISTRO openstlinux-weston and for MACHINE stm32mpx)
  • Add the meta layer in your Yocto environment
PC $>cd [your STM32MPU Distribution path]/build-openstlinuxweston-stm32mpx
PC $>bitbake-layers add-layer [your STM32MPU Distribution path]/layers/meta-java
  • Define at least the following variables in your local.conf file
([your STM32MPU Distribution path]/build-openstlinuxweston-stm32mpx/conf/local.conf)

#Possible provider: cacao-initial-native and jamvm-initial-native
PREFERRED_PROVIDER_virtual/java-initial-native = "cacao-initial-native"

#Possible provider: cacao-native and jamvm-native
PREFERRED_PROVIDER_virtual/java-native = "jamvm-native"

#Optional since there is only one provider for now
PREFERRED_PROVIDER_virtual/javac-native = "ecj-bootstrap-native"


  • Include in your image the openjdk-8 component
PC $>cd [your STM32MPU Distribution path]/layers/meta-st/meta-st-openstlinux/recipes-st/images

Edit the file st-image-weston.bb and add the following line under CORE_IMAGE_EXTRA_INSTALL

  openjdk-8 \
  openjdk-8-demo \
  • Choose XWayland configuration in meta-st/meta-st-openstlinux.
PC $>cd [your STM32MPU Distribution path]/layers/meta-st/meta-st-openstlinux

Three modifications to be done:

1- conf/distro/openstlinux-weston.conf

-DISTRO_FEATURES:remove = " x11 "
+DISTRO_FEATURES:append = " x11 wayland "
# with X11
-#PREFERRED_PROVIDER_virtual/xserver = "${@bb.utils.contains('DISTRO_FEATURES', 'x11 wayland', 'xwayland', 'xserver-xorg', d)}"
+PREFERRED_PROVIDER_virtual/xserver = "${@bb.utils.contains('DISTRO_FEATURES', 'x11 wayland', 'xwayland', 'xserver-xorg', d)}"

2- recipes-st/packagegroups/packagegroup-framework-core-extra.bb

-    ${@bb.utils.contains('DISTRO_FEATURES', 'x11 wayland', 'xf86-input-keyboard', '', d)}   \

3- recipes-graphics/xorg-xserver/xserver-xorg_%.bbappend (new file)

FILESEXTRAPATHS:prepend := "${THISDIR}/${PN}:"
DEPENDS += "libxshmfence"
  • Increase the Rootfs partition size

Update the file ([your STM32MPU Distribution path]/layers/meta-st/meta-st-stm32mp/conf/machine/include/st-machine-common-stm32mp.inc)

IMAGE_ROOTFS_MAXSIZE = "819200"
  • Build the image
PC $>cd [your STM32MPU Distribution path]/build-openstlinuxweston-stm32mpx
PC $>bitbake st-image-weston

3. Compilation and execution of some JAVA demos[edit | edit source]

  • forkjoin benchmark Java application
Board $>cd /usr/lib/jvm/openjdk-8/sample/forkjoin/mergesort
Board $>javac MergeDemo.java
Board $>java MergeDemo 200 100 3 1 1 3
Running with parameters: 200 100 3 1 1 3
Time in milliseconds. Y-axis: number of elements. X-axis parallelism used.
            1    2    3
    200:   10    7    8
    300:   17   12   12
    400:   20   14   14
  Total:   47   33   34
  • For all GUI Java application, user must export DISPLAY variable and launch a XWayland socket.

The same ":N" DISPLAY value is used to launch XWayland socket (only one instance can be run for one "N" value).

Board $>export DISPLAY=:1

Choose 'X' and 'Y' according to your Java application:

Board $>Xwayland :1 -geometry 'X'x'Y'&

Remove some glamor warnings

Board $>export XWAYLAND_NO_GLAMOR=1

Note that some XKEYBOARD not fatal warnings can occur


1- SampleTree Java application Read the README.txt file for details. To execute in a Linux Weston console on the board, with a keyboard and a mouse.

Board $>export DISPLAY=:1
Board $>Xwayland :1 -geometry 350x450&
Board $>cd /usr/lib/jvm/openjdk-8/demo/jfc/SampleTree
Board $>java -jar SampleTree.jar

Sampletree.png


2- GraphicsTest Java applet Read the README.txt file for details. To execute in a Linux Weston console on the board, with a keyboard and a mouse.

Board $>export DISPLAY=:1
Board $>Xwayland :1 -geometry 400x400&
Board $>cd /usr/lib/jvm/openjdk-8/demo/applets/GraphicsTest
Board $>/usr/lib/jvm/openjdk-8/bin/appletviewer example1.html

AppletGraphicTest.png