Registered User mNo edit summary |
Registered User No edit summary |
||
(36 intermediate revisions by 7 users not shown) | |||
Line 1: | Line 1: | ||
{{ApplicableFor | |||
|MPUs list=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x | |||
|MPUs checklist=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x | |||
}} | |||
<noinclude></noinclude> | |||
== Article purpose == | == Article purpose == | ||
The purpose of this article is to provide information about the Linux<sup>®</sup> kernel log including configuration, and to detail usage of dmesg command. | The purpose of this article is to provide information about the Linux<sup>®</sup> kernel log including configuration, and to detail usage of dmesg command. | ||
Line 5: | Line 11: | ||
Linux kernel is able to print log and trace messages, which are by default stored in a ring buffer. | Linux kernel is able to print log and trace messages, which are by default stored in a ring buffer. | ||
The same messages can also be displayed, applying filter, on uart/console using serial port. This is defined in the kernel command-line, with the "console" parameter. See <ref> | The same messages can also be displayed, applying filter, on uart/console using serial port. This is defined in the kernel command-line, with the "console" parameter. See <ref>{{DocSource | domain=Linux kernel | path=admin-guide/serial-console.html | text=Linux Serial Console}}</ref> for detail. | ||
dmesg is a shell command on the kernel console, which also displays the content of the ring buffer, with filter or not (default). | dmesg is a shell command on the kernel console, which also displays the content of the ring buffer, with filter or not (default). | ||
Line 32: | Line 38: | ||
-> Kernel log buffer size (16 => 64KB, 17 => 128KB) | -> Kernel log buffer size (16 => 64KB, 17 => 128KB) | ||
* Or modify kernel arguments<ref> | * Or modify kernel arguments<ref>{{DocSource | domain=Linux kernel | path=admin-guide/kernel-parameters.html | text=The kernel’s command-line parameters}}</ref> in kernel command-line (via bootargs value in device tree, or directly in extlinux uboot config file) | ||
bootargs = "root=/dev/mmcblk0p5 rootwait rw console=ttySTM0,115200 {{highlight|log_buf_len=65536}}"; | bootargs = "root=/dev/mmcblk0p5 rootwait rw console=ttySTM0,115200 {{highlight|log_buf_len=65536}}"; | ||
Line 38: | Line 44: | ||
== Loglevels == | == Loglevels == | ||
As reference, | As reference, see elinux.org<ref>https://elinux.org/Debugging_by_printing#Log_Levels</ref>. | ||
The log level is used by the kernel to determine the importance of a message and to decide whether it should be presented to the user immediately, by printing it to the current console. | The log level is used by the kernel to determine the importance of a message and to decide whether it should be presented to the user immediately, by printing it to the current console. | ||
Line 44: | Line 50: | ||
For this, the kernel compares the log level of the message to the console_loglevel (a kernel variable) and if the priority is higher (i.e. a lower value) than the console_loglevel, the message will be printed to the current console. As example, if console_loglevel=5, all messages with log level 0 to 4 will be displayed. | For this, the kernel compares the log level of the message to the console_loglevel (a kernel variable) and if the priority is higher (i.e. a lower value) than the console_loglevel, the message will be printed to the current console. As example, if console_loglevel=5, all messages with log level 0 to 4 will be displayed. | ||
Note that all messages with loglevel lower or equal to KERN_INFO level are stored in the ring buffer. | |||
=== loglevels values === | === loglevels values === | ||
{| class=" | {| class="st-table" | ||
|+ "Loglevels table" | |+ "Loglevels table" | ||
|- | |- | ||
Line 69: | Line 75: | ||
|} | |} | ||
{{Highlight|'''Important''': | {{Highlight|'''Important''': note that Higher priority message is loglevel 0}} | ||
=== Set loglevel filter value for console === | === Set loglevel filter value for console === | ||
==== Default values ==== | ==== Default values ==== | ||
To determine your current console_loglevel on the target you can verifiy with the following command: | To determine your current console_loglevel on the target you can verifiy with the following command: | ||
{{Board$}} cat /proc/sys/kernel/printk | {{Board$}}cat /proc/sys/kernel/printk | ||
{{green|'''7'''}} {{ | {{green|'''7'''}} {{Orange|'''4'''}} {{STPurple|'''1'''}} {{highlight|'''7'''}} | ||
{{green|'''current'''}} {{ | {{green|'''current'''}} {{Orange|'''default_msg'''}} {{STPurple|'''minimum'''}} {{highlight|'''default_console'''}} | ||
The first integer shows you the current console_loglevel; the second the default log level, see [[#Use_loglevel_in_kernel_source_for_log_and_trace|Use loglevel in the kernel source for log and trace]]. | The first integer shows you the current console_loglevel; the second the default log level, see [[#Use_loglevel_in_kernel_source_for_log_and_trace|Use loglevel in the kernel source for log and trace]]. | ||
Line 82: | Line 88: | ||
This is defined at compilation:<br> | This is defined at compilation:<br> | ||
:- {{green|Current console}} loglevel via {{green|CONFIG_CONSOLE_LOGLEVEL_DEFAULT=7}} (defined in file ''lib/Kconfig.debug'')<br> | :- {{green|Current console}} loglevel via {{green|CONFIG_CONSOLE_LOGLEVEL_DEFAULT=7}} (defined in file ''lib/Kconfig.debug'')<br> | ||
:- {{ | :- {{Orange|Default message}} loglevel via {{Orange|CONFIG_MESSAGE_LOGLEVEL_DEFAULT=4}} (defined in file ''lib/Kconfig.debug'')<br> | ||
:- {{STPurple|Minimum console}} loglevel via {{STPurple|#define CONSOLE_LOGLEVEL_MIN 1}} (defined in file ''include/linux/printk.h'')<br> | :- {{STPurple|Minimum console}} loglevel via {{STPurple|#define CONSOLE_LOGLEVEL_MIN 1}} (defined in file ''include/linux/printk.h'')<br> | ||
:- {{highlight|Default console}} loglevel is {{highlight|equal to CONFIG_CONSOLE_LOGLEVEL_DEFAULT}}<br> | :- {{highlight|Default console}} loglevel is {{highlight|equal to CONFIG_CONSOLE_LOGLEVEL_DEFAULT}}<br> | ||
==== Using kernel command-line ==== | ==== Using kernel command-line ==== | ||
The console loglevel can be also set via a kernel command-line parameter if you want to use a different value than one | The console loglevel can be also set via a kernel command-line parameter if you want to use a different value than one specified by CONFIG_CONSOLE_LOGLEVEL_DEFAULT.<br> | ||
For example: | For example: | ||
root=/dev/mmcblk0p5 rootwait rw console=ttySTM0,115200 {{highlight|loglevel=4}} | root=/dev/mmcblk0p5 rootwait rw console=ttySTM0,115200 {{highlight|loglevel=4}} | ||
In that case only messages with a higher priority than KERN_WARNING (means < 4, KERN_EMERG to KERN_ERR ) will be displayed on the console. | In that case only messages with a higher priority than KERN_WARNING (means < 4, KERN_EMERG to KERN_ERR ) will be displayed on the console. | ||
Note: The command-line is set in one of several extlinux configuration files located in the bootfs partition. The used configuration file path is dependent of the boot device and the board type. For simplicity, you can retrieve the file parsed at boot time from the console once U-Boot takes over the boot sequence. As example : | |||
Boot over mmc0! | |||
Saving Environment to MMC... Writing to redundant MMC(0)... OK | |||
switch to partitions #0, OK | |||
mmc0 is current device | |||
Scanning mmc 0:8... | |||
Found U-Boot script /boot.scr.uimg | |||
4187 bytes read in 7 ms (584 KiB/s) | |||
## Executing script at c6100000 | |||
Executing SCRIPT on target=mmc0 | |||
FOUND {{HighlightParam|/mmc0_extlinux/stm32mp135f-dk_extlinux.conf}} | |||
[...] | |||
Starting kernel ... | |||
Two ways to add this ''loglevel'' command-line parameter (as example with stm32mp135f-dk_extlinux.conf): | |||
* If using SD card, this is possible to edit the file on host PC: | * If using SD card, this is possible to edit the file on host PC: | ||
Insert SD card on host PC | Insert SD card on host PC | ||
Check for mounting boot partition (i.e. /media/$USER/bootfs) | Check for mounting boot partition (i.e. /media/$USER/bootfs) | ||
Open the appropriate extlinux configuration file for edition | |||
{{PC$}} cd /media/$USER/bootfs/ | {{PC$}}cd /media/$USER/bootfs/mmc0_extlinux/ | ||
{{PC$}} gedit | {{PC$}}gedit stm32mp135f-dk_extlinux.conf | ||
Add '''loglevel=8''' at the end of APPEND line | Add '''loglevel=8''' at the end of APPEND line | ||
Save and insert SD card on the board | Save and insert SD card on the board | ||
* If using SD Card or eMMC, this is possible to edit the file directly on the board side: | * If using SD Card or eMMC, this is possible to edit the file directly on the board side: | ||
When software is boot | When software is boot | ||
Mount boot partition | Mount boot partition if not already done | ||
{{Board$}} mount /dev/mmcblk0p4 /boot | {{Board$}}mount /dev/mmcblk0p4 /boot | ||
Update the kernel command line | Update the kernel command line | ||
{{Board$}} cd /boot | {{Board$}}cd /boot | ||
{{Board$}} cd | {{Board$}}cd mmc0_extlinux # (or mmc1_extlinux if booting from eMMC) | ||
Modify extlinux | {{Board$}}vi stm32mp135f-dk_extlinux.conf | ||
Modify the extlinux configuration file to add '''loglevel=8''' at the end of APPEND line | |||
Save and reboot the board | Save and reboot the board | ||
==== Using sysfs in runtime ==== | ==== Using sysfs in runtime ==== | ||
To change your current console_loglevel simply write to this file: | To change your current console_loglevel simply write to this file: | ||
{{Board$}} echo {{ | {{Board$}}echo {{HighlightParam|<''loglevel''>}} > /proc/sys/kernel/printk | ||
or using [[#dmesg command|dmesg command]]. | or using [[#dmesg command|dmesg command]]. | ||
As example: | As example: | ||
{{Board$}} echo {{highlight|8}} > /proc/sys/kernel/printk ''# Temporary increase loglevel to display messages up to loglevel 8'' | {{Board$}}echo {{highlight|8}} > /proc/sys/kernel/printk ''# Temporary increase loglevel to display messages up to loglevel 8'' | ||
:In that case, every kernel messages will appear on your console, as {{highlight|all priority higher than 8 (lower loglevel values)}} will be displayed. | :In that case, every kernel messages will appear on your console, as {{highlight|all priority higher than 8 (lower loglevel values)}} will be displayed. | ||
''' | '''Note that after reboot, this configuration is reset.''' | ||
==== Using menuconfig before compilation ==== | ==== Using menuconfig before compilation ==== | ||
Line 126: | Line 147: | ||
Symbol: '''CONSOLE_LOGLEVEL_DEFAULT''' [={{green|7}}] | Symbol: '''CONSOLE_LOGLEVEL_DEFAULT''' [={{green|7}}] | ||
Location: | Location: | ||
Kernel hacking | -> Kernel hacking | ||
-> printk and dmesg options | |||
{{highlight|(7) Default console loglevel (1-15)}} | {{highlight|(7) Default console loglevel (1-15)}} | ||
Symbol: '''MESSAGE_LOGLEVEL_DEFAULT''' [={{green|4}}] | Symbol: '''MESSAGE_LOGLEVEL_DEFAULT''' [={{green|4}}] | ||
Location: | Location: | ||
Kernel hacking | -> Kernel hacking | ||
-> printk and dmesg options | |||
{{highlight|(4) Default message log level (1-7)}} | {{highlight|(4) Default message log level (1-7)}} | ||
Line 164: | Line 185: | ||
[ 1.046700] {{highlight|stm32-usart 40010000.serial}}: interrupt mode used for rx (no dma) | [ 1.046700] {{highlight|stm32-usart 40010000.serial}}: interrupt mode used for rx (no dma) | ||
== | == earlycon for {{MicroprocessorDevice | device=Class}} == | ||
'''earlycon''' is a Linux kernel debug feature useful to get traces for kernel issues which happen before the normal console is initialized. | |||
It is available on for both {{MicroprocessorDevice | device=1}} (AArch processors type - 32 bits) and {{MicroprocessorDevice | device=2}} (AArch64 processors type - 64 bits). | |||
=== Linux kernel configuration === | |||
Linux kernel config SERIAL_EARLY_CON is enable by default: | |||
Symbol: '''SERIAL_EARLYCON''' [=y] | |||
Type : bool | |||
Defined at drivers/tty/serial/Kconfig:9 | |||
Depends on: TTY [=y] && HAS_IOMEM [=y] && SERIAL_CORE [=y] | |||
Selected by [y]: | |||
... | |||
- SERIAL_STM32_CONSOLE [=y] && TTY [=y] && HAS_IOMEM [=y] && SERIAL_STM32 [=y] | |||
... | |||
Selected by [n]: | |||
... | |||
=== Serial port configuration === | |||
The serial port configuration is done via the '''stdout-path setting''' from the devide tree source file. | |||
=== Linux kernel boot command configuration === | |||
The Linux kernel boot command must contain the command-line parameter '''earlycon''' (for details, refer to {{DocSource | domain=Linux kernel | path=admin-guide/kernel-parameters.html | text=kernel-parameter}} documentation). | |||
For instance, the kernel ''bootargs'' can be modified in the following ways:<br> | |||
* Mount a boot partition from the Linux kernel console, and then update the extlinux configuration file using the vi editor (see man page<ref>http://ex-vi.sourceforge.net/vi.html</ref>, or introduction page<ref>http://ex-vi.sourceforge.net/viin/paper.html</ref> ). | |||
:For example: | |||
{{Board$}}mount /dev/mmcblk0p8 /boot | |||
{{Board$}}vi /boot/mmc0_extlinux/stm32mp135f-dk_extlinux.conf | |||
* | or | ||
* Edit the extlinux configuration file by using UMS (USB Mass Storage): see [[How to use USB mass storage in U-Boot]] for details. | |||
To mount partitions (mmc 0:microSD card / mmc 1: eMMC): | |||
:- Press any key to stop at U-Boot execution when booting the board. | |||
{{Board$}}... | |||
{{Board$}}Hit any key to stop autoboot: 0 | |||
{{Board$}}STM32MP> | |||
:- Then | |||
STM32MP> ums 0 mmc 0 | |||
: | :- Check for the boot partition mounted on your host PC (/media/''$USER''/bootfs)<br> | ||
:- Edit the extlinux configuration file corresponding to your setup (as example: /media/''$USER''/bootfs/mmc0_extlinux/stm32mp135f-dk_extlinux.conf)<br> | |||
: | |||
* Update the kernel command line by adding the '''earlycon''' parameter: | |||
root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw '''earlycon''' console=ttySTM0,115200 | |||
Save and quit file update, and then reboot the board. | |||
{{Warning| | {{Warning | In some cases, to avoid clocking issue during debug with earlycon, which cause the console display to stop, we recommend to also add '''ignore_clk_unused''' in kernel command line}} | ||
}} | |||
=== Get trace === | |||
'''Earlycon traces''' are pushed automatically to the serial console defined as seen previously, and also added to the kernel ring log buffer. | |||
== dmesg command == | == dmesg command == | ||
As reference, | As reference, see man page<ref>http://man7.org/linux/man-pages/man1/dmesg.1.html</ref>. | ||
The Kernel ring buffer can be displayed using ''dmesg'' command. | The Kernel ring buffer can be displayed using ''dmesg'' command. | ||
Line 262: | Line 247: | ||
* It is possible to filter messages following the loglevels: | * It is possible to filter messages following the loglevels: | ||
{{Board$}} dmesg -n {{ | {{Board$}}dmesg -n {{HighlightParam|<''loglevel''>}} | ||
In that case, only messages with a value lower ('''not lower equal''') than the console_loglevel will be printed. | In that case, only messages with a value lower ('''not lower equal''') than the console_loglevel will be printed. | ||
Here, {{ | Here, {{HighlightParam|<''loglevel''>}} can be a numeric value, but also a string: | ||
Supported log levels (priorities): | Supported log levels (priorities): | ||
emerg (0) | emerg (0) | ||
Line 277: | Line 262: | ||
:As example: | :As example: | ||
{{Board$}} dmesg -n {{highlight|8 }} ''# Temporary change loglevel to display messages up to debug level'' | {{Board$}}dmesg -n {{highlight|8 }} ''# Temporary change loglevel to display messages up to debug level'' | ||
or | or | ||
{{Board$}} dmesg -n {{highlight|debug }} | {{Board$}}dmesg -n {{highlight|debug }} | ||
:In that case, every kernel messages will appear on your console, as {{highlight|all priority higher than 8 (lower loglevel values)}} will be displayed. | :In that case, every kernel messages will appear on your console, as {{highlight|all priority higher than 8 (lower loglevel values)}} will be displayed. | ||
* It is possible to clear the dmesg buffer | * It is possible to clear the dmesg buffer | ||
{{Board$}} dmesg {{highlight|-c}} ''# Display the full content of dmesg ring buffer, and then clear it'' | {{Board$}}dmesg {{highlight|-c}} ''# Display the full content of dmesg ring buffer, and then clear it'' | ||
{{Board$}} dmesg {{highlight|-C}} ''# Clear the dmesg ring buffer'' | {{Board$}}dmesg {{highlight|-C}} ''# Clear the dmesg ring buffer'' | ||
== /var/log/messages file system entry == | == /var/log/messages file system entry == | ||
Line 294: | Line 279: | ||
These messages are using the loglevel 7 (KERN_DEBUG). | These messages are using the loglevel 7 (KERN_DEBUG). | ||
Refer to [[How to use the kernel dynamic debug]] article. | |||
==References== | ==References== |
Latest revision as of 16:52, 4 November 2024
1. Article purpose[edit | edit source]
The purpose of this article is to provide information about the Linux® kernel log including configuration, and to detail usage of dmesg command.
2. Introduction[edit | edit source]
Linux kernel is able to print log and trace messages, which are by default stored in a ring buffer.
The same messages can also be displayed, applying filter, on uart/console using serial port. This is defined in the kernel command-line, with the "console" parameter. See [1] for detail.
dmesg is a shell command on the kernel console, which also displays the content of the ring buffer, with filter or not (default).
3. printk function[edit | edit source]
The simplest way to get some debug information from the kernel code is by printing out various information with the kernel's equivalent of printf - the printk function and its derivatives.
printk("My Debugger is Printk\n");
See elinux.org[2] for reference. This information will be sent to the console, and also stored in a ring buffer.
You can also check to the printk-format.txt[3] document provided in the Linux kernel package to get detail about syntax and formatting.
4. Linux kernel ring buffer[edit | edit source]
The Linux kernel also manages a ring buffer to store log and trace messages.
The size of the buffer cannot be modified in runtime, and its default size value is 2^CONFIG_LOG_BUF_SHIFT bytes.
To change it, there are 3 possibles ways:
- Modify CONFIG_LOG_BUF_SHIFT value in defconfig file or use the config fragment file:
In example for 64K : CONFIG_LOG_BUF_SHIFT=16
- or use the Linux kernel menuconfig update
Location:
-> General setup
-> Kernel log buffer size (16 => 64KB, 17 => 128KB)
- Or modify kernel arguments[4] in kernel command-line (via bootargs value in device tree, or directly in extlinux uboot config file)
log_buf_len=65536";bootargs = "root=/dev/mmcblk0p5 rootwait rw console=ttySTM0,115200
This ring buffer can be displayed using dmesg command (see dmesg).
5. Loglevels[edit | edit source]
As reference, see elinux.org[5].
The log level is used by the kernel to determine the importance of a message and to decide whether it should be presented to the user immediately, by printing it to the current console.
For this, the kernel compares the log level of the message to the console_loglevel (a kernel variable) and if the priority is higher (i.e. a lower value) than the console_loglevel, the message will be printed to the current console. As example, if console_loglevel=5, all messages with log level 0 to 4 will be displayed.
Note that all messages with loglevel lower or equal to KERN_INFO level are stored in the ring buffer.
5.1. loglevels values[edit | edit source]
Name | String | Meaning | alias functions | dev alias function |
---|---|---|---|---|
KERN_EMERG | "0" | Emergency messages, system is about to crash or is unstable | pr_emerg | dev_emerg |
KERN_ALERT | "1" | Something bad happened and action must be taken immediately | pr_alert | dev_alert |
KERN_CRIT | "2" | A critical condition occurred like a serious hardware/software failure | pr_crit | dev_crit |
KERN_ERR | "3" | An error condition, often used by drivers to indicate difficulties with the hardware | pr_err | dev_err |
KERN_WARNING | "4" | A warning, meaning nothing serious by itself but might indicate problems | pr_warning | dev_warn |
KERN_NOTICE | "5" | Nothing serious, but notably nevertheless. Often used to report security events | pr_notice | dev_notice |
KERN_INFO | "6" | Informational message e.g. startup information at driver initialization | pr_info | dev_info |
KERN_DEBUG | "7" | Debug messages | pr_debug, pr_devel if DEBUG is defined | dev_dbg |
Important: note that Higher priority message is loglevel 0
5.2. Set loglevel filter value for console[edit | edit source]
5.2.1. Default values[edit | edit source]
To determine your current console_loglevel on the target you can verifiy with the following command:
7 4 1 7 current default_msg minimum default_consolecat /proc/sys/kernel/printk
The first integer shows you the current console_loglevel; the second the default log level, see Use loglevel in the kernel source for log and trace.
This is defined at compilation:
- - Current console loglevel via CONFIG_CONSOLE_LOGLEVEL_DEFAULT=7 (defined in file lib/Kconfig.debug)
- - Default message loglevel via CONFIG_MESSAGE_LOGLEVEL_DEFAULT=4 (defined in file lib/Kconfig.debug)
- - Minimum console loglevel via #define CONSOLE_LOGLEVEL_MIN 1 (defined in file include/linux/printk.h)
- - Default console loglevel is equal to CONFIG_CONSOLE_LOGLEVEL_DEFAULT
5.2.2. Using kernel command-line[edit | edit source]
The console loglevel can be also set via a kernel command-line parameter if you want to use a different value than one specified by CONFIG_CONSOLE_LOGLEVEL_DEFAULT.
For example:
loglevel=4root=/dev/mmcblk0p5 rootwait rw console=ttySTM0,115200
In that case only messages with a higher priority than KERN_WARNING (means < 4, KERN_EMERG to KERN_ERR ) will be displayed on the console.
Note: The command-line is set in one of several extlinux configuration files located in the bootfs partition. The used configuration file path is dependent of the boot device and the board type. For simplicity, you can retrieve the file parsed at boot time from the console once U-Boot takes over the boot sequence. As example :
MMC... Writing to redundant MMC(0)... OK switch to partitions #0, OK mmc0 is current device Scanning mmc 0:8... Found U-Boot script /boot.scr.uimg 4187 bytes read in 7 ms (584 KiB/s) ## Executing script at c6100000 Executing SCRIPT on target=mmc0 FOUND /mmc0_extlinux/stm32mp135f-dk_extlinux.conf [...] Starting kernel ...Boot over mmc0! Saving Environment to
Two ways to add this loglevel command-line parameter (as example with stm32mp135f-dk_extlinux.conf):
- If using SD card, this is possible to edit the file on host PC:
SD card on host PC Check for mounting boot partition (i.e. /media/$USER/bootfs) Open the appropriate extlinux configuration file for edition cd /media/$USER/bootfs/mmc0_extlinux/ gedit stm32mp135f-dk_extlinux.conf Add loglevel=8 at the end of APPEND line Save and insert SD card on the boardInsert
- If using SD Card or eMMC, this is possible to edit the file directly on the board side:
eMMC) vi stm32mp135f-dk_extlinux.conf Modify the extlinux configuration file to add loglevel=8 at the end of APPEND line Save and reboot the boardWhen software is boot Mount boot partition if not already done mount /dev/mmcblk0p4 /boot Update the kernel command line cd /boot cd mmc0_extlinux # (or mmc1_extlinux if booting from
5.2.3. Using sysfs in runtime[edit | edit source]
To change your current console_loglevel simply write to this file:
<loglevel> > /proc/sys/kernel/printkecho
or using dmesg command.
As example:
8 > /proc/sys/kernel/printk # Temporary increase loglevel to display messages up to loglevel 8echo
- In that case, every kernel messages will appear on your console, as all priority higher than 8 (lower loglevel values) will be displayed.
Note that after reboot, this configuration is reset.
[edit | edit source]
As values are defined first at compilation step, this is also possible to set them (CONFIG_CONSOLE_LOGLEVEL_DEFAULT and CONFIG_MESSAGE_LOGLEVEL_DEFAULT) using the Linux kernel Menuconfig tool (Menuconfig or how to configure kernel):
7] Location: -> Kernel hacking -> printk and dmesg options (7) Default console loglevel (1-15) Symbol: MESSAGE_LOGLEVEL_DEFAULT [=4] Location: -> Kernel hacking -> printk and dmesg options (4) Default message log level (1-7)Symbol: CONSOLE_LOGLEVEL_DEFAULT [=
5.3. Use loglevel in kernel source for log and trace[edit | edit source]
5.3.1. Using printk[edit | edit source]
A loglevel information can be added in the printk function call, with the following syntax.
printk(KERN_ERR "something went wrong, return code: %d\n",ret);
When not present, default loglevel value is given by CONFIG_MESSAGE_LOGLEVEL_DEFAULT (usually "4"=KERN_WARNING)
5.3.2. Using dedicated functions[edit | edit source]
In the loglevels table above, there are some alias functions pr_ and dev_.
These functions are defined to replace printk + loglevel info inside, in order to simplify syntax.
pr_err("something went wrong, return code: %d\n",ret);
dev_ functions are taken one more parameter to provide more information about current device or driver where message is coming from.
- Example for pr_info
pr_info("%s%s%s at %s (irq = %d, base_baud = %d) is a %s\n",
port->dev ? dev_name(port->dev) : "",
port->dev ? ": " : "",
port->name,
address, port->irq, port->uartclk / 16, uart_type(port));
will display information below:
[ 0.919488] 40010000.serial: ttySTM0 at MMIO 0x40010000 (irq = 41, base_baud = 6046875) is a stm32-usart
- Example for dev_info
dev_info(&pdev->dev, "interrupt mode used for rx (no dma)\n");
will display information below, including device reference automatically:
stm32-usart 40010000.serial: interrupt mode used for rx (no dma)[ 1.046700]
6. earlycon for STM32 Arm® Cortex® MPUs
[edit | edit source]
earlycon is a Linux kernel debug feature useful to get traces for kernel issues which happen before the normal console is initialized.
It is available on for both STM32MP1 series (AArch processors type - 32 bits) and STM32MP2 series (AArch64 processors type - 64 bits).
6.1. Linux kernel configuration[edit | edit source]
Linux kernel config SERIAL_EARLY_CON is enable by default:
TTY [=y] && HAS_IOMEM [=y] && SERIAL_CORE [=y] Selected by [y]: ... - SERIAL_STM32_CONSOLE [=y] && TTY [=y] && HAS_IOMEM [=y] && SERIAL_STM32 [=y] ... Selected by [n]: ...Symbol: SERIAL_EARLYCON [=y] Type : bool Defined at drivers/tty/serial/Kconfig:9 Depends on:
6.2. Serial port configuration[edit | edit source]
The serial port configuration is done via the stdout-path setting from the devide tree source file.
6.3. Linux kernel boot command configuration[edit | edit source]
The Linux kernel boot command must contain the command-line parameter earlycon (for details, refer to kernel-parameter documentation).
For instance, the kernel bootargs can be modified in the following ways:
- Mount a boot partition from the Linux kernel console, and then update the extlinux configuration file using the vi editor (see man page[6], or introduction page[7] ).
- For example:
mount /dev/mmcblk0p8 /boot
vi /boot/mmc0_extlinux/stm32mp135f-dk_extlinux.conf
or
- Edit the extlinux configuration file by using UMS (USB Mass Storage): see How to use USB mass storage in U-Boot for details.
To mount partitions (mmc 0:microSD card / mmc 1: eMMC):
- - Press any key to stop at U-Boot execution when booting the board.
...
Hit any key to stop autoboot: 0
STM32MP>
- - Then
STM32MP> ums 0 mmc 0
- - Check for the boot partition mounted on your host PC (/media/$USER/bootfs)
- - Edit the extlinux configuration file corresponding to your setup (as example: /media/$USER/bootfs/mmc0_extlinux/stm32mp135f-dk_extlinux.conf)
- Update the kernel command line by adding the earlycon parameter:
root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw earlycon console=ttySTM0,115200
Save and quit file update, and then reboot the board.
6.4. Get trace[edit | edit source]
Earlycon traces are pushed automatically to the serial console defined as seen previously, and also added to the kernel ring log buffer.
7. dmesg command[edit | edit source]
As reference, see man page[8].
The Kernel ring buffer can be displayed using dmesg command. It will display on the console all the content of the ring buffer.
- It is possible to filter messages following the loglevels:
<loglevel>dmesg -n
In that case, only messages with a value lower (not lower equal) than the console_loglevel will be printed.
Here, <loglevel> can be a numeric value, but also a string:
Supported log levels (priorities):
emerg (0)
alert (1)
crit (2)
err (3)
warn (4)
notice (5)
info (6)
debug (7)
- As example:
8 # Temporary change loglevel to display messages up to debug level or dmesg -n debugdmesg -n
- In that case, every kernel messages will appear on your console, as all priority higher than 8 (lower loglevel values) will be displayed.
- It is possible to clear the dmesg buffer
-c # Display the full content of dmesg ring buffer, and then clear it dmesg -C # Clear the dmesg ring bufferdmesg
8. /var/log/messages file system entry[edit | edit source]
An other way to display the content of the Linux kernel log is to look at the content of the file /var/log/messages.
It contains general system activity messages from the start-up. It also provides useful information about origin of the message, and log level.
9. Dynamic debug message[edit | edit source]
These messages are using the loglevel 7 (KERN_DEBUG).
Refer to How to use the kernel dynamic debug article.
10. References[edit | edit source]
- ↑ Linux Serial Console
- ↑ https://elinux.org/Debugging_by_printing
- ↑ https://www.kernel.org/doc/Documentation/printk-formats.txt
- ↑ The kernel’s command-line parameters
- ↑ https://elinux.org/Debugging_by_printing#Log_Levels
- ↑ http://ex-vi.sourceforge.net/vi.html
- ↑ http://ex-vi.sourceforge.net/viin/paper.html
- ↑ http://man7.org/linux/man-pages/man1/dmesg.1.html