Difference between revisions of "Configfs"

[unchecked revision] [quality revision]
m (How to set and manage configfs from Linux kernel drivers and user space)
m
 
Applicable for STM32MP13x lines, STM32MP15x lines

1 Introduction[edit]

Configfs[1] is a RAM-based filesystem that provides the converse of sysfs functionality.

While sysfs provides a filesystem-based view of kernel objects, configfs is a filesystem-based manager of kernel objects or config_items (every object in configfs is a config_item). This means that kernel objects can be created, managed and destroyed from the user space.

2 Installing configs on your target board[edit]

Configfs can be enabled and ready to be used in all STM32MPU Embedded Software distribution, via the Linux® kernel configuration CONFIG_CONFIGFS_FS (set to yes by default):

Symbol: CONFIGFS_FS
Location:
  File systems --->
    Pseudo filesystems -->
      -*- Userspace-driven configuration filesystem

Please refer to Menuconfig or how to configure kernel article for instructions for modifying the configuration and recompiling the Linux kernel image in the Distribution Package context.

3 Getting started[edit]

3.1 How to mount configfs[edit]

Use the following command to mount Configfs at /sys/kernel/config:

 mount -t configfs none /sys/kernel/config

3.2 How to set and manage configfs from Linux kernel drivers and user space[edit]

Refer to the Linux documentation[1] for detailed information.

Configfs is used by the USB framwework. Refer to USB API description for an example.

4 References[edit]


<noinclude>{{ApplicableFor
|MPUs list=STM32MP13x, STM32MP15x
|MPUs checklist=STM32MP13x,STM32MP15x
}}</noinclude>

== Introduction ==
'''Configfs'''<ref name=configfsdoc>{{CodeSource | Linux kernel | Documentation/filesystems/configfs/configfs.txt.rst}}</ref> is a RAM-based filesystem that provides the converse of sysfs functionality.

While sysfs provides a filesystem-based view of kernel objects, configfs is a filesystem-based manager of kernel objects or config_items (every object in configfs is a config_item). This means that kernel objects can be created, managed and destroyed from the user space.

== Installing configs on your target board ==
'''Configfs''' can be enabled and ready to be used in all STM32MPU Embedded Software distribution, via the Linux<sup>&reg;</sup> kernel configuration '''CONFIG_CONFIGFS_FS''' (set to yes by default):
 Symbol: '''CONFIGFS_FS'''
 Location:
   File systems --->
     Pseudo filesystems -->
       {{highlight|-*- Userspace-driven configuration filesystem}}

Please refer to [[Menuconfig or how to configure kernel]] article for instructions for modifying the configuration and recompiling the Linux kernel image in the Distribution Package context.

== Getting started ==
=== How to mount configfs ===
Use the following command to mount '''Configfs''' at ''/sys/kernel/config'':
 {{Board$}} mount -t configfs none /sys/kernel/config

=== How to set and manage configfs from Linux kernel drivers and user space ===
Refer to the Linux documentation<ref name=configfsdoc/> for detailed information.

Configfs is used by the USB framwework. Refer to [[USB_overview#API_description | USB API description]] for an example.

== References ==<references />

<noinclude>

[[Category:OpenSTLinux filesystem|02]]
{{PublicationRequestId | 10267 | 2019-01-14 | AnneJ}}</noinclude>
Line 4: Line 4:
 
}}</noinclude>
 
}}</noinclude>
 
== Introduction ==
 
== Introduction ==
'''Configfs'''<ref name=configfsdoc>{{CodeSource | Linux kernel | Documentation/filesystems/configfs/configfs.txt}}</ref> is a RAM-based filesystem that provides the converse of sysfs functionality.
+
'''Configfs'''<ref name=configfsdoc>{{CodeSource | Linux kernel | Documentation/filesystems/configfs.rst}}</ref> is a RAM-based filesystem that provides the converse of sysfs functionality.
   
 
While sysfs provides a filesystem-based view of kernel objects, configfs is a filesystem-based manager of kernel objects or config_items (every object in configfs is a config_item). This means that kernel objects can be created, managed and destroyed from the user space.
 
While sysfs provides a filesystem-based view of kernel objects, configfs is a filesystem-based manager of kernel objects or config_items (every object in configfs is a config_item). This means that kernel objects can be created, managed and destroyed from the user space.