Pages in category "How to customize software"
The following 35 pages are in this category, out of 35 total.
H
- How to add a customer application
- How to add a new parallel or serial NAND flash memory device in Yocto
- How to adjust USBPHYC settings using USB Eye Diagram
- How to assign an internal peripheral to an execution context
- How to avoid proxy issues
- How to change the CPU frequency
- How to change the GPU frequency
- How to compile the device tree with the Distribution Package
- How to configure a 256MB DDR mapping from STM32 MPU Distribution Package
- How to configure system resources
- How to configure U-Boot for your board
- How to configure UEFI boot with the Distribution Package
- How to configure uniprocessor mode
- How to create a new open embedded layer
- How to create your board device tree
- How to create your own distribution
- How to create your own image
- How to customize the Linux kernel
- How to develop an OP-TEE Trusted Application
- How to disable one CPU
- How to enable secure boot on STM32 MPU
- How to install X-TouchGFX MPU Addon
- How to optimize the boot time
- How to perform Secure Boot from Distribution Package
- How to protect the Cortex-M coprocessor firmware
- How to setup the DDR configuration
- How to tune RGMII GTX clock delay
- How to use LTDC layers from CM33 and CA35 simultaneously
- How to use the DCMIPP ISP
- How to use the secure display feature
- How to write a display panel or bridge driver
- How to write a low resolution and slow interface display panel driver