Registered User m (Update DT file) |
Registered User m (→References) Tag: 2017 source edit |
||
(12 intermediate revisions by 4 users not shown) | |||
Line 1: | Line 1: | ||
{{ApplicableFor | |||
|MPUs list=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x | |||
|MPUs checklist=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x | |||
}} | |||
<noinclude></noinclude> | |||
== Article purpose == | == Article purpose == | ||
The purpose of this article is to explain how to configure the ''CRC'' | The purpose of this article is to explain how to configure the [[CRC internal peripheral|'''CRC''']] using the [[Device tree|device tree]] mechanism, relying on the bindings documentation, that is the description of the required and optional device-tree properties. | ||
The | The peripheral can be assigned to different contexts/software components, depending on the final product needs. Refer to [[How to assign an internal peripheral to an execution context]] for guidelines on this configuration . | ||
== DT bindings documentation == | == DT bindings documentation == | ||
The | The device tree binding documents are stored either in the given applicable components listed below, or in the Linux kernel repository: <br> | ||
* Linux<sup>®</sup> OS : | |||
** CRC device tree bindings: {{CodeSource | Linux kernel | Documentation/devicetree/bindings/crypto/st,stm32-crc.yaml}} | |||
== DT configuration == | == DT configuration == | ||
This hardware description is a combination of STM32 microprocessor and board device tree files. See [[Device tree]] for | This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device-tree file organization. | ||
'''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details. | |||
===DT configuration (STM32 level) === | ===DT configuration (STM32 level) === | ||
The CRC node is | The CRC node is located in the [[STM32 MPU device_tree#Device tree structure|device tree file]] for the software components, supporting the peripheral and listed in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. | ||
{{Warning|This device tree part is related to STM32 microprocessors. It should be kept as is, without being modified by the end-user.}} | {{Warning|This device tree part is related to STM32 microprocessors. It should be kept as is, without being modified by the end-user.}} | ||
=== DT configuration (board level) === | === DT configuration (board level) === | ||
The objective of this chapter is to explain how to enable and configure the [[CRC_internal_peripheral|'''CRC''']] DT nodes for a board.<br> | |||
Peripheral configuration should be done in specific board device tree files (board dts file).<br> | |||
=== DT configuration examples === | === DT configuration examples === | ||
Line 37: | Line 36: | ||
==How to configure the DT using STM32CubeMX== | ==How to configure the DT using STM32CubeMX== | ||
The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree# | The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32_MPU|platform configuration device tree]] files.<br /> | ||
STM32CubeMX may not support all the properties described in DT binding files listed in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties, and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information. | |||
==References== | ==References== | ||
Line 49: | Line 48: | ||
{{PublicationRequestId | 8895 | 2018-09-21 | BrunoB}} | {{PublicationRequestId | 8895 | 2018-09-21 | BrunoB}} | ||
{{ArticleBasedOnModel|Peripheral or framework device tree configuration model}} | {{ArticleBasedOnModel|Peripheral or framework device tree configuration model}} | ||
</noinclude> | </noinclude> |
Latest revision as of 14:28, 28 October 2024
1. Article purpose[edit | edit source]
The purpose of this article is to explain how to configure the CRC using the device tree mechanism, relying on the bindings documentation, that is the description of the required and optional device-tree properties.
The peripheral can be assigned to different contexts/software components, depending on the final product needs. Refer to How to assign an internal peripheral to an execution context for guidelines on this configuration .
2. DT bindings documentation[edit | edit source]
The device tree binding documents are stored either in the given applicable components listed below, or in the Linux kernel repository:
- Linux® OS :
- CRC device tree bindings: Documentation/devicetree/bindings/crypto/st,stm32-crc.yaml
3. DT configuration[edit | edit source]
This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device-tree file organization.
STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.
3.1. DT configuration (STM32 level)[edit | edit source]
The CRC node is located in the device tree file for the software components, supporting the peripheral and listed in the above DT bindings documentation paragraph.
3.2. DT configuration (board level)[edit | edit source]
The objective of this chapter is to explain how to enable and configure the CRC DT nodes for a board.
Peripheral configuration should be done in specific board device tree files (board dts file).
3.3. DT configuration examples[edit | edit source]
&crc1 {
status = "okay";
};
4. How to configure the DT using STM32CubeMX[edit | edit source]
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
STM32CubeMX may not support all the properties described in DT binding files listed in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties, and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.
5. References[edit | edit source]
Please refer to the following links for additional information: