Last edited one month ago

Watchdog overview


This article provides information on the Linux® WDT (Watchdog Timer) framework.
It explains how to activate the WDT interface and, based on examples, how to use it.

1. Framework purpose[edit | edit source]

A Watchdog Timer is a hardware circuit that can reset the computer system in case of a software fault (for example, when the software is blocked in an infinity loop and cannot reload the timer before an elapsed time).

2. System overview[edit | edit source]

Watchdog overview.png

2.1. Component description[edit | edit source]

From client application to hardware, the components are the following:

  • Application (User Space): an application that configures and regularly pings the char device[1].
  • User Space interface: composed of a standard char device[1].
  • Watchdog framework (Kernel Space): this component provides a watchdog common interface [2](through a char device) to configure and control a watchdog hardware block.
  • User driver (Kernel Space): Linux kernel drivers that handle internal peripherals or external devices under watchdog core[3].
  • STM32 peripherals (Hardware): Hardware block for watchdog handling (IWDT).

2.2. API description[edit | edit source]

A userspace daemon notifies the kernel watchdog driver that the userspace is still alive at regular intervals. This is done via the char device[1] special device file ((/dev/watchdog). When such a notification occurs, the driver tells the hardware watchdog that everything is in order, and that the watchdog must wait a little more to reset the system. If the userspace fails (because of a RAM error or a kernel bug), the notifications stop and the hardware watchdog resets the system after the timeout occurs, thus causing a reboot.

3. Configuration[edit | edit source]

3.1. Kernel configuration[edit | edit source]

By default, the Watchdog Timer (WDT[2]) framework is activated in STMicroelectronics deliveries. If a specific configuration is needed, this section indicates how the WDT framework can be activated/inactivated in the kernel.

The WDT framework can be activated in the kernel configuration via Linux® Menuconfig tool. Follow the steps below to configure the kernel via Menuconfig:

[*] Watchdog Timer Support  --->
    [*] Disable watchdog shutdown on close
    [*] Update boot-enabled watchdog until userspace takes over
    <*>   STM32 Independent WatchDoG (IWDG) support

3.2. Device tree configuration[edit | edit source]

DT configuration can be done thanks to STM32CubeMX.

Please refer to the IWDG device tree configuration.

4. How to use the Watchdog framework[edit | edit source]

The Watchdog framework can be used by the userspace application:

  • The kernel provides a simple code example[4]
  • Busybox provides a watchdog daemon[5]
  • Systemd provides a watchdog support[6]

5. How to trace and debug the framework[edit | edit source]

5.1. How to trace[edit | edit source]

For details on dynamic trace usage, refer to How to use the kernel dynamic debug.

Board $> echo "file drivers/watchdog/* +p" > /sys/kernel/debug/dynamic_debug/control

6. Source code location[edit | edit source]

7. References[edit | edit source]

  1. Jump up to: 1.0 1.1 1.2 character device interface, Linux Kernel and Driver Development training document, see Character drivers and Kernel frameworks for device drivers chapter
  2. Jump up to: 2.0 2.1 kernel.org watchdog user api
  3. kernel.org watchdog user api
  4. user example
  5. busybox commands
  6. systemd watchdog configuration