How to debug a user space application with STM32CubeIDE

Revision as of 15:32, 20 April 2021 by Registered User

This article is a guideline to user space project support, which is fully integrated from release 1.6.0 of STM32CubeIDE.

It covers executable, static or shared libraries support from project creation to debug. It also gives some tracks in order to easily use gtk library or to start a new project from standard Eclipse CDT project wizard.

1. Prerequisites[edit source]

Minimum hardware

  • STM32MP15x-based board
  • Linux console
  • Ethernet (or Ethernet over USB) for connection to Linux® Cortex®-A

Minimum software

2. STM32CubeIDE Linux user space[edit source]

From STM32CubeIDE release 1.6.0 it is possible to enrich an STM32MP15x hierarchical project with User Space type project.

STM32MP15 project enriched with Linux user space projects


3. Eclipse CDT STM32 Linux user space[edit source]

From STM32CubeIDE release 1.6.0 it is also possible to easily create a STM32MP15x user space project from standard CDT Eclipse wizard.

In that case, the user space project is not part of any STM32MP15x hierarchical project and appears as a standalone project in Eclipse project explorer view: myCdtProject here after:

CDT Linux user space project'