Template:ArticleMainWriter Template:ArticleFirstDraftVersion Template:ReviewersList
1. Purpose[edit source]
This article explains how to update boot chain (trusted mode) in case of use of a "customised" devicetree.
As exemple, CubeMX is able to generate "customised" devicetree.
This article describes how to update the DTB (devicetree compiled) part of the boot binaries.
2. Rationale[edit source]
The rationale to not use the devicetree provided by OpenSTLinux distribution and prefer a "customised" devicetree is various;
- You made your own board
- You need to swap some IPs from MCU side to MPU side (or reverse)
- For any other reason...
3. Pre-requisites[edit source]
This article only need to update three software of the complete boot chain (trusted mode); Trusted Firmware A (TF-A), u-boot and the Linux kernel.
Modifying those software need to handle :
- need flashlayout and images to flash provided from file IMAGES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz
- Need components sources and patches of the the software to update provided in file SOURCES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz
- Need mkimage for stm32 and dtc utilities which could be provided by file SDK-x86_64-st-image-weston-openstlinux-weston-stm32mp1.tar.xz
- Notice this is optional since 'dtc' and 'mkimage for stm32' could also be provided by your Linux distribution (as Ubuntu, even Ubuntu though WSL)
- Host tools for binary manipulation : tar, patch, ssh/scp, dd and mount loop device
- Those tools are very basic and available in any Linux distribution even on WSL.
- In case of using WSL, mount loop device is only available from WSL2.
- STM32CubeProgrammer: the tool used to flash the images and binaries into target
- Custom devicetree sources:
- For the rest of document the custom devicetree are considered generated by STM32CubeMX and stored in a tarball MyDeviceTree_fromCubeMX.tar.xz with following file tree:
MyDeviceTree_fromCubeMX |-- kernel | |-- stm32mp157c-mydevicetree-mx.dts |-- tf-a | |-- stm32mp15-mx.h | |-- stm32mp157c-mydevicetree-mx.dts |-- u-boot | |-- stm32mp15-mx.h | |-- stm32mp157c-mydevicetree-mx-u-boot.dtsi | |-- stm32mp157c-mydevicetree-mx.dts
4. Prepare your environnement[edit source]
As seen in #Pre-requisites, there are numerus inputs so here a proposition to organize your environment.
Better is to create a dedicated WORKDIR somewhere in your HOME. Then copy all inputs quoted in #Pre-requisites in that just created WORKDIR:
- cd
- mkdir WORKDIR
- cd WORKDIR
- export WORKDIR="$PWD"
- cp <IMAGES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz> $WORKDIR/
- tar xf <IMAGES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz> -C $WORKDIR/
- cp <SOURCES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz> $WORKDIR/
- tar xf <SOURCES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz> -C $WORKDIR/
- cp <MyDeviceTree_fromCubeMX.tar.xz> $WORKDIR/
- tar xf <MyDeviceTree_fromCubeMX.tar.xz> -C $WORKDIR/
- (optional) cp <SDK-x86_64-st-image-weston-openstlinux-weston-stm32mp1.tar.xz> $WORKDIR/
- (optional) tar xf <SDK-x86_64-st-image-weston-openstlinux-weston-stm32mp1.tar.xz> -C $WORKDIR/
5. Kernel device tree update[edit source]
Updating the devicetree of kernel only needs to replace the 'dtb' file of '/boot' partition.
Indeed 'extlinux.conf' explicitly points on the dtb the kernel should use (something like '/boot/<devicetree>.dtb').
Below the procedure to generate and then copy new DTB in target:
5.1. Kernel : unpack and patch sources[edit source]
Run following command into a shell:
- pushd $WORKDIR
- mkdir -p kernel
- tar xf st-image-weston-openstlinux-weston-stm32mp1/sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0/linux-4.19.*.tar.xz -C kernel
- mv kernel/linux-* kernel/kernel-sources/
- pushd kernel/kernel-sources/
- for p in $(ls -1 ../../st-image-weston-openstlinux-weston-stm32mp1/sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0/*.patch); do patch -p1 < $p; done
- popd
- popd
5.2. Kernel : generate DTB[edit source]
- pushd $WORKDIR
- cp -r MyDeviceTree_fromCubeMX/kernel kernel/dts
- ls kernel/dts/
- stm32mp157c-mydevicetree-mx.dts
- pushd $WORKDIR
- gcc -E -nostdinc -I kernel-sources/include/ -I kernel-sources/arch/arm/boot/dts -I dts -undef -D__DTS__ -x assembler-with-cpp -o stm32mp157c-mydevicetree-mx.dts.tmp dts/stm32mp157c-mydevicetree-mx.dts
- dtc -I dts -O dtb -o stm32mp157c-mydevicetree-mx.dtb stm32mp157c-mydevicetree-mx.dts.tmp
- warnings ,most of the case, could be ignored
- popd
- popd
5.3. Kernel : copy DTB on target/bootfs[edit source]
- SCP method (require a up and running target with ssh service):
- scp stm32mp157c-mydevicetree-mx.dtb root@<Target_IP>:/boot/
- mount loop device method:
![]() |
Coming soon |
Then if needed [#update extlinux] of target according this new dtb filename. This is only needed if the filename of the dtb generated is diferent from the one used by extlinux to boot.
6. U-Boot device tree update[edit source]
This operation depends on the use of a mkimage with stm32 support for Windows® which is not officially available.
- The usage of a a cross-compiler for Windows® and mingw64, the latest mkimage version (provided by U-Boot) will allow you to generate a mkimage version
- Upon request, STMicroelectronics may provide an executable binary, without warranty nor support.
Here a procedure to rebuild U-Boot with a new DTS (generated with CubeMX for exemple).
- inputs: u-boot sources + patches, u-boot-nodtb.bin, u-boot dts
- host tools required: tar, patch, gcc (anyone), mkimage (with stm32 support), dtc
Here a zipfile with all inputs files used for testing Below the procedure with a mkimage with support of stm32image:
- U-Boot trusted
######################################### ######################################### ######################################### UBOOT ######################################### ######################################### ################### ################### UNPACK + PATCH ################### [frq09494@lmecxl0985 ~/views/DTC] $ mkdir -p u-boot $ tar xf SOURCES-st-image-weston-openstlinux-weston-stm32mp1-openstlinux-4.19-thud-mp1-19-05-31/st-image-weston-openstlinux-weston-stm32mp1-openstlinux-4.19-thud-mp1-19-05-31/sources/arm-openstlinux_weston-linux-gnueabi/u-boot-stm32mp-2018.11-r0/v2018.11.tar.gz -C u-boot $ mv u-boot/u-boot* u-boot/u-boot-sources/ $ pushd u-boot/u-boot-sources for p in $(ls -1 ../../SOURCES-st-image-weston-openstlinux-weston-stm32mp1-openstlinux-4.19-thud-mp1-19-05-31/st-image-weston-openstlinux-weston-stm32mp1-openstlinux-4.19-thud-mp1-19-05-31/sources/arm-openstlinux_weston-linux-gnueabi/u-boot-stm32mp-2018.11-r0/*.patch); do patch -p1 < $p; done $ popd ################### ################### GENERATE DTB ################### [frq09494@lmecxl0985 ~/views/DTC/u-boot] $ mkdir -p u-boot $ pushd u-boot $ cp -r ../MyDeviceTree_fromCubeMX/u-boot dts [frq09494@lmecxl0985 ~/views/DTC/u-boot] $ ll dts total 36 -rw-r--r-- 1 frq09494 frq09494 25968 Jun 7 17:32 stm32mp157c-mydevicetree-mx.dts -rw-r--r-- 1 frq09494 frq09494 3642 Jun 7 17:32 stm32mp157c-mydevicetree-mx-u-boot.dtsi -rw-r--r-- 1 frq09494 frq09494 3511 Jun 7 17:32 stm32mp15-mx.h ## include dtsi u-boot file into dts of u-boot $ echo '#include "stm32mp157c-mydevicetree-mx-u-boot.dtsi"' >> dts/stm32mp157c-mydevicetree-mx.dts $ gcc -E -nostdinc -I u-boot-sources/include/ -I u-boot-sources/arch/arm/dts -I dts -undef -D__DTS__ -x assembler-with-cpp -o stm32mp157c-mydevicetree-mx.dts.tmp dts/stm32mp157c-mydevicetree-mx.dts $ dtc -I dts -O dtb -o u-boot.dtb stm32mp157c-mydevicetree-mx.dts.tmp ################### ################### REBUILD UBOOT.stm32 ################### [frq09494@lmecxl0985 ~/views/DTC/u-boot] $ cat SOURCES-st-image-weston-openstlinux-weston-stm32mp1-openstlinux-4.19-thud-mp1-19-05-31/st-image-weston-openstlinux-weston-stm32mp1-openstlinux-4.19-thud-mp1-19-05-31/sources/arm-openstlinux_weston-linux-gnueabi/u-boot-stm32mp-2018.11-r0/intermediate-binaries/trusted/u-boot-nodtb.bin u-boot.dtb > u-boot-dtb.bin ## SYS_TEXT_BASE=0xC0100000 is the addr of u-boot in memory (should never change) $ export SYS_TEXT_BASE=0xC0100000 $ mkimage -T stm32image -a $SYS_TEXT_BASE -e $SYS_TEXT_BASE -d u-boot-dtb.bin u-boot.stm32
- Because of 'extlinux' before flashing the new u-boot.stm32, an extlinux entry should be add in bootfs to be able to boot on new devicetree
- First get the 'compatible' of the devicetree from dts file. At the head of the file, look for the 'compatible = ' line. The compatible should looks like something as : "st,stm32mp157c-mydevicetree-mx"
* Add a new entry in extlinux.conf file located in /boot/mmc0_stm32mp157c-dk2_extlinux/. :If the mmc0_<something> directory is not available, add the new entry in /boot/extlinux/extlinux.conf.
menu title Select the boot mode MENU BACKGROUND ../splash.bmp TIMEOUT 20 DEFAULT stm32mp157c-mydevicetree-mx LABEL stm32mp157c-dk2-sdcard KERNEL /uImage FDT /stm32mp157c-dk2.dtb APPEND root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200 LABEL stm32mp157c-dk2-a7-examples-sdcard KERNEL /uImage FDT /stm32mp157c-dk2-a7-examples.dtb APPEND root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200 LABEL stm32mp157c-dk2-m4-examples-sdcard KERNEL /uImage FDT /stm32mp157c-dk2-m4-examples.dtb APPEND root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200 LABEL stm32mp157c-mydevicetree-mx KERNEL /uImage FDT /stm32mp157c-mydevicetree-mx.dtb APPEND root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200
7. TF-A device tree update[edit source]
This operation is not supported. It is currently not possible to modify TF-A device tree without recompiling TF-A module.